Skip to main content

Deploy Full-Weight GR00T N1.7 with TensorRT on JetPack 7.2 and Jetson AGX Orin

This tutorial deploys a finetuned NVIDIA Isaac GR00T N1.7 policy on Jetson AGX Orin using JetPack 7.2 and a full TensorRT inference pipeline. Unlike the older Orin workflow that accelerated only the DiT component, this implementation builds TensorRT engines for all seven model components:

  1. Vision Transformer (ViT)
  2. Large Language Model (LLM)
  3. Vision-language self-attention
  4. State encoder
  5. Action encoder
  6. DiT action expert
  7. Action decoder

The validated workflow performs offline inference with a local LeRobot dataset. It does not open a robot serial port or send actuator commands, making it suitable for checking model conversion and action generation before integrating a physical robot.

GR00T N1.7 full TensorRT deployment on Jetson AGX Orin

Project Repository​

The JetPack 7.2 implementation, conversion scripts, runtime changes, and original deployment notes are available in the following repository:

This guide was validated against repository commit:

93d711e3d56ca054d1cd41b12115a37ae57b46f6

Later commits may improve package versions or command-line options. When reproducing the measured result, start from the pinned commit and review newer changes separately.

Tested Configuration​

ItemTested value
DeviceJetson AGX Orin, compute capability sm_87
JetPack / L4TJetPack 7.2 / L4T R39.2
OS / kernelUbuntu 24.04 / Linux 6.8 Tegra
System CUDACUDA 13.2
System TensorRT10.16.2.10
Python3.12.3
PyTorch2.8.0, Jetson AI Lab CUDA 12.9 wheel
TorchVision0.23.0
Transformers4.57.6
ONNX1.20.1
PyAV / FFmpegPyAV 16.1.0 / FFmpeg 8
TensorRT batch size1
Action horizon16
warning

The repository's older Orin setup targets JetPack 6.2, Python 3.10, CUDA 12.6, and an earlier TensorRT release. Do not run scripts/deployment/orin/install_deps.sh or scripts/activate_orin.sh for this JetPack 7.2 workflow.

note

The PyTorch wheel used by the validated environment carries a CUDA 12.9 runtime. TensorRT continues to use JetPack 7.2's system CUDA 13.2 installation. Keep the activation and library-path order shown in this guide.

Storage and Memory Planning​

Reserve at least 45–50 GB of free storage for the repository, checkpoint, local VLM backbone, dataset, ONNX graphs, TensorRT engines, and temporary build files. The validated TensorRT artifact directory occupies approximately 13 GB.

The tested AGX Orin exposed approximately 29 GB of usable unified memory and did not use swap. Before building engines:

free -h
df -h "${HOME}"
sudo tegrastats

Close browsers, notebooks, desktop applications, and unrelated model services if the TensorRT builder is terminated by the out-of-memory killer.

1. Define Portable Paths​

The project README records paths from the original test machine. Instead of copying machine-specific absolute paths, create a reusable configuration under your own home directory:

mkdir -p "${HOME}/.config/gr00t-jp72"

cat > "${HOME}/.config/gr00t-jp72/paths.sh" <<'EOF'
export GR00T_WORKSPACE="${HOME}/gr00t-jp72"
export GR00T_REPO="${GR00T_WORKSPACE}/Isaac-GR00T-Orin-JP72"
export GR00T_CHECKPOINT="${GR00T_WORKSPACE}/checkpoints/checkpoint-10000"
export GR00T_DATASET="${GR00T_WORKSPACE}/datasets/grab_tube_0_eval"
export GR00T_BACKBONE="${GR00T_WORKSPACE}/models/Qwen/Qwen3-VL-2B-Instruct"
export GR00T_TRT_OUTPUT="${GR00T_WORKSPACE}/artifacts/rebot_trt"
EOF

source "${HOME}/.config/gr00t-jp72/paths.sh"
mkdir -p \
"$(dirname "${GR00T_REPO}")" \
"$(dirname "${GR00T_CHECKPOINT}")" \
"$(dirname "${GR00T_DATASET}")" \
"$(dirname "${GR00T_BACKBONE}")" \
"${GR00T_TRT_OUTPUT}"

Run the following command in every new terminal before using the variables:

source "${HOME}/.config/gr00t-jp72/paths.sh"

You may change the values in paths.sh to place large files on an NVMe SSD. Keep the repository, model, dataset, and output paths separate.

2. Clone the JetPack 7.2 Repository​

source "${HOME}/.config/gr00t-jp72/paths.sh"

git clone https://github.com/jjjadand/Isaac-GR00T-Orin-JP72.git "${GR00T_REPO}"
cd "${GR00T_REPO}"
git checkout 93d711e3d56ca054d1cd41b12115a37ae57b46f6

If the repository already exists, verify its current revision:

git -C "${GR00T_REPO}" rev-parse HEAD
git -C "${GR00T_REPO}" status --short

Do not switch revisions while an ONNX export or engine build is in progress.

3. Prepare the Required Inputs​

3.1 Finetuned GR00T N1.7 Checkpoint​

Copy your finetuned checkpoint into ${GR00T_CHECKPOINT}. The inference checkpoint requires the GR00T configuration, statistics, and model shards. A typical layout is:

checkpoint-10000/
├── config.json
├── embodiment_id.json
├── model-00001-of-00003.safetensors
├── model-00002-of-00003.safetensors
├── model-00003-of-00003.safetensors
├── model.safetensors.index.json
├── processor_config.json
└── statistics.json

Training-state files such as optimizer.pt, scheduler.pt, and trainer_state.json are not required for inference or ONNX export.

Validate the configured path:

source "${HOME}/.config/gr00t-jp72/paths.sh"
test -f "${GR00T_CHECKPOINT}/config.json"
test -f "${GR00T_CHECKPOINT}/processor_config.json"
test -f "${GR00T_CHECKPOINT}/statistics.json"

3.2 Download the Local Qwen3-VL Backbone​

The N1.7 policy still requires the compatible backbone architecture, tokenizer, and image processor. This repository supports a fully local backbone through GR00T_BACKBONE_PATH, so a Hugging Face login is not required during export or inference.

source "${HOME}/.config/gr00t-jp72/paths.sh"

uv tool run --from modelscope modelscope download \
Qwen/Qwen3-VL-2B-Instruct \
--local-dir "${GR00T_BACKBONE}"

Confirm that the main model file and configuration are present:

test -f "${GR00T_BACKBONE}/config.json"
test -f "${GR00T_BACKBONE}/model.safetensors"
ls -lh "${GR00T_BACKBONE}/model.safetensors"

The model.safetensors file is approximately 4.25 GB in the tested download.

3.3 Prepare the Local LeRobot Dataset​

The offline dry-test accepts a local LeRobot v2/v2.1 dataset through --dataset-path. For the validated RS-Rebot example, the minimum layout is:

grab_tube_0_eval/
├── data/chunk-000/episode_000000.parquet
├── videos/chunk-000/observation.images.front/episode_000000.mp4
├── videos/chunk-000/observation.images.side/episode_000000.mp4
└── meta/
├── episodes.jsonl
├── info.json
├── modality.json
├── stats.json
└── tasks.jsonl

The provided example expects:

  • embodiment tag: NEW_EMBODIMENT;
  • camera keys: front and side;
  • state and action dimensions: 7;
  • action horizon: 16.

The checkpoint's processor_config.json and the dataset's meta/modality.json must describe compatible state, action, and video modalities.

tip

Pass the local directory with --dataset-path. Do not provide a local folder to an option that expects a Hugging Face repository ID, because it may trigger an unnecessary Hub request and return an HTTP 401 error.

4. Install the JetPack 7.2 Environment​

4.1 Install System Packages​

JetPack 7.2 must already provide CUDA, TensorRT, cuDNN, and the TensorRT Python bindings.

sudo apt-get update
sudo apt-get install -y --no-install-recommends \
ffmpeg \
libopenblas0-pthread \
python3.12-venv \
python3-dev

Check the platform packages:

cat /etc/nv_tegra_release
/usr/local/cuda-13.2/bin/nvcc --version
dpkg-query -W python3-libnvinfer libnvinfer10 tensorrt

The validated environment reports L4T R39.2, CUDA 13.2, and TensorRT 10.16.

4.2 Create a Dedicated Python Environment​

source "${HOME}/.config/gr00t-jp72/paths.sh"
cd "${GR00T_REPO}"

curl -LsSf https://astral.sh/uv/install.sh | sh
export PATH="${HOME}/.local/bin:${PATH}"

uv venv --python /usr/bin/python3.12 .venv-jp72

Do not reuse the repository's .venv, which may contain packages built for a different Jetson platform.

4.3 Install the Tested Orin PyTorch Wheels​

uv pip install --python "${GR00T_REPO}/.venv-jp72/bin/python" --no-deps \
"https://pypi.jetson-ai-lab.io/jp6/cu129/+f/f36/0db283b1249b3/torch-2.8.0-cp312-cp312-linux_aarch64.whl" \
"https://pypi.jetson-ai-lab.io/jp6/cu129/+f/255/341cb5beb4673/torchvision-0.23.0-cp312-cp312-linux_aarch64.whl"

Install the CUDA 12.9 runtime libraries required by the PyTorch wheel:

uv pip install --python "${GR00T_REPO}/.venv-jp72/bin/python" \
nvidia-cublas-cu12==12.9.2.10 \
nvidia-cuda-cupti-cu12==12.9.79 \
nvidia-cuda-nvrtc-cu12==12.9.86 \
nvidia-cuda-runtime-cu12==12.9.79 \
nvidia-cufft-cu12==11.4.1.4 \
nvidia-curand-cu12==10.3.10.19 \
nvidia-cusolver-cu12==11.7.5.82 \
nvidia-cusparse-cu12==12.5.10.65 \
nvidia-nvjitlink-cu12==12.9.86

4.4 Install the GR00T Dependencies​

uv pip install --python "${GR00T_REPO}/.venv-jp72/bin/python" \
accelerate==1.12.0 \
albumentations==1.4.18 \
av==16.1.0 \
build==1.4.0 \
click==8.1.8 \
cryptography==46.0.7 \
datasets==3.6.0 \
dm-tree==0.1.8 \
einops==0.8.1 \
gitpython==3.1.50 \
gymnasium==1.2.2 \
"huggingface-hub[cli]==0.36.2" \
jsonlines==4.0.0 \
lmdb==1.7.5 \
matplotlib==3.10.1 \
msgpack==1.1.0 \
msgpack-numpy==0.4.8 \
numpy==1.26.4 \
omegaconf==2.3.0 \
onnx==1.20.1 \
onnxscript==0.6.2 \
opencv-python-headless==4.11.0.86 \
pandas==2.2.3 \
peft==0.17.1 \
pytest==9.0.3 \
pytest-timeout==2.4.0 \
pyzmq==27.0.1 \
ruff==0.15.1 \
safetensors==0.7.0 \
scipy==1.15.3 \
termcolor==3.2.0 \
transformers==4.57.6 \
tyro==0.9.17 \
wandb==0.23.0

uv pip install --python "${GR00T_REPO}/.venv-jp72/bin/python" --no-deps \
"https://pypi.jetson-ai-lab.io/jp6/cu129/+f/c46/66317287eb28a/diffusers-0.36.0.dev0-py3-none-any.whl"

uv pip install --python "${GR00T_REPO}/.venv-jp72/bin/python" --no-deps -e "${GR00T_REPO}"

Do not install TorchCodec for this tested configuration. PyAV 16 is used with JetPack 7.2's FFmpeg 8 to decode the dataset videos. Flash Attention is optional and was not installed in the validated environment.

4.5 Expose the System TensorRT Python Package​

Use Python to determine the environment's actual site-packages path instead of hard-coding a username:

GR00T_SITE_PACKAGES="$("${GR00T_REPO}/.venv-jp72/bin/python" -c 'import site; print(site.getsitepackages()[0])')"

printf '%s\n' '/usr/lib/python3.12/dist-packages' \
> "${GR00T_SITE_PACKAGES}/jetpack_system_packages.pth"

5. Activate and Validate​

Run the following block in each new shell:

source "${HOME}/.config/gr00t-jp72/paths.sh"
cd "${GR00T_REPO}"

deactivate 2>/dev/null || true
source .venv-jp72/bin/activate
source scripts/activate_orin_jp72.sh

# Override the original test-machine path configured by the activation script.
export GR00T_BACKBONE_PATH="${GR00T_BACKBONE}"
hash -r

Validate the interpreter, GPU architecture, TensorRT binding, backbone, and video backend:

python - <<'PY'
import os
import sys

import tensorrt
import torch

print("python:", sys.executable)
print("torch:", torch.__version__)
print("torch CUDA:", torch.version.cuda)
print("GPU:", torch.cuda.get_device_name(0))
print("architectures:", torch.cuda.get_arch_list())
print("TensorRT:", tensorrt.__version__)
print("backbone:", os.environ["GR00T_BACKBONE_PATH"])
print("video backend:", os.environ["GR00T_VIDEO_BACKEND"])

assert sys.executable.endswith("/.venv-jp72/bin/python")
assert "sm_87" in torch.cuda.get_arch_list()
assert os.environ["GR00T_VIDEO_BACKEND"] == "pyav"
PY

Expected key values include PyTorch 2.8.0, PyTorch CUDA 12.9, sm_87, TensorRT 10.16.2.10, and the pyav backend.

warning

Use the activated environment's plain python command. Avoid uv run python after installation because it may synchronize the repository's default project environment and replace working Jetson-specific packages.

6. Run the PyTorch Smoke Test​

Before exporting, verify that the checkpoint, local backbone, dataset, video decoder, and CUDA forward pass work together:

python scripts/deployment/standalone_inference_script.py \
--model-path "${GR00T_CHECKPOINT}" \
--dataset-path "${GR00T_DATASET}" \
--embodiment-tag NEW_EMBODIMENT \
--traj-ids 0 \
--steps 1 \
--execution-horizon 16 \
--denoising-steps 4 \
--inference-mode pytorch \
--save-plot-path /tmp/rebot_pytorch_smoke.jpeg

Do not continue to TensorRT export until this command can load one dataset observation and generate an action prediction.

7. Export the Complete Model to ONNX​

Export all seven components with a static batch size of 1:

python scripts/deployment/build_trt_pipeline.py \
--model-path "${GR00T_CHECKPOINT}" \
--dataset-path "${GR00T_DATASET}" \
--embodiment-tag NEW_EMBODIMENT \
--export-mode full_pipeline \
--batch-size 1 \
--output-dir "${GR00T_TRT_OUTPUT}" \
--workspace 4096 \
--steps export

The validated export takes approximately two minutes. Confirm that the ONNX directory contains seven graphs and the export metadata:

find "${GR00T_TRT_OUTPUT}/onnx" -maxdepth 1 -type f \
-printf '%f %s bytes\n' | sort

Keep dit_bf16.onnx.data beside dit_bf16.onnx; it contains external tensor data used by the DiT graph.

8. Build the Seven TensorRT Engines​

Build the engines on the target AGX Orin. TensorRT engines are tied to the GPU architecture, TensorRT version, graph shapes, and batch size.

python scripts/deployment/build_trt_pipeline.py \
--model-path "${GR00T_CHECKPOINT}" \
--dataset-path "${GR00T_DATASET}" \
--embodiment-tag NEW_EMBODIMENT \
--export-mode full_pipeline \
--batch-size 1 \
--output-dir "${GR00T_TRT_OUTPUT}" \
--workspace 4096 \
--steps build

The validated build took approximately 3 minutes 37 seconds and generated:

action_decoder.engine
action_encoder.engine
dit_bf16.engine
llm_bf16.engine
state_encoder.engine
vit.engine
vl_self_attention.engine

Verify the engine directory:

find "${GR00T_TRT_OUTPUT}/engines" -maxdepth 1 -type f \
-printf '%f %s bytes\n' | sort

Rebuild after changing the checkpoint, input camera layout or resolution, action horizon, batch size, GPU, CUDA/TensorRT installation, or ONNX graphs.

9. Verify TensorRT Against PyTorch​

Run the repository's numerical verification stage:

python scripts/deployment/build_trt_pipeline.py \
--model-path "${GR00T_CHECKPOINT}" \
--dataset-path "${GR00T_DATASET}" \
--embodiment-tag NEW_EMBODIMENT \
--export-mode full_pipeline \
--batch-size 1 \
--output-dir "${GR00T_TRT_OUTPUT}" \
--workspace 4096 \
--steps verify

The validated run produced:

ComparisonCosine similarity
ViT output0.995977
Backbone output0.999958
Final action0.997426
Verification statusPASS

Treat these values as a reproduction reference. A different finetuned checkpoint, dataset sample, or dependency revision may produce slightly different values.

10. Run Full-TensorRT Offline Inference​

The following command loads trajectory 0 and predicts two 16-action chunks. It does not initialize the RS-Rebot hardware runner.

python scripts/deployment/standalone_inference_script.py \
--model-path "${GR00T_CHECKPOINT}" \
--dataset-path "${GR00T_DATASET}" \
--embodiment-tag NEW_EMBODIMENT \
--traj-ids 0 \
--steps 32 \
--execution-horizon 16 \
--denoising-steps 4 \
--skip-timing-steps 1 \
--inference-mode trt_full_pipeline \
--trt-engine-path "${GR00T_TRT_OUTPUT}/engines" \
--save-plot-path /tmp/rebot_trt_result.jpeg

A successful run includes messages similar to:

N1.7 full-pipeline TRT engines loaded.
ViT: TRT | LLM: TRT | Action Head: TRT
All inference steps completed for current trajectory-id 0
pred_action_joints vs time (32, 7)
Done

The validated warm inference time was 0.2755 seconds per 16-action prediction chunk, or approximately 3.63 chunks per second. This result applies to the tested checkpoint, dataset shape, engine configuration, and AGX Orin operating conditions.

The script's MSE and MAE values compare model predictions with recorded dataset actions. They are not TensorRT conversion-error metrics; use the cosine verification stage for PyTorch-versus-TensorRT agreement.

Full-TensorRT Inference Demo​

The following video demonstrates the completed GR00T N1.7 TensorRT workflow running on JetPack 7.2 and Jetson AGX Orin.

11. Safe Warnings​

libnvjpeg.so.12 from TorchVision​

The tested dataset path uses PyAV and FFmpeg rather than torchvision.io. This warning does not block the validated inference workflow.

flash_attn is not installed​

The reference PyTorch model uses SDPA during loading and export. Full-pipeline inference replaces the ViT, LLM, and action components with TensorRT engines.

lm_head.weight is newly initialized​

GR00T consumes the backbone hidden states rather than the language-generation head. The finetuned policy checkpoint supplies the weights used by action inference.

12. Troubleshooting​

torch._C has no _dlpack_exchange_api​

The wrong environment is active. Check the interpreter:

which python
python -c "import sys; print(sys.executable)"

The path must end with ${GR00T_REPO}/.venv-jp72/bin/python. Reactivate the environment and run source scripts/activate_orin_jp72.sh again.

Hugging Face HTTP 401​

Confirm that the local backbone override was applied after the repository activation script:

export GR00T_BACKBONE_PATH="${GR00T_BACKBONE}"
export HF_HUB_OFFLINE=1
export TRANSFORMERS_OFFLINE=1

test -f "${GR00T_BACKBONE_PATH}/config.json"
test -f "${GR00T_BACKBONE_PATH}/model.safetensors"

TorchCodec or FFmpeg Import Failure​

Confirm that PyAV is selected:

python -c "import os, av; print(os.environ['GR00T_VIDEO_BACKEND'], av.__version__)"

Expected output begins with pyav 16.1.0.

Engine Shape or Deserialization Error​

Do not copy engines from another GPU or TensorRT installation. Check that export_metadata.json accompanies the engine output and rebuild ONNX and TensorRT artifacts on the target device.

TensorRT Build Runs Out of Memory​

  1. Close unrelated GPU applications and model servers.
  2. Keep --workspace 4096 rather than increasing it immediately.
  3. Build stages sequentially.
  4. Confirm sufficient storage and memory with df -h, free -h, and tegrastats.
  5. Reboot into a clean session if memory remains fragmented after repeated failed builds.

13. Moving Toward Robot Control​

The validated command is intentionally an offline dry-test. Before connecting a physical robot:

  1. compare TensorRT and PyTorch action trajectories on recorded episodes;
  2. confirm joint order, units, scaling, limits, and embodiment metadata;
  3. clamp all generated commands to safe joint and velocity limits;
  4. implement emergency stop, command timeout, and stale-observation detection;
  5. test with actuators disabled or unloaded;
  6. begin with low-speed, short-horizon actions;
  7. record latency, memory, power, temperature, and task success rate.

Do not reuse the offline command as a robot controller without a hardware-specific safety layer.

Reproduction Checklist​

  • JetPack 7.2 / L4T R39.2 is installed.
  • CUDA 13.2 and TensorRT 10.16 are visible.
  • The repository is cloned at the documented revision.
  • .venv-jp72 uses Python 3.12 and the Orin sm_87 PyTorch wheel.
  • The local Qwen3-VL backbone loads without a Hub request.
  • The checkpoint and LeRobot dataset modalities match.
  • The PyTorch smoke test succeeds.
  • Seven ONNX graphs are exported.
  • Seven TensorRT engines are generated on the target Orin.
  • Numerical verification reports PASS.
  • Offline full-TensorRT inference completes and saves the plot.

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...