Skip to main content

Deploy a PREEMPT_RT Real-Time Kernel with a Prebuilt DEB Package on Seeed reComputer Jetson Devices

A real-time kernel, also known as a PREEMPT_RT kernel, is a Linux kernel variant with enhanced real-time scheduling capabilities. It reduces scheduling latency and improves task execution determinism, which is critical for workloads such as motor control, sensor data acquisition, and industrial bus communication (CAN, EtherCAT) in robotics, industrial automation, and edge computing scenarios.

If you prefer to build the PREEMPT_RT kernel from source, please refer to this wiki. This guide takes a much simpler path: a single prebuilt DEB package installs the real-time kernel in about one minute, keeps the original standard kernel untouched as a fallback, and lets you switch between the two kernels at any time.

note

This wiki applies to Seeed reComputer and reServer Jetson devices based on the NVIDIA Orin (T234) module running JetPack 7.2 (Jetson Linux R39.2.0) with the standard kernel. A single DEB package covers all T234-based carrier boards. This wiki has been tested and verified on a reComputer Super.

Prerequisites​

note

For devices still running JetPack 6.2 (Jetson Linux R36.4.3), use the matching package nvidia-l4t-kernel-rt-6.2-36.4.3-2026-08-26.deb instead. The procedures in this wiki are identical; only the kernel version strings differ (5.15.148-tegra / 5.15.148-rt-tegra).

If your device is not running the standard system yet, please refer to the reComputer Super Getting Started wiki first.

Check the Standard Kernel Version​

The DEB package requires the device to run the standard kernel version that matches the package. Open a terminal on the device and run:

uname -r

You should see output similar to:

6.8.12-1021-tegra

If the output is a different version (for example 5.15.148-tegra from an older JetPack release, or 6.8.12-1021-rt-tegra from the real-time kernel), flash the matching standard system image first, then continue with this guide.

Install the Real-Time Kernel DEB Package​

Step 1. Transfer the DEB package to the device (a USB drive or scp both work):

scp nvidia-l4t-kernel-rt-7.2.0-39.2.0-2026-08-26.deb <username>@<device-ip>:~

Step 2. Log in to the device and install the package:

sudo dpkg -i ~/nvidia-l4t-kernel-rt-7.2.0-39.2.0-2026-08-26.deb

The installation takes about one minute and is fully automatic. It places the real-time kernel image at /boot/Image.real-time, installs the matching modules under /lib/modules/6.8.12-1021-rt-tegra/, rebuilds the initrd, and switches the default boot entry to the real-time kernel. The original standard kernel at /boot/Image is left untouched, so it always remains available as a fallback.

Step 3. Reboot the device:

sudo reboot

Verify the Real-Time Kernel​

After the reboot, confirm that the real-time kernel is running:

uname -r
cat /sys/kernel/realtime
zcat /proc/config.gz | grep PREEMPT

You should see output similar to:

6.8.12-1021-rt-tegra
1
CONFIG_PREEMPT_RT=y

The package ships a kernel with the Seeed carrier-board patches already applied, so all peripherals should behave exactly as on the standard system. You can spot-check a few of them:

lsmod | grep nvgpu
ip -br addr
systemctl --failed

systemctl --failed should report no failed services.

Switch Between the Real-Time and Standard Kernels​

You can switch between the two kernels at any time. To switch back to the standard kernel:

sudo nv-update-extlinux generic && sudo reboot

To switch to the real-time kernel again:

sudo nv-update-extlinux real-time && sudo reboot
tip

During boot, press 0 (standard kernel) or 1 (real-time kernel) within 3 seconds in the boot menu to select a kernel for that boot only, without changing the default entry.

Uninstall the Real-Time Kernel​

caution

Make sure the device has been switched back to the standard kernel before uninstalling the package.

sudo nv-update-extlinux generic && sudo reboot
sudo apt remove nvidia-l4t-kernel-rt

Performance Comparison: Real-Time vs Standard Kernel​

To show what the real-time kernel actually brings, the two kernels were compared under three workloads: scheduler latency (cyclictest), GPIO output jitter, and EtherCAT servo motor control — all on the same device, under the same interference, and with the CPU kept under full load.

note

All results below were measured on a Seeed reComputer Super (Orin Nano Super) running JetPack 7.2, under full CPU load.

Principle​

The experiments use a kernel module called spinlock_holder: a kernel thread bound to one CPU core that repeatedly takes a spin_lock() and holds it for a configured duration.

  • On the standard kernel, spin_lock() disables kernel preemption. Every task on that CPU — including the highest-priority SCHED_FIFO real-time task — is frozen until the lock is released.
  • On the PREEMPT_RT kernel, spinlock_t is replaced by a sleepable lock backed by an rt_mutex, so a higher-priority task preempts the lock holder at any time.

This is the difference the experiments make visible: on the standard kernel, a 1-second lock means a 1-second stall for the real-time task; on the real-time kernel, the same interference is almost invisible to it.

info

Why a kernel thread and not a busy-loop user process? User-space load is always schedulable — on both kernels an SCHED_FIFO task outranks it, so nothing interesting shows up. Only a non-preemptible kernel critical section separates the two kernels. The control group below proves this with data.

Test Setup​

ItemValue
DeviceSeeed reComputer Super (Orin Nano Super, 6 cores)
SystemJetPack 7.2 (Jetson Linux R39.2.0)
Standard kernel6.8.12-1021-tegra
Real-time kernel6.8.12-1021-rt-tegra (deployed via DEB package)
Interferencespinlock_holder kernel module, kthread bound to CPU3
Workloadscyclictest, GPIO square wave (SCHED_FIFO), IgH EtherCAT master 1 kHz (SCHED_FIFO 89, same core)

During the experiments, the interference thread keeps the target core pinned at 100% in jtop, while the other cores stay mostly idle:

Cyclictest Latency​

Install rt-tests first:

sudo apt update && sudo apt install -y rt-tests

Generate full system load in one terminal:

stress --cpu 6 --io 4 --vm 2 --vm-bytes 64M &

Then run cyclictest in a second terminal, for 30 seconds (the -S option starts one measurement thread per CPU core, with the interval increasing by 500 µs from thread to thread):

sudo cyclictest -m -S -p90 -i1000 -D30s

The image below shows an example run on the standard kernel: every thread's average latency stays between 8 and 21 µs — deceptively close to the real-time kernel — but the maximum latency spikes to 1,909 µs, more than 60 times the real-time kernel's ceiling, with no way to predict when it happens:

The real-time kernel has a hard ceiling on the maximum latency: no matter how heavy the load gets, it never runs out of control. This determinism is exactly what a real-time kernel is for.

GPIO Square-Wave Jitter​

This test also runs under full CPU load. A kernel thread periodically holds a spinlock on a CPU core while a SCHED_FIFO task on the same core toggles a GPIO pin to output a 2 kHz square wave. Edge timestamps are recorded in a ring buffer and written to a log file at exit, so logging itself never adds jitter. The edge-to-edge statistics and the oscilloscope view show the difference directly (lock held for 300 µs every 1 ms):

Lock hold / periodMetricStandard kernelReal-time kernel
300 µs / 1 msp99 / max / σ306 / 325~547 / 40 µs251 / 257 / 0.56 µs
500 µs / 1 mslost edges / merged pairs25% / 25%0 / 0
500 µs / 1 msp99 / max506 / 529 µs~251 µs

On the standard kernel, edges that fall inside the spinlock window are delayed or swallowed, so the waveform visibly distorts. On the real-time kernel the waveform stays clean.

Standard kernel — the square wave distorts and stops whenever the spinlock is held:

Real-time kernel — a continuous square wave (time base 500 µs/div):

EtherCAT Servo Motor Control​

This test also runs under full CPU load: the target core is kept loaded in all phases. The Jetson device runs an IgH EtherCAT master (1 kHz cycle, SCHED_FIFO 89) that drives an EtherCAT servo motor. The EtherCAT drive has a communication watchdog of about 100 ms: if the process-data frames stop for longer, the drive cuts output and the motor stops. The interference module holds a spinlock for 1,000 ms every 3 s on the master's core — so any freeze longer than the watchdog should, and does, kill the bus on the standard kernel.

A three-phase demo shows the whole story in one run:

PhaseInterferenceStandard kernelReal-time kernel
1 (10 s)CPU load onlyMotor rotates smoothlyMotor rotates smoothly
2 (15 s)+ spinlock (1,000 ms / 3 s)CYCLE BROKEN — SAFE STOP, bus drops out of OP, motor stopsMotor keeps rotating, zero alarms
3 (15 s)spinlock removed, load staysMaster self-recovers in ~4 s, motor restartsNo change

Core metrics over identical runs:

MetricStandard kernelReal-time kernel
Safe stop triggeredOn the first lock windowNever
Slave dropped out of OP1~3 times per 25 s0 times
Master wake-up p50 / p99 / max7 / ~994,000 / ~1,018,000 µs2 / 3 / 12 µs
Cycles over 1 ms (per 5,000)~2,0000
Motor behaviorStops while locked, recovers ~4 s after releaseContinuous sinusoidal motion

Standard kernel output when the lock hits (the master freezes for a full second, then recovers after the lock is released):

############ Phase 2: LOADING spinlock interference ############
*** CYCLE BROKEN (frozen >500ms) — SAFE STOP: disabling motor ***
!!! BUS DROPPED: slave left OP (AL 0x08 -> 0x4) — comm watchdog/error !!!
[STAT] cycles=15000 WKC0=2255 late>1ms=2084 drops(total)=1
wake_us p50/p99/max=7/994615/1018037
############ Phase 3: REMOVING interference ############
+++ cycle restored — re-enabling motor +++

Real-time kernel output under the same interference, for the entire run:

[STAT] cycles=5000  WKC0=131  late>1ms=0 drops(total)=0 wake_us p50/p99/max=2/3/8
[STAT] cycles=10000 WKC0=0 late>1ms=0 drops(total)=0 wake_us p50/p99/max=2/3/9
[STAT] cycles=15000 WKC0=0 late>1ms=0 drops(total)=0 wake_us p50/p99/max=2/3/8
Running: Act=41268 Vel=29970 TgtV=29630 md=9 SW=1237
note

The master has built-in cycle health monitoring: a wake-up delay over 500 ms is treated as "frozen" and triggers a controlled safe stop (standard practice for industrial stacks); the motor re-enables after 4 s without any freeze. On the standard kernel the interference returns every 3 s, so the recovery window never opens.

On the standard kernel, the master stalls for whole seconds — more than 10 times the EtherCAT drive watchdog (~100 ms) — so the bus drops out of OP state and the motor is disabled. On the real-time kernel, the master wake-up jitter stays within a few microseconds, and neither the bus nor the motor is affected by the interference.

On the real-time kernel, the EtherCAT servo motor rotates smoothly for 30 seconds:

On the standard kernel, the motor stops whenever the lock is held (10 s of rotation, 15 s of stall, 15 s of rotation):

Control Group: CPU Load Is Not the Killer​

To prove that the damage comes from the non-preemptible critical section and not from CPU utilization, the same core was loaded by an ordinary SCHED_OTHER user process (busy 1 s / idle 2 s, peaks at 100%) instead of the spinlock module — same core, same rhythm:

MetricStandard + CPU loadReal-time + CPU loadStandard + spinlock
MotorRotatesRotatesStops
Bus drops / safe stops0 / 00 / 01~3 / triggered
wake p99up to 1,879 µs11 µs~994,000 µs
wake max~8,200 µs32 µs~1,018,000 µs
Cycles over 1 ms (per 5,000)28~560~2,000

User-space load never outranks an SCHED_FIFO task on either kernel, so the motor keeps turning in both columns — but the standard kernel is still dragged into millisecond-scale jitter (p99 roughly 170 times worse than the real-time kernel). The kernel spinlock is what turns jitter into a second-long outage. The killer is not CPU usage; it is the non-preemptible kernel critical section.

Reproduce the Experiments​

The complete source code of the GPIO experiment (interference module, square-wave task, and Makefile) is embedded below, so it can be used directly. The EtherCAT demo is built on the open-source ethercat-myctor project with a customized device controller; the complete demo package (controller override, run scripts, and CPU-load generator) is available here: rt_ethercat_demo.zip.

Switching between the two kernels is described in Switch Between the Real-Time and Standard Kernels. After each switch, verify with uname -v — the output should contain SMP PREEMPT_RT or SMP PREEMPT respectively.

Prepare the Real-Time Kernel Source Tree (once)​

note

The real-time DEB package ships the kernel image and modules but no headers package. Kernel modules must be built against a prepared source tree while the real-time kernel is running, otherwise insmod fails with module_layout disagrees.

curl -sL -o ~/public_sources.tbz2 \
https://developer.download.nvidia.cn/embedded/L4T/r39_Release_v2.0/sources/public_sources.tbz2
mkdir -p ~/nvsrc ~/rt-kernel-src
tar xf ~/public_sources.tbz2 -C ~/nvsrc Linux_for_Tegra/source/kernel_src.tbz2
tar xf ~/nvsrc/Linux_for_Tegra/source/kernel_src.tbz2 -C ~/rt-kernel-src --strip-components=1

cd ~/rt-kernel-src/kernel-noble
zcat /proc/config.gz > .config
sed -i 's/^CONFIG_LOCALVERSION=".*"/CONFIG_LOCALVERSION="-1021-rt-tegra"/' .config
make ARCH=arm64 olddefconfig
make ARCH=arm64 -j6 prepare modules_prepare

CONFIG_LOCALVERSION must equal the suffix of uname -r after 6.8.12 (here -1021-rt-tegra), otherwise the module vermagic does not match. For the standard kernel, use -1021-tegra and prepare the tree the same way.

Demo Source Code (GPIO Experiment)​

Create a working directory and place the following three files in it:

mkdir -p ~/rt_demo && cd ~/rt_demo

spinlock_holder.c — the interference module:

// spinlock_holder: PREEMPT_RT demo module (ms and us granularity)
//
// One-shot mode (period = 0): sysfs trigger makes the bound kthread hold a
// spinlock for the configured hold time, once. On a normal kernel
// spin_lock() disables preemption so every task on that CPU freezes for
// the duration; on PREEMPT_RT spinlock_t is a sleepable rt_mutex-backed
// lock and higher priority tasks preempt the holder instead.
//
// Periodic mode (period > 0): the kthread repeats hold/idle cycles.
// Writing any *_us parameter (or period) via sysfs wakes the kthread so
// changes take effect immediately.
#include <linux/module.h>
#include <linux/kernel.h>
#include <linux/slab.h>
#include <linux/kthread.h>
#include <linux/delay.h>
#include <linux/spinlock.h>
#include <linux/wait.h>
#include <linux/sysfs.h>
#include <linux/kobject.h>
#include <linux/sched.h>
#include <linux/ktime.h>

static int demo_cpu = 3;
module_param(demo_cpu, int, 0644);
MODULE_PARM_DESC(demo_cpu, "CPU to bind the holder kthread to (default 3)");

static int hold_ms = 3000;
module_param(hold_ms, int, 0644);
MODULE_PARM_DESC(hold_ms, "critical section length in ms (one-shot default 3000)");

static int period_ms = 0;
MODULE_PARM_DESC(period_ms, "0 = one-shot trigger; >0 = repeat every period_ms (ms mode)");

static int idle_ms = 400;
module_param(idle_ms, int, 0644);
MODULE_PARM_DESC(idle_ms, "ms mode: ms to idle between critical sections");

static int hold_us = 500;
MODULE_PARM_DESC(hold_us, "us mode: critical section length in us");

static int period_us = 1000;
MODULE_PARM_DESC(period_us, "us mode: full period in us (hold_us + idle). >0 selects us mode");

static int idle_us = 700;
module_param(idle_us, int, 0644);
MODULE_PARM_DESC(idle_us, "us mode: idle part of the period in us");

static DEFINE_SPINLOCK(test_lock);
static DECLARE_WAIT_QUEUE_HEAD(trigger_wq);
static atomic_t triggered = ATOMIC_INIT(0);

static struct task_struct *holder_task;
static u64 hold_count;

static void spin_for_ns(u64 ns)
{
u64 end = ktime_get_ns() + ns;
while (ktime_get_ns() < end)
cpu_relax();
}

static void spin_for_ns_periodic(u64 ns)
{
if (ns > (u64)50 * 1000) /* > 50 us left: udelay in chunks */
udelay(ns / 1000);
else if (ns > 0)
spin_for_ns(ns);
}

static void run_critical_section_us(void)
{
u64 t0_ns = ktime_get_ns();
u64 t1_ns;

spin_lock(&test_lock);
spin_for_ns((u64)hold_us * 1000);
spin_unlock(&test_lock);

t1_ns = ktime_get_ns();
hold_count++;

/* log only every 2000 holds to keep dmesg quiet at kHz rates */
if (hold_count % 2000 == 1)
pr_info("spinlock_holder: cpu %d hold #%llu wall %llu us (%s)\n",
smp_processor_id(), hold_count,
div_u64(t1_ns - t0_ns, 1000),
(t1_ns - t0_ns) > (u64)hold_us * 1200
? "stretched by preemption" : "clean");
}

static void run_critical_section_ms(void)
{
u64 t0_ns = ktime_get_ns();
u64 t1_ns;

spin_lock(&test_lock);
mdelay(hold_ms);
spin_unlock(&test_lock);

t1_ns = ktime_get_ns();
hold_count++;

pr_info("spinlock_holder: cpu %d hold #%llu wall %llu ms (%s)\n",
smp_processor_id(), hold_count,
div_u64(t1_ns - t0_ns, 1000000),
(t1_ns - t0_ns) > (u64)hold_ms * 1200000 / 1000
? "stretched by preemption" : "clean");
}

static int holder_fn(void *unused)
{
while (!kthread_should_stop()) {
if (period_us > 0) {
u64 cycle_start = ktime_get_ns();
s64 spent_ns;

run_critical_section_us();
/* busy-wait the remainder of the period for exact rate.
* s64: if hold overran the period, remainder clamps to 0
* instead of wrapping to ~2^64 ns (which would udelay forever). */
spent_ns = (s64)(ktime_get_ns() - cycle_start);
if (spent_ns < (s64)period_us * 1000)
spin_for_ns_periodic((u64)period_us * 1000 - (u64)spent_ns);
} else if (period_ms > 0) {
run_critical_section_ms();
msleep(max(idle_ms, 1));
} else {
wait_event_interruptible(trigger_wq,
atomic_read(&triggered) || kthread_should_stop());
if (kthread_should_stop())
break;
if (atomic_read(&triggered)) {
run_critical_section_ms();
atomic_set(&triggered, 0);
}
}
}
return 0;
}

static int wake_holder(const char *val, const struct kernel_param *kp)
{
int ret = param_set_int(val, kp);
if (ret)
return ret;
atomic_set(&triggered, 1);
wake_up(&trigger_wq);
if (holder_task)
wake_up_process(holder_task);
return 0;
}

static const struct kernel_param_ops wake_ops = { .set = wake_holder, .get = param_get_int };
module_param_cb(period_ms, &wake_ops, &period_ms, 0644);
module_param_cb(period_us, &wake_ops, &period_us, 0644);
module_param_cb(hold_us, &wake_ops, &hold_us, 0644);

static ssize_t trigger_store(struct kobject *kobj, struct kobj_attribute *attr,
const char *buf, size_t count)
{
if (period_us > 0 || period_ms > 0)
return -EBUSY;
atomic_set(&triggered, 1);
wake_up(&trigger_wq);
return count;
}

static struct kobj_attribute trigger_attribute =
__ATTR(trigger, 0220, NULL, trigger_store);

static struct kobject *demo_kobj;

static int __init spinlock_holder_init(void)
{
struct task_struct *t;
int ret;

/* create parked, bind while parked, then start — kthread_run()+bind()
* races and the bind gets rejected with a WARNING in dmesg */
t = kthread_create(holder_fn, NULL, "spinlock_holder");
if (IS_ERR(t))
return PTR_ERR(t);
kthread_bind(t, demo_cpu);
wake_up_process(t);
holder_task = t;

demo_kobj = kobject_create_and_add("spinlock_holder", kernel_kobj);
if (!demo_kobj) {
kthread_stop(t);
return -ENOMEM;
}

ret = sysfs_create_file(demo_kobj, &trigger_attribute.attr);
if (ret) {
kobject_put(demo_kobj);
kthread_stop(t);
return ret;
}

pr_info("spinlock_holder: loaded, cpu %d, us-mode: hold %d us / period %d us%s\n",
demo_cpu, hold_us, period_us,
period_us > 0 ? " [ACTIVE]" : " (inactive; set period_us>0)");
return 0;
}

static void __exit spinlock_holder_exit(void)
{
kthread_stop(holder_task);
kobject_put(demo_kobj);
pr_info("spinlock_holder: unloaded after %llu holds\n", hold_count);
}

module_init(spinlock_holder_init);
module_exit(spinlock_holder_exit);

MODULE_LICENSE("GPL");
MODULE_DESCRIPTION("PREEMPT_RT demo: spinlock critical section vs schedulable tasks (ms/us modes)");

gpio_pwm.c — the SCHED_FIFO square-wave task (requires sudo apt install -y libgpiod-dev):

// gpio_pwm: toggle a GPIO line every half-period from a SCHED_FIFO task.
// Half period is configurable in microseconds (default 500000 = 1s square
// wave). Edges are timestamped (CLOCK_MONOTONIC) into a ring buffer and
// flushed to edges.log so logging itself never adds jitter.
#define _GNU_SOURCE
#define _DEFAULT_SOURCE
#include <gpiod.h>
#include <sys/mman.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <time.h>
#include <sched.h>
#include <unistd.h>
#include <errno.h>
#include <signal.h>

#define CHIP "gpiochip0"
#define LINE 41
#define NBUF (1 << 20) /* 1M edges ring buffer */

static volatile sig_atomic_t stop = 0;
static void on_sigint(int s) { (void)s; stop = 1; }

static double now_sec(void)
{
struct timespec ts;
clock_gettime(CLOCK_MONOTONIC, &ts);
return ts.tv_sec + ts.tv_nsec / 1e9;
}

struct edge { int level; double t; };
static struct edge ring[NBUF];
static size_t nring;

int main(int argc, char **argv)
{
int cpu = argc > 1 ? atoi(argv[1]) : 3;
long half_us = argc > 2 ? atol(argv[2]) : 500000;
struct gpiod_chip *chip;
struct gpiod_line *line;
struct sched_param sp = { .sched_priority = 80 };
cpu_set_t set;
FILE *log;
double t0, target;
int level = 0;
struct sigaction sa = { .sa_handler = on_sigint };
struct timespec req;

sigaction(SIGINT, &sa, NULL);

CPU_ZERO(&set);
CPU_SET(cpu, &set);
if (sched_setaffinity(0, sizeof(set), &set)) { perror("setaffinity"); return 1; }
if (sched_setscheduler(0, SCHED_FIFO, &sp)) { perror("SCHED_FIFO (run as root)"); }
mlockall(MCL_CURRENT | MCL_FUTURE);

chip = gpiod_chip_open_by_name(CHIP);
if (!chip) { perror("gpiod_chip_open"); return 1; }
line = gpiod_chip_get_line(chip, LINE);
if (!line) { perror("gpiod_chip_get_line"); return 1; }
if (gpiod_line_request_output(line, "gpio_pwm", 0)) { perror("request_output"); return 1; }

fprintf(stderr, "gpio_pwm: toggling %s line %d every %ld us on cpu %d (fifo %d). Ctrl-C to stop.\n",
CHIP, LINE, half_us, cpu, sp.sched_priority);

t0 = now_sec();
target = t0;

while (!stop) {
level = !level;
gpiod_line_set_value(line, level);

if (nring < NBUF) {
ring[nring].level = level;
ring[nring].t = now_sec() - t0;
nring++;
} else {
fprintf(stderr, "ring full, stopping\n");
break;
}

target += half_us / 1e6;
req.tv_sec = (time_t)target;
req.tv_nsec = (long)((target - (time_t)target) * 1e9);
clock_nanosleep(CLOCK_MONOTONIC, TIMER_ABSTIME, &req, NULL);
}

gpiod_line_release(line);
gpiod_chip_close(chip);

log = fopen("edges.log", "w");
if (!log) { perror("fopen edges.log"); return 1; }
for (size_t i = 0; i < nring; i++)
fprintf(log, "%d %.6f\n", ring[i].level, ring[i].t);
fclose(log);
fprintf(stderr, "gpio_pwm: stopped, %zu edges written to edges.log\n", nring);
return 0;
}

Makefile:

# Normal kernel:            make
# RT kernel (JP7.2, no headers pkg): make KDIR=~/rt-kernel-src/kernel-noble
obj-m += spinlock_holder.o

KDIR ?= /lib/modules/$(shell uname -r)/build

all: spinlock_holder.ko gpio_pwm

spinlock_holder.ko:
KBUILD_MODPOST_WARN=1 $(MAKE) -C $(KDIR) M=$(CURDIR) modules

gpio_pwm: gpio_pwm.c
$(CC) -O2 -Wall -o $@ $< $(shell pkg-config --cflags --libs libgpiod)

clean:
$(MAKE) -C $(KDIR) M=$(CURDIR) clean
rm -f gpio_pwm

.PHONY: all clean
tip

To use a different GPIO pin, change the CHIP / LINE macros in gpio_pwm.c. List the available lines on your carrier board with gpioinfo gpiochip0, and pick an unused output-capable line on the 40-pin header.

Build the Interference Module for Both Kernels​

# Standard kernel
make
# Real-time kernel
KBUILD_MODPOST_WARN=1 make KDIR=~/rt-kernel-src/kernel-noble

KBUILD_MODPOST_WARN=1 is required for the real-time build: a tree that only ran modules_prepare has no Module.symvers, so modpost reports every kernel symbol as undefined — all false alarms.

Run the Demos​

GPIO demo (oscilloscope on the GPIO pin), under full CPU load:

stress --cpu 6 --io 4 --vm 2 --vm-bytes 64M &
sudo insmod spinlock_holder.ko demo_cpu=3 hold_us=300 period_us=1000
sudo ./gpio_pwm 3 250

EtherCAT demo (three phases: load only, load + spinlock, load only):

sudo ./run_demo.sh 10 15 15

The script brings up the EtherCAT master, waits for the bus, starts the CPU load, loads and removes the spinlock module on schedule (choosing the right .ko by kernel version), and cleans up at the end.

Known Pitfalls​

SymptomCauseFix
insmod: File exists after changing parametersModule parameters only apply at first loadChange via /sys/module/spinlock_holder/parameters/, or rmmod then insmod again
Interference seems loaded but the waveform is cleanThe holder thread stopped without an error ("fake run")Check that the hold # counter in dmesg keeps advancing; if not, rmmod and reload
insmod: Invalid module formatModule built against the other kernelRebuild against the running kernel's tree
modpost: "kfree" ... undefinedPrepared tree has no Module.symversBuild with KBUILD_MODPOST_WARN=1
openssl/opensslv.h: No such fileMissing libssl-devsudo apt install libssl-dev
EtherCAT port shows Link: DOWNPort grabbed by NetworkManagersudo nmcli dev set <interface> managed no
Actuator refuses to activate after repeated watchdog tripsDrive firmware latch-up after many bus dropsPower-cycle the actuator
Everything breaks after interrupting the demo scriptThe spinlock module was left loadedsudo rmmod spinlock_holder, then power-cycle the actuator if needed

Conclusion​

On the standard kernel, a kernel spinlock held for one second freezes every task on that CPU for one second — including a top-priority SCHED_FIFO EtherCAT master. One second of frame loss is ten times the drive watchdog, so the bus drops out of OP and the motor stops, and repeated interference prevents recovery. On the PREEMPT_RT kernel, the same interference costs the real-time task single-digit microseconds. For hard real-time field buses, the real-time kernel is not "faster" — it is immune to being starved by activity inside the kernel, a property no amount of tuning can guarantee on the standard kernel.

References​

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...