Edge Box RPi 200 with Node Red and InfluxDB
Introduction
Deploying InfluxDB on an Edgebox RPi 200, a Raspberry Pi-powered edge controller, enables robust time-series data collection and analysis at the edge of your network. This setup is ideal for IoT applications, providing real-time insights and monitoring capabilities. By leveraging the lightweight yet powerful InfluxDB database, you can efficiently manage and analyze sensor data directly on the Edgebox. The following guide outlines the steps to install, configure, and use InfluxDB on your Edgebox RPi 200, ensuring a seamless integration into your data infrastructure.
Hardware Preparation
| Edge Box RPi 200 |
|---|
![]() |
Software Preparation
Edge Box comes to your hand pre-installed with Raspberry Pi OS. If you are booting this device for the first time, please read our Getting Started Wiki. We have prepared a Getting Started Guide on Node-RED. It is recommended that you review this guide before proceeding to the wiki. In this tutorial, we are going to connect the Host PC running the YABE room temperature simulator with Node-RED running on Edge Box.
Installing InfluxDB on Edgebox RPi 200
This guide covers the steps to install and set up InfluxDB on an Edgebox RPi 200 edge controller.
Step 1: Update the System
First, ensure your system is up-to-date by running the following command: SSH to EdgeBox and
sudo apt update
Step 2: Add the InfluxDB Repository
Add the InfluxDB GPG key and repository to your system.
Add the GPG key:
curl https://repos.influxdata.com/influxdata-archive.key | gpg --dearmor | sudo tee /usr/share/keyrings/influxdb-archive-keyring.gpg >/dev/null
Add the repository to the sources list:
echo "deb [signed-by=/usr/share/keyrings/influxdb-archive-keyring.gpg] https://repos.influxdata.com/debian stable main" | sudo tee /etc/apt/sources.list.d/influxdb.list
Step 3: Update Package List
Update the package list to include the InfluxDB repository:
sudo apt update
Step 4: Install InfluxDB
Install InfluxDB version 1
sudo apt install influxdb
Start InfluxDB Server
Enable and start the InfluxDB service:
Step 1. Unmask the service:
sudo systemctl unmask influxdb
Step 2. Enable the service:
sudo systemctl enable influxdb
Step 3. Start the service:
sudo systemctl start influxdb
Testing InfluxDB
Access the InfluxDB CLI tool to perform basic database operations.
Step 1. Open terminal :
influx
Step 2. Create a database:
CREATE DATABASE data
Step 3. Use the database:
USE data
Step 4. Insert a sample data point:
INSERT room,temperature=30.1 humidity=80.2
Step 5. Query the inserted data:
SELECT * FROM room
Adding Authentication to InfluxDB
Step 1. Open terminal:
influx
Step 2. Create an admin user with all privileges (replace <password> with your secure password):
CREATE USER admin WITH PASSWORD '<password>' WITH ALL PRIVILEGES
Step 3. Exit the InfluxDB CLI:
exit
Step 4. Edit the InfluxDB configuration to enable authentication:
sudo nano /etc/influxdb/influxdb.conf
Under the [HTTP] section, add or modify the following lines:
auth-enabled = true
pprof-enabled = true
pprof-auth-enabled = true
ping-auth-enabled = true
enabled=true
bind-address=":8086"
Step 5. Restart the InfluxDB service to apply the changes:
sudo systemctl restart influxdb
Step 6. Connect to InfluxDB with the admin user:
influx -username admin -password <password>
Make sure to replace <password> with the password you set for the admin user.
Sending Data to InfluxDB via Node-RED
Step 1. Open your Node-RED in your browser (typically http://<your-edgebox-ip>:1880).
Step 2. Install the node-red-contrib-influxdb using the Node-RED manage palette.
Step 3. Drag and drop an inject node, a function node, and an influxdb out node onto the flow canvas, and connect them as follows:
[Inject Node] -> [Function Node] -> [InfluxDB Out Node]
Function Node
This node formats the data to be sent to InfluxDB.
Step 1. Double-click the function node.
Step 2. Enter a name (e.g., Format Data for InfluxDB).
Step 3. Enter the following code in the function editor:
msg.payload = [
{
temperature: 30.1,
humidity: 80.2
}
];
return msg;
Step 4. Click "Done".
InfluxDB Out Node
This node sends the formatted data to InfluxDB.
Step 1. Double-click the influxdb out node.
Step 2. Enter the following details:
- Name: labdata
- Database: data (previously created)
- Measurement: lab
Step 3. Click the pencil icon to add a new InfluxDB server configuration.
Step 4. Enter the following details:
- Name: InfluxDB
- Version: 1.8-flux
- URL:
http://localhost:8086 - Username: admin
- Password:
<password>(the password you created)
Step 5. Click "Add" and then "Done".
Step 6. Click "Deploy" to save and deploy your flow.
Test the Flow
-
Click the button on the
injectnode to trigger the flow manually. -
Check your InfluxDB database to see if the data has been successfully written by running the following commands on terminal:
influx -username admin -password <password>
USE data
SELECT * FROM lab
Make sure to replace <password> with the password you set for the admin user.
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.