Skip to main content

Firmware Update

SenseCAP ONE Weather Sensor Firmware Update

tip

This firmware update is intended exclusively for the SenseCAP ONE V2 weather station.

V1 vs V2 Weather Stations

V1 and V2 weather stations can be identified by the SKU on the white label or by the base design.

Additionally, the USB Type-C port is located differently: on V1, it is on the same side as the white label, while on V2, it is on the opposite side.

Product NameV1 SKUV2 SKU
S200None101991044
S500101990693101991021
S600-ANone101991232
S700101990787101991022
S700-ANone101991050
S700-BNone101991102
S700-CNone101991141
S800None101991023
S900101990784None
S1000101990902101991024

SenseCAP ONE Configuration Tool

SenseCAP ONE Configuration Tool offers a graphical interface for you to configure the device. And you can download the tool from the GitHub link below:

<https://github.com/Seeed-Solution/SenseCAP-One-Configuration-Tool/releases>

Select the software for the respective operating system, Windows, macOS, or Linux based on your needs.

The next image shows the main interface of the SenseCAP ONE Configuration Tool.

Firmware Update Procedure

  1. Open SenseCAP One Configuration Tool
  1. Connect the device to your computer via the Type-C cable

  2. Open the software, select the correct COM port for the device, and click "Connect"

  1. After connecting, click "Firmware Update"
  1. Select the target board and the corresponding firmware file
  • Select the Master board or Slave Board1
  • Click "Local File" and browse to the firmware folder

  • Click "Update"

  1. Press the Reset button on the device (located next to the Type-C port) after clicking "Update".

The update process will begin a few seconds after pressing the button.

  1. Once the update is complete, press the Reset button again, then click "OK" on the screen.
  1. Repeat the above steps to flash another firmware onto Slave Board 1.

  2. Close the Firmware Update window after completion, Click "Disconnect".

This completes all the firmware upgrade steps for the weather station.

Firmware Resources

2025-04

Loading Comments...