How to flash OS if I replace the CM4 with non-eMMC version
If you want to use a Compute Module 4 without eMMC on the reTerminal, then you need to insert a micro-SD and flash the OS of your choice. Follow the steps below according to your operating system.
-
Step 1. Insert a micro-SD card to the computer using a micro-SD card reader connected to the computer, or by using a built-in card reader on a laptop
-
Step 2. Download Raspberry Pi Imager software by visiting this link
You can choose to download for either Windows, Mac or Ubuntu
- Step 3. Open Raspberry Pi Imager software

- Step 4. Press CTRL + SHIFT + X on the keyboard to open Advanced options window

Here you can set a hostname, enable SSH, set a password, configure wifi, set locale settings and more
- Step 5. Click CHOOSE OS and select your preferred OS

You can select OS such as 64-bit Ubuntu by navigating into Other general purpose OS

-
Step 6. Click CHOOSE STORAGE and select the connected micro-sd card
-
Step 7. Finally, click WRITE

Please wait a few minutes until the flashing process is complete.
- Step 8. Eject the micro-SD card from computer and insert it into the reTerminal.

Note: You need to open the shell of the reTerminal to access the micro-sd card slot