Skip to main content

Get Started with Wio Tracker L1

tip

The Wio Tracker L1 Series share the same hardware framework. Although the video guide was for the L1 Pro, it is applicable to all other products in the L1 series.

Video Tutorial

Part 1 Unboxing

When using the L1, L1 Lite or L1 E-Ink models for the first time, after connecting to USB power supply, lift the power switch upwards to turn it on.

Part 2 Firmware Flashing

note

Please don't use NRF-OTA to update the firmware, it may cause the device to be completely dead.

Part 3 Device Usage

Four-way Joystick

L1 E-Ink firmware currently don't support the four-way joystick. If you want to use the joystick, please purchase other models.

pir

Only the 2.7 firmware support the menu bar. If you want to use the menu bar, follow the Flash Firmware Tutorial to update firmware.

pir

Buzzer

If you want to turn on or off the buzzer, please first update the firmware to 2.7 version. Because only the 2.7 version firmware has the menu bar.

  • Turn on the buzzer Setting (icon shaped like the gear) -> Notification -> Buzzer Action -> Disable
  • Turn off the buzzer Setting (icon shaped like the gear) -> Notification -> Buzzer Action -> All enabled

Part 4 Phone Connection

Part 5 Different States

Get Started

note

When the device is in the states below, please don't manually reboot or turn off it. Or else the device can be dead.

  1. Not finishing the message transmission process
  2. Being configured

Flash Firmware

note

Please don't use NRF-OTA to update the firmware, it may cause the device to be completely dead.

Visit Meshtastic Web Flasher.

For L1, L1 Lite and L1 Pro, select the target device to Seeed Wio Tracker L1 and choose the latest firmware, then click Flash.

pir

pir

For L1 E-Ink, select the target device to Seeed Wio Tracker L1 E-Ink and choose the latest firmware, then click Flash.

pir

pir

Switch on the device, click Enter DFU Mode, there will be a serial port named Tracker L1, click and connect it, and there should be a driver named Tracker L1 display.

pir

Drag the UF2 file to the DFU drive. Firmware should be flashed after the file is downloaded and the device reboots.

Power on the device

Connect the USB cable to activate the device. Lift the power switch upwards to turn it on.

tip

If the device doesn't respond when you press the button, please charge it first. Do not use the fast-charging charger.

Connect via App

  • Select the target device on the Bluetooth panel.

pir

  • Enter the code on the display and then click OK to connect the device.

pir

Connect via Website

If you want to text messages and communicate with other nodes in the website, you can connect the device to the Meshtastic Website now.

Step 1: Open the Website

Click here to go to the webstite.

pir

Step 2: Add the new device

Click "+ New Connection".

pir

There are two ways to connect. You can choose your preferred method.

Method 1: Via Bluetooth

Choose bluetooth method. Choose the device ID in the pop-up window.

pir

Method 2: Via Serial

Choose serial method. Open the device manager to see which port the device is connected to. Choose that port in the pop-up window.

pir

Your device will be shown in the list. Click to connect. If the connection succeed, you can see the device status directly on the website.

pir

Configure the LoRa

In order to start communicating over the mesh, you must set your region. This setting controls which frequency range your device uses and should be set according to your regional location.

pir

Region List

Region CodeDescriptionFrequency Range (MHz)Duty Cycle (%)Power Limit (dBm)
UNSETUnsetN/AN/AN/A
USUnited States902.0 - 928.010030
EU_868European Union 868MHz869.4 - 869.651027

Refer to LoRa Region by Country for a more comprehensive list.

info

EU_868 has to adhere to an hourly duty cycle limitation of 10%, calculated every minute on a rolling 1-hour basis. Your device will stop transmitting if you reach it, until it is allowed again.

Now that you have set the LoRa region on your device, you can continue with configuring any LoRa Configs to suit your needs.

Configure GPS

Please set GPS enabled. You can adjust the update inerval and broadcast interval to obtain a more up-to-date location information.

pir

For IOS, please turn on the Accurate Location. Otherwise, the positioning may deviate.

pir

Sensor connection

pir

You can add sensor to the device via the grove interface. The following sensors have been verified to be compatible with the Grove interface on the device.

Sensor typeSensor Model
Environmental SensorPressureBMP085
TemperatureMCP9808 、PCT2075
Temperature & HumiditySHT31/SHTC3/SHT4X、AHT10
Temperature & Humidity & PressureBME280
OtherHeart Rate & SpO₂MAX30102
I2C KeyboardCardKB
  • Enable Telemetry to get sensor data. If you want to show sensor data on the OLED screen, enale on screen

pir

The OLED will show sensor data if you enable on screen.

pir

Screen Connection

  • E-Ink Screen Click here to get the compatible E-Ink screen.

pir

  • OLED Screen Click here to get the compatible OLED screen. The current OLED driver is SSD1306.

pir

Virtual Keyboard

pir

The 2.7 version firmware now support virtual keyboard! You can type message directly on the device to communicate with other device. Follow the Flash Firmware Tutorial to update firmware.

pir

FAQ

Device bricked & Bootloader installation

Description:

The device is not responding, no LED, can not pair with your App. If you found the device completely dead after flashing your own firmware, you can try re-install the bootloader too.

note

When you are flashing the bootloader, please make sure the cable connection is stable and DO NOT disconnect it during the flash process.

  • Step 1: Click here to download Bootloader

  • step 2: Enter DFU mode

    Double click the RST button to enter DFU mode. The disk name "Tracker L1" will pop out.

    pir

  • step 3: Paste the bootloader file

    Cover all the files in the disk with the downloaded bootloader file.

  • step 4: Flash the firmware

    When you have completed the above steps, then you can follow this step to flash the application firmware. You may need to enter the DFUmode manually

Unable to enter DFU & Entering DFU Mode Manually

Connect the device to your PC, double-press the Reset button. The yellow LED will stay solid, and a new USB drive named Tracker L1 will appear on your PC.

Exiting DFU Mode

Press the Reset button once to exit DFU mode.

Device automatically turn off

Description

  • After the device turning on, it will turn off or reboot automatically after a while.
  • The serial port log ran for a while and then stopped.

This is possibly caused by manually and forcely rebooting or turning off the device when the device is in the following states:not finishing the messages transmission process, being configured......

Troubleshoot

click here to see the video. You need to perform a flash erase, and the re-flash the latest firmware.

Factory Reset

If you want to restore to the default settings, you can do the factory reset. There are two methods for you to do the factory reset.

  • click here to see the video. You need to perform a flash erase, and the re-flash the latest firmware.

  • Click the Factory Reset Button on the App. The device will reboot with the factory configuration automatically.

    pir

NodeDB Reset

NodeDB is the local database that stores information about nodes discovered in the current Mesh network, including:

  • Node ID
  • User Name
  • Location Information
  • Signal Information (SNR)
  • Last Seen Time

When to reset

Reset NodeDB when:

  • The node list contains outdated, duplicate, or invalid entries.
  • You move to a different Mesh environment and want to rediscover nearby nodes.
  • Node information in the app appears incorrect or incomplete.
danger

Resetting NodeDB only clears the node database stored on the device. It does not perform a factory reset and does not remove the device's basic configuration.

Method 1: Reset from the Device

  1. Open the menu on the device.
  2. Go to Node Actions / Settings.
  3. Select Reset NodeDB.
  4. Confirm the reset.

Example Screens

Step 1: Press the device button to enter the menu.

Device button to enter the menu

Step 2: Find Reset NodeDB in the menu.

Reset NodeDB option in the device menu

Method 2: Reset from the App

  1. Open the app and connect to the target device.
  2. Go to Settings.
  3. Tap Device.
  4. Scroll to the bottom of the Device Config page and find Reset NodeDB.
  5. Tap it and confirm the action.

App Path

Settings > Device > Reset NodeDB

Example Screens

Step 1: Open Device from the Settings page.

Device entry in Settings

Step 2: Tap Reset NodeDB on the Device Config page.

Reset NodeDB button in Device Config

tip

Please note the difference between the following options:

  • Reset NodeDB: Only clears the node database.
  • Factory Reset: Restores the device to factory settings and removes more configuration data.

What happens after reset

After Reset NodeDB is executed, the device clears the currently stored node list. As the device continues running, it will rediscover and record nearby nodes again.

You may observe the following:

  • The node list may temporarily become empty or smaller.
  • Nodes will gradually reappear as the device continues operating.
  • Previously stored historical node records will no longer be available.

Notes

  • Before resetting, make sure the issue is actually related to an abnormal node list.
  • If the problem is only a delay in node display, wait for a while first to see whether it recovers automatically.
  • If the issue remains after resetting NodeDB, continue troubleshooting the device configuration or other possible causes.
  • Use Factory Reset carefully to avoid accidentally removing device configuration.

Signal Quality

  • SNR reflects the quality of the communication link. Normal device usually operates above -7 dB. Device with a SNR lower than -10 dB indicates poor performance.

  • RSSI is determined jointly by the device and its surrounding environment. Normal device usually operates above -110 dBm. Device with an RSSI lower than -115 dBm is considered to have poor performance.

    To achieve the best signal effect, please use the device in an open, unobstructed area with minimal interference for use.

Compatible Antenna

If you need a antenna replacement for L1 Pro, click here to get one.

Resources

Resource

Loading Comments...