go2rtc on reComputer
Introduction
go2rtc is an open-source WebRTC framework designed to facilitate real-time media streaming over the internet. It is developed by the XTLS team and aims to combine WebRTC with other media protocols like RTSP, RTMP, and HLS for efficient real-time video and audio transmission.
WebRTC (Web Real-Time Communication) is a widely used protocol for establishing peer-to-peer connections and enabling real-time media exchange such as video calls, live broadcasts, and other real-time applications. go2rtc makes it easier to implement WebRTC in environments where different media protocols need to be converted into WebRTC streams for low-latency and scalable transmission.
Prerequisites
Hardware Requirements
| reComputer R1125 | reComputer AI R2130 | reComputer AI Industrial R2145 |
|---|---|---|
![]() | ![]() | ![]() |
| reComputer Industrial R20xx | reComputer Industrial R21xx |
|---|---|
![]() | ![]() |
Download and run go2rtc
Update system
Please use the following command to run.
sudo apt update
sudo apt upgrade -y
Download go2rtc
Please use the following command to run.
wget https://nightly.link/AlexxIT/go2rtc/workflows/build/master/go2rtc_linux_arm64.zip
tar -xvzf go1.24.0.linux-arm64.tar.gz
chmod +x go2rtc_linux_arm64
Create go2rtc.yaml
Please use the following command to run.
nano go2rtc.yaml
Please fill in the following configuration with your actual IP address.
streams:
stream1:
url: rtsp://admin:[email protected]:554/cam/realmonitor?channel=1&subtype=1
protocol: rtsp
codec: h264
server:
api: :1984
rtsp: :8554
webrtc: :8555
Run go2rtc
Please use the following command to run.
./go2rtc_linux_arm64

Open port 1984 on the host, and click the Streambutton.

Result
Once we have configured everything, we can view the live feed from the current camera.

Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.