Building a smart home control centre around Home Assistant
In this article, we will detail how to set up Home Assistant on Seeed Studio's new product LinkStar H68K and deploy the ESPHome environment. ESPHome is a very common service in Home Assistant. Due to the system limitations of soft routing, we will use ESPHome as an example to guide you through a clever method of installing this service.
Getting Started
If you want to follow this tutorial through everything, you will need to prepare the following.
| LinkStar H68K with Wi-Fi 6 | reRouter CM4 1432 (Optional) | XIAO ESP32C3 |
|---|---|---|
![]() | ![]() | ![]() |
| Get One Now | Get One Now | Get One Now |
*The reRouter CM4 1432 is also compatible with this tutorial. You can purchase LinkStar or reRouter.
The aim of this project is to install Home Assitant and ESPHome using LinkStar's Docker service, and then configure a LinkStar hotspot to connect to LinkStar using the XIAO ESP32C3's WiFi capabilities to complete the network.
Then combined with the vast Grove ecosystem, you can make even more possibilities in Home Assistant.
The content of this tutorial will broadly go through the following steps.
- Configure the Docker environment in LinkStar OpenWRT
- Installation and configuration of Home Assistant, ESPHome
- Add Seeed Studio XIAO ESP32C3 to ESPHome
- Grove Modules with ESPHome and Home Assistant
Configure the Docker environment in LinkStar OpenWRT
Step 1. Install OpenWRT for LinkStar
We have detailed how to install various systems for LinkStar in the LinkStar Wiki. In this tutorial, we will take the OpenWRT system as an example and explain how to install the Home Assistant Container while ensuring that LinkStar acts as a soft route.
Please select above the system location where you would like to install OpenWRT for LinkStar.
Step 2. Configure the LinkStar network
Please connect to LinkStar via a network cable and enter the IP address: 192.168.100.1 in your browser to access the operating backend of OpenWRT.
The initial account password is:
Account: root
Password: password
Next we need to get LinkStar connected to the internet.
You need to purchase a LinkStar with wireless networking, so you can choose to connect a network cable to the LinkStar or to WiFi.
- If it is a wired network, please configure your network according to your network operator's instructions.

- If you want to use a wireless LAN, you can search for a network in the Wireless options.

After that, just enter your network password, click Save and Apply.
Make sure you have a good network state before continuing with the next steps.
Step 3. Allocate more space to Docker
By default, docker is only about 250MB in size, which is not enough for us to install the image, so first we need to expand the capacity for Docker.
Click System --> Disk Man --> EDIT.

In the last line, write the size of the storage space to be added in the END SECTOR column. In my case, it's +20G. Then click NEW button.

Choose the ext4 format, then click FORMAT button.


When it is done, you'll see a new 20GB space is added. However, it's a free space now, you need to mount it to the Docker.
Then choose System --> Mount Points, find Mount Point section, click ADD button.

Choose the new space you've just created.

Choose the Mount Point Use as Docker data (/opt). Don't forget to check the checkbox Enable this mount, then click SAVE & APPLY button.

All settings for the expansion are complete, just need to reboot to make it valid.
Choose System --> Reboot, click the PERFORM REBOOT button. Wait for OpenWRT to reboot and login again.

Installation and configuration of Home Assistant, ESPHome
Step 4. Install Home Assistant with Docker
A better way to install Home Assistant in OpenWRT is to do it on Docker, which ensures that LinkStar is stable as a soft route and also allows Home Assistant to be deployed.
Then all we need to do is pull the specific Home Assistant image. This image will serve us well in installing the ESPHome service later on.
homeassistant/qemuarm-64-homeassistant:latest

We use the downloaded image to create a Container.

On the page where the container is created, we need to make some simple settings.
- Container Name: your container name
- Docker Image: choose just downloaded qemuarm-64-homeassistant image
- Network: choose host mode
- Environment Variables(-e): your environment variable

Once you have filled in the above, save and apply. You will see that the Container has been created. Let we start it.

Step 5. Install ESPHome with Docker
As we are installing the Home Assistant Container, we cannot simply download the ESPHome service via the Add-on shop, so a compromise is needed.
Repeating the above steps, we download the ESPHome image.
esphome/esphome:latest

On the page where the container is created, we need to make some simple settings.
- Container Name: your container name
- Docker Image: choose just downloaded esphome image
- Network: choose host mode
- Environment Variables(-e): your environment variable

Once you have filled in the above, save and apply. You will see that the Container has been created. You also need to start it.

Step 6. Add the ESPHome service to Home Assistant
In order to achieve the same effect as downloading ESPHome in Home Assistant, we need to modify the configuration file under Home Assistant.
Go to the Home Assistant Container.

We go to the terminal in Home Assistant.

Enter the following command in the terminal.
vi configuration.yaml
Add following content to the end of configuration.yaml.
# Example configuration.yaml entry
panel_iframe:
esphome:
title: "ESPHome"
url: "http://192.168.100.1:6052"
icon: mdi:chip
Exit the docker container by type exit in the Home Assistant Container shell. Once this is done, we restart the Home Assistant container.
Create a new browser page, enter IP address 192.168.100.1:8123 and register your Home Assistant account and you will see ESPHome appear in the toolbar on the left.

Add Seeed Studio XIAO ESP32C3 to ESPHome
- Step 1. Click + NEW DEVICE

- Step 2. Click CONTINUE

- Step 3. Enter a Name for the device and enter WiFi credentials such as Network name and Password. Then click NEXT

- Step 4. Select ESP32-C3 and click

- Step 5. Click SKIP because we will configure this board manually

- Step 6. Click EDIT under the newly created board

- Step 7. This will open a YAML file and this file will be used to set all the board configurations. Edit the content under esp32 as follows
esp32:
board: seeed_xiao_esp32c3
variant: esp32c3
framework:
type: arduino
version: 2.0.5
platform_version: 5.2.0
Note: Here we are using the latest version of Arduino core for ESP32 and ESP32 support for PlatformIO

- Step 8. then, please click on the Save button in the top right corner.
LinkStar H68K do not support recognition of external MCU devices, we need to download the compiled firmware first and then upload the firmware via another PC.
- Step 9. Click on the Install button in the top right hand corner. Then select the last item Manual download.

- Step 10. Select Modern format.

It will then take a long time to download and compile, so please be patient. Once everything is ready, the firmware will be automatically downloaded to your computer.

-
Step 11. To upload the firmware to XIAO ESP32C3 there are couple options here we show 2 ways of doing it:
- Option 1: using the ESPhome Web tool to upload.
Make sure you have the right drivers installed. Below are the drivers for common chips used in ESP devices.
- CP2102 drivers: Windows & Mac
- CH342, CH343, CH9102 drivers: Windowns, Mac
- CH340, CH341 drivers: Windowns, Mac
Open the ESPhome Web tool with Chrome or Edge web browser.
Click CONNECT.

select the XIAO ESP32 serial port in the popup window.

Click INSTALL and then select the .bin file downloaded from above steps.


- Option 2: Using the esphome-flasher tool.
If you are still unable to upload firmware using method one after installing the driver and changing browsers, then you can try using method two. Please refer to the official tutorial for specific installation methods and instructions.
If you wish to observe the log messages of the XIAO ESP32C3, you can also view them through the View Logs button of this software.

Once the upload is complete, you can disconnect the XIAO ESP32C3 from the PC (unless you have a need to view the logs) and simply power the XIAO separately.
If all goes well, the XIAO ESP32C3 will search for and connect to the WiFi you have set up for it.
Just like me, I use LinkStar H68K's network. You can find it in the network options and see the IP address assigned to it by LinkStar H68K.

- Step 12. If you see the board status as ONLINE, that means the board is successful connected to WiFi

- Step 13. Connect to XIAO ESP32C3
If you do not have many Home Assistant devices on your LAN, Home Assistant can automatically search for and add your ESP devices to the Devices tab. You can see this device inside the Devices & Services tab in Settings.


If it does not automatically search, you can also connect to the XIAO ESP32C3 based on its IP address.
Click ADD INTEGRSTION and search for esphome.

Then enter the IP address of the XIAO ESP32C3 with port number 6053. Then click on SUBMIT.

If the IP address and port number entered are correct, then you will see that you are asked to enter the Encryption key, which we asked to save in yaml file.
Then click on SUBMIT.

At this point, the steps to add the device have been successfully completed.
Grove Modules with ESPHome and Home Assistant
Now we will connect Grove modules to Seeed Studio XIAO ESP32C3 so that we can display sensor data or control the devices using Home Assistant!
Connect Grove Modules to XIAO ESP32C3
In order to use Grove modules with Seeed Studio XIAO ESP32C3, we will use a Grove Shield for Seeed Studio XIAO and connect XIAO ESP32C3 on it.

After that, the Grove connectors on the board can be used to connect Grove modules
Pin Definitions
You need to follow the table below to use the appropriate internal pin numbers when connecting the Grove modules to the Grove connectors on Grove Shield for Seeed Studio XIAO.
| Internal Pin Number | Pin Mapping |
|---|---|
| 2 | D0 |
| 3 | D1 |
| 4 | D2 |
| 5 | D3 |
| 6 | D4 |
| 7 | D5 |
| 21 | D6 |
| 20 | D7 |
| 8 | D8 |
| 9 | D9 |
| 10 | D10 |
| 6 | SDA |
| 7 | SCL |
For example, if you want to connect a Grove module to D0 port, you need to define the pin on ESPHome as 2

Grove Compatibility List with ESPHome
Currently the following Grove modules are supported by ESPHome
Now we will select 6 Grove modules from the above table and explain how they can be connected with ESPHome and Home Assistant.
Grove - Temperature and Humidity Sensor (AHT20)
Setup Configuration
- Step 1. Connect Grove - Temperature and Humidity Sensor (AHT20) to one of the I2C connectors on the Grove Shield for Seeed Studio XIAO

- Step 2. Inside the xiao-esp32c3.yaml file that we created before, add the following at the end of the file and push it OTA to XIAO ESP32C3
i2c:
sda: 6
scl: 7
sensor:
- platform: aht10
temperature:
name: "Temperature"
humidity:
name: "Humidity"
You can learn more about the AHT10 component here. It allows you to use AHT10, AHT20 and AHT21 based sensors. Here we add the I²C Bus component because AHT20 communicates using I2C protocol.
Visualize on Dashboard
- Step 1. On the Overview page of Home Assistant, click the 3 dots and click Edit Dashboard

- Step 2. Click + ADD CARD

- Step 3. Select By ENTITY, type temperature and select the check box next to Temperature

- Step 4. Repeat the same for Humidity

- Step 5. Click CONTINUE

- Step 6. Click ADD TO DASHBOARD

Now your Home Assistant dashboard will look like below

- Step 7. You can also visualize sensor data as gauges. Click Gauge under BY CARD

- Step 8. Select Temperature from the drop-down menu

- Step 9. Click SAVE

- Step 10. Repeat the same for Humidity

Now your dashboard will look like below

For the Grove - VOC and eCO2 Gas Sensor (SGP30) and Grove - CO2 & Temperature & Humidity Sensor (SCD41) in this wiki, you can follow a similar procedure to visualize the sensor data on the dashboard
Grove - VOC and eCO2 Gas Sensor (SGP30)
Setup configuration
- Step 1. Connect Grove - VOC and eCO2 Gas Sensor (SGP30) to one of the I2C connectors on the Grove Shield for Seeed Studio XIAO

- Step 2. Inside the xiao-esp32c3.yaml file that we created before, add the following at the end of the file and push it OTA to XIAO ESP32C3
i2c:
sda: 6
scl: 7
sensor:
- platform: sgp30
eco2:
name: "eCO2"
accuracy_decimals: 1
tvoc:
name: "TVOC"
accuracy_decimals: 1
You can learn more about the SGP30 component here.
Grove - CO2 & Temperature & Humidity Sensor (SCD41)
Setup configuration
- Step 1. Connect Grove - CO2 & Temperature & Humidity Sensor (SCD41) to one of the I2C connectors on the Grove Shield for Seeed Studio XIAO

- Step 2. Inside the xiao-esp32c3.yaml file that we created before, add the following at the end of the file and push it OTA to XIAO ESP32C3
i2c:
sda: 6
scl: 7
sensor:
- platform: scd4x
co2:
name: "CO2"
temperature:
name: "Temperature"
humidity:
name: "Humidity"
You can learn more about the SGP4x component here
Grove - Relay
Setup configuration
- Step 1. Connect Grove - Relay to one of the Digital ports on the Grove Shield for Seeed Studio XIAO. Here we select D0 port

- Step 2. Inside the xiao-esp32c3.yaml file that we created before, add the following at the end of the file and push it OTA to XIAO ESP32C3
switch:
- platform: gpio
pin: 2
name: "Relay"
You can learn more about the Relay component here
Visualize on Dashboard
- Step 1. Under + ADD CARD that we mentioned before, select BY ENTITY, type relay, select it and click CONTINUE

- Step 2. Click ADD TO DASHBOARD

Now you can turn the relay ON/OFF using the toggle switch

Grove - mini PIR motion sensor
Setup configuration
- Step 1. Connect Grove - mini PIR motion sensor to one of the Digital ports on the Grove Shield for Seeed Studio XIAO. Here we select D0 port

- Step 2. Inside the xiao-esp32c3.yaml file that we created before, add the following at the end of the file and push it OTA to XIAO ESP32C3
binary_sensor:
- platform: gpio
pin: 2
name: "PIR Sensor"
device_class: motion
You can learn more about the PIR component here
Visualize on Dashboard
- Step 1. Under + ADD CARD that we mentioned before, select BY ENTITY, type pir, select it and click CONTINUE

- Step 2. Click ADD TO DASHBOARD

Now if a motion is detected, it will show as Detected

What Next?
Congratulations, you have learned to complete the deployment of Home Assistant on LinkStar and are able to use the ESPHome plugin. For anything similar to not being able to install a Home Assistant Container with Add-on, you can use this method to install other Home Assistant plugin.
We also look forward to having you join our team of creators and bring us more useful examples!
Of course, there is more to the XIAO ESP32C3 than just support for the MR24HPCB1 in Home Assistant, and you can find more tutorials for your own use in this document.
- Connect Grove Modules to Home Assistant using ESPHome (Odyssey)
- XIAO ESP32C3 accesses Home Assistant via ESPHome service
Get your creative juices flowing!
Troubleshooting
FAQ1: I got the following error while uploading firmware using ESPhome Web tool, how can I fix it?

A: If this prompt appears while uploading, disconnect the XIAO ESP32C3 from the PC. Then, hold the BOOT BUTTON, connect the board to your PC while holding the BOOT button, and then release it to enter bootloader mode. At this point it is sufficient to reconnect and upload the firmware again.
FAQ2: I can't install esphome flasher under Linux following the tutorial of esphome flasher?
A: When executing the following commands, you need to select your system version, otherwise an error will occur. For example, my computer is Ubuntu 22.04, then the command that should be executed is as follows.
sudo apt install python3
pip3 install -U \
-f https://extras.wxpython.org/wxPython4/extras/linux/gtk3/ubuntu-22.04/ \
wxPython
pip3 install esphomeflasher
FAQ3: I filled in the correct WiFi and password, why don't I see the IP address of the XIAO ESP32C3?
A: When you encounter this problem, please check that the XIAO ESP32C3's antenna is connected in place. If the antenna is already connected, please make sure that the XIAO is not further than 3m from the LinkStar if possible (unless you have replaced the antenna with a more powerful one). If you still do not see XIAO, you can use the esphome flasher software to check the XIAO log information and check the XIAO connection through the logs. You can re-plug the xiao to let it try to search for WiFi and connect again.
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.