Skip to main content

iSpy on reComputer

Introduction

iSpy is an open-source video surveillance application, designed to work with consumer webcams and IP cameras. It was originally launched in 2007 and has evolved into a full-featured monitoring solution.

pir

Prerequisites

Hardware Requirements

reComputer R1125reComputer AI R2130reComputer AI Industrial R2145
reComputer Industrial R20xxreComputer Industrial R21xx

Download iSpy

Update system

Please use the following command to run.

sudo apt update
sudo apt upgrade -y

Download docker and docker compose

Please use the following command to install docker.

wget https://get.docker.com -O get-docker.sh
chmod +x
sudo sh get-docker.sh
sudo systemctl start docker
sudo systemctl enable docker
docker --version

The result is shown as below:

pir

Please use the following command to install docker compose.

sudo curl -L "https://github.com/docker/compose/releases/download/$(curl -s https://api.github.com/repos/docker/compose/releases/latest | jq -r .tag_name)/docker-compose-$(uname -s)-$(uname -m)" -o /usr/local/bin/docker-compose
sudo chmod +x /usr/local/bin/docker-compose
docker-compose --version

The result is shown as below:

pir

Create docker-compose.yaml

Please use the following command to create docker-compose.yaml.

cd ~ && nano docker-compose.yaml

Then input the following content into the YAML file.

services:
agentdvr:
image: mekayelanik/ispyagentdvr:latest
container_name: AgentDVR
restart: unless-stopped
environment:
- PUID=1000
- PGID=1000
- TZ=America/New_York
- AGENTDVR_WEBUI_PORT=8090
ports:
- "8090:8090"
- "3478:3478/udp"
- "50000-50100:50000-50100/udp"
volumes:
- /appdata/AgentDVR/config/:/AgentDVR/Media/XML/
- /appdata/AgentDVR/media/:/AgentDVR/Media/WebServerRoot/Media/
- /appdata/AgentDVR/commands:/AgentDVR/Commands/

Please use the following command to create necessary folder.

sudo mkdir -p /appdata/AgentDVR/config /appdata/AgentDVR/media /appdata/AgentDVR/commands

Configure iSpy

Run docker compose

Please use the following command to init database.

sudo docker compose up -d

The result is shown as below.

pir

Configure

Open the localhost:8090 port:

pir

Add a camera by following the steps below:

pir

pir

pir

pir

pir

Result

Once we have configured everything, we can view the live feed from the current camera.

pir

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...