Skip to main content

Getting Started with reComputer Robotics J601

Robotics & Physical AI · NVIDIA Jetson AGX Thor

Connect perception and control on one robotics carrier board

The reComputer Robotics J601 carrier board supports NVIDIA Jetson AGX Thor T5000 and T4000 modules for multi-camera perception, sensor fusion, and embodied AI development. Combine high-speed Ethernet, GMSL2 camera expansion, and isolated robotics I/O with the Jetson software platform.

reComputer Robotics J601 carrier board for NVIDIA Jetson AGX Thor modules
Up to 2070 TFLOPSAI performance with a Jetson AGX Thor T5000 module
Up to 4× 10GbEFour RJ45 ports with T5000; three with T4000
Up to 8× GMSL2Multi-camera input through two GMSL extension boards
19–48 V DCWide-range input through an XT30 power connector

Choose Your Jetson Configuration​

The J601 is a carrier board. Select a compatible Jetson AGX Thor module, NVMe SSD, and cooling solution for your build. The J6015 and J6014 names below identify the module-specific configurations and BSP packages used in this guide.

T5000 configuration

reComputer Robotics J6015

Use the T5000 BSP for the configuration with four active 10GbE ports and four isolated CAN interfaces.

AGX Thor T50004× 10GbE4× CAN FD
T4000 configuration

reComputer Robotics J6014

Use the T4000 BSP for the configuration with three active 10GbE ports and two isolated CAN interfaces.

AGX Thor T40003× 10GbE2× CAN FD

Compatible modules: NVIDIA Jetson AGX Thor T5000 and NVIDIA Jetson AGX Thor T4000.

Why reComputer Robotics J601​

Multi-Camera PerceptionGMSL extension boards support up to eight GMSL2 cameras for surround perception and sensor fusion.
High-Speed NetworkingUp to four 10GbE RJ45 connections carry data between sensors, compute nodes, and development systems.
Robotics I/OIsolated CAN FD, RS-232/422/485, I2C, I2S, and digital I/O connect controllers, sensors, and actuators.
Modular ExpansionM.2 Key M supports an NVMe 2280 SSD; Key E and Key B support compatible Wi-Fi/Bluetooth and 4G/5G modules.
Development ConnectivityFour USB 3.2 Type-A ports and HDMI 2.1 connect peripherals and a display, with separate debug and recovery USB-C ports.
Physical AI WorkflowsBuild on Jetson with frameworks such as NVIDIA Isaac, ROS, PyTorch, and Hugging Face, following each framework's platform requirements.

Specifications​

Interface / PropertyJ601 Carrier Board
Module CompatibilityNVIDIA Jetson AGX Thor T5000 / T4000
PCB Size168 mm x 155 mm (without the Jetson AGX Thor module)
Display1x HDMI 2.1
USB4x USB 3.2 Type-A (10Gbps, Host), 1x USB 2.0 Type-C (Debug), 1x USB 3.0 Type-C (Recovery)
Ethernet4x RJ45 10GbE with T5000; 3x RJ45 10GbE with T4000
M.2 Key M1x M.2 Key M for PCIe Gen 4 NVMe 2280 SSD
M.2 Key E1x M.2 Key E for M.2 2230 Wi-Fi module
M.2 Key B1x M.2 Key B for 4G/5G module
Serial1x RS-232/422/485 (DB9 connector)
JST Ports4x CAN with T5000 or 2x CAN with T4000, 1x RS-485, 1x I2S, 1x I2C, 4x GPI, and 4x GPO
Audio1x microphone input and 1x audio output
Fan1x 4-pin fan connector (12V PWM)
RTC1x RTC 2-pin header
LEDs1x green PWR LED, 1x green SSD LED, and 1x RGB USR LED
Buttons1x Recovery button and 1x Reset button
GMSL2x Mini-Fakra connectors for up to 8x GMSL2 cameras
Operating Temperature-10°C to 60°C with thermal grease; -10°C to 55°C with a thermal pad
Power SupplyXT30, 19V to 48V DC
JetPackJetPack 7.1

Hardware Overview​

IndicatorColorRole
PWRGreenPower indicator
SSDGreenStorage activity indicator
USRRGBUser-controllable status LED

For connector pinouts, wiring, interface tests, and RGB LED control, open Hardware & I/O.

Flash JetPack​

This workflow installs JetPack 7.1 (L4T 38.4.0) to an NVMe SSD on the J601 carrier board. Choose the BSP for the installed module: J6015 for T5000 or J6014 for T4000.

caution

Flashing erases data on the target NVMe SSD. Back up important data before starting, and keep power and USB connected until flashing completes.

1

Prepare the Equipment

Step 1 · Set up the Ubuntu host and target hardware

Prepare the following equipment:

  • J601 carrier board with a Jetson AGX Thor T5000 or T4000 module and suitable cooling
  • NVMe M.2 2280 SSD installed in the Key M slot
  • 19–48 V DC power supply connected through XT30
  • Physical Ubuntu 22.04 or 24.04 host PC with at least 220 GB of free storage
  • USB Type-C data cable
  • HDMI display, keyboard, and mouse for first boot
tip

A native Ubuntu host provides the most reliable flashing experience. Seeed Jetson DevelopTool also supports Windows through WSL2; follow its installation guide for host setup.

2

Enter Force Recovery Mode

Step 2 · Connect J4 and verify the installed module

  1. With the board powered off, connect the host PC to the USB 3.0 Type-C recovery/flashing port (J4). The USB 2.0 Type-C debug port (J3) is a separate connector.
  2. Press and hold RECOVERY.
  3. Connect the 19–48 V DC power supply through XT30.
  4. Release RECOVERY after two seconds.
  5. Run the following command on the Ubuntu host:
lsusb
ConfigurationModuleExpected recovery USB ID
J6015AGX Thor T50000955:7026 NVIDIA Corp.
J6014AGX Thor T40000955:7226 NVIDIA Corp.
J601 USB-C flashing port and recovery button connectionsUbuntu host lsusb output while a J601 is in Force Recovery Mode

If the expected ID is missing, check the data cable and recovery port, then repeat the recovery sequence before continuing.

3

Prepare the Matching BSP

Step 3 · Choose software or command-line flashing

Install and launch Seeed Jetson DevelopTool, then prepare the firmware:

  1. Open Flash Center and select reComputer J601 and JetPack 7.1 (L4T 38.4.0).
Jetson DevelopTool Flash Center with reComputer J601 selected
  1. Confirm the recovery wiring from Step 2.
J601 power and USB connections for Jetson DevelopTool
  1. Click Detect Device, confirm the installed module, and click Next.
Jetson DevelopTool detecting the AGX Thor module
  1. Click Download / Prepare BSP. The tool downloads the firmware, verifies its SHA-256 checksum, and extracts the package.
Jetson DevelopTool downloading and preparing the J601 BSP
Watch the Jetson DevelopTool flashing tutorial
4

Flash the NVMe SSD

Step 4 · Use the same flashing method and module selection

Click Start Flash in Jetson DevelopTool and wait for the interface to report success. Keep the power supply and USB data cable connected throughout the process.

5

Complete the First Boot

Step 5 · Configure Ubuntu and check your interfaces

Connect the HDMI display, keyboard, and mouse, and complete Ubuntu's initial system configuration. If the setup screen does not appear after flashing, power-cycle the board after the flashing tool reports success.

Example Jetson Ubuntu first-boot configuration screen

Continue with Hardware & I/O to verify your peripherals, or explore the perception demo. Seeed's carrier-board device-tree and BSP sources are available in Linux_for_Tegra.

Optional: Explore Other Jetson Carrier Boards

After completing setup, you can explore firmware downloads and flashing instructions for other Seeed Jetson carrier boards.

Applications​

Start with a camera-and-LiDAR perception example for reComputer Robotics J601.

Video preview of the J601 camera and LiDAR perception demo
DetectionSensor FusionBEV

Multi-Camera & LiDAR Perception

Replay six camera streams and LiDAR data while Jetson runs TensorRT detection, road segmentation, geometric bird's-eye-view fusion, and pose-aligned local mapping, with synchronized browser views.

Watch the Perception Demo​

The repository documents validation on JetPack 7.2 / L4T R39.2, CUDA 13.2, and TensorRT 10.16.2. Follow its environment and deployment instructions; this page's JetPack 7.1 flash package is a separate software baseline. Build TensorRT engines on the target device for the installed software versions.

The demo uses recorded nuScenes data and geometric camera/LiDAR fusion. Its local map uses dataset-provided poses; segmentation accuracy on nuScenes has not been evaluated. See the repository for validation conditions and dataset/model licenses.

Resources​

Use these resources for board integration, mechanical design, and BSP development.

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible.

Loading Comments...