Skip to main content

Use an SPI Display on reComputer J4012 Classic

Introduction​

This wiki introduces how to connect and drive an SPI display on the Seeed reComputer J4012 Classic. It covers the basic workflow of using an SPI display through the 40-pin header, including hardware wiring, SPI interface configuration, device node checking, dependency installation, compiling a C++ demo, and running a simple display test.

In this guide, an ST7789 SPI LCD display is used as an example. For other SPI display modules, such as ST7735 or ILI9341, the overall workflow is similar, but the wiring details, display resolution, initialization sequence, and driver parameters may be different.

The method in this guide can also be used as a reference for other SPI display applications.

Hardware Preparation​

Required Hardware​

ItemDescription
reComputer J4012 ClassicJetson-based edge AI computer
SPI display moduleThis guide uses an ST7789 SPI LCD display as an example
Dupont wiresUsed to connect the display to the 40-pin header
HDMI display or SSH terminalUsed to configure and test the device

Required Software​

SoftwareDescription
JetPack / UbuntuOperating system running on reComputer J4012 Classic
g++Used to compile the C++ demo
spidevLinux SPI userspace interface
sysfs GPIOUsed to control GPIO pins such as DC and RES

Hardware Connection​

40-pin Header​

The reComputer J4012 Classic provides a 40-pin expansion header. SPI signals and GPIO pins can be used through this header to connect small display modules.

40-pin header pinout

Figure 1. 40-pin header pinout of reComputer J4012 Classic

SPI Display Wiring Example: ST7789​

In this guide, an ST7789 SPI display is used as the example display module. Connect the display to the 40-pin header according to the table below.

ST7789 PinJ4012 Classic 40-pin PinFunctionDescription
GNDPin 6GNDGround
VCCPin 13.3VPower input for the display
SCLPin 23SPI SCLKSPI clock signal
SDAPin 19SPI MOSISPI data from J4012 Classic to the display
RESPin 31GPIO / PQ.06Hardware reset signal
DCPin 29GPIO / PQ.05Data / command selection
CSPin 24SPI CSSPI chip select
BLKPin 173.3VBacklight power, always on

ST7789 SPI display wiring

Figure 2. Wiring between reComputer J4012 Classic and ST7789 SPI display

Enable SPI Interface​

Before running the display demo, the SPI interface on the 40-pin header should be enabled.

Open the Jetson-IO configuration tool:

sudo /opt/nvidia/jetson-io/jetson-io.py

Select the 40-pin header configuration menu.

Jetson-IO main menu

Figure 3. Jetson-IO main menu

Configure header pins manually

Figure 4. Select "Configure header pins manually"

Enable spi1 function

Figure 5. Enable spi1 function on the 40-pin header

Save the configuration and reboot the device:

sudo reboot

After the device reboots, load the spidev kernel module:

sudo modprobe spidev

This step makes sure the Linux userspace SPI driver is available before checking or accessing /dev/spidev*.

Check SPI Device​

After the device reboots, check whether the SPI device node has been generated:

ls /dev/spidev*

If SPI is enabled correctly, you may see output similar to the following:

/dev/spidev0.0
/dev/spidev0.1

Check SPI device node

Figure 6. SPI device node generated successfully

In this guide, the ST7789 display uses the SPI signals connected to Pin 19, Pin 23, and Pin 24. The example code uses /dev/spidev0.0 by default. If your system generates a different SPI device node, please modify the SPI device path in the code.

Install Dependencies​

Update the package list:

sudo apt update

Install the C++ compiler:

sudo apt install -y g++

Check whether the SPI device node exists:

ls /dev/spidev*

GPIO Control​

Before running the display demo, export the GPIO pins used by DC and RES. The demo controls these two pins through the sysfs GPIO interface.

In this guide:

Signal40-pin PinGPIO nameGPIO number
DCPin 29PQ.05453
RESPin 31PQ.06454

When exporting GPIO through /sys/class/gpio/export, use the GPIO number instead of the GPIO name. In this guide, GPIO 453 corresponds to PQ.05, and GPIO 454 corresponds to PQ.06:

sudo sh -c 'echo 453 > /sys/class/gpio/export'
sudo sh -c 'echo 454 > /sys/class/gpio/export'

After exporting, the corresponding GPIO nodes should appear as PQ.05 and PQ.06. Check whether the GPIO nodes exist:

ls /sys/class/gpio/PQ.05
ls /sys/class/gpio/PQ.06

Run the ST7789 Display Demo​

This section uses a C++ demo to verify that the ST7789 SPI display can work correctly on the reComputer J4012 Classic.

The demo performs the following operations:

  1. Opens the SPI device /dev/spidev0.0.
  2. Configures SPI mode, bits per word, and SPI speed.
  3. Controls the DC and RES pins through sysfs GPIO.
  4. Initializes the ST7789 display controller.
  5. Continuously fills the screen with different RGB565 colors.

The wiring used in this demo is shown below.

Signal40-pin PinGPIO / Device
SPI SCLKPin 23SPI clock
SPI MOSIPin 19SPI MOSI
SPI CSPin 24SPI CS
RESPin 31/sys/class/gpio/PQ.06
DCPin 29/sys/class/gpio/PQ.05
BLKPin 173.3V

Create a file named st7789_spi.cpp:

nano st7789_spi.cpp

Add the following C++ demo code:

#include <iostream>
#include <fcntl.h>
#include <unistd.h>
#include <sys/ioctl.h>
#include <linux/spi/spidev.h>
#include <cstdint>
#include <cstring>

int spi_fd = -1;
int dc_fd = -1;
int res_fd = -1;

// GPIO paths for reComputer J4012 Classic
// DC -> Pin 29 -> PQ.05
// RES -> Pin 31 -> PQ.06
const char* DC_DIR_PATH = "/sys/class/gpio/PQ.05/direction";
const char* DC_VAL_PATH = "/sys/class/gpio/PQ.05/value";
const char* RES_DIR_PATH = "/sys/class/gpio/PQ.06/direction";
const char* RES_VAL_PATH = "/sys/class/gpio/PQ.06/value";

bool write_file(const char* path, const char* value)
{
int fd = open(path, O_WRONLY);
if (fd < 0) {
std::cerr << "open failed: " << path << std::endl;
return false;
}

write(fd, value, strlen(value));
close(fd);
return true;
}

bool init_gpios()
{
if (!write_file(DC_DIR_PATH, "out")) return false;
if (!write_file(RES_DIR_PATH, "out")) return false;

dc_fd = open(DC_VAL_PATH, O_WRONLY);
res_fd = open(RES_VAL_PATH, O_WRONLY);

if (dc_fd < 0 || res_fd < 0) {
std::cerr << "open gpio value failed" << std::endl;
return false;
}

return true;
}

void gpio_write(int fd, int value)
{
lseek(fd, 0, SEEK_SET);
write(fd, value ? "1" : "0", 1);
}

void WriteCommand(uint8_t cmd)
{
gpio_write(dc_fd, 0);
write(spi_fd, &cmd, 1);
}

void WriteData(uint8_t data)
{
gpio_write(dc_fd, 1);
write(spi_fd, &data, 1);
}

void WriteDataBuf(const uint8_t* data, size_t len)
{
gpio_write(dc_fd, 1);

const size_t CHUNK_SIZE = 4096;
size_t bytes_sent = 0;

while (bytes_sent < len) {
size_t current_chunk = (len - bytes_sent > CHUNK_SIZE) ? CHUNK_SIZE : (len - bytes_sent);

struct spi_ioc_transfer tr;
std::memset(&tr, 0, sizeof(tr));

tr.tx_buf = (unsigned long)(data + bytes_sent);
tr.rx_buf = 0;
tr.len = current_chunk;
tr.speed_hz = 24000000;
tr.bits_per_word = 8;

if (ioctl(spi_fd, SPI_IOC_MESSAGE(1), &tr) < 0) {
std::cerr << "SPI chunk transfer failed at " << bytes_sent << std::endl;
return;
}

bytes_sent += current_chunk;
}
}

void ST7789_Reset()
{
gpio_write(res_fd, 0);
usleep(200000);

gpio_write(res_fd, 1);
usleep(200000);
}

void ST7789_Init()
{
ST7789_Reset();

WriteCommand(0x11); // Sleep Out
usleep(120000);

WriteCommand(0x3A); // Pixel Format Set
WriteData(0x05); // RGB565

WriteCommand(0x36); // Memory Access Control
WriteData(0x08); // Default direction

WriteCommand(0x21); // Display Inversion ON

WriteCommand(0x29); // Display ON
usleep(20000);
}

void ST7789_SetWindow(uint16_t x0, uint16_t y0, uint16_t x1, uint16_t y1)
{
WriteCommand(0x2A); // Column Address Set
WriteData(x0 >> 8);
WriteData(x0 & 0xFF);
WriteData(x1 >> 8);
WriteData(x1 & 0xFF);

WriteCommand(0x2B); // Row Address Set
WriteData(y0 >> 8);
WriteData(y0 & 0xFF);
WriteData(y1 >> 8);
WriteData(y1 & 0xFF);

WriteCommand(0x2C); // Memory Write
}

void ST7789_FillColor(uint16_t color)
{
const int width = 240;
const int height = 320;

ST7789_SetWindow(0, 0, width - 1, height - 1);

uint8_t screen_buf[height * width * 2];

uint8_t high = color >> 8;
uint8_t low = color & 0xFF;

for (int i = 0; i < height * width * 2; i += 2) {
screen_buf[i] = high;
screen_buf[i + 1] = low;
}

WriteDataBuf(screen_buf, sizeof(screen_buf));
}

bool init_spi()
{
spi_fd = open("/dev/spidev0.0", O_RDWR);
if (spi_fd < 0) {
std::cerr << "open /dev/spidev0.0 failed" << std::endl;
return false;
}

uint8_t mode = SPI_MODE_0;
uint8_t bits = 8;
uint32_t speed = 24000000;

ioctl(spi_fd, SPI_IOC_WR_MODE, &mode);
ioctl(spi_fd, SPI_IOC_WR_BITS_PER_WORD, &bits);
ioctl(spi_fd, SPI_IOC_WR_MAX_SPEED_HZ, &speed);

return true;
}

uint16_t Rainbow_HSV_To_RGB565(int h)
{
float r = 0, g = 0, b = 0;

int sector = h / 60;
float fractional = (h % 60) / 60.0f;

float x = 1.0f - fractional;
float y = fractional;

switch (sector) {
case 0: r = 1.0f; g = y; b = 0.0f; break;
case 1: r = x; g = 1.0f; b = 0.0f; break;
case 2: r = 0.0f; g = 1.0f; b = y; break;
case 3: r = 0.0f; g = x; b = 1.0f; break;
case 4: r = y; g = 0.0f; b = 1.0f; break;
case 5: r = 1.0f; g = 0.0f; b = x; break;
default: r = 0.0f; g = 0.0f; b = 0.0f; break;
}

uint8_t R8 = static_cast<uint8_t>(r * 255);
uint8_t G8 = static_cast<uint8_t>(g * 255);
uint8_t B8 = static_cast<uint8_t>(b * 255);

return ((R8 >> 3) << 11) | ((G8 >> 2) << 5) | (B8 >> 3);
}

int main()
{
uint16_t color = 0x001F;
int i = 0;

std::cout << "Init SPI..." << std::endl;
if (!init_spi()) return -1;

std::cout << "Init GPIO..." << std::endl;
if (!init_gpios()) return -1;

std::cout << "Init ST7789..." << std::endl;
ST7789_Init();

std::cout << "Fill 240x320 Color..." << std::endl;

while (1) {
color = Rainbow_HSV_To_RGB565(i++ % 360);
ST7789_FillColor(color);
usleep(10000);
}

close(spi_fd);
close(dc_fd);
close(res_fd);

return 0;
}

Compile the demo:

g++ st7789_spi.cpp -o st7789_spi

Run the demo:

sudo ./st7789_spi

If the wiring and SPI configuration are correct, the ST7789 display should continuously refresh with different colors.

ST7789 display demo result

Figure 7. ST7789 display demo result

Code Explanation​

SPI Initialization​

The demo opens /dev/spidev0.0 and configures the SPI interface as follows.

ParameterValue
SPI device/dev/spidev0.0
SPI modeSPI_MODE_0
Bits per word8
SPI speed24000000 Hz

If your system generates a different SPI device node, modify the following line in the demo code:

spi_fd = open("/dev/spidev0.0", O_RDWR);

For example, if your device node is /dev/spidev1.0, change it to:

spi_fd = open("/dev/spidev1.0", O_RDWR);

GPIO Control​

The demo uses sysfs GPIO to control the DC and RES pins.

Signal40-pin Pinsysfs GPIO path
DCPin 29/sys/class/gpio/PQ.05
RESPin 31/sys/class/gpio/PQ.06

The DC pin is used to switch between command mode and data mode. The RES pin is used to reset the ST7789 display.

ST7789 Initialization​

The demo initializes the ST7789 display with the following commands.

CommandDescription
0x11Sleep Out
0x3APixel Format Set
0x05RGB565 format
0x36Memory Access Control
0x21Display Inversion On
0x29Display On

Screen Fill Test​

The demo uses RGB565 format to fill the full screen. The display resolution used in the demo is:

const int width = 240;
const int height = 320;

If your ST7789 display uses a different resolution, modify these values according to the actual screen size.

SPI Data Transfer​

The full screen buffer is larger than a single small SPI transfer. Therefore, the demo sends display data in chunks:

const size_t CHUNK_SIZE = 4096;

This avoids transfer size limitations and makes the full-screen refresh more stable.

Troubleshooting​

No /dev/spidev* Device Found​

Possible causes:

  1. The SPI interface is not enabled.
  2. The Jetson-IO configuration was not saved.
  3. The device was not rebooted after enabling SPI.
  4. The device tree does not expose the SPI device node.
  5. The system image does not include the expected SPI configuration.

Suggested checks:

ls /dev/spidev*

If no SPI device is found, run Jetson-IO again and check whether SPI is enabled.

Permission Denied When Accessing SPI or GPIO​

If you see a permission error when running the C++ demo, try running it with sudo:

sudo ./st7789_spi

You can also check the permission of the SPI device and GPIO nodes:

ls -l /dev/spidev*
ls -l /sys/class/gpio/PQ.05/value
ls -l /sys/class/gpio/PQ.06/value

GPIO Path Does Not Exist​

If /sys/class/gpio/PQ.05 or /sys/class/gpio/PQ.06 does not exist, the GPIO pins may not have been exported correctly.

Please check the available GPIO nodes:

ls /sys/class/gpio/

Then export the GPIO pins again:

sudo sh -c 'echo 453 > /sys/class/gpio/export'
sudo sh -c 'echo 454 > /sys/class/gpio/export'

SPI Can Be Opened but the Display Shows Nothing​

Possible causes:

  1. The display wiring is incorrect.
  2. The SPI device path is incorrect.
  3. The CS, DC, or RES pins are not connected correctly.
  4. The display controller is not ST7789.
  5. The display requires a different initialization sequence.
  6. The backlight pin is not powered.

Suggested checks:

  1. Confirm that VCC is connected to Pin 1.
  2. Confirm that GND is connected to Pin 6.
  3. Confirm that BLK is connected to Pin 17 and the backlight is on.
  4. Confirm that SCL, SDA, and CS are connected to Pin 23, Pin 19, and Pin 24.
  5. Confirm that RES and DC are connected to Pin 31 and Pin 29.
  6. Reduce the SPI speed and test again.
  7. Confirm the display controller model from the display module datasheet.

Backlight Is On but No Image Is Displayed​

If the backlight is on but no image is displayed, the power wiring may be correct, but SPI communication or display initialization may be incorrect.

Please check:

  1. Whether the correct SPI device is used.
  2. Whether the DC and RES pins are configured correctly.
  3. Whether the display driver matches the ST7789 controller.
  4. Whether the screen resolution is correct.
  5. Whether the display module requires row or column offset settings.

Image Color Is Abnormal​

Possible causes:

  1. RGB and BGR color order mismatch.
  2. Display inversion setting is different.
  3. The MADCTL parameter is not suitable for your panel.
  4. The display module uses a slightly different ST7789 initialization sequence.

Suggested solutions:

  1. Try changing the MADCTL value.
  2. Try enabling or disabling display inversion.
  3. Check the ST7789 display module datasheet.
  4. Confirm whether your module uses RGB or BGR color order.

Image Direction Is Incorrect​

If the image is rotated or mirrored, modify the MADCTL command parameter in the initialization function:

WriteCommand(0x36);
WriteData(0x08);

The correct value depends on the display module orientation.

Display Refresh Is Slow​

Possible causes:

  1. SPI clock speed is too low.
  2. The program refreshes the full screen every time.
  3. The display module has limited refresh performance.
  4. The C++ demo uses a simple full-screen fill method for verification.

Suggested solutions:

  1. Increase SPI clock speed gradually.
  2. Avoid unnecessary full-screen refresh.
  3. Refresh only changed areas if your application supports it.
  4. Use the current color fill test only as a basic hardware verification demo.

Summary​

In this wiki, we introduced how to connect an SPI display to the Seeed reComputer J4012 Classic through the 40-pin header. The general SPI display workflow includes wiring the display, enabling the SPI interface, checking the SPI device node, installing dependencies, compiling a C++ demo, and running a display test. JetPack 5 uses sysfs GPIO, JetPack 6 uses libgpiod with manual pinmux configuration, and JetPack 7 uses libgpiod with GPIO pins configured directly in the Jetson Expansion Header Tool.

The ST7789 SPI LCD was used as the example display module in this guide. For other SPI displays, the overall process is similar, but the display driver, resolution, initialization sequence, and wiring details should be adjusted according to the actual display module.

Resources​

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...