Skip to main content

Getting started with SO-ARM100 and SO-ARM101 robotic arm with LeRobot

tip

This tutorial maintenance has been updated to the latest version of lerobot, if you want to refer to the tutorial of the previous version, please click here.

Introduction

The SO-10xARM is a fully open-source robotic arm project launched by TheRobotStudio. It includes the follower arm and the leader robotic arm, and also provides detailed 3D printing files and operation guides. LeRobot is committed to providing models, datasets and tools for real-world robotics in PyTorch. Its aim is to reduce the entry barrier of robotics, enabling everyone to contribute and benefit from sharing datasets and pretrained models. LeRobot integrates cutting-edge methodologies validated for real-world application, centering on imitation learning. It has furnished a suite of pre-trained models, datasets featuring human-gathered demonstrations, and simulation environments, enabling users to commence without the necessity of robot assembly. In the forthcoming weeks, the intention is to augment support for real-world robotics on the most cost-effective and competent robots presently accessible.

Projects Introduction

The SO-ARM10x and reComputer Jetson AI intelligent robot kit seamlessly combine high-precision robotic arm control with a powerful AI computing platform, providing a comprehensive robot development solution. This kit is based on the Jetson Orin or AGX Orin platform, combined with the SO-ARM10x robotic arm and the LeRobot AI framework, offering users an intelligent robot system applicable to multiple scenarios such as education, research, and industrial automation. This wiki provides the assembly and debugging tutorial for the SO ARM10x and realizes data collection and training within the Lerobot framework.

Main Features

  1. Open-source and low-cost: It is an open-source, low-cost robotic arm solution from TheRobotStudio
  2. Integration with LeRobot: Designed for integration with LeRobot platform
  3. Abundant learning resources: Provides comprehensive open-source learning resources like assembly and calibration guides, and tutorials for testing, data collection, training and deployment to assist users in quickly getting started and developing robotic applications.
  4. Compatible with Nvidia: Deploy this arm kit with reComputer Mini J4012 Orin NX 16 GB.
  5. Multi-Scene Application: It is applicable to fields such as education, scientific research, automated production, and robotics, helping users achieve efficient and precise robot operations in various complex tasks.

What's news:

  • Wiring optimization: Compared to SO-ARM100, SO-ARM101 features improved wiring that prevents disconnection issues previously seen at joint 3. The new wiring design also no longer limits the range of motion of the joints.
  • Different gear ratios for the leader arm: The leader arm now uses motors with optimized gear ratios, improving performance and eliminating the need for external gearboxes.
  • New functionality support: The leader arm can now follow the follower arm in real-time, which is crucial for the upcoming learning policy, where a human can intervene and correct the robot’s actions.
caution

Seeed Studio is only responsible for the quality of the hardware itself. The tutorials are strictly updated in accordance with the official documentation. If you encounter software issues or environment dependency problems that cannot be resolved, in addition to checking the FAQ section at the end of this tutorial, please promptly report the issue to the LeRobot platform or the LeRobot Discord channel.

Specification

TypeSO-ARM100SO-ARM101
Arm KitArm Kit ProArm KitArm Kit Pro
Leader Arm12x ST-3215- C001 (7.4V) motors with 1:345 gear ratio for all joints12x ST-3215-C018/ST-3215-C047 (12V) motors with 1:345 gear ratio for all joints

1x ST-3215- C001 (7.4V) motor with 1:345 gear ratio for joint 2 only
2x ST-3215-C044 (7.4V) motors with 1:191 gear ratio for joints 1 and 3
3x ST-3215-C046 (7.4V) motors with 1:147 gear ratio for joints 4, 5, and gripper (joint 6)

Follower ArmSame as SO-ARM100
Power Supply5.5 mm × 2.1 mm DC 5 V 4 A5.5 mm × 2.1 mm DC 12 V 2 A5.5 mm × 2.1 mm DC 5 V 4 A

5.5 mm × 2.1 mm DC 12 V 2 A (Follower Arm)
5.5 mm × 2.1 mm DC 5 V 4 A (Leader Arm)

Angle Sensor12-bit magnetic encoder
Recommended Operating Temperature0 °C to 40 °C
CommunicationUART
Control MethodPC
danger

If you purchase the Arm Kit version, both power supplies are 5V. If you purchase the Arm Kit Pro version, please use the 5V power supply for the calibration and every step of the Leader robotic arm, and the 12V power supply for the calibration and every step of the Follower robotic arm.

Bill of Materials(BOM)

PartAmountIncluded
Servo Motos12
Motor Control Board2
USB-C Cable 2 pcs1
Power Supply22
Table Clamp4
3D printed parts of the arm1Option

Initial System Environment

For Ubuntu x86:

  • Ubuntu 22.04
  • CUDA 12+
  • Python 3.10
  • Torch 2.6+

For Jetson Orin:

  • Jetson JetPack 6.0 and 6.1, not support 6.1
  • Python 3.10
  • Torch 2.3+

Table of Contents

A. 3D Printing Guide

B. Install LeRobot

C. Configure the motors

D. Assembly

E. Calibrate

F. Teleoperate

G. Add cameras

H. Record the dataset

I. Visualize the dataset

J. Replay an episode

K. Train a policy

L. Evaluate your policy

3D Printing Guide

caution

Following the official update of SO101, SO100 will no longer support it and the source files will be deleted as per the official, but the source files can still be found in our Makerworld. However, for users who have previously purchased SO100, the tutorials and installation methods remain compatible. The print of SO101 is fully compatible with the motor kit installation of SO100.

Step 1: Choose a printer

The STL files provided are ready to print on many FDM printers. Below are the tested and suggested settings though others may work.

  • Material: PLA+
  • Nozzle Diameter and Precision: 0.4mm nozzle diameter at 0.2mm layer height or 0.6mm nozzle at 0.4mm layer height.
  • Infill Density: 15%

Step 2: Set up the printer

  • Ensure that the printer is calibrated and the bed level is correctly set using the printer specific instructions.
  • Clean the print bed, making sure it is free from dust, or grease. If cleaning the bed using water, or other liquid, dry the bed.
  • If your printer recommends it, use a standard glue stick and apply a thin, even layer of glue across the print area of the bed. Avoid clumping or uneven application.
  • Load the printer filament using printer specific instructions.
  • Ensure the printer settings match the ones suggested above (most printers have multiple settings so choose the ones that most closely match).
  • Set for supports everywhere but ignore slopes greater than 45 degrees to the horizontal.
  • There should be no supports in the screw holes with horizontal axes.

Step 3: Print the parts

All the parts for the leader or follower are for easy 3D printing already contained in a single file, correctly orientated for z upwards to minimize supports.

  • For printer bed sizes of 220mmx220mm (such as the Ender), print these files:

  • For printer bed sizes of 205mm x 250mm (such as the Prusa/Up):

Install LeRobot

Environments such as pytorch and torchvision need to be installed based on your CUDA.

  1. Install Miniconda: For Jetson:
wget https://repo.anaconda.com/miniconda/Miniconda3-latest-Linux-aarch64.sh
chmod +x Miniconda3-latest-Linux-aarch64.sh
./Miniconda3-latest-Linux-aarch64.sh
source ~/.bashrc

Or, For X86 Ubuntu 22.04:

mkdir -p ~/miniconda3
cd miniconda3
wget https://repo.anaconda.com/miniconda/Miniconda3-latest-Linux-x86_64.sh -O ~/miniconda3/miniconda.sh
bash ~/miniconda3/miniconda.sh -b -u -p ~/miniconda3
rm ~/miniconda3/miniconda.sh
source ~/miniconda3/bin/activate
conda init --all
  1. Create and activate a fresh conda environment for lerobot
conda create -y -n lerobot python=3.10 && conda activate lerobot
  1. Clone Lerobot:
git clone https://github.com/Seeed-Projects/lerobot.git ~/lerobot
  1. When using miniconda, install ffmpeg in your environment:
conda install ffmpeg -c conda-forge
tip

This usually installs ffmpeg 7.X for your platform compiled with the libsvtav1 encoder. If libsvtav1 is not supported (check supported encoders with ffmpeg -encoders), you can:

  • [On any platform] Explicitly install ffmpeg 7.X using:
conda install ffmpeg=7.1.1 -c conda-forge
  • [On Linux only] Install ffmpeg build dependencies and compile ffmpeg from source with libsvtav1, and make sure you use the corresponding ffmpeg binary to your install with which ffmpeg.

If you encounter an error like this, you can use this command too.

  1. Install LeRobot with dependencies for the feetech motors:
cd ~/lerobot && pip install -e ".[feetech]"

For Jetson Jetpack 6.0+ devices (please make sure to install Pytorch-gpu and Torchvision from step 5 before executing this step):

conda install -y -c conda-forge "opencv>=4.10.0.84"  # Install OpenCV and other dependencies through conda, this step is only for Jetson Jetpack 6.0+
conda remove opencv # Uninstall OpenCV
pip3 install opencv-python==4.10.0.84 # Then install opencv-python via pip3
conda install -y -c conda-forge ffmpeg
conda uninstall numpy
pip3 install numpy==1.26.0 # This should match torchvision
  1. Check Pytorch and Torchvision

Since installing the lerobot environment via pip will uninstall the original Pytorch and Torchvision and install the CPU versions of Pytorch and Torchvision, you need to perform a check in Python.

import torch
print(torch.cuda.is_available())

If the printed result is False, you need to reinstall Pytorch and Torchvision according to the official website tutorial.

If you are using a Jetson device, install Pytorch and Torchvision according to this tutorial.

Configure the motors

The servo calibration and initialization process for SO-ARM101 is the same as that of SO-ARM100 in terms of both method and code. However, please note that the gear ratios for the first three joints of the SO-ARM101 Leader Arm differ from those of SO-ARM100, so it’s important to distinguish and calibrate them carefully.

To configure the motors designate one bus servo adapter and 6 motors for your leader arm, and similarly the other bus servo adapter and 6 motors for the follower arm. It's convenient to label them and write on each motor if it's for the follower F or for the leader L and it's ID from 1 to 6. We use F1–F6 to represent joints 1 to 6 of the Follower Arm, and L1–L6 to represent joints 1 to 6 of the Leader Arm. The corresponding servo model, joint assignments, and gear ratio details are as follows:

Servo ModelGear RatioCorresponding Joints
ST-3215-C044(7.4V)1:191L1
ST-3215-C001(7.4V)1:345L2
ST-3215-C044(7.4V)1:191L3
ST-3215-C046(7.4V)1:147L4–L6
ST-3215-C001(7.4V) / C018(12V) / C047(12V)1:345F1–F6
danger

You now should plug the 5V or 12V power supply to the motor bus. 5V for the STS3215 7.4V motors and 12V for the STS3215 12V motors. Note that the leader arm always uses the 7.4V motors, so watch out that you plug in the right power supply if you have 12V and 7.4V motors, otherwise you might burn your motors! Now, connect the motor bus to your computer via USB. Note that the USB doesn't provide any power, and both the power supply and USB have to be plugged in.

The following are the code calibration steps, please calibrate with the reference wiring servo in the picture above

Find USB ports associated to your arms To find the correct ports for each arm, run the utility script twice:

lerobot-find-port

Example output:

Finding all available ports for the MotorBus.
['/dev/ttyACM0', '/dev/ttyACM1']
Remove the usb cable from your MotorsBus and press Enter when done.

[...Disconnect corresponding leader or follower arm and press Enter...]

The port of this MotorsBus is /dev/ttyACM1
Reconnect the USB cable.
tip

Remember to remove the usb, otherwise the interface will not be detected.

Example output when identifying the follower arm's port (e.g., /dev/tty.usbmodem575E0031751 on Mac, or possibly /dev/ttyACM0 on Linux):

Example output when identifying the leader arm's port (e.g., /dev/tty.usbmodem575E0032081, or possibly /dev/ttyACM1 on Linux):

You might need to give access to the USB ports by running:

sudo chmod 666 /dev/ttyACM0
sudo chmod 666 /dev/ttyACM1

Configure your motors

danger

Please use a 5V power supply for calibrating Leader motors (ST-3215-C046, C044, 001).

Leader Arm Joint 6 CalibrationLeader Arm Joint 5 CalibrationLeader Arm Joint 4 CalibrationLeader Arm Joint 3 CalibrationLeader Arm Joint 2 CalibrationLeader Arm Joint 1 Calibration
fig1fig2fig3fig4fig5fig6
danger

If you buy the Arm Kit version (ST-3215-C001), use a 5V power supply. If you buy the Arm Kit Pro version, please use a 12V power supply to calibrate the servo (ST-3215-C047/ST-3215-C018).

Follower Arm Joint 6 CalibrationFollower Arm Joint 5 CalibrationFollower Arm Joint 4 CalibrationFollower Arm Joint 3 CalibrationFollower Arm Joint 2 CalibrationFollower Arm Joint 1 Calibration
fig1fig2fig3fig4fig5fig6
tip

Again, please make sure that the servo joint IDs and gear ratios strictly correspond to those of the SO-ARM101.

Connect the usb cable from your computer and the power supply to the follower arm’s controller board. Then, run the following command.

lerobot-setup-motors \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 # <- paste here the port found at previous step

You should see the following instruction.

Connect the controller board to the 'gripper' motor only and press enter.

As instructed, plug the gripper’s motor. Make sure it’s the only motor connected to the board, and that the motor itself is not yet daisy-chained to any other motor. As you press [Enter], the script will automatically set the id and baudrate for that motor.

You should then see the following message:

'gripper' motor id set to 6

Followed by the next instruction:

Connect the controller board to the 'wrist_roll' motor only and press enter.

You can disconnect the 3-pin cable from the controller board, but you can leave it connected to the gripper motor on the other end, as it will already be in the right place. Now, plug in another 3-pin cable to the wrist roll motor and connect it to the controller board. As with the previous motor, make sure it is the only motor connected to the board and that the motor itself isn’t connected to any other one.

caution

Repeat the operation for each motor as instructed.

tip

Check your cabling at each step before pressing Enter. For instance, the power supply cable might disconnect as you manipulate the board.

When you are done, the script will simply finish, at which point the motors are ready to be used. You can now plug the 3-pin cable from each motor to the next one, and the cable from the first motor (the ‘shoulder pan’ with id=1) to the controller board, which can now be attached to the base of the arm.

Do the same steps for the leader arm.

lerobot-setup-motors \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM0 # <- paste here the port found at previous step

Assembly

tip
  • The dual-arm assembly process of SO-ARM101 is the same as that of SO-ARM100. The only differences are the addition of cable clips on SO-ARM101 and the different gear ratios of the joint servos on the Leader Arm. So both SO100 and SO101 can be installed by referring to the following content
  • Before assembly, please check your motor model and reduction ratio again. If you have purchased SO100, you can ignore this step. If you have purchased SO101, please check the following table to distinguish F1 to F6 and L1 to L6.
Servo ModelGear RatioCorresponding Joints
ST-3215-C044(7.4V)1:191L1
ST-3215-C001(7.4V)1:345L2
ST-3215-C044(7.4V)1:191L3
ST-3215-C046(7.4V)1:147L4–L6
ST-3215-C001(7.4V) / C018(12V) / C047(12V)1:345F1–F6
danger

If you purchased the SO101 Arm Kit Standard Edition, all power supplies are 5V. If you purchased the SO101 Arm Kit Pro Edition, the Leader Arm should be calibrated and operated at every step using a 5V power supply, while the Follower Arm should be calibrated and operated at every step using a 12V power supply.

Assemble Leader Arm

Step 1Step 2Step 3Step 4Step 5Step 6
fig1fig2fig3fig4fig5fig6
Step 7Step 8Step 9Step 10Step 11Step 12
fig1fig2fig3fig4fig5fig6
Step 13Step 14Step 15Step 16Step 17Step 18
fig1fig2fig3fig4fig5fig6
Step 19Step 20
fig1fig2

Assemble Follower Arm

tip
  • The steps for assembling the Follower Arm are generally the same as those for the Leader Arm. The only difference lies in the installation method of the end-effector (gripper and handle) after Step 12.
Step 1Step 2Step 3Step 4Step 5Step 6
fig1fig2fig3fig4fig5fig6
Step 7Step 8Step 9Step 10Step 11Step 12
fig1fig2fig3fig4fig5fig6
Step 13Step 14Step 15Step 16Step 17
fig1fig2fig3fig4fig5

Calibrate

tip

The SO100 and SO101 codes are compatible. Users of SO100 can directly utilize SO101's parameters and code for operation.

danger

If you purchased the SO101 Arm Kit Standard Edition, all power supplies are 5V. If you purchased the SO101 Arm Kit Pro Edition, the Leader Arm should be calibrated and operated at every step using a 5V power supply, while the Follower Arm should be calibrated and operated at every step using a 12V power supply.

Next, you need to connect the power supply and data cable to your SO-10x robot for calibration to ensure that the leader and follower arms have the same position values when they are in the same physical position. This calibration is essential because it allows a neural network trained on one SO-10x robot to work on another. If you need to recalibrate the robotic arm, delete the files under ~/.cache/huggingface/lerobot/calibration/robots or ~/.cache/huggingface/lerobot/calibration/teleoperators and recalibrate the robotic arm. Otherwise, an error prompt will appear. The calibration information for the robotic arm will be stored in the JSON files under this directory.

tip

On PC (Linux) and Jetson devices, the first USB device you plug in typically maps to ttyACM0, and the second maps to ttyACM1. Double-check which port is mapped to the leader and follower before running commands.

Manual calibration of follower arm

Please connect the interfaces of the 6 robot servos via a 3-pin cable and connect the chassis servo to the servo drive plate, then run the following command or API example to calibrate the robot arm:

Interface permissions are given first

sudo chmod 666 /dev/ttyACM*

Then calibrate the follower arm

lerobot-calibrate \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \# <- The port of your robot
--robot.id=my_awesome_follower_arm # <- Give the robot a unique name

The video below shows how to perform the calibration. First you need to move the robot to the position where all joints are in the middle of their ranges. Then after pressing enter you have to move each joint through its full range of motion.

Manual calibration of leader arm

Do the same steps to calibrate the leader arm, run the following command or API example:

lerobot-calibrate \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \# <- The port of your robot
--teleop.id=my_awesome_leader_arm # <- Give the robot a unique name

(Optional) Middle-position calibration with the Seeed Studio SoARM quick tool

When calibrating or running the robot, if you see errors like:

Magnitude 30841 exceeds 2047 (max for sign_bit_index=11)

This usually means the current position / zero-offset of a servo is abnormal, causing the read angle to exceed the expected range. In that case, you can use Seeed Studio’s SoARM tool to do a middle-position calibration (write the current position to the middle value 2048), and then redo the full-arm calibration.

1) Clone the tool from GitHub and install dependencies

git clone https://github.com/Seeed-Projects/Seeed_RoboController.git
cd Seeed_RoboController
pip install -r requirements.txt

2) Middle-position calibration and verification

Script locations:

  • src/tools/servo_middle_calibration.py: middle-position calibration (write current position as 2048)
  • src/tools/servo_disable.py: disable servo torque (easier to rotate joints by hand)
  • src/tools/servo_center_test.py: move to 2048 to verify the calibration result

Run in order (the commands will interactively ask you to select a port):

  1. (Optional) Disable torque to adjust joints manually:
python -m src.tools.servo_disable
  1. Do middle-position calibration (set current position to 2048):
python -m src.tools.servo_middle_calibration
  1. Verify: move the servo to 2048 and check if it returns to the expected middle position:
python -m src.tools.servo_center_test

After the middle-position calibration, return to the lerobot-calibrate steps above and redo the full-arm calibration.

Teleoperate

Simple teleop Then you are ready to teleoperate your robot! Run this simple script (it won't connect and display the cameras):

Note that the id associated with a robot is used to store the calibration file. It’s important to use the same id when teleoperating, recording, and evaluating when using the same setup.

sudo chmod 666 /dev/ttyACM*
lerobot-teleoperate \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=my_awesome_leader_arm

The teleoperate command will automatically:

  1. Identify any missing calibrations and initiate the calibration procedure.
  2. Connect the robot and teleop device and start teleoperation.

Add cameras

If using RealSense D435i/D405

RealSense depth cameras can provide RGB-D perception for LeRobot and are suitable for tasks such as object recognition, point cloud reconstruction, and tabletop manipulation. The recommended models here are RealSense D405 and RealSense D435i.

RealSense D405

The RealSense D405 is a short-range stereo depth camera designed for high-precision close-range tasks such as tabletop robotic manipulation, with a typical working range of 7 cm to 50 cm.

RealSense D435i

The RealSense D435i combines depth sensing, RGB imaging, and an IMU, making it suitable for mid- to close-range applications such as 3D reconstruction, SLAM, and robotic environment perception.

1. Switch to the Camera Branch

Current camera support is available on the DepthCameraSupport branch:

git checkout DepthCameraSupport
git pull origin DepthCameraSupport

Confirm the current branch:

git branch --show-current

Expected output:

DepthCameraSupport

2. Install LeRobot in Editable Mode

If you only use RealSense:

pip install -e ".[realsense]"

3. Detect Cameras

lerobot-find-cameras realsense

This step will output:

  • Camera model
  • Serial number
  • USB information
  • Default stream configuration

4. RealSense Example

Dual RealSense test:

lerobot-teleoperate \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--robot.cameras='{
d435i_color: {
type: realsense_d435i_color,
serial_number_or_name: "419522072950",
width: 640,
height: 480,
fps: 30,
color_mode: rgb,
color_stream_format: rgb8,
rotation: 0,
warmup_s: 1
},
d435i_depth: {
type: realsense_d435i_depth,
serial_number_or_name: "419522072950",
width: 640,
height: 480,
fps: 30,
max_depth_m: 2.0,
depth_alpha: 0.2,
rotation: 0,
warmup_s: 5
},
d405_color: {
type: realsense_d405_color,
serial_number_or_name: "409122273421",
width: 640,
height: 480,
fps: 30,
color_mode: rgb,
color_stream_format: rgb8,
rotation: 0,
warmup_s: 1
},
d405_depth: {
type: realsense_d405_depth,
serial_number_or_name: "409122273421",
width: 640,
height: 480,
fps: 30,
depth_alpha: 0.03,
rotation: 0,
warmup_s: 5
}
}' \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=my_awesome_leader_arm \
--display_data=true

5. Parameter Notes

  • depth_alpha controls the scaling factor of the depth image and can be adjusted based on the display result and target distance range.
  • If you connect three or more depth cameras, it is recommended to reduce fps to 15 to improve overall stability.
  • It is recommended to keep the resolution at 640x480 for a better balance of stability and real-time performance.
If using Orbbec Gemini2/Gemini336 cameras

Orbbec Gemini 2 is a high-performance RGB-D camera for robotics applications, providing synchronized RGB and depth streams with precise depth-to-color alignment. Combined with stereo depth sensing and a built-in 6-axis IMU, it is well suited for robotic tasks such as object detection, 3D perception, mapping, and navigation. Its compact design and full Orbbec SDK support make it suitable for both research and real-world deployment.

Gemini 336 is a new member of the Gemini 330 series. It inherits the strong depth performance of Gemini 335 and further improves depth imaging quality in reflective indoor areas, dark regions in high-dynamic scenes, and bright outdoor environments. For robotics applications, it can provide more stable, high-quality depth data for tasks such as perception, localization, and manipulation.

1. Switch to the Camera Branch

Current camera support is available on the DepthCameraSupport branch:

git checkout DepthCameraSupport
git pull origin DepthCameraSupport

Confirm the current branch:

git branch --show-current

Expected output:

DepthCameraSupport

2. Install LeRobot in Editable Mode

If you only use Orbbec:

pip install -e ".[orbbec]"

3. Detect Cameras

lerobot-find-cameras orbbec

This step will output:

  • Camera model
  • Serial number
  • USB information
  • Default stream configuration

4. Orbbec Example

Single Orbbec test:

lerobot-teleoperate \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--robot.cameras='{
orbbec_color: {
type: orbbec_color,
serial_number_or_name: "CP9JA530003A",
width: 640,
height: 480,
fps: 30,
color_mode: rgb,
rotation: 0,
warmup_s: 1
},
orbbec_depth: {
type: orbbec_depth,
serial_number_or_name: "CP9JA530003A",
width: 640,
height: 400,
fps: 30,
depth_alpha: 0.2,
rotation: 0,
warmup_s: 5
}
}' \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=my_awesome_leader_arm \
--display_data=true

5. Parameter Notes

  • depth_alpha controls the scaling factor of the depth image. A good starting point is 0.2, then you can fine-tune it based on the display result.
  • If you connect three or more depth cameras, it is recommended to reduce fps to 15 for better stability.
  • It is recommended to keep the resolution at 640x480 for more stable display and data transfer.

6. Common Issues

If you see the following error:

No Orbbec camera found for 'XXXX'

it usually means the serial number in the configuration does not match the currently connected device. Run:

lerobot-find-cameras orbbec

Then confirm the actual serial and update serial_number_or_name in your command.

If using a regular camera

tip

The SO100 and SO101 codes are compatible. Users of SO100 can directly utilize SO101's parameters and code for operation.

To instantiate a camera, you need a camera identifier. This identifier might change if you reboot your computer or re-plug your camera, a behavior mostly dependant on your operating system.

To find the camera indices of the cameras plugged into your system, run the following script:

lerobot-find-cameras opencv # or realsense for Intel Realsense cameras

The terminal will print out the following information.

--- Detected Cameras ---
Camera #0:
Name: OpenCV Camera @ 0
Type: OpenCV
Id: 0
Backend api: AVFOUNDATION
Default stream profile:
Format: 16.0
Width: 1920
Height: 1080
Fps: 15.0
--------------------
(more cameras ...)

You can find the pictures taken by each camera in the outputs/captured_images directory.

warning

When using Intel RealSense cameras in , you could get this error: , this can be solved by running the same command with permissions. Note that using RealSense cameras in is unstable.macOSError finding RealSense cameras: failed to set power statesudomacOS.

Then you will be able to display the cameras on your computer while you are teleoperating by running the following code. This is useful to prepare your setup before recording your first dataset.

lerobot-teleoperate \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=my_awesome_leader_arm \
--display_data=true

If you have more cameras, you can change --robot.cameras to add cameras. You should note the format of the index_or_path, which is determined by the last digit of the camera ID output by python -m lerobot.find_cameras opencv.

tip

Images in the fourcc: "MJPG" format are compressed. You can try higher resolutions, and you may also attempt the YUYV format. However, the latter will reduce the image resolution and FPS, leading to lag in the robotic arm's operation. Currently, under the MJPG format, it can support 3 cameras at a resolution of 1920*1080 while maintaining 30FPS. That said, connecting 2 cameras to a computer via the same USB HUB is still not recommended.

For example, you want to add a side camera:

lerobot-teleoperate \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=my_awesome_leader_arm \
--display_data=true
tip

Images in the fourcc: "MJPG" format are compressed. You can try higher resolutions, and you may also attempt the YUYV format. However, the latter will reduce the image resolution and FPS, leading to lag in the robotic arm's operation. Currently, under the MJPG format, it can support 3 cameras at a resolution of 1920*1080 while maintaining 30FPS. That said, connecting 2 cameras to a computer via the same USB HUB is still not recommended.

tip

If you find bug like this.

You can downgrade the rerun version to resolve the issue.

pip3 install rerun-sdk==0.23

Record the dataset

  • If you want to save the dataset locally, you can run it directly:
lerobot-record \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=my_awesome_leader_arm \
--display_data=true \
--dataset.repo_id=seeedstudio123/test \
--dataset.num_episodes=5 \
--dataset.single_task="Grab the black cube" \
--dataset.push_to_hub=false \
--dataset.episode_time_s=30 \
--dataset.reset_time_s=30

Among them, repo_id can be modified customarily, and push_to_hub=false. Finally, the dataset will be saved in the ~/.cache/huggingface/lerobot directory in the home folder, where the aforementioned seeedstudio123/test folder will be created.

  • If you want to use the Hugging Face hub features for uploading your dataset and you haven't previously done it, make sure you've logged in using a write-access token, which can be generated from the Hugging Face settings:
huggingface-cli login --token ${HUGGINGFACE_TOKEN} --add-to-git-credential

Store your Hugging Face repository name in a variable to run these commands:

HF_USER=$(huggingface-cli whoami | head -n 1)
echo $HF_USER

Record 5 episodes and upload your dataset to the hub:

lerobot-record \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \
--teleop.type=so101_leader \
--teleop.port=/dev/ttyACM1 \
--teleop.id=my_awesome_leader_arm \
--display_data=true \
--dataset.repo_id=${HF_USER}/record-test \
--dataset.num_episodes=5 \
--dataset.single_task="Grab the black cube" \
--dataset.push_to_hub=true \
--dataset.episode_time_s=30 \
--dataset.reset_time_s=30

You will see a lot of lines appearing like this one:

INFO 2024-08-10 15:02:58 ol_robot.py:219 dt:33.34 (30.0hz) dtRlead: 5.06 (197.5hz) dtWfoll: 0.25 (3963.7hz) dtRfoll: 6.22 (160.7hz) dtRlaptop: 32.57 (30.7hz) dtRphone: 33.84 (29.5hz)

Record function

The record function provides a suite of tools for capturing and managing data during robot operation.

1. Data Storage

  • Data is stored using the LeRobotDataset format and is stored on disk during recording.
  • By default, the dataset is pushed to your Hugging Face page after recording.
  • To disable uploading, use: --dataset.push_to_hub=False

2. Checkpointing and Resuming

  • Checkpoints are automatically created during recording.
  • To resume after an interruption, re-run the same command with: --resume=true

⚠️ Critical Note: When resuming, set --dataset.num_episodes to the number of additional episodes to record (not the targeted total number of episodes in the dataset).

  • To start recording from scratch, manually delete the dataset directory.

3. Recording Parameters

Set the flow of data recording using command-line arguments:

ParameterDescriptionDefault
--dataset.episode_time_sDuration per data episode (seconds)60
--dataset.reset_time_sEnvironment reset time after each episode (seconds)60
--dataset.num_episodesTotal episodes to record50

4. Keyboard Controls During Recording

Control the data recording flow using keyboard shortcuts:

KeyAction
→ (Right Arrow)Early-stop current episode/reset; move to next.
← (Left Arrow)Cancel current episode; re-record it.
ESCStop session immediately, encode videos, and upload dataset.
tip

If keyboard not work, you may need install other version of pynput.

pip install pynput==1.6.8

Tips for Gathering Data

  • Task Suggestion: Grasp objects at different locations and place them in a bin.
  • Scale: Record ≥50 episodes (10 episodes per location).
  • Consistency:
    • Keep cameras fixed.
    • Maintain identical grasping behavior.
    • Ensure manipulated objects are visible in camera feeds.
  • Progression:
    • Start with reliable grasping before adding variations (new locations, techniques, camera adjustments).
    • Avoid rapid complexity increases to prevent failures.

💡 Rule of Thumb: You should be able to do the task yourself by only looking at the camera images.

If you want to dive deeper into this important topic, you can check out the blog post we wrote on what makes a good dataset.

Troubleshooting

Linux-specific Issue:
If Right Arrow/Left Arrow/ESC keys are unresponsive during recording:

Visualize the dataset

tip

The SO100 and SO101 codes are compatible. Users of SO100 can directly utilize SO101's parameters and code for operation.

If you uploaded your dataset to the hub with --control.push_to_hub=true, you can visualize your dataset online by copy pasting your repo id given by:

echo ${HF_USER}/so101_test  

If you didn't upload with --dataset.push_to_hub=false, you can also visualize it locally with:

lerobot-dataset-viz \
--repo-id ${HF_USER}/so101_test \

If you upload with --dataset.push_to_hub=false, you can also visualize it locally with:

lerobot-dataset-viz \
--repo-id seeed_123/so101_test \

Here, seeed_123 is the custom repo_id name defined when collecting data.

Replay an episode

tip

The SO100 and SO101 codes are compatible. Users of SO100 can directly utilize SO101's parameters and code for operation.

A useful feature is the replay function, which allows you to replay any episode that you’ve recorded or episodes from any dataset out there. This function helps you test the repeatability of your robot’s actions and assess transferability across robots of the same model.

You can replay the first episode on your robot with either the command below or with the API example:

lerobot-replay \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.id=my_awesome_follower_arm \
--dataset.repo_id=${HF_USER}/record-test \
--dataset.episode=0

Your robot should replicate movements similar to those you recorded.

Train And Evaluate

ACT

Refer toACT

To train a policy to control your robot, use the lerobot-train script.

Train

lerobot-train \
--dataset.repo_id=${HF_USER}/so101_test \
--policy.type=act \
--output_dir=outputs/train/act_so101_test \
--job_name=act_so101_test \
--policy.device=cuda \
--wandb.enable=false \
--steps=300000

If you want to train on a local dataset, make sure the repo_id matches the one used during data collection and add --policy.push_to_hub=False.

lerobot-train \
--dataset.repo_id=seeedstudio123/test \
--policy.type=act \
--output_dir=outputs/train/act_so101_test \
--job_name=act_so101_test \
--policy.device=cuda \
--wandb.enable=false \
--policy.push_to_hub=false\
--steps=300000

Let's explain it:

  • Dataset specification: We provide the dataset via the parameter --dataset.repo_id=${HF_USER}/so101_test.
  • Training steps: We modify the number of training steps using --steps=300000. The algorithm defaults to 800000 steps, and you can adjust it based on the difficulty of your task and by observing the loss during training.
  • Policy type: We provide the policy with policy.type=act. Similarly, you can switch between policies such as [act, diffusion, pi0, pi0fast, pi0fast, sac, smolvla]., which will load the configuration from configuration_act.py. Importantly, this policy will automatically adapt to your robot's (e.g., laptop and phone) motor states, motor actions, and the number of cameras, as this information is already stored in your dataset.
  • Device selection: We provide policy.device=cuda because we are training on an Nvidia GPU, but you can use policy.device=mps for training on Apple Silicon.
  • Visualization tool: We provide wandb.enable=true to visualize training charts using Weights and Biases. This is optional, but if you use it, ensure you have logged in by running wandb login.

Evaluate

tip

The SO100 and SO101 codes are compatible. Users of SO100 can directly utilize SO101's parameters and code for operation.

You can use the record function from lerobot/record.py but with a policy checkpoint as input. For instance, run this command to record 10 evaluation episodes:

lerobot-record \
--robot.type=so100_follower \
--robot.port=/dev/ttyACM0 \
--robot.cameras="{ up: {type: opencv, index_or_path: /dev/video10, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: intelrealsense, serial_number_or_name: 233522074606, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \
--robot.id=my_awesome_follower_arm \
--display_data=false \
--dataset.repo_id=${HF_USER}/eval_so100 \
--dataset.single_task="Put lego brick into the transparent box" \
--policy.path=${HF_USER}/my_policy

such as:

lerobot-record \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \
--robot.id=my_awesome_follower_arm \
--display_data=false \
--dataset.repo_id=seeed/eval_test123 \
--dataset.single_task="Put lego brick into the transparent box" \
--policy.path=outputs/train/act_so101_test/checkpoints/last/pretrained_model
  1. The --policy.path parameter indicates the path to the weight file of your policy training results (e.g., outputs/train/act_so101_test/checkpoints/last/pretrained_model). If you upload the model training result weight file to Hub, you can also use the model repository (e.g., ${HF_USER}/act_so100_test).

  2. The dataset name dataset.repo_id starts with eval_. This operation will separately record videos and data during evaluation, which will be saved in the folder starting with eval_, such as seeed/eval_test123.

  3. If you encounter File exists: 'home/xxxx/.cache/huggingface/lerobot/xxxxx/seeed/eval_xxxx' during the evaluation phase, please delete the folder starting with eval_ first and then run the program again.

  4. When encountering mean is infinity. You should either initialize with stats as an argument or use a pretrained model, please note that keywords like front and side in the --robot.cameras parameter must be strictly consistent with those used when collecting the dataset.

SmolVLA

SmolVLA is Hugging Face’s lightweight foundation model for robotics. Designed for easy fine-tuning on LeRobot datasets, it helps accelerate your development!

Set Up Your Environment

Install SmolVLA dependencies by running:

pip install -e ".[smolvla]"

Finetune SmolVLA on your data

Use smolvla_base, our pretrained 450M model, and fine-tune it on your data. Training the model for 20k steps will roughly take ~4 hrs on a single A100 GPU. You should tune the number of steps based on performance and your use-case.

If you don’t have a gpu device, you can train using our notebook on Google Colab.

Pass your dataset to the training script using --dataset.repo_id. If you want to test your installation, run the following command where we use one of the datasets we collected for the SmolVLA Paper.

lerobot-train \
--policy.path=lerobot/smolvla_base \
--dataset.repo_id=${HF_USER}/mydataset \
--batch_size=64 \
--steps=20000 \
--output_dir=outputs/train/my_smolvla \
--job_name=my_smolvla_training \
--policy.device=cuda \
--wandb.enable=true
tip

You can start with a small batch size and increase it incrementally, if the GPU allows it, as long as loading times remain short.

Fine-tuning is an art. For a complete overview of the options for finetuning, run

lerobot-train --help

Evaluate the finetuned model and run it in real-time

Similarly for when recording an episode, it is recommended that you are logged in to the HuggingFace Hub. You can follow the corresponding steps: Record a dataset. Once you are logged in, you can run inference in your setup by doing:

lerobot-record \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \ # <- Use your port
--robot.id=my_blue_follower_arm \ # <- Use your robot id
--robot.cameras="{ front: {type: opencv, index_or_path: 8, width: 640, height: 480, fps: 30, fourcc: "MJPG"}}" \ # <- Use your cameras
--dataset.single_task="Grasp a lego block and put it in the bin." \ # <- Use the same task description you used in your dataset recording
--dataset.repo_id=${HF_USER}/eval_DATASET_NAME_test \ # <- This will be the dataset name on HF Hub
--dataset.episode_time_s=50 \
--dataset.num_episodes=10 \
# <- Teleop optional if you want to teleoperate in between episodes \
# --teleop.type=so100_leader \
# --teleop.port=/dev/ttyACM0 \
# --teleop.id=my_red_leader_arm \
--policy.path=HF_USER/FINETUNE_MODEL_NAME # <- Use your fine-tuned model

Depending on your evaluation setup, you can configure the duration and the number of episodes to record for your evaluation suite.

LIBERO

LIBERO is a benchmark designed to study lifelong robot learning. The idea is that robots won’t just be pretrained once in a factory, they’ll need to keep learning and adapting with their human users over time. This ongoing adaptation is called lifelong learning in decision making (LLDM), and it’s a key step toward building robots that become truly personalized helpers.

Evaluating with LIBERO

At LeRobot, we ported LIBERO into our framework and used it mainly to evaluate SmolVLA, our lightweight Vision-Language-Action model.

LIBERO is now part of our multi-eval supported simulation, meaning you can benchmark your policies either on a single suite of tasks or across multiple suites at once with just a flag.

To Install LIBERO, after following LeRobot official instructions, just do: pip install -e ".[libero]"

Single-suite evaluation

Evaluate a policy on one LIBERO suite:

lerobot-eval \
--policy.path="your-policy-id" \
--env.type=libero \
--env.task=libero_object \
--eval.batch_size=2 \
--eval.n_episodes=3
  • --env.task picks the suite (libero_object, libero_spatial, etc.).
  • --eval.batch_size controls how many environments run in parallel.
  • --eval.n_episodes sets how many episodes to run in total.

Multi-suite evaluation

Benchmark a policy across multiple suites at once:

lerobot-eval \
--policy.path="your-policy-id" \
--env.type=libero \
--env.task=libero_object,libero_spatial \
--eval.batch_size=1 \
--eval.n_episodes=2
  • Pass a comma-separated list to --env.task for multi-suite evaluation.

Example training command

lerobot-train \
--policy.type=smolvla \
--policy.repo_id=${HF_USER}/libero-test \
--dataset.repo_id=HuggingFaceVLA/libero \
--env.type=libero \
--env.task=libero_10 \
--output_dir=./outputs/ \
--steps=100000 \
--batch_size=4 \
--eval.batch_size=1 \
--eval.n_episodes=1 \
--eval_freq=1000 \

Note on rendering

LeRobot uses MuJoCo for simulation. You need to set the rendering backend before training or evaluation:

  • export MUJOCO_GL=egl → for headless servers (e.g. HPC, cloud)
Pi0

Refer to Pi0

pip install -e ".[pi]"

Train

lerobot-train \
--policy.type=pi0 \
--dataset.repo_id=seeed/eval_test123 \
--job_name=pi0_training \
--output_dir=outputs/pi0_training \
--policy.pretrained_path=lerobot/pi0_base \
--policy.compile_model=true \
--policy.gradient_checkpointing=true \
--policy.dtype=bfloat16 \
--steps=20000 \
--policy.device=cuda \
--batch_size=32 \
--wandb.enable=false

Evaluate

lerobot-record \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30,fourcc: "MJPG"}}" \
--robot.id=my_awesome_follower_arm \
--display_data=false \
--dataset.repo_id=seeed/eval_test123 \
--dataset.single_task="Put lego brick into the transparent box" \
--policy.path=outputs/pi0_training/checkpoints/last/pretrained_model
Pi0.5

Refer to Pi0.5

pip install -e ".[pi]"

Train

lerobot-train \
--dataset.repo_id=seeed/eval_test123 \
--policy.type=pi05 \
--output_dir=outputs/pi05_training \
--job_name=pi05_training \
--policy.pretrained_path=lerobot/pi05_base \
--policy.compile_model=true \
--policy.gradient_checkpointing=true \
--wandb.enable=false \
--policy.dtype=bfloat16 \
--steps=3000 \
--policy.device=cuda \
--batch_size=32

Evaluate

lerobot-record \
--robot.type=so101_follower \
--robot.port=/dev/ttyACM0 \
--robot.cameras="{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30,fourcc: "MJPG"}}" \
--robot.id=my_awesome_follower_arm \
--display_data=false \
--dataset.repo_id=seeed/eval_test123 \
--dataset.single_task="Put lego brick into the transparent box" \
--policy.path=outputs/pi05_training/checkpoints/last/pretrained_model
GR00T N1.5

Refer to the official documentation: GR00T N1.5.

GR00T N1.5 is an open foundation model from NVIDIA for more general robot reasoning and skill learning. It is a cross-embodiment model: it can take multimodal inputs such as language and images, and execute manipulation tasks across different environments.

In LeRobot, the key is to set the policy type to --policy.type=groot. Note that GR00T N1.5 has higher environment requirements (it depends on FlashAttention and requires a CUDA GPU). It is recommended to first get ACT / Pi0 running end-to-end, and then try GR00T.

Installation (important)

According to the current official docs, GR00T N1.5 requires flash-attn and can only be used on CUDA-capable hardware.

Recommended order:

  1. Prepare your base environment first (Python, CUDA, drivers, etc.). Do not install lerobot yet.
  2. Install PyTorch for your CUDA version (different CUDA versions may require a different --index-url; follow the PyTorch install page).
pip install "torch>=2.2.1,<2.8.0" "torchvision>=0.21.0,<0.23.0"
  1. Install the build dependencies for flash-attn, then install flash-attn itself.
pip install ninja "packaging>=24.2,<26.0"
pip install "flash-attn>=2.5.9,<3.0.0" --no-build-isolation
python -c "import flash_attn; print(f'Flash Attention {flash_attn.__version__} imported successfully')"
  1. Install LeRobot with the groot optional dependencies (lerobot[groot]).
pip install "lerobot[groot]"
tip

If flash-attn installation fails, it is usually due to (1) a PyTorch/CUDA mismatch, (2) missing build dependencies, or (3) an environment that is too new/too old. Cross-check the official GR00T docs and the PyTorch install instructions first.

Training (fine-tuning)

The official docs provide a multi-GPU example with accelerate launch --multi_gpu .... If you only have a single GPU, you can still start by getting a single-process run working first (exact support/arguments depend on the official docs).

accelerate launch \
--multi_gpu \
--num_processes=$NUM_GPUS \
$(which lerobot-train) \
--output_dir=$OUTPUT_DIR \
--save_checkpoint=true \
--batch_size=$BATCH_SIZE \
--steps=$NUM_STEPS \
--save_freq=$SAVE_FREQ \
--log_freq=$LOG_FREQ \
--policy.push_to_hub=true \
--policy.type=groot \
--policy.repo_id=$REPO_ID \
--policy.tune_diffusion_model=false \
--dataset.repo_id=$DATASET_ID \
--wandb.enable=true \
--wandb.disable_artifact=true \
--job_name=$JOB_NAME

On-robot validation (evaluation)

After training, you can evaluate and record replays with lerobot-record like other policies. The official docs include a bimanual example; SO101 single-arm users do not need left_arm_port/right_arm_port-style arguments.

lerobot-record \
--robot.type=bi_so_follower \
--robot.left_arm_port=/dev/ttyACM1 \
--robot.right_arm_port=/dev/ttyACM0 \
--robot.id=bimanual_follower \
--robot.cameras='{ right: {"type": "opencv", "index_or_path": 0, "width": 640, "height": 480, "fps": 30}, left: {"type": "opencv", "index_or_path": 2, "width": 640, "height": 480, "fps": 30}, top: {"type": "opencv", "index_or_path": 4, "width": 640, "height": 480, "fps": 30} }' \
--display_data=true \
--dataset.repo_id=${HF_USER}/eval_groot_bimanual \
--dataset.num_episodes=10 \
--dataset.single_task="Grab and handover the red cube to the other arm" \
--policy.path=${HF_USER}/groot-bimanual \
--dataset.episode_time_s=30 \
--dataset.reset_time_s=10

License: Apache 2.0 (same as the original GR00T repository).

(Optional) Parameter-Efficient Fine-Tuning (PEFT)

PEFT (Parameter-Efficient Fine-Tuning) is a family of methods and tools that help a large pretrained model adapt to new tasks without updating all parameters. For pretrained LeRobot policies (e.g., SmolVLA, Pi0), you can often train only a small set of “adapter” parameters (e.g., LoRA) to reduce VRAM usage and training cost, while still achieving performance close to full fine-tuning.

Install

After installing LeRobot with the optional peft dependencies, you can use PEFT-related arguments in training.

pip install -e ".[peft]"
pip install "lerobot[peft]"

More concepts and methods: 🤗 PEFT documentation.

Example: Fine-tune SmolVLA with LoRA (LIBERO libero_spatial sub-task)

This example fine-tunes lerobot/smolvla_base with LoRA on the HuggingFaceVLA/libero dataset. Argument names depend on the LeRobot version; it’s recommended to also check lerobot-train --help.

lerobot-train \
--policy.path=lerobot/smolvla_base \
--policy.repo_id=${HF_USER}/my_libero_smolvla_peft \
--dataset.repo_id=HuggingFaceVLA/libero \
--env.type=libero \
--env.task=libero_spatial \
--output_dir=outputs/train/my_libero_smolvla_peft \
--job_name=my_libero_smolvla_peft \
--policy.device=cuda \
--steps=10000 \
--batch_size=32 \
--optimizer.lr=1e-3 \
--peft.method_type=LORA \
--peft.r=64

Key PEFT arguments

  • --peft.method_type: Select the PEFT method. LoRA (Low-Rank Adapter) is one of the most common options.
  • --peft.r: LoRA rank. Higher rank usually increases capacity, but also increases parameter count and VRAM usage.

Choose which layers/modules to inject LoRA into (optional)

By default, PEFT usually injects LoRA into the most important projection layers (e.g., attention q_proj, v_proj), and may also cover state/action projections. If you want to customize, use --peft.target_modules.

Common patterns:

  1. Provide a list of module-name suffixes (example):
--peft.target_modules="['q_proj', 'v_proj']"
  1. Provide a regex (example; adjust to the actual module names in the model):
--peft.target_modules='(model\\.vlm_with_expert\\.lm_expert\\..*\\.(down|gate|up)_proj|.*\\.(state_proj|action_in_proj|action_out_proj|action_time_mlp_in|action_time_mlp_out))'

Fully train some modules (optional)

If you want some modules to be fully trained (instead of only injecting LoRA), use --peft.full_training_modules. For example, only fully train state_proj:

--peft.full_training_modules="['state_proj']"

Learning rate suggestion (rule of thumb)

LoRA learning rates are often ~10× higher than full fine-tuning. For example, if full fine-tuning commonly uses 1e-4, LoRA can start from 1e-3. If you use a learning-rate scheduler, the final learning rate is often around 1e-4 as a reference.

(Optional) Multi-GPU training with Accelerate

Training steps

Method 1: Use CLI flags.

  1. Install accelerate in your lerobot environment.

pip install accelerate

  1. Launch multi-GPU training with accelerate launch and the --multi_gpu and --num_processes flags.

accelerate launch \

--multi_gpu \

--num_processes=2 \

$(which lerobot-train) \

--dataset.repo_id=${HF_USER}/my_dataset \

--policy.type=act \

--policy.repo_id=${HF_USER}/my_trained_policy \

--output_dir=outputs/train/act_multi_gpu \

--job_name=act_multi_gpu \

--wandb.enable=true

Key accelerate flags:

  • --multi_gpu: Enable multi-GPU training.
  • --num_processes: Number of GPUs to use (usually equals the number of available GPUs on the machine).
  • --mixed_precision=fp16: Use fp16 mixed precision (if your hardware supports it, you can also use bf16).

Please note: bf16 requires hardware support and is not available on all GPUs.

PrecisionHardware support
fp16Supported by almost all NVIDIA GPUs
bf16Only supported by some newer GPUs (Ampere and later)

If your GPU does not support bf16, choose fp16 in the Accelerate configuration, or specify fp16 explicitly.

Method 2: Use an accelerate config file (optional).

If you train on multiple GPUs frequently, you can save the configuration to avoid repeatedly typing the same flags.

accelerate config saves your hardware configuration (number of GPUs, mixed precision, etc.) into a config file, so you don’t have to re-enter those options when running accelerate launch later. It does not change LeRobot’s training logic; it only reduces repeated CLI inputs.

If you only use multi-GPU occasionally (or this is your first time), skipping this is completely fine.

In the interactive configuration, for the common “single machine + multiple GPUs” scenario, typical choices are:

  • Compute environment: This machine
  • Number of machines: 1
  • Number of processes: Number of GPUs you want to use
  • GPU ids to use: press Enter (use all GPUs)
  • Mixed precision: prefer fp16; choose bf16 only if you know your GPU supports it

accelerate config


accelerate launch $(which lerobot-train) \

--dataset.repo_id=${HF_USER}/my_dataset \

--policy.type=act \

--policy.repo_id=${HF_USER}/my_trained_policy \

--output_dir=outputs/train/act_multi_gpu \

--job_name=act_multi_gpu \

--wandb.enable=true

How multi-GPU affects hyperparameters (and how to adjust)

LeRobot does not automatically adjust learning rate or training steps based on the number of GPUs, to avoid silently changing training behavior. This differs from some other distributed training frameworks.

If you want to adjust hyperparameters for multi-GPU, a common approach is:

  • Steps: effective batch size increases (batch_size × num_gpus), so you can reduce steps roughly proportional to 1 / num_gpus to keep a similar total number of samples seen.

accelerate launch --num_processes=2 $(which lerobot-train) \

--batch_size=8 \

--steps=50000 \

--dataset.repo_id=lerobot/pusht \

--policy=act

  • Learning rate: since each step uses more samples, you can often scale the learning rate linearly with the number of GPUs: new_lr = single_gpu_lr × num_gpus

accelerate launch --num_processes=2 $(which lerobot-train) \

--optimizer.lr=2e-4 \

--dataset.repo_id=lerobot/pusht \

--policy=act

These are not strict rules; they are common heuristics. If you’re unsure, you can also keep the learning rate and steps unchanged as long as training remains stable.

For advanced configuration and troubleshooting, see the Accelerate documentation: Accelerate.

(Optional) Asynchronous Inference

When asynchronous inference is not enabled, LeRobot’s control flow can be understood as conventional sequential / synchronous inference: the policy first predicts a segment of actions, then executes that segment, and only after that waits for the next prediction.

For larger models, this can cause the robot to noticeably pause while waiting for the next action chunk.

The goal of asynchronous inference is to let the robot execute the current action chunk while computing the next one in advance, thereby reducing idle time and improving responsiveness.

Asynchronous inference is applicable to policies supported by LeRobot, including chunk-based action policies such as ACT, OpenVLA, Pi0, and SmolVLA.

Since inference is decoupled from actual control, asynchronous inference also helps leverage machines with stronger compute resources to perform inference for the robot.

You can read more about asynchronous inference in the blog by Hugging Face

Let us first introduce some basic concepts:

  • Client: connects to the robotic arm and cameras, collects observation data (such as images and robot poses), sends these observations to the server, and receives the action chunks returned by the server and executes them in order.

  • Server: the device that provides compute resources. It receives camera data and robotic arm data, performs inference (that is, computation) to produce action chunks, and sends them back to the client. It can be the same device connected to the robotic arm and cameras, another computer on the same local network, or a rented cloud server on the Internet.

  • Action chunk: a sequence of robotic arm action commands obtained by policy inference on the server side.

Three deployment scenarios for asynchronous inference

  1. Single-machine deployment

The robot, cameras, client, and server are all on the same device.

This is the simplest case: the server can listen on 127.0.0.1, and the client can also connect to 127.0.0.1:port. The command example in the official documentation is for this scenario.

  1. LAN deployment

The robot and cameras are connected to a lightweight device, while the policy server runs on another high-compute machine in the same local network.

In this case, the server must listen on an address that is accessible by other machines, and the client must also connect to the server’s LAN IP, rather than 127.0.0.1.

  1. Cross-network / cloud deployment

The policy server runs on a publicly accessible cloud host, and the client connects to it over the public Internet.

This approach can use the stronger GPU of the cloud host. When network conditions are good, the round-trip network time (network latency) can sometimes be relatively small compared with inference time, but this depends on your actual network environment.

Security note: the LeRobot async inference pipeline has a risk related to unauthenticated gRPC + pickle deserialization. If there is important information or important services on the server, it is not recommended to expose the service directly to the Internet in a public deployment. A safer approach is to use VPN or SSH tunneling, or at least restrict the allowed source IPs in the security group to your own client public IP.

Getting started with asynchronous inference deployment

Step 1: Environment setup

First, use pip to install the additional dependencies required for asynchronous inference. Both the client and the server need to have lerobot installed along with the extra dependencies:

pip install -e ".[async]"

Step 2: Network configuration and checks

  1. Proxy issues

If your current terminal is configured to use a proxy and the connection behaves abnormally, you can temporarily unset the proxy environment variables:

unset http_proxy https_proxy ftp_proxy all_proxy HTTP_PROXY HTTPS_PROXY FTP_PROXY ALL_PROXY

Note: the command above only affects the current terminal session. If you open another terminal window, you need to run it again.

  1. Open the port in the firewall / security group

Single-machine deployment: this can usually be skipped.

LAN deployment: you need to open the listening port on the server side.

Example for opening the listening port on a LAN setup (run on the server side):

sudo ufw allow 8080/tcp

Cloud deployment: you need to open this port in the cloud server security group, and it is recommended to restrict the source IPs as much as possible.

If you are running on a cloud server:

Open port 8080 in the server management console’s security group, or use another port that is already open. Different cloud service platforms handle this differently; refer to your cloud provider’s documentation.

  1. Confirm the IP address

This step can be skipped for single-machine deployment (the IP address for a single machine is always 127.0.0.1).

If this is a LAN deployment:

You need to confirm and remember the LAN IP address of the server side. When the client connects, what should be filled in is the LAN IP of the machine running policy_server, not the client’s own IP.

Linux / Jetson / Raspberry Pi:

hostname -I

If multiple addresses are shown, generally choose the one corresponding to the current LAN network interface, for example 192.168.x.x.

You can also use:

ip addr

to view the inet field under the currently connected network interface.

Windows:

ipconfig

Find a field like IPv4 Address . . . . . . . . . . . : 192.168.14.140; that is the LAN IP address of that machine.

macOS:

ifconfig

Find the inet field corresponding to the currently connected network interface; that is the LAN IP address.

We need to remember the server-side LAN IP address. We will use <LAN IP address> to refer to it.

If this is a cloud server deployment:

Look for the public IP in the server control panel. It is usually called one of the following:

Public IPv4

External IP

Public IP address

EIP

Public IP

We need to remember the public IP address. We will use<server public IP>to refer to it.

  1. Connection test

Single-machine deployment: this step can be skipped

LAN / cloud deployment: it is recommended to test from the client side whether the server port is reachable. Example tests are as follows:

LAN example: run on the client side

nc -vz <LAN IP address> 8080

Cloud example: run on the client side

nc -vz <server public IP> 8080

Step 3: Start the service

Scenario A: Single-machine deployment

Start the local service in one terminal:

python -m lerobot.async_inference.policy_server \
--host=127.0.0.1 \
--port=8080

After it starts successfully, you need to keep this terminal open. You will need to open a new terminal to run other commands.

Scenario B: LAN deployment

Run on the server side:

python -m lerobot.async_inference.policy_server \
--host=0.0.0.0 \
--port=8080

In this case, when the client connects, the --server_address should be the server-side LAN IP address, that is,<LAN IP address>:8080.

Scenario C: Cloud server deployment

Run on the server side:

python -m lerobot.async_inference.policy_server \
--host=0.0.0.0 \
--port=8080

In this case, when the client connects, the --server_address should be the server’s public IP address, that is, <server public IP>:8080.

Step 4: Choose inference parameters

Run on the client side:

python -m lerobot.async_inference.robot_client \
--server_address=<ip address>:8080 \
--robot.type=so100_follower \
--robot.port=/dev/tty.usbmodem585A0076841 \
--robot.id=follower_so100 \
--robot.cameras="{ laptop: {type: opencv, index_or_path: 0, width: 1920, height: 1080, fps: 30}, phone: {type: opencv, index_or_path: 0, width: 1920, height: 1080, fps: 30}}" \
--task="dummy" \
--policy_type=your_policy_type \
--pretrained_name_or_path=user/model \
--policy_device=cuda \
--actions_per_chunk=50 \
--chunk_size_threshold=0.5 \
--aggregate_fn_name=weighted_average \
--debug_visualize_queue_size=True

Parameter explanations:

  • --server_address

Specifies the address and port of the policy server. <ip address> should be replaced with 127.0.0.1 (local machine), <LAN IP address>(LAN), or<server public IP> (cloud server).

  • --robot.type, --robot.port, --robot.id, --robot.cameras

Hardware device parameters. These should be kept consistent with the parameters used during dataset collection.

  • --task

The task description. Vision-language policies such as SmolVLA can determine the action target based on the task text.

  • --policy_type

Replace this with the specific policy name, for example:

  • smolvla

  • act

  • --pretrained_name_or_path

This value should be replaced with the model path on the server side, or a model path on Hugging Face.

  • --policy_device

Specifies the inference device used on the server side.

It can be cuda, mps, or cpu.

  • --actions_per_chunk=50

Specifies how many actions are output in each inference.

The larger this value is:

Advantage: the action buffer is more sufficient, making it less likely to run out Disadvantage: the prediction horizon is longer, so control error may accumulate more noticeably

  • --chunk_size_threshold=0.5

Specifies when to request the next action chunk from the server.

This is a threshold, usually in the range 0 to 1.

It can be understood as: when the remaining proportion of the current action queue falls below this threshold, the client will send a new observation in advance and request the next action chunk.

Setting it to 0.5 here means:

when the current action chunk is about half consumed

the client starts requesting the next action chunk

The larger this value is, the more frequently requests are sent, and the more responsive the system becomes, but the load on the server also increases.

The smaller this value is, the closer the behavior gets to synchronous inference.

  • --aggregate_fn_name=weighted_average

Specifies the aggregation method for overlapping action intervals.

In asynchronous inference, when the old action chunk has not yet been fully executed, the new action chunk may already have arrived.

In that case, the two chunks overlap over part of the time interval, and an aggregation function is needed to combine them into the final executed action.

The meaning of weighted_average is:

use a weighted average to fuse the overlapping part.

This usually makes action switching smoother and reduces abrupt changes.

  • --debug_visualize_queue_size=True

Whether to visualize the action queue size at runtime.

When enabled, it allows you to see more directly whether the queue frequently hits the bottom, which helps you tune actions_per_chunk and chunk_size_threshold.

Step 5: Adjust parameters based on robot behavior

In asynchronous inference, there are two additional parameters that need adjustment which do not exist in synchronous inference:

Parameter Suggested initial value Description

actions_per_chunk 50 How many actions the policy outputs at one time. Typical values: 10–50.

chunk_size_threshold 0.5 When the remaining proportion of the action queue is ≤ chunk_size_threshold, the client sends a new action chunk request. The value range is [0, 1].

When --debug_visualize_queue_size=True, the change in action queue size will be plotted at runtime.

What asynchronous inference needs to balance is: the speed at which the server generates action chunks must be greater than or equal to the speed at which the client consumes action chunks. Otherwise, the action queue will empty, and the robot will begin to stutter again (this can be seen as the curve hitting the bottom in the queue visualization).

The speed at which the server generates action chunks is affected by factors such as model size, device type, VRAM / memory, and GPU compute power.

The speed at which the client consumes action chunks is affected by the configured execution fps.

If the queue frequently runs empty, you need to increase actions_per_chunk, increase chunk_size_threshold, or reduce fps.

If the queue curve fluctuates frequently but the remaining actions in the queue are always sufficient, you can appropriately decrease chunk_size_threshold.

In general:

the empirical range for actions_per_chunk is 10–50

the empirical range for chunk_size_threshold is 0.5–0.7; when tuning, it is recommended to start from 0.5 and gradually increase it

If you encounter the following error:

Try running the following command to resolve it:

pip install datasets==2.19

Training should take several hours. You will find checkpoints in outputs/train/act_so100_test/checkpoints.

To resume training from a checkpoint, below is an example command to resume from last checkpoint of the act_so101_test policy:

lerobot-train \
--config_path=outputs/train/act_so101_test/checkpoints/last/pretrained_model/train_config.json \
--resume=true

Upload policy checkpoints

Once training is done, upload the latest checkpoint with:

huggingface-cli upload ${HF_USER}/act_so101_test \
outputs/train/act_so101_test/checkpoints/last/pretrained_model

You can also upload intermediate checkpoints with:

CKPT=010000
huggingface-cli upload ${HF_USER}/act_so101_test${CKPT} \
outputs/train/act_so101_test/checkpoints/${CKPT}/pretrained_model

FAQ

  • If you are following this documentation/tutorial, please git clone the recommended GitHub repository https://github.com/Seeed-Projects/lerobot.git. The repository recommended in this documentation is a verified stable version; the official Lerobot repository is continuously updated to the latest version, which may cause unforeseen issues such as different dataset versions, different commands, etc.

  • If you encounter the following error when calibrating servo IDs:

    `Motor ‘gripper’ was not found, Make sure it is connected`

    Please carefully check whether the communication cable is properly connected to the servo and whether the power supply is providing the correct voltage.

  • If you encounter:

    Could not connect on port "/dev/ttyACM0"

    And you can see ACM0 exists when running ls /dev/ttyACM*, it means you forgot to grant serial port permissions. Enter sudo chmod 666 /dev/ttyACM* in the terminal to fix it.

  • If you encounter:

    No valid stream found in input file. Is -1 of the desired media type?

    Please install ffmpeg 7.1.1 using conda install ffmpeg=7.1.1 -c conda-forge.

  • If you encounter:

    ConnectionError: Failed to sync read 'Present_Position' on ids=[1,2,3,4,5,6] after 1 tries. [TxRxResult] There is no status packet!

    You need to check whether the robotic arm on the corresponding port is powered on, and whether the data cables of the bus servos are loose or disconnected. If a servo's light is not on, it means the cable of the previous servo is loose.

  • If you encounter the following error when calibrating the robotic arm:

    Magnitude 30841 exceeds 2047 (max for sign_bit_index=11)

    Power off and restart the robotic arm, then try calibrating again. This method can also be used if the MAX angle reaches a value of tens of thousands during calibration. If this doesn't work, you need to recalibrate the corresponding servos, including median calibration and ID writing.

  • If you encounter during the evaluation phase:

    File exists: 'home/xxxx/.cache/huggingface/lerobot/xxxxx/seeed/eval_xxxx'

    Please delete the folder starting with eval_ first and then run the program again.

  • If you encounter during the evaluation phase:

    `mean` is infinity. You should either initialize with `stats` as an argument or use a pretrained model

    Please note that keywords like "front" and "side" in the --robot.cameras parameter must be strictly consistent with those used when collecting the dataset.

  • If you have repaired or replaced parts of the robotic arm, please completely delete the files under ~/.cache/huggingface/lerobot/calibration/robots or ~/.cache/huggingface/lerobot/calibration/teleoperators and recalibrate the robotic arm. Otherwise, error messages may appear, as calibration information is stored in JSON files in these directories.

  • Training ACT on 50 sets of data takes approximately 6 hours on a laptop with an RTX 3060 (8GB), and about 2-3 hours on computers with RTX 4090 or A100 GPUs.

  • During data collection, ensure the camera position, angle, and ambient lighting are stable. Reduce the amount of unstable background and pedestrians captured by the camera, as excessive changes in the deployment environment may cause the robotic arm to fail to grasp properly.

  • For the data collection command, ensure the num-episodes parameter is set to collect sufficient data. Do not manually pause midway, as the mean and variance of the data are calculated only after data collection is complete, which are necessary for training.

  • If the program indicates it cannot read image data from the USB camera, ensure the USB camera is not connected through a hub. The USB camera must be directly connected to the device to ensure fast image transmission speed.

  • If you find bug like AttributeError: module 'rerun' has no attribute 'scalar'. Did you mean: 'scalars'?, You can downgrade the rerun version to resolve the issue.

pip3 install rerun-sdk==0.23
tip

If you encounter software issues or environment dependency problems that cannot be resolved, in addition to checking the FAQ section at the end of this tutorial, please promptly report the issue to the LeRobot platform or the LeRobot Discord channel.

Citation

Chinese Document

TheRobotStudio Project: SO-ARM10x

Huggingface Project: Lerobot

Dnsty: Jetson Containers

Jetson AI Lab

Diffusion Policy

ACT or ALOHA

TDMPC

VQ-BeT

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...