Log in to Raspberry Pi OS/ Ubuntu OS or Other OS using SSH over Wi-Fi/ Ethernet
If you want to log in to the Raspberry Pi OS using SSH over Wi-Fi/ Ethernet, you can follow the steps below. First set up Wi-Fi/Ethernet on the reTerminal and then SSH using Windows/Mac/Linux.
Step 1: Set up Wi-Fi/Ethernet on the reTerminal
caution
If you have configured WiFi and enabled SSH using Raspberry Pi Imager, you can skip step 1
- 1. If you have a Wi-Fi connection, click the Wi-Fi icon on the top right corner of the Raspberry Pi OS Desktop, select your Wi-Fi network and enter the password using the on-screen virtual keyboard
Note: The location of the Wi-Fi setting might be different for other OS
- 2. If you don't have a Wi-Fi connection, you can connect an ethernet cable from your router to the ethernet port of the reTerminal
Note: Make sure the reTerminal and your computer is connected to the same network
-
3. Touch on the Raspberry Pi icon at the top left corner and navigate to
Preferences > Raspberry Pi Configurationand click on Interfaces tab -
4. Select Enable which is next to SSH and click OK

Now let's configure the software on the computer. Please follow according to your operating system
Step 2: Configure SSH using Windows/Mac/Linux
For Windows
- 1. Open Command Prompt and type the following
ssh pi@raspberrypi.local
- 2. Type yes for the prompt

- 3. Enter the password as follows
raspberry
- 4. If you have sucessfully logged into the Raspberry Pi OS, you will see the following output

For Mac/Linux
- 1. Open Terminal on the computer and type the following
ssh pi@raspberrypi.local
- 2. Type yes for the following message
ECDSA key fingerprint is SHA256:XXXXXXX.
Are you sure you want to continue connecting (yes/no/[fingerprint])?
- 3. When it asks for the password, type the following
raspberry
- 4. If you have sucessfully logged into the Raspberry Pi OS, you will see the following output