Skip to main content

Make DIY BSP from Orin Nano DevKit to reComputer Classic / Super

This guide shows how to clone a full development environment from an NVIDIA Jetson Orin Nano Developer Kit, swap in Seeed reComputer board firmware, build a Hybrid BSP, and complete the flash.

Two target boards are supported:

  • reComputer Classic (J4011/J4012, board config recomputer-orin-j401)
  • reComputer Super (board config recomputer-orin-super-j401)

Both share the same core idea—keep the DevKit's full APP, regenerate the target board's QSPI—but differ in pinmux, camera overlay, and disk layout details. Differences are presented in tabs below; shared steps are written once.

This flow has been validated with JetPack 6.2 / L4T 36.4.3, Orin Nano 8GB (SKU 0005).

Related docs:

What You Are Building​

GoalArtifactPurpose
A. Same-carrier clonemfi_jetson-orin-nano-devkit-nvme.tar.gzReflash DevKit with a full environment clone
B. Target Bundlemfi_recomputer-orin-j401.tar.gz (Classic)
mfi_recomputer-orin-super-j401.tar.gz (Super)
Flash target board: target board-level QSPI + DevKit full APP (including /home)
C. Safe fallbackOfficial BSP + migrate /home onlyUse when Hybrid results are abnormal
danger

Do not flash the DevKit mfi_jetson-orin-nano-devkit-nvme package directly onto the target board.

Do not treat editing a single .dtb inside the mfi directory as board adaptation.

Do not flash a Classic Hybrid bundle onto Super, or vice versa—their pinmux and camera overlays differ.

Prerequisites​

Hardware​

  • Source: Orin Nano Developer Kit (this example uses module SKU 0005 = Orin Nano 8GB, NVMe boot)
  • Target: Seeed reComputer Classic J4011/J4012 or reComputer Super (module should ideally also be 0005)
  • Host: Ubuntu 22.04 x86_64, USB Type-C cable (flash port)
  • Disk: reserve ≥ 100GB free space (backup + dual mfi + snapshots)
danger

The reComputer Classic series has insufficient cooling to support MAXN Super mode. If you flash JetPack 6.2 onto a Classic device, do not enable MAXN.

Host Dependencies​

sudo apt-get update -y
sudo apt-get install -y \
build-essential flex bison libssl-dev \
sshpass abootimg nfs-kernel-server \
libxml2-utils qemu-user-static

Before backup/flash:

sudo systemctl stop udisks2.service
sudo service nfs-kernel-server start
lsusb | grep 0955:7523 # must show NVIDIA Corp. APX

Board Comparison​

ItemDevKitreComputer ClassicreComputer Super
board-namejetson-orin-nano-devkit-nvmerecomputer-orin-j401recomputer-orin-super-j401
Config filep3768-0000-p3767-0000-a0-nvme.confrecomputer-orin-j401.confrecomputer-orin-super-j401.conf
PinmuxNVIDIA DevKit (DP)Classic HDMISuper HDMI
Camera overlayNVIDIA dynamicSeeed dual IMX219Seeed quad IMX219
SKU0005 main DTB...-0005-nv(-super).dtbStill uses tegra234-p3768-0000+p3767-0005-nv-super.dtb
Final mfiDevKit onlyClassic onlySuper only

Example backup board_spec:

3767-300-0005-V.2-1-1-jetson-orin-nano-devkit-nvme-

1. Prepare the Linux_for_Tegra Workspace​

Download the Seeed L4T working package from the table in Creating a Custom BSP Package from Jetson Development Environment (JetPack 6.2 / L4T 36.4.3 plus in this example).

sudo tar xpf L4T_36.4.3_plus.tar.gz
# Adjust the archive name to match your download

cd Linux_for_Tegra/
sudo ./apply_binaries.sh
cd ..

export ARCH=arm64
export CROSS_COMPILE="$PWD/aarch64--glibc--stable-2022.08-1/bin/aarch64-buildroot-linux-gnu-"
export PATH="$PWD/aarch64--glibc--stable-2022.08-1/bin:$PATH"
export INSTALL_MOD_PATH="$PWD/Linux_for_Tegra/rootfs/"

cd Linux_for_Tegra/source
./nvbuild.sh
./do_copy.sh
./nvbuild.sh -i

Verification:

test -f Linux_for_Tegra/recomputer-orin-j401.conf
test -f Linux_for_Tegra/jetson-orin-nano-devkit-nvme.conf
ls Linux_for_Tegra/kernel/dtb/tegra234-j401-*-recomputer.dtb
ls Linux_for_Tegra/kernel/dtb/tegra234-dcb-p3767-0000-hdmi.dtbo

2. Back Up the Full DevKit Environment​

2.1 Put the Source Device in Recovery Mode​

Connect the DevKit flash port to the host with a USB Type-C data cable and enter Recovery mode. On the host, lsusb should show 0955:7523 APX.

For Recovery mode steps, see: Flash JetPack to a Selected Product

During backup the device may briefly switch to 0955:7035 (Linux for Tegra / initrd). That is normal.

2.2 Backup Command​

cd Linux_for_Tegra
sudo ./tools/backup_restore/l4t_backup_restore.sh \
-e nvme0n1 -b -c jetson-orin-nano-devkit-nvme
warning

Do not use the target board name for the first backup when the source is a DevKit. That will corrupt board_spec and later baselines.

2.3 Verification​

ls -lah tools/backup_restore/images/
head -5 tools/backup_restore/images/nvpartitionmap.txt

You should see:

  • board_spec contains jetson-orin-nano-devkit-nvme
  • nvme0n1p1.tar.zst (or the later converted large APP) is GB-scale
  • QSPI0.img exists (this is DevKit QSPI; Hybrid must not reuse it as target board QSPI)

Recommended: snapshot immediately:

sudo cp -a tools/backup_restore/images ~/backup_images_dk_sku0005

3. Build DevKit Same-Carrier DIY BSP (Optional)​

Put the device back into APX. On the host, lsusb should show 0955:7523 APX:

cd Linux_for_Tegra
sudo ./tools/kernel_flash/l4t_initrd_flash.sh \
--use-backup-image --no-flash --network usb0 --massflash 5 \
jetson-orin-nano-devkit-nvme internal

Artifacts:

  • mfi_jetson-orin-nano-devkit-nvme/
  • mfi_jetson-orin-nano-devkit-nvme.tar.gz
danger

For DevKit reflash only. Do not flash the target board with this package.

Its APP can be used as the data source for the Hybrid bundle, but its QSPI cannot be reused.

4. Required Reading: The QSPI Trap​

With --use-backup-image, convert_backup_image_to_initrd_flash places:

Backup contentDestination
NVMe / APPtools/kernel_flash/images/external/
Source QSPI0.imgtools/kernel_flash/images/internal/

Therefore:

Wrong approachResult
Only edit mfi/.../rootfs or one .dtbIneffective (what actually flashes is bak / QSPI)
DevKit backup, then directly swap target board name + --use-backup-imageStill flashes DevKit QSPI (DP pinmux); HDMI/USB may be wrong
Change conf, then --flash-only--flash-only does not rebuild images from conf

What really differs on the target board is HDMI pinmux + DCB/camera overlay in the board conf:

Key contents of recomputer-orin-j401.conf:

PINMUX_CONFIG="tegra234-mb1-bct-pinmux-p3767-hdmi-a03.dtsi"
PMC_CONFIG="tegra234-mb1-bct-padvoltage-p3767-hdmi-a03.dtsi"
OVERLAY_DTB_FILE+=",tegra234-dcb-p3767-0000-hdmi.dtbo,tegra234-p3767-camera-p3768-imx219-dual-seeed.dtbo"
DCE_OVERLAY_DTB_FILE="tegra234-dcb-p3767-0000-hdmi.dtbo"

For SKU 0005, the main DTB filename is still NVIDIA's *-0005-nv-super.dtb. Do not force-switch to *-0000-recomputer.dtb (that path is for NX 16GB).

5. Hybrid BSP: Build the Target Bundle​

Core idea:

  1. APP: keep using the DevKit backup (full user environment)
  2. QSPI: regenerate with the target board conf (without --use-backup-image)
  3. Assemble into the target board mfi
DevKit backup APP  ──►  external/ (nvme0n1p1_bak.img, etc.)
Target conf new QSPI ──► internal/ (QSPI shards, not DevKit monolithic QSPI0.img)
└──► mfi_recomputer-orin-<target>(.tar.gz)

5.1 Prepare APP-only (Remove DevKit QSPI)​

cd Linux_for_Tegra
sudo cp -a ~/backup_images_dk_sku0005 \
tools/backup_restore/images_app_only
sudo rm -f tools/backup_restore/images_app_only/QSPI0.img
sudo sed -i '/qspi/Id' tools/backup_restore/images_app_only/nvpartitionmap.txt

Convert APP-only into initrd flash external images (use the backup tool's convert step, or reuse the large APP already under tools/kernel_flash/images/external/ from the DevKit mfi pack step).

5.2 Generate Target Board QSPI​

Device must be in APX. Module parameters should match the backup (this example: 3767 / 0005 / 300 / V.2):

cd Linux_for_Tegra
sudo BOARDID=3767 BOARDSKU=0005 FAB=300 BOARDREV=V.2 CHIP_SKU=00:00:00:D5 \
./tools/kernel_flash/l4t_initrd_flash.sh \
--external-device nvme0n1p1 \
-c tools/kernel_flash/flash_l4t_t234_nvme.xml \
-p "-c bootloader/generic/cfg/flash_t234_qspi.xml --no-systemimg" \
--no-flash --massflash 5 --showlogs --network usb0 \
recomputer-orin-j401 internal

Logs should show HDMI pinmux, e.g. tegra234-mb1-bct-pinmux-p3767-hdmi-a03.

Recommended: save the new QSPI internal:

sudo cp -a tools/kernel_flash/images/internal ~/j401_qspi_internal_save
info

The QSPI internal (SKU 0005 / L4T 36.4.3) generated in this guide is available for direct download:

wget -O j401_qspi_internal_save.tar.gz \
https://files.seeedstudio.com/wiki/reComputer-Jetson/FAQ/dk-to-classic/j401_qspi_internal_save.tar.gz
mkdir -p Linux_for_Tegra/tools/kernel_flash/images/internal
tar xpf j401_qspi_internal_save.tar.gz -C Linux_for_Tegra/tools/kernel_flash/images/internal/

Place the downloaded files into Linux_for_Tegra/tools/kernel_flash/images/internal/ to skip the QSPI generation step above.

Reuse prerequisites: target board is reComputer Classic J4011/J4012, module SKU 0005, L4T 36.4.3. If any condition does not match, regenerate QSPI per this section.

5.3 Assemble mfi​

The final directory should satisfy:

PathContent
mfi_recomputer-orin-j401/recomputer-orin-j401.confPresent
.../tools/kernel_flash/images/internal/New J401 QSPI (no DevKit monolithic QSPI0.img, or hash differs from DevKit; flash.idx is often multi-line shards)
.../tools/kernel_flash/images/external/nvme0n1p1_bak.imgGB-scale APP

Optional archive:

cd Linux_for_Tegra
sudo tar czf mfi_recomputer-orin-j401.tar.gz mfi_recomputer-orin-j401

6. Flash to the Target Board​

6.1 Put Target in APX​

lsusb → 0955:7523 NVIDIA Corp. APX

6.2 Flash Command​

If the extracted directory already exists locally, do not run tar xpf again:

cd Linux_for_Tegra/mfi_recomputer-orin-j401
sudo ./tools/kernel_flash/l4t_initrd_flash.sh \
--flash-only --massflash 1 --network usb0 --showlogs

Only when another PC has only the .tar.gz:

sudo tar xpf mfi_recomputer-orin-j401.tar.gz
cd mfi_recomputer-orin-j401
sudo ./tools/kernel_flash/l4t_initrd_flash.sh \
--flash-only --massflash 1 --network usb0 --showlogs
warning

If /mnt/external/...: Permission denied appears while writing recovery or APP, this is an NFS permission issue—see Tech Note B.

6.3 Normal Messages During Flash​

LogMeaning
p3768-0000-p3767-0000-a0.conf: No such file or directoryCommon with --flash-only; images are prebuilt, continue
rpcbind already runningSafe to ignore
blockdev: cannot open /dev/mmcblk0boot0Orin Nano has no such partition; usually harmless
RCM-boot + SSH readyNormal flash entry
DTB ...-0005-nv-super.dtbCorrect for SKU0005
Multiple internal lines + Starting to flash to qspiFlashing target board QSPI
tar ... zstd ... nvme0n1p1_bak.imgRestoring APP (longest step; may take tens of minutes)
Successfully flash the qspiQSPI flash complete
Successfully flash the external deviceExternal device flash complete
Flashing success / Flash is successfulFlash succeeded
warning

Do not power off or unplug until you see a successful completion message.

7. Post-Flash Checks​

Release the Recovery button or jumper and power-cycle after a successful flash. If lsusb still reports 0955:7523 APX, the device remains in Recovery and has not booted Linux.

After a normal boot, run:

cat /proc/device-tree/model
ls /boot/kernel_tegra234*.dtb
ls /boot/*.dtbo | grep -E 'hdmi|imx219' || true

# Whether peripherals actually work (more important than model / dtbo filenames)
xrandr 2>/dev/null | head -20
lsusb | head
ip -br link
ls /boot/*.dtbo 2>/dev/null | head -40
sudo dmesg | grep -iE 'dtb|overlay|hdmi|tegra234' | tail -30

# Whether the original DevKit user environment survived (CUDA example)
nvcc --version
info

Without sudo, dmesg may report Operation not permitted. That is a permissions issue; use sudo.

How to Interpret Results (SKU 0005)​

1) /proc/device-tree/model still shows DevKit — normal for SKU 0005

Example:

NVIDIA Jetson Orin Nano Engineering Reference Developer Kit Super

Reason: the target board conf for SKU 0005 selects NVIDIA's tegra234-p3768-0000+p3767-0005-nv-super.dtb. It does not switch to tegra234-j401-*-recomputer.dtb, so the model string still looks like the official DevKit. Do not conclude "flashed the wrong DevKit bundle" from this line alone.

2) DTB filenames under /boot

Commonly visible:

/boot/kernel_tegra234-p3768-0000+p3767-0000-nv.dtb
/boot/kernel_tegra234-p3768-0000+p3767-0005-nv.dtb

You may not see a *-0005-nv-super.dtb filename; the actual boot DTB is often chosen by UEFI/QSPI. The /boot listing is reference only.

3) Empty grep hdmi|imx219 — not a failure by itself

After Hybrid flash, /boot/*.dtbo often still contains the generic overlay list from the DevKit backup. You may not see tegra234-dcb-p3767-0000-hdmi.dtbo or Seeed camera overlays. Seeed HDMI/camera settings mostly take effect through the new target board QSPI / UEFI overlay path.

4) Judge by "does it work?"

CheckHealthy example
USBHubs, mouse, Bluetooth, USB Ethernet enumerated (lsusb shows multiple devices)
Wired EthernetClassic: enP8p1s0 etc. are UP; Super: see Tech Note C
Wi‑FiwlP1p1s0 is UP
DisplayDesktop works; or xrandr has output
User environmentOriginal DevKit users, software, and data remain
CUDAnvcc --version works (this example 12.6), indicating APP clone is intact

Classic should focus on validating the dual camera configuration (imx219-dual-seeed).

On device: model / DTB

On device: CUDA installed on the original DevKit still works

When to Edit extlinux.conf​

Only if HDMI / USB / boot is abnormal, try adding under LABEL primary in /boot/extlinux/extlinux.conf:

FDT /boot/kernel_tegra234-p3768-0000+p3767-0005-nv-super.dtb

(If that file is missing under /boot, try ...-0005-nv.dtb, or copy from BSP kernel/dtb/ first.)

sudo reboot

If still abnormal, use Section 8 fallback.

8. Fallback (Official Path)​

If Hybrid flash leaves partitions/UEFI/peripherals abnormal:

  1. Flash the official target board BSP per Seeed's flow (do not flash the DevKit mfi).
  2. Extract /home from backup (nvme0n1p1.tar.zst) or follow Migrate /home Data from Jetson Orin Nano Developer Kit to reComputer.
  3. Restore /home on the target board, then reinstall system-level software as needed (/usr, /etc, Docker, etc. need separate handling).

Pros: cleanest board firmware. Cons: not a full / disk clone.

9. Key Paths Quick Reference​

TypePath (under Linux_for_Tegra/)
DK mfimfi_jetson-orin-nano-devkit-nvme.tar.gz
Classic Bundle mfimfi_recomputer-orin-j401.tar.gz
Super Bundle mfimfi_recomputer-orin-super-j401.tar.gz
Classic confrecomputer-orin-j401.conf
Super confrecomputer-orin-super-j401.conf
HDMI DCBkernel/dtb/tegra234-dcb-p3767-0000-hdmi.dtbo
Classic dual IMX219kernel/dtb/tegra234-p3767-camera-p3768-imx219-dual-seeed.dtbo
Super quad IMX219kernel/dtb/tegra234-p3767-camera-p3768-imx219-quad-seeed.dtbo
J401 DTBkernel/dtb/tegra234-j401-p3768-0000+p3767-*-recomputer.dtb
SKU0005 DTBkernel/dtb/tegra234-p3768-0000+p3767-0005-nv-super.dtb

10. Flow Overview​

[Host] Extract L4T + apply_binaries + nvbuild
│
▼
[DevKit APX] backup -c jetson-orin-nano-devkit-nvme
│
├─► (optional) --use-backup-image → mfi_jetson-orin-nano-devkit-nvme
│
├─► snapshot backup_images_dk_sku0005
│ │
│ ├─ APP-only (remove QSPI)
│ └─► external APP
│
└─► [APX] target board conf → generate QSPI
│ │
│ ├─ Classic: recomputer-orin-j401 internal
│ └─ Super: recomputer-orin-super-j401-nvme external
│
▼
assemble mfi_recomputer-orin-<target>
│
▼
[target APX] --flash-only
│
▼
check display/USB/NVMe/user environment

11. FAQ​

Q: Both the directory and .tar.gz exist—do I still need to extract?
A: No. If mfi_recomputer-orin-* directory exists, cd into it and run --flash-only.

Q: Target board module is not 0005?
A: Change BOARDSKU, pick the matching DTB per p3767_super_overlay in the target board conf, then regenerate QSPI.

Q: I only want to keep /home, not clone the whole disk?
A: Use Section 8 fallback. It is simpler and more reliable.

Q: Can I rename and flash the Classic Hybrid bundle onto Super?
A: No. Their pinmux and camera overlays differ. Regenerate the corresponding QSPI.

Q: Why not use --use-backup-image directly?
A: It may also reuse the DevKit QSPI0.img. Hybrid should reuse only the APP.

Q: What if source and target drive capacities differ? (Super)
A: Generate GPT for the target drive and replace only the APP payload. The expanded APP must fit the new APP partition.

Q: Why does the DIY BSP wiki example use recomputer-orin-j401?
A: That example assumes source and target are both Seeed boards. When the source is an official DevKit, backup must first use jetson-orin-nano-devkit-nvme, then follow this Hybrid tutorial to adapt to the target board.

Tech Notes​

Tech Note A. Super First-Boot Consistency​

Check three consistency requirements before archiving:

  1. root=PARTUUID=... in boot.img must match the APP partition unique GUID in the external GPT;
  2. the /boot/efi UUID in the DevKit APP /etc/fstab must match the FAT UUID of the new esp.img;
  3. if the cloned DevKit kernel crashes in lan743x on the Super LAN7430, preinstall:
/etc/modprobe.d/blacklist-lan743x-super-hybrid.conf
blacklist lan743x
install lan743x /bin/false

The first two mismatches prevent root mounting or enter maintenance mode. Changing the live PARTUUID with sgdisk in a repair initrd is a recovery measure, not a reproducible build step. Regenerate GPT and boot.img together, then patch the APP before creating the final archive.

Tech Note B. NFS Permission Denied​

If /mnt/external/...: Permission denied appears while writing recovery or APP, ensure that the NFS client can traverse every parent directory in the mfi path.

For example, if the user home directory mode is 750, temporarily use 751 during flashing and restore it immediately afterward:

sudo chmod 751 /home/$USER
# Re-enter APX and flash
sudo chmod 750 /home/$USER

Mode 751 adds traversal permission only; it does not allow other users to list the directory. Do not use 777.

Tech Note C. Super lan743x Wired Ethernet Limitation​

The cloned DevKit RT kernel used in this test triggered a kernel Oops while loading lan743x for the Super LAN7430. The final Hybrid BSP blacklists lan743x (see Tech Note A item 3), so onboard wired Ethernet is temporarily unavailable; Wi-Fi is not affected.

This is a source APP/kernel driver compatibility limitation, not a Super QSPI or pinmux failure. Port or upgrade a compatible driver and run stress tests before relying on wired Ethernet in production.

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...