How to use MID360 LiDAR on reComputer
Introduction
MID360 LIDAR sensors provide high-precision 3D point cloud data for various applications. This guide focuses on setting up the MID360 on a reComputer J30/40 device running ROS Noetic.
This wiki provides a step-by-step guide to install and set up MID360 LiDAR on reComputer J30/40 Jetson using ROS, and visualize point cloud data.
Prerequisites
-
reComputer J30/40 series: Already completed the installation of the JetPack 5.x system and the ROS Noetic environment according to the tutorial.
-
MID360 LIDAR

Getting Started
Install SDK2
-
Step 1: Install Livox-SDK2
git clone https://github.com/Livox-SDK/Livox-SDK2.git
cd ./Livox-SDK2/
mkdir build
cd build
cmake .. && make -j8
sudo make install -
Step 2: Install livox_ros_driver2:
git clone https://github.com/Livox-SDK/livox_ros_driver2.git ~/ws_livox/src/livox_ros_driver2
cd ~/ws_livox/src/livox_ros_driver2
source /opt/ros/noetic/setup.sh
./build.sh ROS1
Configure reComputer IP Address
The default IP address for the MID360 LiDAR is 192.168.1.2xx, the target host machine IP address is 192.168.1.50. After connecting the hardware, you need to manually configure the IP address of the reComputer.
-
Step 1: Open Ethernet Settings.
-
Step 2: Select Manual Settings in the IPv4 field and enter the IP address 192.168.1.50 and mask 255.255.255.0.
-
Step 3: Configuration Parameters. Next, modify the
~/src/livox_ros_driver2/config
files in thelivox_ros_driver2
. The blue underlined parts should be consistent with the static IP. The red underlined parts should be set as192.168.1.1xx
, where the last two digits correspond to the last two digits of the MID360 broadcast code. For example, if your broadcast code is 47MDL1C0010081 (14 characters), then the IP address should be set as192.168.1.181
.livox_ros_driver2/config/MID360_config.json
livox_ros_driver2/launch_ROS1/rviz_MID360.launch
livox_ros_driver2/launch_ROS1/msg_MID360.launch
Running Lidar Code
Start Lidar:
cd ~/ws_livox/
source devel/setup.bash
roslaunch livox_ros_driver2 msg_MID360.launch
Open a new terminal:
cd ~/ws_livox/
source devel/setup.bash
roslaunch livox_ros_driver2 rviz_MID360.launch

Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.