Skip to main content

Quick Start

Power Connection

Powered by a power adapter

The reComputer R1225 is supplied with a nominal AC voltage of 12~24 V or DC voltage of 9~36V. The power supply is connected via the 2-pin power terminal block connector. To ground the reComputer R1225, the ground wire can be secured to the screw located at the top left corner of the power terminal.

note

The power solution utilizes a bridge rectifier diode for reverse polarity protection and is compatible with both AC and DC inputs. This ensures that regardless of how the power supply's positive and negative terminals are connected, the circuit will not be damaged. By using a bridge rectifier, the output voltage polarity remains fixed irrespective of the input DC polarity, providing effective reverse polarity protection.

PoE power supply

With the PoE module installed, the ETH0 port of reComputer R1225 can support PoE power supply, providing a convenient and efficientway to power the device over Ethernet. This option simplifies the installation process and reduces the amount of cabling required, making it an ideal solution for applications with limited power sources or where power outlets are not readily available.

  • PoE input: Range 44~57V; Typical 48V
  • PoE output: 12V, 1.1A Max.
tip

It's worth noting that the PoE module provided with the reComputer R1225 is compliant with the IEEE 802.3af standard and can provide a maximum power supply of 12.95W. Therefore, if there is a need to connect high-power peripherals such as SSD or 4G modules, the PoE power supply may not be sufficient. In this case, it's recommended to use the AC/DC terminal for power supply instead to ensure stable and reliable operation of the device.

Access the SenseCAP Gateway OS

The SenseCAP Gateway OS is a multi‑protocol IoT gateway operating system designed for industrial indoor scenarios. Built on OpenWrt, it delivers a standardized software foundation that encompasses three core capabilities: LoRaWAN gateway functionality, industrial bus data acquisition, and building compliance reporting. You can also access the source code on our GitHub via the link HERE.

Access via router

  • Step 1: Connect your R1225 to an Ethernet cable, and connect your PC to the same router
note

Your PC and device should be connected to the same router/network.

Network Connection Diagram

When using the R1225 for the first time, if there are routers and Ethernet cables nearby, you can choose to connect the R1225 to the network via a wired connection.

pir

tip

If Wi-Fi is configured, you can access the LuCI interface via the R1225’s IP address without an Ethernet cable, as long as your computer and the R1225 are on the same network.

  • Step 2: Get IP Address of your device

Check the IP Address of your device on your router admin page.

  • Step 3: Get your device Username and Password

    • Username:admin
    • Password:null (No password required for first-time login)
  • Step 4: Login Luci

Input the IP Address of your device in a browser to enter the Luci page. Then input your device username and password to login, and click the Login button.

pir

Access via device AP hotspot

caution

When the R1225 is turned on for the first time, its Wi-Fi hotspot remains active for 5 minutes by default. After this time, the R1225’s hotspot will automatically turn off.

  • Step 1: Turn on R1225

Plug in the reComputer R1225 LoRaWAN Gateway, and the device will power on automatically.

  • Step 2: Connect to the AP hotspot

    • SSID : R1225-XXXX (last 4 digits of the SN)
    • Password : 1234567890

pir

When the reComputer R1225 is powered on for the first time, it automatically enables hotspot mode. The default SSID for the hotspot is “R1225-XXXX (last 4 digits of the SN)”, and the default password is “1234567890”,connect your computer to this AP hotspot.

  • Step 3: Get IP Address of your device

After connecting to the AP with the SSID R1225-XXXX, click the details icon in the upper-right corner.

pir

Click to open the “Network and Internet” page in the system settings, then scroll down to the bottom to find the IP address.

pir

  • Step4 : Get your device Username and Password

    • Username:admin
    • password:null (No password required for first-time login)
  • Step5 : Login Luci

Input the IP Address (192.168.2.1) in your browser to enter the Local Console.
Then input your device username and password, and click the Login button.

pir

R1225 Network Configuration

Ethernet Connection

Ethernet is plug-and-play and requires no configuration.

WIFI Connection

  • Step 1: Click on Network - Wi-Fi

pir

  • Step 2: Click on the Scan button to scan the WIFI

pir

  • Step 3: Select your Wi-Fi to join the network

pir

  • Step 4: Submit the Wi-Fi password, and then click Submit and Save

pir

pir

  • Step 5: Click Save & Apply to apply your settings

pir

Cellular Connection (for 4G version)

  • Step 1: Plug your SIM card into the Nano-SIM card slot

Please use a paperclip and insert it into the small hole next to the SIM card slot.

pir

  • Step 2: Login the Luci page, and click on Network - LTE

pir

  • Step 3: Setup the APN info, and click Save & Apply to apply your settings

pir

R1225 LoRaWAN Configuration

  • Step 1: Click on LoRa - LoRa Network

pir

  • Step 2: Check the Enable LoRa functionality

pir

  • Step 3: Click Save & Apply to apply your settings

Channel Plan Settings

  • Step 1: Navigate to LoRa > Channel Plan

pir

  • Step 2: Select Region and Channel-plan

pir

  • Step 3: Click Save & Apply to apply your settings

Select the built-in Chirpstack platform

tip

R1225 comes with ChirpStack (open-source LoRaWAN network server) pre-installed.

  • Step 1: Select Platform Type - ChirpStack

  • Step 2: Check the EUI

pir

  • Step 3: Click Open ChirpStack Application Server in the lower-left corner

pir

  • Step 4: Log in to the Chirpstack Cloud Platform

    • Username/email: admin

    • Password: admin

The default username and password are both “admin”

Then click Submit to go to the Chirpstack platform interface

pir

Bind R1225 LoRaWAN Gateway

  • Step 5: Navigate to Gateway > Add gateway

pir

  • Step 6: Enter the Gateway Name and Gateway ID (EUI: 64)

    • Gateway name: A name of your gateway

    • Gateway ID(EUI64): Gateway EUI can be found on the device label or Local Console

    • Stats interval(secs): The expected interval in seconds in which the gateway sends its statistics

pir

Then click Submit

Checking the Gateway Connection Status

Upon completion of all configuration steps, the gateway should be displayed as Online on the ChirpStack platform.

pir

Gateway data

Navigate to Gateways, choose the gateway you want to check.

pir

Loading Comments...