Frigate NVR and Hailo on reComputer AI box & Industrial box connect with Home Assistant
Introduction
Frigate NVR is an open-source Network Video Recorder (NVR) designed specifically for real-time object detection using AI models. It is lightweight, powerful, and works seamlessly with cameras via the RTSP protocol.
Home Assistant (HA) is an open-source platform for smart home automation that enables you to control and automate devices in your home.
In this guide, we'll walk you through how to install Frigate on a reComputer AI box & Industrial box equipped with Hailo PCIe, and how to connect it to your existing Home Assistant setup using MQTT with minimal hassle.
Prerequisites
Hardware Requirements
| reComputer AI R2130 | reComputer AI Industrial R2145 | reComputer Industrial R20xx | reComputer Industrial R21xx |
|---|---|---|---|
![]() | ![]() | ![]() | ![]() |
Install Hailo PCIe Driver
Step 1: Raspberry Pi Configuration
sudo apt update
sudo raspi-config
- Navigate to
6 Advanced Options > A8 PCIe Speed - Select
Yesto enable PCIe Gen 3 - Exit and select
Finish

Append the following line to the end of /boot/firmware/config.txt:
dtoverlay=pciex1-compat-pi5,no-mip
Step 2: Install PCIe Driver
sudo apt update
sudo apt install dkms
git clone https://github.com/hailo-ai/hailort-drivers
cd hailort-drivers/linux/pcie
git checkout 24e7ff2fb58fab7029024c1a1d3f2d1914f56d7b
sudo make install_dkms
Step 3: Install Firmware
cd ../..
./download_firmware.sh
sudo mkdir -p /lib/firmware/hailo
sudo cp hailo8_fw*.bin /lib/firmware/hailo/hailo8_fw.bin
Step 4: Fix PCIe Descriptor Size Issue
Create /etc/modprobe.d/hailo_pci.conf with this content:
options hailo_pci force_desc_page_size=4096
Step 5: Reboot and Verify
sudo reboot
ls /dev/hailo*
Expected output:
/dev/hailo0
Install Frigate NVR with Docker
Prerequisites
Make sure your camera is configured for RTSP streaming at 1920x1080 resolution.
Update System
sudo apt update
Install Docker
curl -fsSL get.docker.com | bash
sudo usermod -aG docker $USER
sudo reboot
Pull Frigate Image
docker pull ghcr.io/blakeblackshear/frigate:0.15.0-rc2-h8l
Create Directory Structure
mkdir -p ~/frigate/config
mkdir -p ~/frigate/data/db
mkdir -p ~/frigate/data/storage
cd ~/frigate
Create Docker Compose File (frigate.yml)
nano frigate.yml
services:
frigate-hailo:
container_name: frigate-hailo
privileged: true
restart: unless-stopped
image: ghcr.io/blakeblackshear/frigate:0.15.0-rc2-h8l
shm_size: 1024mb
devices:
- /dev/hailo0:/dev/hailo0
volumes:
- /etc/localtime:/etc/localtime:ro
- ./config/:/config
- ./data/db/:/data/db
- ./data/storage:/media/frigate
- type: tmpfs
target: /tmp/cache
tmpfs:
size: 1g
ports:
- 5000:5000
Create Frigate Config File (config/config.yml)
nano config/config.yml
database:
path: /data/db/frigate.db
go2rtc:
streams:
home:
- rtsp://admin:[email protected]:554/cam/realmonitor?channel=1&subtype=0
cameras:
home:
ffmpeg:
inputs:
- path: rtsp://admin:[email protected]:554/cam/realmonitor?channel=1&subtype=0
roles:
- record
- detect
mqtt:
enabled: False
objects:
track:
- person
- cat
detectors:
hailo8l:
type: hailo8l
device: PCIe
model:
width: 300
height: 300
model_type: ssd
path: /config/model_cache/h8l_cache/ssd_mobilenet_v1.hef
version: 0.15-1
Start Frigate
docker compose -f frigate.yml up -d
Access Web UI
Visit: http://<your-device-ip>:5000

Home Assistant Integration
Step 1: HACS Setup
Assuming you're running Home Assistant (HA Green, HA Yellow, or similar standalone devices):
- Install HACS if not already installed.
- In HACS, install the Frigate integration from the community store.
Configure it using the IP d port of your Frigate AI box
Step 2: Install MQTT Add-on
Follow the official MQTT integration guide to install and configure the MQTT broker add-on.
Step 3: Update Frigate Config for MQTT
mqtt:
host: <HA IP>
port: 1883
topic_prefix: frigate
client_id: frigate
user: <HA User Name>
password: <HA Password>
Example:
mqtt:
host: 10.0.0.136
port: 1883
topic_prefix: frigate
client_id: frigate
user: kasun
password: HiezenburgCook
full example :
database:
path: /data/db/frigate.db
go2rtc:
streams:
home:
- rtsp://admin:[email protected]:554/cam/realmonitor?channel=1&subtype=0
cameras:
home:
ffmpeg:
inputs:
- path: rtsp://admin:[email protected]:554/cam/realmonitor?channel=1&subtype=0
roles:
- record
- detect
mqtt:
host: core-mosquitto
port: 1883
topic_prefix: frigate
client_id: frigate
user: kasun
password: HiezenburgCook
objects:
track:
- person
- cat
detectors:
hailo8l:
type: hailo8l
device: PCIe
model:
width: 300
height: 300
model_type: ssd
path: /config/model_cache/h8l_cache/ssd_mobilenet_v1.hef
version: 0.15-1
Step 4: Restart Frigate
docker compose -f frigate.yml down
sudo docker compose -f frigate.yml up -d
Step 5: Confirm MQTT is Working (optional)
- Check HA logs or MQTT add-on logs to verify messages from Frigate
- In HA, you can now use Frigate events in automations, e.g., motion alerts, detected objects, etc.
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.