Skip to main content

reComputer R1000 with balena

What is balena?​

balena is an Internet of Things (IoT) platform designed to help developers build, deploy, and manage IoT applications across a fleet of devices. It supports a wide range of device architectures and includes features for containerized application deployment, making it possible to easily update your IoT software and HostOS, fix bugs and introduce new features on your IoT applications. balena provides a unified way to push code updates, manage device configurations and ensure devices run reliably and securely in the field, regardless of their location or network conditions.

pir

Getting Start​

Before you start this project, you may need to prepare your hardware and software in advance as described here.

Hardware Preparation​

reComputer R1000

Software​

Hardware Configuration​

Step 1: You need to set the switch on the side of the R1000 to boot mode, then power on the device

Switch PositionModeDescriptionnRPI-BOOT
imageNormal modeBoot from eMMCLow
imageFlash modeBoot from USBHigh

Step 2: Please use a USB Type-c cable to connect reComputer R1000 to your computer.

pir

Image File Acquisition​

Step 1: Go to balenaCloud, create a free account, and then create a fleet,Default device type choose Raspberry Pi CM4 IO Board

pir

Step 2: Click "Add device", select the version information and configuration information you want, and then download the balenaOS image file in the lower right corner.

pir
note

It is recommended to download the balenaOS image file first and then burn it. If you directly click "Flash" in the lower right corner of the window to burn it, it may fail to burn.

Steps for Flashing balena OS​

Step 1: Open the rpiboot software, and then the system will show the new disk

Step 2: Open the flash tool balenaEtcher, select the previously downloaded balena image file, then select the target disk, and finally click Burn.

pir

Change Configure​

Step 1:Copy the reComputer-R100x.dtbo file to the resin-boot => overlays folder

pir

Step 2:Add the following content to the config.txt file:

dtparam=i2c_arm=on
dtoverlay=i2c1,pins_44_45
dtoverlay=i2c3,pins_2_3
dtoverlay=i2c6,pins_22_23
dtoverlay=audremap,pins_18_19
dtoverlay=reComputer-R100x,uart2
pir

Step 3:Set the reComputer R1000 DIP switch to normal mode, then power on again. After a while, you can see the new device has been added successfully on balenaCloud.

pir

If the device is Online (Heartbeat only). This is due to the firewall restrictions in my area. If you have the same problem, you can connect a VPN to the device so that it can be displayed normallyOnline.

Deployment test​

Step 1:Enter the following command to download the resources and deploy them:

balena login
git clone https://github.com/mpous/seeed-recomputer-r100x.git
cd seeed-recomputer-r100x
balena push recomputerR1000
pir
pir

Step 2:After the deployment is completed, a unicorn will appear on the terminal and the status of all services will change to Running.

pir
pir

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...