reComputer R1000 with FIN to create a Top Level Graphic
Introduction
FIN Framework (FIN) is a software framework with application suites that can integrate, control, manage, analyze, visualize and connect. Its capabilities can be integrated by OEMs into a range of products and services.
This article will show you how to use the Graphics Builder of FIN Framwork, and to create a Top Level Graphic using the Graphics Builder.
Getting Start
Before you start this project, you may need to prepare your hardware and software in advance as described here.
Hardware Preparation
| reComputer R1000 |
|---|
![]() |
Software Preparation
- Regarding how to install FIN Framwork, you can refer to this wiki.
Steps of create a Top Level Graphic
Create new Top Level Graphic
Step 1: We create three sites. For how to create sites under Equip Tree, you can refer to this wiki. And please keep the system context in the home directory.

Step 2: Click Graphics Builder => New, and a pop-up window named Create a Graphic will appear. You need to fill in the Graphic Name and Select sites to include in Top Level graphic properties, among which the optional site is the site we created in the first step. Finally, click OK and our newly created Graphic will appear on the right side. Click it and then click Edit to enter the editing page.

Configure new Top Level Graphic
Step 1: Import the floor plan. First select IMAGE in the TYPE column in the lower left corner, and then you can import the background image. There are two ways to import background images. The first way is to drag it directly from the folder into the edit box; the second way is to click BROWSE in the lower left corner. If you have imported a certain image before, you can click here find that picture. After importing, right-click the mouse and select Arrange => Send to back to move the image to the bottom layer.

Step 2: Since we selected three site, the system will automatically generate three labels. For the sake of beauty, we will place them in the lower right corner and align them.

Step 3: We can add a label to explain some information. We find the label control on the left and drag it into the workspace, adjust its size, and then change the text and text size of label in the lower right corner.

Step 4: Add Graphic include to put our tags together and set a background color to make the visual effect more beautiful

Step 5: Draw the polygon. Use the polygon Tool at the top to draw a polygon to mark the location of our site. After drawing, you can also use the Edit polygon Tool tool to adjust the polygon.

Step 6: Add Virtual points. Switch to the Virtual points panel on the left, select the virtual point that matches the site we selected, and drag it into the drawn polygon.

Step 7: Make the polygon transparent.

Step 8: After saving the settings, click Graphics Builder => Menu and a new interface will appear on the right. Click Top Level Graphic => Create in the new interface and a popup named Edit Top Level Record will appear. window, select the Graphic we set, and finally click APPLY. After returning to the main interface, you can see the Top Level Graphic we set.

Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.