Qt for reTerminal with Python

Introduction
This wiki explains how to build your own user interface using Qt for Python on the reTerminal. Here we have used PySide2 for the development. PySide2 is the official Python module from the Qt for Python project, which provides access to the complete Qt5 framework.Qt for Python allows you to build interactive user interfaces in a more user friendly way! It is also very flexible to use and has a short learning curve.
By following the guide below, you will be able to create an application to control the STA and USR LEDs on the reTerminal just by clicking buttons on the LCD. So let's get started!
Prepare Development Environment
On reTerminal
- Step 1. Access reTerminal using the onboard LCD, external display or SSH as explained here and type the following on a terminal window
sudo apt install qml-module-qtquick-shapes python3-pyside2.qtqml python3-pyside2.qtcore python3-pyside2.qtnetwork python3-pyside2.qtgui python3-pyside2.qtwidgets python3-pyside2.qtquick qtquickcontrols2-5-dev qml-module-qtcharts qml-module-qtquick-controls qml-module-qtquick-controls2
- Step 2. Install compile tools to install the QtQuick.Studio component manually
sudo apt install qt5-qmake
Note: We have to install QtQuick.Studio manually because default Debian and Ubuntu OS don't have this module
- Step 3. Install the QtQuick.Studio module
git clone https://github.com/Pillar1989/qtquickdesigner-components.git
cd qtquickdesigner-components
qmake
make
sudo make install
Note: Because the latest QtQuick.Studio module cannot work on the current Raspberry Pi OS, we had port it to Debian GNU/Linux 10 (buster)
We can ignore the following prompt error.
Some of the required modules (qtHaveModule(quick)) are not available.
Skipped.
Now we have finished installing the necessary packages on the reTerminal
On Host PC
- Step 1. Download and install Microsoft Visual Studio Code
Note: Download the installer which is suitable for your operating system
- Step 2. Click on the Extensions tab on the left navigation menu and type remote development in the search box

-
Step 3. Select Remote Development and click Install
-
Step 4. Press F1 on the keyboard, type ssh and select Remote-SSH:Connect to Host...

- Step 5. Enter the following
Note: pi is the username and 192.xxx.xx.xx is the IP address of the reTerminal
- Step 6. Enter the password for the user
Now you have sucessfully logged in to reTerminal using SSH
- Step 7. Install Python extension as step 2 before

- Step 8. Install Qt for Python extension

- Step 9. Navigate to
File > Open Folder...and select any folder that you want to open
Note: Later we will use Visual Studio Code to create files inside the reTerminal and build our project
Now we have successfully finished preparing the development environment
Build the Project
Next let's move on to building the project. The workflow is as follows:
- Design the UI on a graphic designer software
- Create a .qml file and build the UI based on the positions of the UI elements obtained from the graphic designer software
- Create another .qml for the full screen UI application
- Create a python file and write the functions that will be used to control the LEDs
- Create a Python file to run the app
- Create a script to run the python file
- Create a Desktop shortcut to open the created app by double clicking on an icon
The files we need to create are as follows:
- LedGui.qml - UI with graphical elements
- App.qml - Full screen UI application
- ledControl.py - LEDs controlling functions
- main.py - Run the app
- led_start.sh - Run the Python file
- led.desktop - Open the app
Design the UI
First we need to design the UI. To do this, we will use a free online graphic designer software called Gravit Designer
-
Step 1. Click this link to open Gravit Designer
-
Step 2. Click Get Started, create a free account or directly log in with Facebook or Google
-
Step 3. Set the canvas size as 1280 x 720px and click Create!

Note: We set it to 1280x720px because that's the resolution of the reTerminal LCD
- Step 4. Select the Rectangle shape

- Step 5. Draw a rectangle for the title bar of the UI by holding down on the left mouse button, drag the mouse and release

-
Step 6. Draw a rectangle for the title bar of the UI by holding down on the left mouse button, drag the mouse and release
-
Step 7. Draw the following shapes for the buttons of the UI

- Step 8. Select the shape and under INSPECTOR tab, select Fills

- Step 9. Click on a color to fill the selected shape

- Step 10. Fill the remaining shapes as follows

- Step 11. Add a close button

- Step 12. Click on the Text tool

- Step 13. Place a text block and type "LED TEST"

- Step 14. Click on the text block, change the size and color

- Step 15. Repeat the same to obtain the following

Now we have finished designing the UI
Build the UI on qml
Now we will transfer the design from Gravit Designer to qml and build the UI
-
Step 1. Connect to reTerminal using SSH via Microsoft Visual Code, open a folder as mentioned before.
-
Step 2. Right click and select New Folder

- Step 3. Type a name for the folder and enter the folder

- Step 4. Right click on the folder and select New File

- Step 4. Type a name for the file with .qml extension as follows

Note: Make sure the first letter is Upper Case
- Step 5. Enter the .qml file and copy the following codes
// import libraries
import QtQuick 2.8
import QtQuick.Controls 2.1
/* The Item type is the base type for all visual items in Qt Quick. Here 1280 and 720 are chosen
for the dimensions because the resolution of reTerminal LCD is 1280x720 */
Item {
// identify the qml
id: ledControl
// define width and height of the app
width: 1280
height: 720
// Rectangle block for the heading
Rectangle {
id: titleBlock
x: 0 // Rectangle block position in x-axis
y: 0 // Rectangle block position in y-axis
width: 1280 // Rectangle block width
height: 175 // Rectangle block height
color: "green" // Rectangle block color
/* You can also enter **hexadecimal values** for the color field */
}
// left top button (ON)
Button {
id: staGreenOn
x: 159
y: 272
width: 200
height: 91
text: "ON" // text inside the button
font.pointSize: 28 // text font
palette.button: "green" // button color
palette.buttonText: "white" // text color
// Used to access the button control class in the Python file and turn on the LED
onClicked:
{
_Setting.staGreenOn()
}
}
// left bottom button (OFF)
Button {
id: staGreenOff
x: 159
y: 496
width: 200
height: 91
text: "OFF"
font.pointSize: 28
palette.button: "green"
palette.buttonText: "white"
onClicked:
{
_Setting.staGreenOff()
}
}
// middle top button (ON)
Button {
id: staRedOn
x: 540
y: 272
width: 200
height: 91
text: "ON"
font.pointSize: 28
palette.button: "red"
palette.buttonText: "white"
onClicked:
{
_Setting.staRedOn()
}
}
// middle bottom button (OFF)
Button {
id: staRedOff
x: 540
y: 496
width: 200
height: 91
text: "OFF"
font.pointSize: 28
palette.button: "red"
palette.buttonText: "white"
onClicked:
{
_Setting.staRedOff()
}
}
// right top button (ON)
Button {
id: usrGreenOn
x: 918
y: 272
width: 200
height: 91
text: "ON"
font.pointSize: 28
palette.button: "green"
palette.buttonText: "white"
onClicked:
{
_Setting.usrGreenOn()
}
}
// right bottom button (OFF)
Button {
id: usrGreenOff
x: 918
y: 496
width: 200
height: 91
text: "OFF"
font.pointSize: 28
palette.button: "green"
palette.buttonText: "white"
onClicked:
{
_Setting.usrGreenOff()
}
}
// close button
Button {
id: close
x: 1200
y: 0
width: 80
height: 31
palette.button: "red"
palette.buttonText: "white"
text: "X"
onClicked:
{
_Setting.closeWindow()
}
}
// heading
Text {
id: title
x: 500
y: 37
color: "white"
text: "LED TEST"
font.pixelSize: 60
}
// STA GREEN text
Text {
id: staGreen
x: 135
y: 400
text: "STA GREEN"
font.pixelSize: 45
}
// STA RED text
Text {
id: staRed
x: 547
y: 400
text: "STA RED"
font.pixelSize: 45
}
// USR GREEN text
Text {
id: usrGreen
x: 891
y: 400
text: "USR GREEN"
font.pixelSize: 45
}
}
Obtain Location and Size of Shapes
Inside the Gravit Designer, select a shape block and obtain the position and size from the INSPECTOR tab

Obtain Location and Size of Text
Inside the Gravit Designer, select a text block and obtain the position and size from the INSPECTOR tab

Build the Fullscreen UI
Next, let's build the fullscreen UI
- Step 1. Open the Root folder that we created before and create a new .qml file under that folder

- Step 2. Open the .qml file and copy the following codes
// import library
import QtQuick.Controls 2.1
// properties of the application window containing UI elements
ApplicationWindow {
id: application
width: 1280
height: 720
visible: true
visibility: "FullScreen"
// initialize the first window of the application
property var iniITEM: "LedGui.qml"
// stack-based navigation model
StackView {
id: stackview
initialItem: iniITEM
}
}
Now we have finished building the fullscreen app
Methods to Control the LEDs
Next we will create a python file to obtain the methods to control the LEDs on the reTerminal
- Step 1. Open the root folder that we created before and create a new .py python file under that folder

- Step 2. Enter the .py file and copy the following codes
# import libraries
import sys
import os
from PySide2.QtCore import *
# class to handle button controls
class Setting(QObject):
# staGreen ON/OFF
@Slot()
def staGreenOn(self):
# turn ON
os.system("sudo sh -c 'echo 255 > /sys/class/leds/usr_led2/brightness'")
@Slot()
def staGreenOff(self):
# turn OFF
os.system("sudo sh -c 'echo 0 > /sys/class/leds/usr_led2/brightness'")
# staRed
@Slot()
def staRedOn(self):
os.system("sudo sh -c 'echo 255 > /sys/class/leds/usr_led1/brightness'")
@Slot()
def staRedOff(self):
os.system("sudo sh -c 'echo 0 > /sys/class/leds/usr_led1/brightness'")
# usrGreen
@Slot()
def usrGreenOn(self):
os.system("sudo sh -c 'echo 255 > /sys/class/leds/usr_led0/brightness'")
@Slot()
def usrGreenOff(self):
os.system("sudo sh -c 'echo 0 > /sys/class/leds/usr_led0/brightness'")
# close
@Slot()
def closeWindow(self):
sys.exit()
Now we have completed the python file used to control the LEDs
Prepare Python File to Run the APP
Now we need to create a Python file that can be used to run the app that we have built
- Step 1. Open the Root folder that we created before and create a new .py file under that folder

- Step 2. Enter the created file and copy the following codes
# import libraries
from PySide2.QtQml import QQmlApplicationEngine
from PySide2.QtWidgets import *
from PySide2.QtCore import *
from ledControl import Setting
# launch the app
if __name__ == '__main__':
app = QApplication([])
engine = QQmlApplicationEngine()
# location of the fullscreen app that we created before
url = QUrl("./App.qml")
context = engine.rootContext()
seting = Setting()
context.setContextProperty("_Setting", seting)
engine.load(url)
app.exec_()
Prepare a Script to Run the Python file
- Step 1. Open the Root folder that we created before and create a new .sh file under that folder

- Step 2. Open the created file and enter the following
#!/bin/bash
cd $HOME/ledApp
DISPLAY=:0 python3 main.py
Note: Here $HOME/ledApp is the location of the main.py file
- Step 3. Open a terminal window inside the reTerminal and navigate to the root directory of the app
example:
cd /ledApp
- Step 4. Make the led_start.sh an executable file
chmod +x led_start.sh
Prepare a Desktop File to Launch the App
- Step 1. Open the Root folder that we created before and create a new .desktop file under that folder

- Step 2. Open the created file and enter the following
[Desktop Entry]
Encoding=UTF-8
Name=LED Test
Comment=IconTest Link
Exec=/home/pi/ledApp/led_start.sh
Type=Application
Categories=Application;Development;
Note: Exec is the location of the script that we created before
- Step 3. Open a terminal window inside the reTerminal and navigate to the root directory of the app
example:
cd /ledApp
- Step 4. Make the led_start.sh an executable file
chmod +x led.desktop
Launch the App
-
Step 1. Navigate to the ledApp folder using the reTerminal LCD
-
Step 2. Double click on the LED Test file
You will see the output as follows

Now you can click on the buttons and you will see the LEDs light up!
Debugging the App
Let's go through the process of debugging your app while developing
-
Step 1. Log in to reTerminal via SSH using Microsoft Visual Studio Code as mentioned before
-
Step 2. Log in to reTerminal via SSH using a SSH application such as MobaXterm with X11 server feature
Note: X11 is needed to forward the reTerminal display and pop up on the PC
- Step 3. After writing all the codes on Microsoft Visual Studio Code to the reTerminal, run the main.py file using MobaXterm
python3 main.py
Direct Test
Follow the steps above to set up your environment, copy the code directly and run it.
git clone https://github.com/lakshanthad/Python_ReTerminalQt5_LED_UI
cd Python_ReTerminalQt5_LED_UI
python3 main.py
Finally you will see the output displayed on a new window. If there are any errors in the code, they will be dislpayed in the MobaXterm terminal window.
Bonus Demo
If you want to experience a more interesting demo with Qt for Python, you can checkout this GitHub repo

Resources
- [GitHub] Python_ReTerminalQt5_LED_UI
- [Webpage] Qt Documentation
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.