Skip to main content

Utils

Interpolation Functions

reachy_mini.utils.interpolation.minimum_jerk

Source

Compute the minimum jerk interpolation function from starting position to goal position.


reachy_mini.utils.interpolation.linear_pose_interpolation

Source

Linearly interpolate between two poses in 6D space.


reachy_mini.utils.interpolation.time_trajectory

Source

Compute the time trajectory value based on the specified interpolation method.


reachy_mini.utils.interpolation.delta_angle_between_mat_rot

Source

Compute the angle (in radians) between two 3x3 rotation matrices P and Q.

This is equivalent to the angular distance in axis-angle space. It is computed via the trace of the relative rotation matrix.

Parameters:

NameDescription
PA 3x3 rotation matrix.
QAnother 3x3 rotation matrix.

Returns:

The angle in radians between the two rotations.

References:


reachy_mini.utils.interpolation.distance_between_poses

Source

Compute three types of distance between two 4x4 homogeneous transformation matrices.

The result combines translation (in mm) and rotation (in degrees) using an arbitrary but emotionally satisfying equivalence: 1 degree ≈ 1 mm.

Parameters:

NameDescription
pose1A 4x4 homogeneous transformation matrix representing the first pose.
pose2A 4x4 homogeneous transformation matrix representing the second pose.

Returns:

A tuple of:

  • translation distance in meters
  • angular distance in radians
  • unhinged distance in magic-mm (translation in mm + rotation in degrees)

reachy_mini.utils.interpolation.compose_world_offset

Source

Compose an absolute world-frame pose with a world-frame offset.

  • translations add in world: t_final = t_abs + t_off
  • rotations compose in world: R_final = R_off @ R_abs

This rotates the frame in place (about its own origin) by a rotation defined in world axes, and shifts it by a world translation.

Parameters:

NameTypeDescription
T_abs(4,4) ndarrayAbsolute pose in world frame.
T_off_world(4,4) ndarrayOffset transform specified in world axes (dx,dy,dz in world; dR about world axes).
reorthonormalizeboolIf True, SVD-orthonormalize the resulting rotation to fight drift.

Returns:

NameTypeDescription
T_final(4,4) ndarrayResulting pose in world frame.

reachy_mini.utils.interpolation.InterpolationTechnique

Source

Enumeration of interpolation techniques.


Hardware Configuration

reachy_mini.utils.hardware_config.parser.MotorConfig

Source

Motor configuration.


reachy_mini.utils.hardware_config.parser.SerialConfig

Source

Serial configuration.


reachy_mini.utils.hardware_config.parser.ReachyMiniConfig

Source

Reachy Mini configuration.


reachy_mini.utils.hardware_config.parser.parse_yaml_config

Source

Parse the YAML configuration file and return a ReachyMiniConfig.


Rerun Visualization

reachy_mini.utils.rerun.Rerun

Source

Rerun logging for Reachy Mini.

Methods

log_camera

Source

Log the camera image to Rerun.


log_movements

Source

Log the movement data to Rerun.


set_absolute_path_to_urdf

Source

Set the absolute paths in the URDF file. Rerun cannot read the "package://" paths.


start

Source

Start the Rerun logging thread.


stop

Source

Stop the Rerun logging thread.


reachy_mini.utils.rerun.UrdfEntityPaths

Source

Helper for constructing link/joint entity paths that match the native URDF logger.


Wireless Version Utilities

reachy_mini.utils.wireless_version.utils.call_logger_wrapper

Source

Run a command asynchronously, streaming stdout and stderr to logger in real time.

Parameters:

NameDescription
commandlist or tuple of command arguments (not a string)
loggerlogger object with .info and .error methods

reachy_mini.utils.wireless_version.update.update_reachy_mini

Source

Update reachy_mini package and restart daemon.

Parameters:

NameDescription
loggerLogger for streaming output.
pre_releaseIf True, install pre-release from PyPI (ignored if git_ref set).
git_refIf set, install from this GitHub tag/branch instead of PyPI.

reachy_mini.utils.wireless_version.startup_check.check_and_fix_venvs_ownership

Source

For wireless units, check if files under venvs_path are owned by user pollen and fix if needed.

Parameters:

NameDescription
venvs_pathPath to the virtual environments directory (default: /venvs)
custom_loggerOptional logger to use instead of the module logger

reachy_mini.utils.wireless_version.startup_check.check_and_update_bluetooth_service

Source

info

Check if bluetooth service needs updating and update if different.

Compares the source bluetooth_service.py with the installed version at /bluetooth/bluetooth_service.py. If they differ, copies the new version and restarts the bluetooth service. Also syncs the commands/ folder.


reachy_mini.utils.wireless_version.startup_check.check_and_update_wireless_launcher

Source

info

Check if wireless daemon service needs updating and update if different.

Compares the source reachy-mini-daemon.service with the installed version. If they differ, copies the new version and reloads systemd.


reachy_mini.utils.wireless_version.startup_check.check_and_sync_apps_venv_sdk

Source

info

Check if apps_venv SDK matches daemon install source and sync if needed.

Compares both version AND install source (PyPI vs git ref). If daemon was installed from a git ref, apps_venv will be synced to the same ref.


reachy_mini.utils.wireless_version.update_available.is_update_available

Source

Check if an update is available for the given package.


reachy_mini.utils.wireless_version.update_available.get_pypi_version

Source

Get the latest version of a package from PyPI.


reachy_mini.utils.wireless_version.update_available.get_local_version

Source

Get the currently installed version of a package.


Core Utilities

reachy_mini.utils.create_head_pose

Source

Create a homogeneous transformation matrix representing a pose in 6D space (position and orientation).

Parameters:

NameTypeDescription
xfloatX coordinate of the position.
yfloatY coordinate of the position.
zfloatZ coordinate of the position.
rollfloatRoll angle
pitchfloatPitch angle
yawfloatYaw angle
mmboolIf True, convert position from millimeters to meters.
degreesboolIf True, interpret roll, pitch, and yaw as degrees; otherwise as radians.

Returns:

np.ndarray — A 4x4 homogeneous transformation matrix representing the pose.


URDF Parsing

reachy_mini.utils.parse_urdf_for_kinematics.get_data

Source

Generate the urdf_kinematics.json file.

Loading Comments...