Install the Daemon from a Specific Branch
This guide explains how to install the Reachy Mini daemon from a specific GitHub branch before it is officially released. Use this for testing new features or bug fixes.
Starting from v1.3.0, you can install a branch directly from Settings → Reachy Mini Update in the web dashboard.
Prerequisites
- SSH access to your Reachy Mini robot (
[email protected], password:root) - The robot must be connected to your Wi-Fi network (or accessible through its hotspot)
Option A: Local Development Setup
This option is intended for active development and fast debugging cycles. It allows you to safely test changes without affecting the system-wide installation.
Avoid installing dashboard apps with this option—any changes made to the local reachy_mini version won't be propagated correctly.
Steps:
Step 1: Connect to the robot via SSH:
ssh [email protected]
# Password: root
Step 2: Clone the Reachy Mini repository with the specific branch:
git clone -b <branch-name> https://github.com/pollen-robotics/reachy_mini.git
cd reachy_mini
Step 3: Set up the virtual environment:
uv venv --python /venvs/mini_daemon/bin/python .venv
source .venv/bin/activate
uv sync --extra gstreamer --extra wireless-version
Step 4: Stop the system daemon service:
sudo systemctl stop reachy-mini-daemon
This step must be repeated after each reboot since the system service restarts automatically.
Step 5: Start the local daemon for testing:
reachy-mini-daemon --wireless-version
Now you can modify the code in ~/reachy_mini and test your changes without affecting the system installation.
Option B: System-Wide Custom Installation
This option installs a branch build of reachy-mini as the system-wide daemon. It's better suited for thorough, end-to-end testing and supports seamless app installation from the dashboard.
Steps:
Step 1: Connect to the robot via SSH:
ssh [email protected]
# Password: root
Step 2: Activate the daemon's virtual environment:
source /venvs/mini_daemon/bin/activate
Step 3: Install the specific branch:
pip install --no-cache-dir --force-reinstall \
"reachy_mini[gstreamer,wireless-version] @ git+https://github.com/pollen-robotics/reachy_mini.git@<branch-name>"
Replace <branch-name> with the branch you want to test (e.g., develop, feature/my-feature, bugfix/issue-123).
We have to use pip here and not uv because uv pip install does not work correctly with git lfs.
Step 4: (Only for versions ≤ 1.2.13) Repeat steps 2 and 3 using /venvs/apps_venv.
Step 5: Restart the daemon service:
sudo systemctl restart reachy-mini-daemon
Step 6: Verify the installation was successful:
pip show reachy-mini | grep Version
This should display the version corresponding to your installed branch.
Rolling Back to Factory Version
If you encounter issues with the branch installation, you can restore the factory daemon:
Step 1: Trigger the SOFTWARE_RESET command** via Bluetooth to reinstall the original factory daemon
Step 2: Refer to the Reset Guide for detailed step-by-step instructions
Important Notes
- Backup your work before switching between different branch installations
- Test thoroughly in local development mode before doing system-wide installations
- Monitor system logs after installation:
journalctl -u reachy-mini-daemon -f - Performance impact: Some development branches may have reduced performance or stability