Building & Publishing Apps
Reachy Mini has an app ecosystem powered by Hugging Face Spaces. You can build Python apps, publish them, and any Reachy Mini owner can install them in one click from the dashboard.
For a step-by-step tutorial with screenshots, see the blog post: Make and Publish Your Reachy Mini Apps.
Using AI Agents
If you use an AI coding agent (Claude Code, Cursor, Copilot, etc.), it can build apps for you. Point it to the project's AGENTS.md:
I'd like to create a Reachy Mini app. Start by reading https://github.com/pollen-robotics/reachy_mini/blob/main/AGENTS.md
The repository includes a skills/ directory with detailed guides that AI agents use to build apps correctly:
| Skill | What it covers |
|---|---|
create-app.md | App creation workflow and templates |
ai-integration.md | Building LLM-powered apps |
control-loops.md | Real-time reactive apps (tracking, games) |
motion-philosophy.md | Choosing between goto_target and set_target |
interaction-patterns.md | Antennas as buttons, head as controller |
symbolic-motion.md | Defining motion mathematically (dances, rhythms) |
How Apps Work
The Reachy Mini daemon manages your app's entire lifecycle:
- You send a "start app" request (from the dashboard or REST API).
- The daemon launches your app as a Python subprocess (
python -u -m your_app.main). - Your app receives a connected
ReachyMiniinstance and astop_event. - When stopped, the daemon sends
SIGINTto your process, which triggers graceful shutdown. - After the app exits, the daemon returns the robot to its default position.
Key constraints:
- Only one app can run at a time.
- Your app runs inside the daemon's subprocess — it does not manage its own hardware connections.
- On the Wireless robot, your app runs in a shared virtual environment at
/venvs/apps_venv/.
Creating an App
Always use the CLI tool to create apps — it generates the correct structure, metadata, and entry points:
# Install reachy-mini if not already done
uv pip install reachy-mini
# Create and publish in one step (recommended)
reachy-mini-app-assistant create my_app_name /path/to/destination --publish
# Or create locally first
reachy-mini-app-assistant create my_app_name /path/to/destination
Never create app folders manually. The assistant handles boilerplate, Hugging Face tags, entry points, and the correct package structure. Manual creation leads to subtle issues that are hard to debug.
Choose a Template
| Template | Command | Use when |
|---|---|---|
| Default | reachy-mini-app-assistant create my_app . | Most apps. Minimal working structure. |
| Conversation | reachy-mini-app-assistant create --template conversation my_app . | LLM integration, speech, making the robot talk. Includes audio pipeline, LLM tools, movement fusion and all the plumbing. |
Generated Structure
my_app/
├── index.html # Hugging Face Space landing page
├── style.css # Landing page styles
├── pyproject.toml # Package config with entry points
├── README.md # Must contain reachy_mini_python_app tag
└── my_app/
├── __init__.py
├── main.py # Your app logic
└── static/ # Optional web UI
├── index.html
├── style.css
└── main.js
The ReachyMiniApp Contract
Your app is a class that extends ReachyMiniApp and implements a run() method. Here's the minimal structure:
import threading
import time
import numpy as np
from reachy_mini import ReachyMini, ReachyMiniApp
from reachy_mini.utils import create_head_pose
class MyApp(ReachyMiniApp):
def run(self, reachy_mini: ReachyMini, stop_event: threading.Event):
t0 = time.time()
while not stop_event.is_set():
t = time.time() - t0
# Move the head
yaw = 30.0 * np.sin(2.0 * np.pi * 0.2 * t)
head_pose = create_head_pose(yaw=yaw, degrees=True)
# Move the antennas
a = np.deg2rad(25.0 * np.sin(2.0 * np.pi * 0.5 * t))
antennas = np.array([a, -a])
reachy_mini.set_target(head=head_pose, antennas=antennas)
time.sleep(0.02)
if __name__ == "__main__":
app = MyApp()
try:
app.wrapped_run()
except KeyboardInterrupt:
app.stop()
Key points
run(reachy_mini, stop_event): The only method you must implement. TheReachyMiniinstance is already connected and ready. Pollstop_eventin your main loop to exit gracefully.wrapped_run(): Called from the__main__block. It handles connecting to the robot, starting optional services, and calling yourrun()method.stop(): Sets thestop_event. The daemon calls this viaSIGINTwhen stopping your app.__main__block: Required. The daemon runs your app as a module (python -m my_app.main), so this block is the actual entry point.
The pyproject.toml Entry Point
The daemon discovers your app through a standard Python entry point. The assistant generates this for you:
[project.entry-points."reachy_mini_apps"]
my_app = "my_app.main:MyApp"
The group name is reachy_mini_apps (with underscores). The value points to your class (module.main:ClassName).
Any additional dependency for your project should be added in this file.
Optional: Web UI for Your App
If you want a settings page or any web interface for your app, set custom_app_url on your class:
class MyApp(ReachyMiniApp):
custom_app_url: str | None = "http://0.0.0.0:8042"
def run(self, reachy_mini: ReachyMini, stop_event: threading.Event):
# Define FastAPI routes on self.settings_app
@self.settings_app.post("/my_endpoint")
def my_endpoint():
return {"status": "ok"}
# Your main loop...
When custom_app_url is set, the app automatically starts a FastAPI web server that serves files from the static/ directory inside your package. The dashboard shows a settings icon to open this UI. The page can be accessed from http://localhost:8042 with a lite or http://reachy-mini.local:8042 with a wireless.
Set custom_app_url = None if your app doesn't need a web UI.
For a working example with a toggle and sound playback, see the template app.
Testing Your App
1. Validate structure
reachy-mini-app-assistant check /path/to/my_app
This checks that your app has the correct structure, entry points, and metadata.
2. Run directly
You can run your app's main.py directly for quick iteration (make sure the daemon is running):
python -m my_app.main
3. Test through the dashboard
Install your app locally and test it through the dashboard, as users would:
# Install in development mode
uv pip install -e /path/to/my_app
# Start the daemon
reachy-mini-daemon # Lite
reachy-mini-daemon --sim # Simulation
Then open http://127.0.0.1:8000/ — your app appears in the installed list.
Publishing to Hugging Face
1. Log in to Hugging Face
uv pip install --upgrade huggingface_hub
hf auth login
Use a token with Write permissions.
2. Publish
If you used --publish when creating the app, it's already a Hugging Face Space with a Git remote. Just push:
git add . && git commit -m "my changes" && git push
If you created without --publish, you can publish later:
reachy-mini-app-assistant publish /path/to/my_app
3. Discoverability
For your app to appear in the Reachy Mini app store, its README.md must contain the reachy_mini_python_app tag in the YAML frontmatter:
---
tags:
- reachy_mini_python_app
---
The assistant adds this automatically. If you create the README manually, don't forget it.
Installing Apps
From the dashboard
Open the Reachy Mini dashboard and click Install on any community app. This is the easiest way.
Via the REST API
# Install from Hugging Face
curl -X POST http://localhost:8000/api/apps/install \
-H "Content-Type: application/json" \
-d '{"url": "https://huggingface.co/spaces/<user>/<app_name>"}'
# Start an app
curl -X POST http://localhost:8000/api/apps/start-app/<app_name>
# Stop the current app
curl -X POST http://localhost:8000/api/apps/stop-current-app
# List installed apps
curl http://localhost:8000/api/apps/list
Replace localhost with reachy-mini.local or the robot's IP address for the Wireless version.
Offline / manual deployment for a Wireless unit
If you don't have internet access on the robot (e.g., at a conference), you can install your app directly:
# Copy and install your app on the robot
scp -r /path/to/my_app pollen@reachy-mini.local:/tmp/my_app
ssh pollen@reachy-mini.local "/venvs/apps_venv/bin/pip install /tmp/my_app"
After updating code manually, restart the daemon or the app for changes to take effect.
Debugging Apps
Viewing logs
If you run the daemon in a terminal, app logs (stdout/stderr) appear there directly.
reachy-mini-daemon # Lite
reachy-mini-daemon --sim # Simulation
# App logs will print here
App output is captured by the daemon and available via journalctl:
ssh pollen@reachy-mini.local
# Live logs
sudo journalctl -u reachy-mini-daemon -f
# Recent logs, filtered (daemon logs are noisy with HTTP access logs)
sudo journalctl -u reachy-mini-daemon --since '5 min ago' | grep -v "uvicorn\|GET \|POST "
Common issues
| Problem | Solution |
|---|---|
| "An app is already running" | Stop the current app first: curl -X POST http://localhost:8000/api/apps/stop-current-app |
| Daemon in a bad state | Restart it: sudo systemctl restart reachy-mini-daemon (wait ~30s before starting an app) |
| App not picking up code changes | Restart the app. If you deployed manually, also clear bytecode: rm -rf __pycache__ |
Tip: log everything at startup
A useful debugging practice is logging your configuration when the app starts:
import logging
import sys
logger = logging.getLogger(__name__)
def run(self, reachy_mini, stop_event):
logger.info("=" * 50)
logger.info("MY APP STARTING")
logger.info(f" Python: {sys.version}")
logger.info("=" * 50)
# ...
App Configuration
The app subprocess inherits the daemon's environment variables. There is no special injection mechanism — your app sees whatever the daemon process sees.
If your app needs runtime configuration (API keys, server URLs, etc.), the recommended approach is to use the app's web UI. Set custom_app_url on your class and add a settings page where users can enter values (API keys, server addresses, etc.) directly from their browser. This is the most user-friendly option and works across all platforms. See Optional: Web UI for Your App above for how to set this up.
Other approaches:
- Config file: Read from a known path (e.g.,
.envsee example here). - Hardcoded defaults: Simple and debuggable for development.
Using Audio in Your App
Audio recording, playback, and direction-of-arrival detection work the same way inside an app as in a standalone script — use the SDK methods directly (start_recording(), get_audio_sample(), push_audio_sample(), play_sound()).
Refer to the official examples for working code:
- Sound Recording: Record from the mic array and save to WAV.
- Sound Playback: Play a WAV file or push real-time audio (e.g., from a TTS engine).
- Sound Direction of Arrival: Detect who is speaking and make the robot look at them.
For details on how audio streams differ between Wireless and Lite, see Media Architecture.
Further Reading
- Blog post: Make and Publish Your Reachy Mini Apps — full walkthrough with screenshots
- API Reference: Apps API — auto-generated reference for
ReachyMiniApp,AppManager, and related classes - REST API: REST API Reference — full HTTP endpoint documentation
- Example apps: Browse community apps on Hugging Face for inspiration
| App | Key Patterns | Link |
|---|---|---|
| Conversation App | LLM tools, audio pipeline, control loops | GitHub |
| Marionette | Motion recording, safe torque, HF datasets | HF Space |
| Radio | Antenna interaction pattern | HF Space |
| Simon | No-GUI pattern (antenna to start) | HF Space |
| Hand Tracker | Camera-based real-time control loop | HF Space |
| Spaceship Game | Head-as-joystick, antenna buttons | HF Space |