Skip to main content

Python SDK Reference

💡 Reminder: The SDK now auto-detects whether it should connect over USB/localhost or over the network, so ReachyMini() works out of the box. You can still force a mode with ReachyMini(connection_mode="localhost_only" | "network") if needed.

Movement

Basic Control (goto_target)

Smooth interpolation between points. You can control head, antennas, and body_yaw.

from reachy_mini import ReachyMini
from reachy_mini.utils import create_head_pose
import numpy as np

with ReachyMini() as mini:
# Move everything at once
mini.goto_target(
head=create_head_pose(z=10, mm=True), # Up 10mm
antennas=np.deg2rad([45, 45]), # Antennas out
body_yaw=np.deg2rad(30), # Turn body
duration=2.0, # Take 2 seconds
method="minjerk" # Smooth acceleration
)

Interpolation methods: linear, minjerk (default), ease_in_out, cartoon.

Instant Control (set_target)

Bypasses interpolation. Use this for high-frequency control (e.g., following a joystick or generated trajectory).

Sensors & Media

The media architecture is described in detail in the Media Architecture section. Although accesssing audio and video from the SDK is similar across Reachy Mini versions, the underlying implementation differs.

Camera 📷

The frames of the camera can be accessed as follows :

from reachy_mini import ReachyMini

with ReachyMini(media_backend="default") as mini:
frame = mini.media.get_frame()

The returned frame is a numpy array with shape (height, width, 3) and data type uint8.

IMU 🧭

⚠️ The IMU is only available with the wireless version of Reachy Mini

Take a look at this example

with ReachyMini() as mini:
imu_data = mini.imu
accel_x, accel_y, accel_z = imu_data["accelerometer"] # (m/s^2)
gyro_x, gyro_y, gyro_z = imu_data["gyroscope"] # (rad/s)
quat_w, quat_x, quat_y, quat_z = imu_data["quaternion"] # (w, x, y, z)
temperature = imu_data["temperature"] # (°C)

Audio 🎙️ 🔊

Audio inputs (microphones) and outputs (speaker) is handled as follows:

from reachy_mini import ReachyMini
from scipy.signal import resample
import time

with ReachyMini(media_backend="default") as mini:
# Initialization - After this point, both audio devices (input/output) will be seen as busy by other applications!
mini.media.start_recording()
mini.media.start_playing()

# Record
samples = mini.media.get_audio_sample()

# Resample (if needed)
samples = resample(samples, mini.media.get_output_audio_samplerate()*len(samples)/mini.media.get_input_audio_samplerate())

# Play
mini.media.push_audio_sample(samples)
time.sleep(len(samples) / mini.media.get_output_audio_samplerate())

# Get Direction of Arrival
# 0 radians is left, π/2 radians is front/back, π radians is right.
doa, is_speech_detected = mini.media.get_DoA()
print(doa, is_speech_detected)

# Release audio devices (input/output)
mini.media.stop_recording()
mini.media.stop_playing()

Audio data format:

  • get_audio_sample() returns a numpy array with shape (samples, 2) and data type float32, sampled at 16kHz.
  • push_audio_sample() expects a numpy array with shape (samples, 1 or 2) and data type float32, sampled at 16kHz.

In both cases, the channels and samplerate information can be reliably retrieved with get_input/output_audio_samplerate() and get_input/output_channels().

⚠️ Note: push_audio_sample() is non-blocking, meaning it returns immediately while audio plays in the background. If you need to wait for playback completion, calculate the duration based on sample length and sample rate.

Media Backend Options

Choose the appropriate media backend based on your Reachy Mini version and requirements:

Reachy Mini Lite:

  • media_backend="default" - Uses OpenCV for camera and Sounddevice for audio (recommended for most users)
  • media_backend="gstreamer" - Uses GStreamer for both camera and audio (installation required)

Reachy Mini Wireless:

  • Local execution (running on the robot with SSH): Automatically uses "gstreamer"
  • Remote execution (controlling from your computer): Automatically uses "webrtc". With this backend, GStreamer runs locally on the Raspberry Pi, and streams both audio and video on the remote computer using WebRTC.

💡 Tip: For wireless setups, the backend is automatically selected based on whether you're running locally or remotely. No need to specify the media_backend value !

💡 Tip: For wireless setups, the WebRTC backend is requires a specific installation see gstreamer-installation.md. For now only the Linux platform is supported as a client. Other platforms (Windows, macOS) will be supported in future releases.

Recording Moves

You can record a motion by moving the robot (compliant mode) or sending commands, and save it for later replay.

from reachy_mini import ReachyMini
with ReachyMini() as mini:
mini.start_recording()
# ... robot moves ...
recorded_data = mini.stop_recording()

Next Steps

❓ Troubleshooting

Encountering an issue? 👉 Check the Troubleshooting & FAQ Guide

Loading Comments...