Skip to main content

Quickstart Guide

Follow this guide to get your Reachy Mini up and running, either on real hardware or in simulation.

1. Prerequisites

Important

Make sure you have installed Reachy Mini on your computer following our installation guide.

Virtual Environment

Ensure you have created and activated your Python virtual environment. Remember to activate it every time you open a new terminal!

Run SDK directly on Wireless Reachy Mini (Optional)

If you want to run the SDK directly on your wireless Reachy Mini instead of remotely on your computer, you can connect via SSH into it.

Step 1: SSH Connection

Open a terminal and run:

ssh pollen@reachy-mini

When prompted, use these default credentials:

  • Username: pollen
  • Password: root

Step 2: Activate the Python virtual environment

After connecting, activate the virtual environment:

source /venvs/apps_venv/bin/activate

Step 3: Run scripts locally

When running scripts on Reachy Mini itself, use the standard ReachyMini() constructor. Auto mode will keep the connection on localhost unless you explicitly override it:

from reachy_mini import ReachyMini

with ReachyMini() as mini:
# Your code here

Benefits of running locally: Lower latency, no network dependency, and direct access to all robot resources.

Drawbacks: Lower CPU power, and no GUI available.

2. Ensure the Robot Server is running (Daemon)

info

The Daemon is a background service that handles the low-level communication with motors and sensors. It must be running for your code to work.

  • On Reachy Mini (Wireless): The daemon is running when the robot is powered on. Ensure your computer and Reachy Mini are on the same network.
Reachy Mini Lite (USB)

You have two options:

  • Open a terminal and run:
    reachy-mini-daemon
Simulation (No robot needed)

You have two options:

  • Open a terminal and run:

Linux & Windows:

reachy-mini-daemon --sim

macOS:

mjpython -m reachy_mini.daemon.app.main --sim
macOS Users

uv may have compatibility issues with MuJoCo on macOS. If you encounter installation or runtime problems, it's recommended to use pip directly instead of uv for MuJoCo-related packages.

Verification

Open http://localhost:8000 in your browser. If you see the Reachy Dashboard, you are ready!

3. Your First Script

Important

Keep the daemon terminal open and running! The daemon must stay active for your robot to work.

Create your Python script

Step 1

Open a new terminal window

Step 2

Create a new file called hello.py and copy-paste the following code into it:

info

The constructor now auto-detects Lite vs Wireless and switches between localhost and network automatically. Only override it for advanced cases, e.g. ReachyMini(connection_mode="network").

from reachy_mini import ReachyMini

# Connect to the running daemon
with ReachyMini() as mini:
print("Connected to Reachy Mini!")

# Wiggle antennas
print("Wiggling antennas...")
mini.goto_target(antennas=[0.5, -0.5], duration=0.5)
mini.goto_target(antennas=[-0.5, 0.5], duration=0.5)
mini.goto_target(antennas=[0, 0], duration=0.5)

print("Done!")
Step 3

Save the file and run your script:

In your new terminal, run:

python hello.py

🎉 If everything went well, your robot should now wiggle its antennas!

❓ Troubleshooting

Encountering an issue? 👉 Check the Troubleshooting & FAQ Guide

Using an AI Coding Agent?

info

If you're using an AI agent like Claude Code, Codex, or Copilot, you can start building apps right away. Just paste this prompt:

I'd like to create a Reachy Mini app. Start by reading https://github.com/pollen-robotics/reachy_mini/blob/develop/AGENTS.md

This guide gives your AI agent everything it needs to know about the SDK, best practices, and available tools.

Next Steps

Loading Comments...