Skip to main content

reBot Arm B601-DM GraspNet Visual Grasping on Jetson

This wiki explains how to deploy the reBot Arm B601-DM visual grasping demo on NVIDIA Jetson. The demo combines an RGB-D camera, YOLO instance segmentation, GraspNet 6-DoF grasp pose estimation, eye-in-hand calibration, and real robot control, so the arm can select and grasp common objects on a table.

Version 1.0 of this guide focuses on a reliable single-Jetson deployment and daily operation flow. The default setup uses Orbbec Gemini 2 as the RGB-D camera, YOLO11n-seg TensorRT for target filtering, and GraspNet for generic 6-DoF grasp pose generation.

reBot Arm B601-DM Bundle with Jetson Orin

What You Will Build​

The runtime pipeline is:

Orbbec Gemini 2 RGB-D camera
|
YOLO instance segmentation for target filtering
|
GraspNet 6-DoF grasp pose estimation
|
Eye-in-hand calibration transform
|
reBot Arm IK trajectory and gripper force control
|
Optional base rotation and object placement

The project provides three practical ways to use the system:

ModeEntry pointTypical use
Web UIscripts/grasp_web.pyLive video, target selection, grasp preview, real grasp, offset tuning
CLIscripts/grasp.pyHeadless grasping or scripted testing
HTTP APIscripts/grasp_curl.sh and scripts/grasp_api_client.pyRemote control, automation, integration with other apps

Hardware and System Preparation​

Prepare the following hardware before starting:

  • reBot Arm B601-DM
  • NVIDIA Jetson device running JetPack 6.x or JetPack 7.x
  • Orbbec Gemini 2 RGB-D camera
  • USB2CAN adapter for the robot CAN bus
  • USB 3.0 cable for the camera
  • ArUco marker for hand-eye calibration, DICT_4X4_50, ID 0, 0.1 m edge length
  • A stable table, enough clearance around the arm, and an emergency power-off method
warning

This demo drives a real robotic arm. During all motion tests and grasp tests, keep hands, cables, and loose objects away from the arm workspace. Start with --dry-run, read-only checks, and small jog values before enabling full robot execution.

Connect the hardware:

  1. Connect Gemini 2 to Jetson through USB 3.0.
  2. Connect the USB2CAN adapter to the reBot Arm CAN bus and then to Jetson.
  3. Power on the reBot Arm.
  4. Confirm the devices are visible:
lsusb
ls /dev/ttyUSB* /dev/ttyACM* 2>/dev/null || true

Set temporary device permissions for first bring-up:

sudo chmod a+rw /dev/bus/usb/*/*
sudo chmod 666 /dev/ttyUSB0 2>/dev/null || true
sudo chmod 666 /dev/ttyACM0 2>/dev/null || true

For serial devices, it is also recommended to add the current user to dialout, then log out and log back in:

sudo usermod -aG dialout $USER

Deploy the Project on Jetson​

Step 1. Install system packages and Miniconda

sudo apt update
sudo apt install -y git wget curl build-essential cmake libusb-1.0-0-dev python3-pip

wget https://repo.anaconda.com/miniconda/Miniconda3-latest-Linux-aarch64.sh
bash Miniconda3-latest-Linux-aarch64.sh
source ~/.bashrc

Step 2. Clone the project

git clone https://github.com/jjjadand/reBot-DevArm-Grasp.git rebot_grasp-jetson
cd rebot_grasp-jetson

If you are using an internal package instead of the public repository, copy that project directory to Jetson and run the remaining commands from the project root.

Step 3. Create the Python environment

Use Python 3.10 on JetPack 6.x. Use Python 3.12 on JetPack 7.x / Thor.

# JetPack 6.x
conda create -y -n graspnet python=3.10

# JetPack 7.x / Thor
# conda create -y -n graspnet python=3.12

conda activate graspnet
python -m pip install -U pip wheel setuptools

Check your JetPack and CUDA versions:

cat /etc/nv_tegra_release
nvcc --version

Step 4. Install Jetson-compatible PyTorch

Do not install the generic PyPI CPU/GPU PyTorch package on Jetson. Install a wheel that matches your JetPack, Python, and CUDA versions. For reComputer users, you can also follow the dedicated guide: Install Pytorch for reComputer Jetson.

Common starting points are:

# JetPack 6.x, CUDA 12.x, Python 3.10
pip install --extra-index-url https://pypi.jetson-ai-lab.io/jp6/cu126 torch torchvision

# JetPack 7.x / Thor, CUDA 13.x, Python 3.12
pip install --extra-index-url https://pypi.jetson-ai-lab.io/sbsa/cu130 torch torchvision

Verify CUDA from Python:

python - <<'PY'
import torch
print("torch:", torch.__version__)
print("cuda available:", torch.cuda.is_available())
print("device:", torch.cuda.get_device_name(0) if torch.cuda.is_available() else "none")
PY

cuda available must be True before continuing.

Step 5. Install Python dependencies

pip install -r requirements-graspnet-jetson.txt

Step 6. Install robot, GraspNet, and GraspNet API SDKs

mkdir -p sdk

git clone https://github.com/Seeed-Projects/reBotArm_control_py.git sdk/reBotArm_control_py
pip install -e sdk/reBotArm_control_py

git clone https://github.com/graspnet/graspnet-baseline.git sdk/graspnet-baseline
git clone https://github.com/graspnet/graspnetAPI.git sdk/graspnetAPI
pip install -e sdk/graspnetAPI

Download the GraspNet pretrained checkpoint from the GraspNet download page and place it here:

sdk/graspnet-baseline/checkpoints/checkpoint-rs.tar

Step 7. Set CUDA paths and build GraspNet CUDA operators

Set the CUDA path for your JetPack version:

# JetPack 6.x example
export CUDA_HOME=/usr/local/cuda-12.6

# JetPack 7.x / Thor example
# export CUDA_HOME=/usr/local/cuda-13.0

export PATH="$CUDA_HOME/bin:$PATH"
export LD_LIBRARY_PATH="$CUDA_HOME/lib64:$LD_LIBRARY_PATH"

Build the CUDA extensions used by GraspNet:

bash scripts/install_graspnet_cuda_ops.sh
bash scripts/install_graspnet_cuda_ops.sh --check

If you change JetPack, Python, CUDA, or PyTorch later, rebuild with:

bash scripts/install_graspnet_cuda_ops.sh --force

Step 8. Install the Orbbec camera SDK

The project includes a helper that installs pyorbbecsdk2 into the active Python environment:

bash scripts/install_pyorbbecsdk.sh

If you need to build the SDK locally, clone the source tree first and run the source mode:

git clone https://github.com/orbbec/pyorbbecsdk.git sdk/pyorbbecsdk
bash scripts/install_pyorbbecsdk.sh --from-source

Install Orbbec udev rules when the SDK source tree is available:

sudo bash sdk/pyorbbecsdk/scripts/env_setup/install_udev_rules.sh
sudo udevadm control --reload-rules
sudo udevadm trigger

Step 9. Download YOLO weights and export TensorRT on the target Jetson

TensorRT engine files are device-specific. Always export the .engine on the Jetson that will run the demo.

mkdir -p models
wget https://github.com/ultralytics/assets/releases/download/v8.3.0/yolo11n-seg.pt -O models/yolo11n-seg.pt

yolo export model=models/yolo11n-seg.pt format=engine imgsz=640 half=True device=0 workspace=4

The expected output is:

models/yolo11n-seg.engine

If FP16 export fails on your platform, export without half=True:

yolo export model=models/yolo11n-seg.pt format=engine imgsz=640 device=0 workspace=4

Verify and Calibrate​

Run these checks in order before attempting a real grasp.

1. Check the RGB-D camera

conda activate graspnet
cd ~/rebot_grasp-jetson

python scripts/verify_pyorbbec_stream.py
python scripts/verify_pyorbbec_stream.py --preview --seconds 10

The text-only check should report RGB and depth frame information. The preview check should show RGB and depth windows when a desktop display is available.

2. Check the robot connection

Start with read-only mode:

python scripts/verify_rebot_arm_motion.py --read-only

Then run a small joint6 jog after confirming the arm path is clear:

python scripts/verify_rebot_arm_motion.py --deg 5

3. Check the GraspNet stack

python scripts/verify_graspnet_stack.py

If the camera is not connected yet but you only want to check Python, CUDA, GraspNet, and YOLO files:

python scripts/verify_graspnet_stack.py --skip-camera

4. Perform eye-in-hand calibration

This project uses eye-in-hand calibration: the camera is mounted on the end effector, and the ArUco marker is fixed on the table. The default config expects a DICT_4X4_50, ID 0, 0.1 m marker. The repository includes printable marker files such as aruco100x100.pdf.

Automatic collection:

python scripts/collect_handeye_eih.py

Manual collection with gravity compensation:

python scripts/collect_handeye_eih.py --manual

Calibration results are saved under the active camera directory:

config/calibration/orbbec_gemini2/hand_eye.npz
config/calibration/orbbec_gemini2/intrinsics.npz

Verify the saved calibration:

python scripts/verify_handeye_calibration.py

Recalibrate whenever the camera mount, gripper, ArUco board size, or table geometry changes.

Run the Web Demo​

The Web UI is the recommended first user interface. It provides live MJPEG video, target selection, grasp preview, real grasp execution, compensation tuning, base jog, gripper control, ready pose, and reset operations.

Start in preview mode first. This does not execute real robot motion:

conda activate graspnet
cd ~/rebot_grasp-jetson

python scripts/grasp_web.py \
--host 0.0.0.0 \
--port 8090 \
--num-point 12000 \
--cloud-crop-nsample 32

Open the Web UI from a browser:

http://<jetson_ip>:8090

Use preview mode to confirm camera stream, YOLO detections, target filtering, and grasp-point generation. Click the infer or refresh control in the Web UI to update GraspNet preview.

When the scene is stable and the verification steps have passed, start with real robot execution:

python scripts/grasp_web.py \
--host 0.0.0.0 \
--port 8090 \
--enable-robot \
--num-point 12000 \
--cloud-crop-nsample 32

For first real tests, disable post-grasp placement so the arm only performs the grasp and recovery motion:

python scripts/grasp_web.py \
--host 0.0.0.0 \
--port 8090 \
--enable-robot \
--no-place-after-grasp \
--num-point 12000 \
--cloud-crop-nsample 32

Useful startup options:

OptionPurpose
--enable-robotAllow real arm and gripper motion
--target-class cupPreselect a target class
--no-yoloDisable YOLO filtering and run full-scene GraspNet
--camera-type orbbec_gemini2Force the camera driver
--no-place-after-graspSkip base rotation and placement after grasp
--num-point 12000Lower GraspNet point count for Jetson memory
--cloud-crop-nsample 32Lower CloudCrop samples for Jetson memory
--graspnet-interval 2.0Set automatic GraspNet update interval when enabled

The normal Web UI workflow is:

  1. Click Ready to move the arm to the ready pose.
  2. Select a target class, or leave it empty to use detected objects.
  3. Click Infer or Refresh to compute a grasp pose.
  4. Check that the grasp marker looks reasonable in the video.
  5. Adjust gripper, camera, or base compensation if needed.
  6. Click Real Grasp only when the arm path is clear.
  7. Use Reset if the scene changes or the robot needs to return to a safe state.

Compensation values are used to correct small mechanical and calibration errors. After tuning in the Web UI, persist the values in config/compensation.json or copy stable values into your deployment notes. Use small increments, for example 0.005 m for position offsets and 1 to 2 degrees for rotation offsets.

CLI and API Usage​

For a headless dry-run, use:

python scripts/grasp.py --dry-run --camera-type orbbec_gemini2 --target-class cup

For full-scene GraspNet without YOLO filtering:

python scripts/grasp.py --dry-run --camera-type orbbec_gemini2 --no-yolo

For real CLI execution:

python scripts/grasp.py --camera-type orbbec_gemini2 --target-class cup

Disable placement during CLI commissioning:

python scripts/grasp.py \
--camera-type orbbec_gemini2 \
--target-class cup \
--no-place-after-grasp

To inspect GraspNet live output without executing the robot:

python scripts/graspnet_camera_demo.py --auto --target-class cup
python scripts/graspnet_camera_demo.py --auto --no-yolo --no-visualizer

For HTTP automation, start the Web service with the helper:

bash scripts/grasp_curl.sh serve --enable-robot --no-auto-graspnet

In another terminal:

bash scripts/grasp_curl.sh state
bash scripts/grasp_curl.sh ready
bash scripts/grasp_curl.sh target bottle
bash scripts/grasp_curl.sh infer
bash scripts/grasp_curl.sh grasp
bash scripts/grasp_curl.sh reset

The same operations can be called directly with curl:

BASE=http://127.0.0.1:8090

curl -s "$BASE/state"
curl -s -X POST "$BASE/ready" -H "Content-Type: application/json" -d "{}"
curl -s -X POST "$BASE/target" -H "Content-Type: application/json" -d '{"class_name":"bottle"}'
curl -s -X POST "$BASE/infer" -H "Content-Type: application/json" -d "{}"
curl -s -X POST "$BASE/grasp" -H "Content-Type: application/json" -d "{}"

Other useful endpoints:

EndpointMethodPurpose
/stateGETCurrent detection, grasp, and Web runtime state
/robot/stateGETRobot joints, TCP pose, gripper state
/stream.mjpgGETMJPEG camera stream
/compensationPOSTSet gripper, camera, and base compensation
/joint/limitsGETRead joint positions and limits
/joint/jogPOSTJog one joint, often joint1 for base tests
/move/jointsPOSTMove all joints to absolute positions
/move/posePOSTMove TCP to a target pose through IK or trajectory mode
/gripperPOSTOpen, close, release, or read gripper state
/auto_graspPOSTRun a background target-search and grasp cycle

Configuration and Tuning​

The main configuration file is:

config/default.yaml

Default camera settings:

camera:
type: orbbec_gemini2
color_width: 1280
color_height: 720
depth_width: 1280
depth_height: 720
fps: 30

Default detection and GraspNet settings:

yolo:
model_name: "yolo11n-seg.engine"
device: "auto"

graspnet:
checkpoint: "checkpoint-rs.tar"

Default placement behavior:

grasp_pipeline:
place:
enabled: true
base_joint: joint1
base_delta_deg: 90.0
base_direction: auto
base_rotate_duration: 2.5
base_safety_margin_deg: 5.0
return_home: false

If the gripper consistently misses the object, tune in this order:

SymptomFirst tuning target
Gripper is too far in front or behindgrasp_forward_offset / Web gripper forward
Gripper misses left or rightgrasp_lateral_offset or camera X/Y compensation
Gripper is too high or lowgrasp_vertical_offset or camera Z compensation
Wrist angle is wrongGripper roll, pitch, yaw compensation
All grasps shift in the same directionCamera or base compensation

Demo Video​

Troubleshooting​

torch.cuda.is_available() returns False: reinstall a JetPack-matched PyTorch wheel. Generic PyPI torch is not suitable for Jetson deployment.

No module named pointnet2._ext or No module named knn_pytorch.knn_pytorch: rebuild GraspNet CUDA operators:

bash scripts/install_graspnet_cuda_ops.sh --force

pyorbbecsdk import failed or the camera cannot open: reinstall the SDK and check USB permissions:

bash scripts/install_pyorbbecsdk.sh
sudo chmod a+rw /dev/bus/usb/*/*
python scripts/verify_pyorbbec_stream.py

YOLO .engine fails to load: re-export it on the same Jetson. Engine files should not be copied between Jetson models, JetPack versions, or TensorRT versions.

ArUco marker is not detected: confirm the marker dictionary is DICT_4X4_50, ID is 0, marker edge length is 0.1 m, lighting is stable, and the marker is flat and fully visible.

The robot connects but motion fails: run verify_rebot_arm_motion.py --read-only, confirm the USB2CAN device, check motor power, and test a small --deg 5 jog before retrying grasp execution.

GraspNet runs out of memory: reduce --num-point, reduce --cloud-crop-nsample, close desktop applications, and avoid running multiple heavy inference processes at the same time.

Resources​

Tech Support & Product Discussion​

Thank you for choosing our products! We provide several support channels for questions, discussion, and issue reporting.

Loading Comments...