Skip to main content

Build a reCamera and NVIDIA Jetson VLM Event Gateway

Introduction​

This guide deploys a complete two-stage vision demo:

  1. A reCamera Basic runs YOLOv8 continuously.
  2. Only after it detects a person, it sends that frame to an NVIDIA Jetson.
  3. Qwen3-VL on the Jetson decides whether the frame contains a person wearing clearly red clothing.
  4. The Jetson broadcasts either a red-person alert or a scene description over WebSocket.
  5. The reCamera also provides a 1920×1080 H.264 RTSP stream with person boxes.
reCamera Basic                     NVIDIA Jetson                         Client
YOLOv8 person detector :8080 llama-server + Qwen3-VL
| :8000 Vision Gateway
+-- HTTP Base64 JPEG -----------> analyze -> structured VLM result
+-- RTSP :8554/live0 +---------------- WebSocket /ws ----> app

This architecture keeps continuous object detection on the low-power reCamera and invokes the larger vision-language model only when a person is present. It reduces Jetson inference requests while still providing natural-language scene understanding to downstream applications.

note

The prebuilt application in this project targets reCamera Basic with the SG2002 RISC-V SoC. It does not run on the aarch64-based reCamera Pro.

Hardware Preparation​

ItemPurpose
reCamera 2002 SeriesRuns YOLOv8 person detection and the RTSP stream
NVIDIA Jetson Orin deviceRuns llama.cpp, Qwen3-VL, and Vision Gateway
Development computerCopies the application to reCamera and subscribes to RTSP/WebSocket output
LAN or USB/Ethernet networkConnects reCamera, Jetson, and the client

Software Requirements​

  • reCamera Basic (SG2002/RISC-V), not reCamera Pro.
  • NVIDIA Jetson Orin with JetPack, CUDA, and at least 8 GB unified memory recommended.
  • Both devices on the same trusted LAN, with mutually reachable IP addresses.
  • Git and Python 3.10+ on the Jetson.
  • A compatible Qwen3-VL GGUF language model and its matching mmproj file.

Download the demo repository on the Jetson or development computer:

git clone https://github.com/yyling0101-a11y/reCamera-VLM-Gateway.git

This guide uses /home/nvidia/recamera_vl and these placeholders:

JETSON_IP    Jetson LAN address, for example 192.168.4.33
RECAMERA_IP reCamera LAN address
caution

The llama.cpp multimodal subsystem changes quickly and its own documentation warns that breaking changes are expected. Pin a tested llama.cpp commit for a reproducible deployment. A multimodal model normally requires both the language GGUF and a matching projector. See the official multimodal documentation and server documentation.

Set Up NVIDIA Jetson​

Step 1: Check JetPack and CUDA​

On the Jetson:

uname -m
cat /etc/nv_tegra_release
nvcc --version

Expected architecture is aarch64. If nvcc is missing, install a JetPack release that includes the CUDA development toolkit before continuing. You can monitor the device with:

sudo tegrastats

Optional UI monitor:

sudo python3 -m pip install jetson-stats
jtop

Step 2: Install Build Dependencies​

sudo apt update
sudo apt install -y git cmake build-essential ninja-build pkg-config \
libssl-dev python3-venv curl
mkdir -p /home/nvidia/recamera_vl
cd /home/nvidia/recamera_vl

OpenSSL is useful when llama-server itself must fetch HTTPS images. This demo sends Base64 data URIs, so it does not rely on remote image fetching.

Step 3: Build llama.cpp with CUDA​

git clone https://github.com/ggml-org/llama.cpp.git
cd llama.cpp

# Recommended: replace this with a commit you have tested and record it.
git rev-parse HEAD

cmake -S . -B build \
-DGGML_CUDA=ON \
-DCMAKE_CUDA_ARCHITECTURES=87 \
-DLLAMA_OPENSSL=ON \
-DCMAKE_BUILD_TYPE=Release
cmake --build build --config Release -j2 --target llama-server llama-cli

Jetson Orin uses compute capability 8.7. If a different Jetson is used, select the appropriate CUDA architecture. Low-memory devices may need -j1.

Verify the output and CUDA backend:

file build/bin/llama-server
build/bin/llama-server --list-devices

The list should contain a CUDA device rather than CPU only.

Step 4: Prepare the Qwen3-VL Model​

Obtain the language GGUF and corresponding multimodal projector from the same trusted model release. Do not mix projectors between model variants or revisions. Review its license and checksum before deployment.

Example layout matching the filenames used below:

/home/nvidia/recamera_vl/models/Qwen3-VL-4B-Instruct-GGUF/
├── Qwen3VL-4B-Instruct-Q8_0.gguf
└── mmproj-Qwen3VL-4B-Instruct-Q8_0.gguf
caution

Q8 may be tight on an 8 GB Jetson once CUDA, KV cache, the projector, and the OS are included. A publisher-provided Q4 variant can reduce memory use. Never rename an unrelated file to match this example.

Step 5: Start llama-server​

Create /home/nvidia/recamera_vl/start_qwen3_vl.sh:

#!/usr/bin/env bash
set -euo pipefail

BASE=/home/nvidia/recamera_vl
MODEL="$BASE/models/Qwen3-VL-4B-Instruct-GGUF/Qwen3VL-4B-Instruct-Q8_0.gguf"
MMPROJ="$BASE/models/Qwen3-VL-4B-Instruct-GGUF/mmproj-Qwen3VL-4B-Instruct-Q8_0.gguf"

exec "$BASE/llama.cpp/build/bin/llama-server" \
--model "$MODEL" \
--mmproj "$MMPROJ" \
--alias qwen3-vl \
--host 0.0.0.0 \
--port 8080 \
--n-gpu-layers all \
--ctx-size 4096 \
--parallel 1 \
--flash-attn auto

Then run:

chmod +x /home/nvidia/recamera_vl/start_qwen3_vl.sh
/home/nvidia/recamera_vl/start_qwen3_vl.sh

Flags can change between llama.cpp revisions. If a flag is rejected, use build/bin/llama-server --help from the same build rather than copying flags from another release.

In another terminal:

curl http://127.0.0.1:8080/health
curl http://127.0.0.1:8080/v1/models

If memory is insufficient, try --ctx-size 2048, a smaller official quantization, or --no-mmproj-offload (slower). Quantized KV-cache flags may also be available; confirm their names with --help.

Step 6: Install and Start Vision Gateway​

Clone this repository to /home/nvidia/reCamera-VLM-Gateway, then:

cd /home/nvidia
git clone https://github.com/yyling0101-a11y/reCamera-VLM-Gateway.git
cd reCamera-VLM-Gateway
python3 -m venv .venv
source .venv/bin/activate
python -m pip install --upgrade pip
python -m pip install -r vision_gateway/requirements.txt
chmod +x vision_gateway/start.sh
./vision_gateway/start.sh

The bundled script expects llama-server at 127.0.0.1:8080, model alias qwen3-vl, and starts a single worker at 0.0.0.0:8000. Keep one worker because inference serialization and WebSocket connections are in process memory.

Verify:

curl http://127.0.0.1:8000/health
curl http://127.0.0.1:8000/api/v1/status

The health response should show status: ok, busy: false, and the llama-server URL.

Step 7: Test Image Analysis and WebSocket​

From the repository root:

base64 -w 0 vision_gateway/image.jpg > /tmp/vision-image.b64
curl http://127.0.0.1:8000/api/v1/analyze \
-H 'Content-Type: application/json' \
--data-binary "{\"image_base64\":\"$(</tmp/vision-image.b64)\"}"

A successful response contains red_person_detected, message, and processing_ms.

Subscribe from a browser or application before sending another image:

const ws = new WebSocket("ws://JETSON_IP:8000/ws");
ws.onmessage = e => console.log(JSON.parse(e.data));
setInterval(() => ws.readyState === WebSocket.OPEN && ws.send("ping"), 30000);

Events are either:

{"type":"red_person_detected","message":"发现了红色衣服的人","request_id":"...","timestamp":0}

or:

{"type":"scene_description","message":"...","request_id":"...","timestamp":0}

Set Up reCamera​

Step 1: Connect to reCamera​

Complete the reCamera Getting Started guide first. Connect reCamera and Jetson to the same LAN, then confirm their IP addresses. The default USB network address of reCamera is commonly 192.168.42.1, but use the address assigned by your actual network when communicating with Jetson.

note

Camera resources are exclusive. The default sscma-node service must be stopped before the standalone C++ application can access the camera.

Step 2: Deploy and Start the Application​

From your computer:

git clone https://github.com/yyling0101-a11y/reCamera-VLM-Gateway.git
cd reCamera-VLM-Gateway
scp -r recamera root@RECAMERA_IP:/home/recamera/person-vl
ssh root@RECAMERA_IP

On reCamera:

cd /home/recamera/person-vl
chmod +x run.sh bin/person_vl
killall sscma-node 2>/dev/null || true
JETSON_VL_URL=http://JETSON_IP:8000/api/v1/analyze ./run.sh

The bundled binary targets reCamera Basic (SG2002/RISC-V) and the video SDK requires root. A person detection queues one JPEG upload; the default cooldown is 10 seconds.

View the annotated stream using RTSP-over-TCP:

ffplay -rtsp_transport tcp rtsp://RECAMERA_IP:8554/live0

Verify the Complete Demo​

Walk into view wearing red primary clothing, then repeat the test without red clothing. Confirm all three outputs:

  • reCamera prints [vl] response ... http=200.
  • the WebSocket receives red_person_detected or scene_description.
  • RTSP shows the person box.
tip

The Gateway intentionally allows only one VLM inference at a time. If multiple cameras are used, increase VL_COOLDOWN_SECONDS or add an external request queue.

Resources​

Technical Support and Product Discussion​

Thank you for choosing our products! We provide different levels of support to ensure your experience with our products is as smooth as possible. We offer multiple communication channels to meet different preferences and needs.

Loading Comments...