Frequent Ask Questions
If you encounter a situation where the usb-connected device fails to recognize reCamera during the network configuration for reCamera, as well as the problem of network connection failure after configuring the network, please refer to this article.
It is necessary to modify and configure the computer network environment, including installing drivers on the Windows system, querying network cards on the Linux system, and configuring network priorities on the Mac system.
Set up the working environment
USB NET setup
To use USB networking, we enabled UsbNcm and DHCP by default on the system.
UsbNcm is driver-free on Linux, macOS, and the latest Windows systems. You can log in to recamera's terminal directly using ssh [email protected] ,passwd = recamera .
Windows
Make sure the Ncm driver is correctly installed on your computer, as shown in the image. You can check this by going to: Device Manager -> Network adapters.

If your machine does not have this driver, follow the steps below to install Ncm.
Install NCM for windows
step1:
Press win+x and select Device Manager.
Find the unrecognized device in other devices and select Update driver.

step2:
Select Browse my computer for drivers

step3::
Select Let me pick from a list of available drivers on my computer

step4::
Select Network adapters and then click next

step5:Selet Microsoft -> UsbNcm Host Device then click Next.

step6:When the alert bar pops up, select Yes

step7:Enter ping 192.168.42.1 in a terminal window.
The following output shows that you have successfully connected to the reCamera.

Linux
No extra setup, just plug in a USB cable. Enter ifconfig, and you will see the usb1 network adapter. For example: 192.168.42.89. The ip of the device is 192.168.42.1

MacOS
Check the usb network adapter in System Settings -> Network. The ip of the device is 192.168.42.1
Computer network error
windows
If your Windows 10 System computer has network access issues after using the USB network of reCamera.
Press win+x click Control Panel. Select All Control Panel Items -> Network Connections.

Right mouse click UsbNcm Host Device. Select Properties -> TCP/IPv4 -> Properties -> Advanced -> Uncheck Automatic metric -> Enter 255 in the Interface metric field -> click ok
Then your network is back up.

MAC
If your computer is running MacOS. You only need to set the priority of the computer network card UsbNcm network card last

The specific Settings are as follows:
step1: Select System Settings

step2: You will see this order, and we are about to change it.

step3: Drag all the way to the bottom, and click it.

step4: Select Set Service Order

step5: Drag NCM below Wi-Fi and then click ok

step6: Finally, you should see the Settings shown

Resources
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.