OS Update/Upgrade Guideline with Web
Connect the recamera to your computer using the type-c cable, and go to http://192.168.42.1/#/system in your computer's browser, or replace the IP address if you are visiting the device via network. Before upgrading, make sure reCamera has access to the internet by checking ip_address/#/network.
Click System Configuration, and if a new firmware is released, click Apply to update/upgrade the device system. The button text would be "Check" if there is no new firware auto detected.

Wait for the progress bar to complete.

Click Restart to complete the system update/upgrade. Refresh the browser around 30 seconds to reconnect to the device.

The system will automatically check if there is a new version of firmware that can be updated/upgrade.

OS Version management by command
Device management by OTA
Update/Upgrade to latest OTA version
You can check out the latest version of the reCamera OS here.
Manually update/upgrade the latest OTA firmware:
#Upgrade to the latest firmware version
sudo /mnt/system/upgrade.sh latest https://github.com/Seeed-Studio/reCamera-OS/releases/latest
sudo /mnt/system/upgrade.sh start
or
Update/Upgrade or rollback to any specific OTA version
If you have a speicific version you would like to deploy, you can use the command below.
#E.g. install 0.1.4 as an example
sudo /mnt/system/upgrade.sh latest https://github.com/Seeed-Studio/reCamera-OS/releases/tag/0.1.4
sudo /mnt/system/upgrade.sh start
If you are developing OS and you have your own branch in github, you can also update/upgrade the system version with your branch link.
sudo /mnt/system/upgrade.sh latest https://github.com/your-user-name/reCamera-OS/releases/your-version-file-address
sudo /mnt/system/upgrade.sh start
For OS version 0.1.3 and below
If you would like to OTA with upgrade.sh but your version is 0.1.3 and below, please follow the below steps:
- Connect device with computer by USB-type C cable, then visit 192.168.42.1/#/terminal. Find the upgrade.sh script in the folder
cd /mnt/system
ls

- Change the permission of this script
sudo rootfs_rw on
sudo chmod +x upgrade.sh

- Delete the old
upgrade.shfile and check if it is removed successfully.
sudo rm upgrade.sh
ls

- Go to Github and download the latest
upgrade.shscript.

- Change folder permission
sudo chmod 777 /mnt/system

- Open your desktop/pc terminal, then copy the downloaded script to reCamera under the same folder.
sudo scp your_folder_address/upgrade.sh [email protected]:/mnt/system/

- Go back to the web page to check if the new
upgrade.shis in

- Change back the folder permission for safety
sudo chmod 755 /mnt/system

- Now you can try OTA command to do any version control.
Device management by local package
You can also update/upgrade the firmware manually using the local ota package. The ota firmwares can be downloaded here. Use tools like scp to transfer the files to reCamera.
sudo scp sg2002_reCamera_0.1.3_emmc_ota.zip recamera@ip_address:~/
Then use the bash to deploy.
sudo /mnt/system/upgrade.sh start sg2002_reCamera_0.1.3_emmc_ota.zip
If you don't have enough permissions to dump files into recamera, you can can change system files to be readable or writable by typing rootfs_rw on/off.
Manually restore factory Settings
This command can restore reCamera to facotry settings. If you use this, all of your user data will be removed such as Node-RED flow and local storage.
sudo /mnt/system/upgrade.sh recovery
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.