Skip to main content

Troubleshoot API Calls

Login​

Login returns iStatus=-1, what should I do?​

The password is incorrect. Verify that the username and password are correct. The default username is admin.

Login returns iStatus=-3, what should I do?​

Repeated failed logins have triggered an IP-based lockout. Wait for sWaittime seconds for the lockout to expire, then try again.

Login succeeds but subsequent APIs return 401, what should I do?​

The Token is missing or expired. Ensure the request header includes Cookie: token=<JWT_TOKEN> and that the Token has not exceeded its 24-hour lifetime. If expired, log in again.

How long is the Token valid?​

The Token is valid for 24 hours by default (Max-Age=86400). After it expires, log in again to obtain a new one.

Network​

The device becomes inaccessible after changing network settings, what should I do?​

Changing the IP address, gateway, or Wi-Fi parameters may cause the device address to change. Access the device via the new address, or recover via a direct network connection.

What is the difference between /network/wlan and /network/wifi?​

/network/wlan is for wireless IPv4 configuration (address, gateway, mask, DNS). /network/wifi is for current Wi-Fi connection info, connecting, and disconnecting.

What should I put in sSsid when connecting to Wi-Fi?​

sSsid is the unique identifier of the Wi-Fi network. Call /network/wifi-list first, then use the sBssid value from the list to connect.

HTTPS​

The browser warns about an untrusted certificate when accessing HTTPS, what should I do?​

The device uses a self-signed certificate. For local testing, you can proceed past the warning. For production deployment, install a trusted certificate.

Cannot access the device via HTTP after enabling HTTPS, what should I do?​

After enabling HTTPS, use https://<DEVICE_IP> for all subsequent access.

API Paths​

Why do some paths start with /api/v1/ and others with /cgi-bin/?​

Most endpoints require the CGI base path /cgi-bin/entry.cgi. Serial port and file endpoints are direct paths that bypass the CGI layer and are accessed at /api/v1/....

Why does an endpoint return 404?​

The current firmware version may not implement that endpoint, or the path may be constructed incorrectly. Verify whether the path needs /cgi-bin/entry.cgi and check the firmware version.

For the full list of response status codes, see API Error Codes. For general API usage, start with the API Introduction.

Technical Support and Product Discussion​

Thank you for choosing our products! We are here to provide you with various support to ensure your experience with our products is as smooth as possible. We offer multiple communication channels to meet different preferences and needs.

Loading Comments...