Skip to main content

Using the MIPI DSI Interface on reCamera Pro

There is a MIPI DSI interface on the rear side of the device for connecting MIPI screens.

Connect the MIPI Screen​

Open the rear cover of the base board, locate the 22PIN MIPI DSI interface as shown below.

note

Please power off the device before plugging in the MIPI screen!!!

BASE_BOARD_PIN

Locate the TCON end of the MIPI screen cable and insert it inward as shown in the figure below: CONNECT_MIPI_SCREEN

Power On​

After connecting the MIPI screen, power on the device, and the real-time camera image will be displayed on the MIPI screen. SHOW_GIF

note

The screen requires separate power supply; the device does not provide dedicated power output for the screen.

The screen link is as follows:

Raspberry Pi Touch Display 2
Raspberry Pi Touch Display 2

Technical Support and Product Discussion​

Thank you for choosing our products! We are here to provide you with various support to ensure your experience with our products is as smooth as possible. We offer multiple communication channels to meet different preferences and needs.

Loading Comments...