🗃️ API
7 items
📄️ Convert and Quantize Models
Convert ONNX models to the RKNN format for reCamera Pro and create an INT8-quantized model with a representative calibration dataset.
📄️ Flash the Debian 13 Image to reCamera Pro
Flash the Debian 13 image to reCamera Pro
📄️ Develop reCamera Pro Applications with AI Coding Agents
Install and use the reCamera Pro Development Skill to convert ONNX models, build native RKNN applications, and develop camera, audio, GStreamer, and RTSP workflows through natural-language conversations.