📄️ OS Version control
Version control such as upgrade or rollback
📄️ reCamera OS Structure
in depth look at the operating system (OS) structure of the reCamera
📄️ Develop with Node-RED
Providing documentation and info for Node-RED deployments
📄️ Linux Fundamentals
Basic linux command for reCamera
📄️ Develop with C/C++
Providing documentation and info for C/C++ developers
📄️ Make the C++ program auto-start on boot.
This wiki demonstrates how to set a program to launch automatically at startup.
📄️ Real-time YOLO object detection using reCamera based on Cpp
This wiki demonstrates how to use YOLO to detect objects in real time on reCamera with C++.
📄️ reCamera connects to XIAO via HTTP
This wiki demonstrates how to connect to XIAO via HTTP on reCamera to run C++ project.