reComputer Industrial RK FAQ
This page contains verified answers for the reComputer Industrial RK. Each answer states the product variant and firmware mode it applies to, together with the date it was last verified against current official sources.
Before you begin
- Confirm the exact product variant and the SoC it is based on (RK3588 or RK3576).
- Check the current firmware version before applying version-specific steps.
- Answers on this page were last verified on 2026-11-01; re-check the linked official sources if you are reading this later.
OS & Firmware
How do I debug a newly delivered board?
Applies to: reComputer RK3576 boards
Last verified: 2026-11-01
The firmware and the image are already on the device when it ships. Once the device arrives, power it up as described and complete the initial configuration; it is then ready to use and to start developing, which takes roughly 10 to 20 minutes from the moment you receive the device.
References:
Hardware & Interfaces
Does the reComputer RK3576 Industrial support a UPS and a TPM module?
Applies to: reComputer RK3576 Industrial; the exact scope is confirmed together with the answer.
Last verified: 2026-11-01
The device supports a UPS module, and that module is about to go on sale. For the TPM module, the RK3576 has a built-in hardware security mechanism, so no TPM module has to be added.
- Secure boot: the chip carries a BootROM code in ROM; at boot it verifies the digital signatures of the subsequent loaders step by step. The hash of the public key can be programmed into the one-time OTP memory or the eFuse of the chip for verification. Rockchip also provides tools such as rksecure to manage the secure boot state.
- ARM TrustZone: the RK3576 supports ARM TrustZone, which splits the CPU and memory resources into a Secure World and a Normal World
- The RK3576 integrates a dedicated hardware crypto module (Crypto IP) that supports the standard algorithms AES, DES/3DES, RSA, ECC and SHA
References:
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.