Skip to main content

Getting Started with reComputer Super

The reComputer Super Series supercharges the reComputer Classic, delivering up to a 1.7x boost of 157 TOPS in AI performance. It features models with Jetson Orin Nano (11410311, 11410312) and Jetson Orin NX (11410313, 11410314). Designed for both development and production, it comes with a rich array of interfaces, including M.2 Key E/M, dual RJ45 Ethernet, Mini-PCIe, 4xUSB 3.2, HDMI 2.1, 4xCSI, and CAN. With pre-installed Jetpack 6.2 and Linux OS BSP, it enables immediate market entry. It also supports a wide range of LLM & Physical AI frameworks, such as NVIDIA, Hugging Face, ONNX, PyTorch, and ROS2/1 at the edge seamlessly, even merging these multimodal capacity with robotics application to enrich Physical AI development.

Key Features

🚀 ​Performance Boost

  • 1.7x AI performance boost over reComputer Classic, delivering ​157 TOPS
  • Powered by ​Jetson Orin Nano (Models: 11410311, 11410312) and ​Jetson Orin NX (Models: 11410313, 11410314)

🔌 ​Rich Connectivity & Interfaces

  • M.2 Key E/M + ​Mini-PCIe for expandability
  • Dual RJ45 Ethernet ports for high-speed networking
  • 4x USB 3.2, ​HDMI 2.1, ​4x CSI (Camera Serial Interface)
  • CAN bus support for industrial/robotics applications

🛠️ ​Ready for Development & Production

  • Pre-installed ​Jetpack 6.2 and ​Linux OS BSP for out-of-the-box deployment
  • Seamless edge AI integration with frameworks:
    • NVIDIA, ​Hugging Face, ​ONNX, ​PyTorch
    • ROS2/1 for robotics applications
  • Supports ​multimodal AI and ​Physical AI development

🤖 ​Edge AI & Robotics Optimized

  • Merges ​LLM (Large Language Model) capabilities with ​Physical AI at the edge
  • Ideal for robotics, industrial automation, and real-time AI inference
  • Accelerates ​market entry with pre-configured software stack
tip

⚠️ Power & Accessory Guidelines

1. ​Power Adapter

  • Jetson Orin Nano: 12V 5A (5525 barrel jack)
  • Jetson Orin NX: 19V 4.74A (5525 barrel jack)
  • Always use ​official adapters and meet power requirements.

2. ​AC Power Cord

  • Use ​region-specific cloverleaf cords.

3. ​Accessories

  • Only ​officially recommended accessories (e.g., cameras, wireless modules) for optimal performance and compatibility.

Specifications

Jetson Orin Super System on Module
SpecificationsreComputer Super J3010reComputer Super J3011reComputer Super J4011reComputer Super J4012
ModuleNVIDIA Jetson Orin™ Nano 4GBNVIDIA Jetson Orin™ Nano 8GBNVIDIA Jetson Orin™ NX 8GBNVIDIA Jetson Orin™ NX 16GB
AI Performance34 TOPS67 TOPS117 TOPS157 TOPS
GPU512-core NVIDIA Ampere architecture GPU with 16 Tensor Cores1024-core NVIDIA Ampere architecture GPU with 32 Tensor Cores
CPU6-core Arm® Cortex®-A78AE v8.2 64-bit CPU
1.5MB L2 + 4MB L3
6-core Arm® Cortex®-A78AE v8.2 64-bit CPU 1.5MB L2 + 4MB L38-core Arm® Cortex®-A78AE v8.2 64-bit CPU 2MB L2 + 4MB L3
CPU Max Frequency1.7 GHz (MAXN_SUPER)2 GHz
Memory4GB 64-bit LPDDR5
34 GB/s
8GB 128-bit LPDDR5
68 GB/s
8GB 128-bit LPDDR5 102.4GB/s16GB 128-bit LPDDR5 102.4GB/s
DL Accelerator/1x NVDLA v22x NVDLA v2
Video Encoder1080p30 supported by 1-2 CPU cores1x 4K60 (H.265) | 3x 4K30 (H.265)
6x 1080p60 (H.265) | 12x 1080p30 (H.265)
Video Decoder1x 4K60 (H.265)
2x 4K30 (H.265)
5x 1080p60 (H.265)
11x 1080p30 (H.265)
1x 8K30 (H.265)
2x 4K60 (H.265)
4x 4K30 (H.265)
9x 1080p60 (H.265)
18x 1080p30 (H.265)
CSIUp to 4 cameras
(8 via virtual channels)
8 lanes MIPI CSI-2
D-PHY 2.1 (up to 20Gbps)
Mechanical69.6mm x 45mm
260-pin SO-DIMM connector
Carrier Board
Storage1x M.2 KEY M PCIe (M.2 NVMe 2280 SSD 128G included)
NetworkingM.2 KEY E1x M.2 Key E for WiFi/Bluetooth module
Mini PCIe1x mini-PCIe for LTE 4G module
Ethernet2x RJ45 Gigabit Ethernet
I/OUSB4x USB 3.2 Type-A (5Gbps);
1x USB 2.0 Type-C (Device Mode/Debug);
Camera4x mipi CSI(2-lane 15-Pin)
CAN1 x CAN(4-Pin Header)
Display1x HDMI 2.1
Fan1x 4 pin Fan Connector (5V PWM);
1x 4-Pin Fan Connector (12V PWM);
Extension Port1x 40-Pin extension header;
1x 12-Pin control and UART header;
RTC1x RTC 2-pin;
1x RTC Socket
LED2x LED(PWR and ACT)
Pinhole Button1x PWR;
1x RESET;
DIP Switch1x REC
Antenna Hole4x Antenna Hole
Power12-19V 5525 Barrel DC Jack
Jetpack VersionJetpack 6.2
Mechanical Dimensions130mm x 120mm x 66mm
InstallationDesk, Wall-mounting
Operating Temperature-10℃~60℃
Warranty2 Year
CertificationCE,FCC,RoHS,REACH,Telec, KC, Vibration Test(GB/T 2423)

Flash JetPack OS

Supported Module

Prerequisites

  • Ubuntu host PC
  • reComputer Super
  • USB Type-C data transmission cable
info

We recommend that you use physical ubuntu host devices instead of virtual machines. Please refer to the table below to prepare the host machine.

JetPack Version Ubuntu Version (Host Computer)
18.04 20.04 22.04
JetPack 6.x

Prepare the Jetpack Image

Here, we need to download the system image to our Ubuntu PC corresponding to the Jetson module we are using:

Jetpack VersionJetson Module GMSL Download Link1SHA256
6.2 Orin Nano 4GBDownload8FF204A65C006717ED45241186C14B4
FAA8ACE5BEBCDCE755F94C3CBF1311C38
Orin Nano 8GBDownload7EC06C0D17E33AE43D3C69EED791F64
CB9CFDC497E01D525E18EBAC1547A0236
Orin NX 8GBDownload06B175484220DA7A63CC7CDAAE339F7E
FF8997180AF1C4B836D1098CBD8A169D
Orin NX 16GBDownload CF37D028D6466DCC13201367E6358A6
9B7B5305CAE2A2B785E3ECFD3D8C66304
danger

The Jetpack6 image file is approximately 14.1GB in size and should take around 60 minutes to download. Please kindly wait for the download to complete.

info

To verify the integrity of the downloaded firmware, you can compare the SHA256 hash value.

On an Ubuntu host machine, open the terminal and run the command sha256sum <File> to obtain the SHA256 hash value of the downloaded file. If the resulting hash matches the SHA256 hash provided in the wiki, it confirms that the firmware you downloaded is complete and intact.

Enter Force Recovery Mode

info

Before we can move on to the installation steps, we need to make sure that the board is in force recovery mode.

Step-by-Step

Step 1. Switch the switch to the RESET mode.

Step 2. Power up the reComputer Super by connecting the power cable.

Step 3. Connect the Super to the Ubuntu host PC with a USB Type-C data transmission cable.

Step 4. On the Linux host PC, open a Terminal window and enter the command lsusb. If the returned content has one of the following outputs according to the Jetson SoM you use, then the board is in force recovery mode.

  • For Orin NX 16GB: 0955:7323 NVidia Corp
  • For Orin NX 8GB: 0955:7423 NVidia Corp
  • For Orin Nano 8GB: 0955:7523 NVidia Corp
  • For Orin Nano 4GB: 0955:7623 NVidia Corp

The below image is for Orin Nano 8GB

Flash to Jetson

Step 1: Extract the downloaded image file:

cd <path-to-image>
sudo tar xpf mfi_xxxx.tar.gz
# For example: sudo tar xpf mfi_recomputer-super-orin-nx-16g-j401-6.2-36.4.3-2025-05-22.tar.gz

Step 2: Execute the following command to flash jetpack system to the NVMe SSD:

cd mfi_xxxx
sudo ./tools/kernel_flash/l4t_initrd_flash.sh --flash-only --massflash 1 --network usb0 --showlogs

You will see the following output if the flashing process is successful

note

The flash command may run for 2-10 minutes.

Step 3: Connect the monitor using an HDMI cable and complete the initialization configuration of the reComputer Super system:

info

Please complete the System Configuration according to your needs.

Resources

reComputer Robotics J401 Carrier Board Datasheet Schematic 3D File Mechanical Document-reComputer Super Mechanical Document-reComputer Super PCBA Seeed Nvidia Jetson Success Cases Seeed Jetson One Pager

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...