Configure reComputer R1100
Overview
Learn how to configure and test hardware components on the reComputer R1100 series after installing devices. This wiki covers GPIO mapping, USER LED testing, SPI communication, Wi-Fi and Bluetooth scanning, LoRa®, 4G, Zigbee over Mini-PCIe, RS485, RS232, DI/DO testing,UPS for safe shutdown and more.

Query GPIO Mappings and Offsets
To check GPIO mappings and offsets, follow these steps:
- Run the following command in the terminal
cat /sys/kernel/debug/gpio
This command will display GPIO mappings and offsets, providing essential information for debugging or configuring GPIO pins.
Control LED Indicators
The reComputer R1100 provides three LED indicators in red, blue, and green. You can control them using the following commands:
1. Navigate to the LED directory
cd /sys/class/leds/
ls
This will list the available LEDs.
2. Enable LEDs by writing to the brightness file
Switch to superuser mode first:
sudo su
Then, turn on the LEDs:
echo 1 > /sys/class/leds/led-red/brightness
echo 1 > /sys/class/leds/led-blue/brightness
echo 1 > /sys/class/leds/led-green/brightness
This will light up the corresponding LED.
3. Turn off LEDs (optional)
To turn off a specific LED, use:
echo 0 > /sys/class/leds/led-red/brightness
echo 0 > /sys/class/leds/led-blue/brightness
echo 0 > /sys/class/leds/led-green/brightness
Testing SPI Communication
To verify SPI communication, you can perform a loopback test by shorting the TPM module's MISO and MOSI pins. This method ensures that data sent on MOSI (Master Out, Slave In) is received on MISO (Master In, Slave Out).
Step-by-Step Guide
1. Connect to the Internet
Make sure your device is connected to a network before proceeding.
2. Clone the spidev-test repository
git clone https://github.com/rm-hull/spidev-test.git
3. Navigate into the directory
cd spidev-test
4. Compile the spidev_test.c program
gcc spidev_test.c -o spidev_test
5. Run the SPI test
./spidev_test -D /dev/spidev0.1 -v -p "hello"
-D /dev/spidev0.1→ Specifies the SPI device-v→ Enables verbose output-p "hello"→ Sends the string"hello"
6. Loopback Test (Optional)
- Short the TPM module's MISO and MOSI pins before running the test.
- If the SPI bus is functioning correctly, the output should show the transmitted data being received correctly.
Wi-Fi Scanning
To list available Wi-Fi networks and their details, run:
sudo iwlist wlan0 scan
- This command scans for all nearby Wi-Fi networks and displays their SSIDs, signal strength, and encryption type.
Bluetooth Scanning
To scan for Bluetooth devices, follow these steps:
Open the Bluetooth control interface:
sudo bluetoothctl
Enable scanning:
scan on
- This starts scanning for nearby Bluetooth devices.
LoRa® over Mini-PCIe
LoRa® SPI Configuration
Clone the SX1302_HAL repository:
cd ~
git clone https://github.com/Lora-net/sx1302_hal
Navigate to the cloned directory:
cd sx1302_hal
Modify the configuration file:
Open the I2C device configuration file:
sudo vim ./libloragw/inc/loragw_i2c.h
Change this line:
#define I2C_DEVICE "/dev/i2c-1"
To:
#define I2C_DEVICE "/dev/i2c-3"
Compile the code:
sudo make
Modify the reset script:
Open the reset_lgw.sh script:
sudo vim ./tools/reset_lgw.sh
Update the pin configurations:
SX1302_RESET_PIN=580 # SX1302 reset
SX1302_POWER_EN_PIN=578 # SX1302 power enable
SX1261_RESET_PIN=579 # SX1261 reset (LBT/Spectral Scan)
Copy the reset script to the packet forwarder directory:
cp ~/sx1302_hal/tools/reset_lgw.sh ~/sx1302_hal/packet_forwarder/
Update the default SPI port in the LoRaWAN® configuration file:
Modify the global_conf.json.sx1250.US915 file:
sed -i 's/spidev0.0/spidev0.1/g' global_conf.json.sx1250.US915
Start the LoRaWAN® module:
cd ~/sx1302_hal/packet_forwarder
sudo ./lora_pkt_fwd -c global_conf.json.sx1250.US915
LoRa® USB Configuration
If you are using a LoRa® USB module instead of LoRa® SPI, follow these steps. Most commands remain the same as for LoRa® SPI, except for the final step.
Pull up the SX1302 Reset Pin
echo 1 > /sys/class/gpio/gpio580/value
Start the LoRaWAN® USB module
cd ~/sx1302_hal/packet_forwarder
sudo ./lora_pkt_fwd -c global_conf.json.sx1250.EU868.USB
LoRa® USB is now configured and running on reComputer R1100
4G Cellular over Mini-PCIe
To interact with a 4G module using AT commands via minicom, follow these steps:
Open Minicom with the appropriate serial port and baud rate:
sudo minicom -D /dev/ttyUSB2 -b 115200
This command opens Minicom with the specified serial port (/dev/ttyUSB2) at a baud rate of 115200.
Send AT commands to the 4G module:
Once Minicom is open, you can start sending AT commands to the 4G module. For example:
AT
This command checks if the module is responsive. If the module is working properly, you should receive an "OK" response.
Dial a phone number using the 4G module:
To dial a phone number, use the ATD command followed by the phone number:
ATD<phone_number>;
- Replace
<phone_number>with the desired phone number you want to dial. - Make sure to include a semicolon (;) at the end of the command to indicate the end of the phone number.
Zigbee over Mini-PCIe
To test Zigbee communication between two Zigbee modules, follow these steps:
Check Available Serial Ports
Run the following command to check the available serial ports:
cat /dev/ttyUSB*
Install a Serial Communication Tool
Install CuteCom, a graphical serial terminal, using:
sudo apt-get install cutecom
Configure the First Zigbee Module (Coordinator)
- Open CuteCom and configure it for the first serial port.
- Settings:
- Baud Rate: 115200
- Enable "Hex output" at the bottom of the interface.
Steps to Configure as a Coordinator:
-
Set as Coordinator: Send command:
55 04 00 05 00 05- Expected response:
55 04 00 05 00 05 -
Reset Device:
-
Press the reset button, or
-
Send command:
55 07 00 04 00 FF FF 00 04
-
-
Network Formation:
- Send command:
55 03 00 02 02
Configure the Second Zigbee Module (Router)
- Open another instance of CuteCom and configure it for the second serial port using the same settings.
Steps to Configure as a Router:
-
Set as Router: Send command:
55 04 00 05 01 04- Expected response:
55 04 00 05 00 05 -
Reset Device:
-
Press the reset button, or
-
Send command:
55 07 00 04 00 FF FF 00 04
-
-
Network Formation: Send command:
55 03 00 02 02
Check Device Status
To verify the device status, send:
55 03 00 00 00
Expected response:
55 2A 00 00 00 01 XX XX XX XX
XXrepresents device-specific information.
Enter Transparent Mode
If network formation is successful, enable transparent mode by sending:
55 07 00 11 00 03 00 01 13
Both modules must be in transparent mode for direct communication.
To exit transparent mode, send:
+++
Additional Notes
-
If router configuration fails, the device may already be a coordinator. To leave the network, send:
55 07 00 04 02 XXXX XX -
To test transmission power, use:
-
Query power:
55 04 0D 00 00 0D -
Set power:
55 04 0D 01 XXXX
-
Ensure you replace /dev/ttyUSB* with the correct serial port for each Zigbee module.
Follow these steps carefully to establish successful Zigbee communication between the two modules.
Here’s the corrected and well-structured version with improved grammar, readability, and formatting:
RS485 Testing
The reComputer R1100 includes two RS485 ports. Below are their corresponding COM ports and device files:
| RS485 Port | COM Port | Silkscreen Label | Device File |
|---|---|---|---|
| RS485_1 | COM1 | A1 / B1 / GND | /dev/ttyACM0 |
| RS485_2 | COM2 | A2 / B2 / GND | /dev/ttyACM1 |
Steps to Test RS485 Functionality
Connect the RS485 Ports
Physically connect RS485_1 (A & B) to RS485_2 (A & B).
Run the RS485 Test Program
We provide a test program to verify data transmission and measure the speed between the two RS485 ports.
Run the following commands to download and execute the test program:
git clone https://github.com/ackPeng/R1100_TEST.git
cd R1100_TEST
gcc -o serial_test serial_test.c
./serial_test /dev/ttyACM0 /dev/ttyACM1 115200
Test Description
- This program sends 1MB of data from RS485_1 to RS485_2.
- It records the completion time and calculates the actual baud rate.
- Note: The actual baud rate may be slightly lower than the theoretical baud rate, which is expected.
Follow these steps carefully to verify RS485 communication on reComputer R1100.
RS232 Testing
The reComputer R1100 features two RS232 ports. Below are the corresponding COM ports and device files:
| RS232 Port | COM Port | Pin Mapping | Device File |
|---|---|---|---|
| RS232_1 | COM3 | RX3/TX3/GND | /dev/ttyACM2 |
| RS232_2 | COM4 | RX4/TX4/GND | /dev/ttyACM3 |
Testing RS232 Communication
Follow these steps to test RS232 functionality:
-
Connect the ports:
- Connect TX of RS232_1 to RX of RS232_2.
- Connect RX of RS232_1 to TX of RS232_2.
-
Run the test program:
-
Clone the test program repository:
git clone https://github.com/ackPeng/R1100_TEST.git -
Navigate to the directory:
cd R1100_TEST -
Compile the test program:
gcc -o serial_test serial_test.c -
Run the test:
./serial_test /dev/ttyACM2 /dev/ttyACM3 115200
-
This test sends 1MB of data from RS232_1 to RS232_2 and measures the completion time and baud rate. Note that the actual baud rate may be slightly lower than the theoretical value, which is normal.
DI (Digital Input) Testing
The reComputer R1100 includes two Digital Input (DI) ports, which can be configured based on user requirements.
| Number of DI Ports | DI Port | Corresponding Extended GPIO |
|---|---|---|
| 2 | DI1 | GPIO530 |
| DI2 | GPIO531 |
DI Port Specifications
- Input Type: PNP
- Supported Input Voltage: 5VDC – 24VDC
- Current: Up to 1000mA
Steps to Test DI Functionality
Ensure Proper Connection
Make sure the DI port of the reComputer R1100 is properly connected to the external load, also make sure that the G_D port is connected to the power supply GND.
Check the GPIO Status
Run the following commands to check the status of GPIO530 (corresponding to DI1):
echo 530 > /sys/class/gpio/export
echo in > /sys/class/gpio/gpio530/direction
cat /sys/class/gpio/gpio530/value
Interpret the GPIO Value
- If the external level is HIGH, the output of
/sys/class/gpio/gpio530/valuewill be 0. - If the external level is LOW, the output of
/sys/class/gpio/gpio530/valuewill be 1.
DO (Digital Output)
The reComputer R1100 includes two Digital Output (DO) ports, which can be configured based on user requirements.
| Number of DO Ports | DO Port | Corresponding Extended GPIO |
|---|---|---|
| 2 | DO1 | GPIO532 |
| DO2 | GPIO533 |
DO Port Specifications
- Output Type: Transistor
- Supported Output Voltage: Up to 60VDC
- Current Capacity: 500mA
Steps to Test DO Functionality
Ensure Proper Connection
Confirm that the DO port of the reComputer R1100 is properly connected to the external load.
Since the DO port is an open collector output and has no drive capability, please use an external resistor to pull it up to the power supply.
Set the Output Level
Run the following commands to set the output to HIGH or LOW:
echo 532 > /sys/class/gpio/export
echo out > /sys/class/gpio/gpio532/direction
echo 1 > /sys/class/gpio/gpio532/value # Set output to HIGH
echo 0 > /sys/class/gpio/gpio532/value # Set output to LOW
USB Hub Testing
To verify the functionality of the USB hub, follow these steps:
Check if the USB Hub is Detected
Run the following command to list all connected USB devices, including hubs:
lsusb
Verify USB Hub Detection
- This command will display information about all USB devices connected to your system, including USB hubs.
- If the USB hub is functioning properly, its details should appear in the command output.
- If the hub is not listed, there may be an issue with the hub itself or its connection to the system.
Troubleshooting (If the USB Hub is Not Detected)
- Check the physical connection of the USB hub.
- Try connecting the hub to a different USB port.
- Restart the device and rerun
lsusb. - If the issue persists, the hub may be faulty.
RTC (Real-Time Clock) Testing
To verify the RTC functionality on reComputer R1100, follow these steps:
Disable Automatic Time Synchronization
Before testing the RTC, stop and disable automatic time sync to avoid conflicts:
sudo systemctl stop systemd-timesyncd
sudo systemctl disable systemd-timesyncd
Manually Set the RTC Time
Set the RTC to a specific date and time (e.g., November 12, 2024, at 12:00 PM):
sudo hwclock --set --date "2024-11-12 12:00:00"
Sync RTC Time to the System
Update the system time to match the RTC time:
sudo hwclock --hctosys
Verify the RTC Time
Check the current time stored in the RTC:
sudo hwclock -r
This command will display the RTC time.
Test RTC Retention
-
Disconnect the power source from the RTC.
-
Wait a few minutes.
-
Reconnect the power and check the RTC time again using:
sudo hwclock -r -
If the time remains correct, the RTC is functioning properly.
Watchdog Timer Testing
To test the watchdog timer on reComputer R1100, follow these steps:
Install Watchdog Software
Ensure the watchdog package is installed:
sudo apt install watchdog
Configure the Watchdog
Edit the watchdog configuration file:
sudo apt-get install vim # Install Vim if not already installed
sudo vim /etc/watchdog.conf
Modify the configuration as follows:
watchdog-device = /dev/watchdog
# Set the hardware timeout (default is 1 minute)
watchdog-timeout = 120
# Set the interval between tests (should be shorter than watchdog-timeout)
interval = 15
# Set system load limits
max-load-1 = 24
# max-load-5 = 18
# max-load-15 = 12
# Enable real-time priority
realtime = yes
priority = 1
Start the Watchdog Service
Enable and start the watchdog service:
sudo systemctl start watchdog
Test the Watchdog by Simulating a System Hang
Trigger a kernel crash to see if the watchdog automatically reboots the system:
sudo su
echo 1 > /proc/sys/kernel/sysrq
echo "c" > /proc/sysrq-trigger
Monitor the System
Check if the system automatically reboots after the specified timeout period.
If the reboot occurs as expected, the watchdog is functioning properly.
Controlling the Buzzer via GPIO
The buzzer is mapped to GPIO 587. Use the following commands to turn it on and off:
Turn on the buzzer:
echo 587 > /sys/class/gpio/export
echo out > /sys/class/gpio/gpio587/direction
echo 1 > /sys/class/gpio/gpio587/value
Turn off the buzzer:
echo 587 > /sys/class/gpio/export
echo out > /sys/class/gpio/gpio587/direction
echo 0 > /sys/class/gpio/gpio587/value
CSI Camera Testing
To test the CSI camera on reComputer R1100, follow these steps:
Modify the Configuration File
Edit the config.txt file to enable the camera module:
sudo nano /boot/firmware/config.txt
Add the following line at the end of the file:
dtoverlay=imx219,cam0
Restart the System
Reboot to apply the changes:
sudo reboot
Check Camera Detection
After restarting, verify if the camera is detected:
libcamera-jpeg --list-cameras
Test the Camera
Run the following command to activate the camera:
rpicam-hello --timeout 0
If the camera preview starts successfully, the setup is complete!
TPM 2.0 Connection Check
If you have connected a TPM 2.0 module to your device, you can verify its detection using the following command:
ls /dev | grep tpm
Interpreting the Output:
- If you see
tpm0andtpmrm0in the output, it confirms that the TPM (Trusted Platform Module) is successfully detected and available. - This indicates that the TPM hardware is recognized and accessible, allowing you to proceed with TPM-related functionalities or applications.
If the devices are listed, your TPM module is properly connected and ready for use.
Interacting with ATECC608A and Generating a Random Serial Number
To communicate with the ATECC608A device and generate a random serial number, follow these steps:
Clone the atecc-util Repository:
git clone https://github.com/wirenboard/atecc-util.git
Navigate to the atecc-util Directory:
cd atecc-util
Clone the cryptoauthlib Repository:
git clone https://github.com/wirenboard/cryptoauthlib.git
Compile the ATECC Utility:
make
Generate a Random Serial Number:
./atecc -b 1 -s 192 -c 'serial'
-b 1→ Uses slot 1.-s 192→ Sets the serial number size to 192 bits.-c 'serial'→ Generates a random serial number.
Expected Output:
The generated serial number will be displayed, for example:
01235595d3d621f0ee
This method enables interaction with the ATECC608A device, allowing you to perform operations like generating random serial numbers efficiently.
Interacting with EEPROM
To read and write data to an EEPROM (Electrically Erasable Programmable Read-Only Memory), follow these steps:
Grant Full Permissions to the EEPROM Device File:
sudo chmod 777 /sys/bus/i2c/devices/6-0050/eeprom
Write Data to the EEPROM:
echo "This is a test string" > /sys/bus/i2c/devices/6-0050/eeprom
Read the EEPROM Contents in Hexadecimal Format:
cat /sys/bus/i2c/devices/6-0050/eeprom | hexdump -C
Checking SSD Detection
To list all connected disks, including the SSD, use the following command:
sudo fdisk -l
This command will display a list of all detected storage devices. Look for entries that represent your SSD, typically labeled as:
/dev/sda/dev/sdb/dev/sdc, etc.
Once you identify the correct SSD entry, you can proceed with partitioning, formatting, or other disk management tasks as needed.
UPS for Safe Shutdown
A GPIO6 connection between the CPU and DC power-in is used to notify the CPU when the power supply is down. The CPU must execute urgent tasks via a script before the supercapacitor’s energy is depleted and then initiate a safe shutdown ($shutdown).
Alternative Shutdown Method
Another way to use this function is to trigger a shutdown when the GPIO pin changes state. The specified GPIO pin is configured as an input key, generating KEY_POWER events. These events are handled by systemd-logind, which automatically initiates a system shutdown.
To enable this function, refer to /boot/overlays/README, then modify /boot/firmware/config.txt by adding:
dtoverlay=gpio-shutdown,gpio_pin=6,active_low=1
- For UPS functionality details, please contact us.
- The alarm signal is active LOW.
Python Code for Safe Shutdown
The following Python script demonstrates how to detect the working mode of the supercapacitor UPS via GPIO6. When the system detects a power-off event, it automatically saves data and shuts down safely.
import RPi.GPIO as GPIO
import time
import os
num = 0
GPIO.setmode(GPIO.BCM) # Set GPIO numbering mode
GPIO.setup(6, GPIO.IN, pull_up_down=GPIO.PUD_UP) # Set GPIO6 as input with pull-up resistor
GPIO.add_event_detect(6, GPIO.FALLING, bouncetime=500) # Add debounce time for stabilization
while True:
if GPIO.event_detected(6):
print("...External power off detected...")
os.system("sync") # Ensure data is written to disk
print("...Saving data...")
time.sleep(3)
os.system("sync") # Save data again
while num < 5:
print(f"--- {5 - num} seconds remaining ---")
num += 1
time.sleep(1)
os.system("sudo shutdown -h now") # Execute system shutdown
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.