Skip to main content

Getting Started with Raspberry Pi

caution

This wiki is wrote for ReSpeaker 2-Mics Pi HAT v2, to distinguish the v1 and v2 device, please refer to How to Distinguish ReSpeaker 2-Mics Pi HAT Hardware Revisions.

On the latest Raspberry Pi OS, the traditional method of driver installation (For v1 device) is no longer available and may lead to the following known issues:

  • The desktop environment may be corrupted after installation.
  • The ReSpeaker device may not able to be detected by aplay / arecord.

We have therefore re-released a new wiki on this issue, if you are using the more modern Raspberry Pi OS rather than previous releases, please follow these steps to get your ReSpeaker working.

Driver installation and configuration

1. Connect ReSpeaker 2-Mics Pi HAT to Raspberry Pi

Mount ReSpeaker 2-Mics Pi HAT on your Raspberry Pi, make sure that the pins are properly aligned when stacking the ReSpeaker 2-Mics Pi HAT.

Raspberry Pi Connection

connection picture1

Raspberry Pi Zero Connection

connection picture2

2. Setup the driver on Raspberry Pi

Make sure that you are running the latest Raspberry Pi OS on your Pi. (updated at 2024.11.19)

Prepare for Raspberry Pi Zero W
## Install kernel 
sudo apt install flex bison libssl-dev bc build-essential libncurses5-dev libncursesw5-dev linux-headers-6.6.51+rpt-rpi-v6
git clone --depth=1 --branch rpi-6.6.y https://github.com/raspberrypi/linux.git

## Make target directory
mkdir ~/tlv320aic3x_i2c_driver
cd ~/tlv320aic3x_i2c_driver
## Copy code
cp ~/linux/sound/soc/codecs/tlv320aic3x.c ~/tlv320aic3x_i2c_driver/
cp ~/linux/sound/soc/codecs/tlv320aic3x.h ~/tlv320aic3x_i2c_driver/
cp ~/linux/sound/soc/codecs/tlv320aic3x-i2c.c ~/tlv320aic3x_i2c_driver/
## Modify Makefile
nano Makefile
-------------------
obj-m += snd-soc-tlv320aic3x-i2c.o
snd-soc-tlv320aic3x-i2c-objs := tlv320aic3x.o tlv320aic3x-i2c.o

KDIR := /lib/modules/$(shell uname -r)/build
PWD := $(shell pwd)

all:
$(MAKE) -C $(KDIR) M=$(PWD) modules

clean:
$(MAKE) -C $(KDIR) M=$(PWD) clean

install:
sudo cp snd-soc-tlv320aic3x-i2c.ko /lib/modules/$(shell uname -r)/kernel/sound/soc/codecs/
sudo depmod -a

-------------------

## Compile the driver
make
sudo make install
sudo modprobe snd-soc-tlv320aic3x-i2c

## Check logs
lsmod | grep tlv320
dmesg | grep tlv320

  • Step 1: Get Device Tree Source (DTS) for the ReSpeaker 2-Mics Pi HAT (V2.0), compile it and install the device tree overlay.
git clone https://github.com/Seeed-Studio/seeed-linux-dtoverlays.git  
cd seeed-linux-dtoverlays/
make overlays/rpi/respeaker-2mic-v2_0-overlay.dtbo
sudo cp overlays/rpi/respeaker-2mic-v2_0-overlay.dtbo /boot/firmware/overlays/respeaker-2mic-v2_0.dtbo
echo "dtoverlay=respeaker-2mic-v2_0" | sudo tee -a /boot/firmware/config.txt

Note: If your kernel version is greater than 4.0, you don't need to add dtoverlay=i2s-mmap.

config example

  • Step 2: Reboot your Pi.
sudo reboot
  • Step 3: Check if the device is detected by aplay / arecord.

The expected output for aplay should be:

$ aplay -l
**** List of PLAYBACK Hardware Devices ****
card 0: vc4hdmi0 [vc4-hdmi-0], device 0: MAI PCM i2s-hifi-0 [MAI PCM i2s-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 1: vc4hdmi1 [vc4-hdmi-1], device 0: MAI PCM i2s-hifi-0 [MAI PCM i2s-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0
card 2: seeed2micvoicec [seeed2micvoicec], device 0: 1f000a4000.i2s-tlv320aic3x-hifi tlv320aic3x-hifi-0 [1f000a4000.i2s-tlv320aic3x-hifi tlv320aic3x-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0

The expected output for arecord should be:

$ arecord -l
**** List of CAPTURE Hardware Devices ****
card 2: seeed2micvoicec [seeed2micvoicec], device 0: 1f000a4000.i2s-tlv320aic3x-hifi tlv320aic3x-hifi-0 [1f000a4000.i2s-tlv320aic3x-hifi tlv320aic3x-hifi-0]
Subdevices: 1/1
Subdevice #0: subdevice #0

Where the card 2 is the index of the ReSpeaker 2-Mics Pi HAT, depending on your system this number may differ. To access the ReSpeaker in this example, you can use arecord -D plughw:2,0 or aplay -D plughw:2,0.

3. Configure sound settings and adjust the volume with alsamixer

alsamixer is a terminal user interface mixer program for the Advanced Linux Sound Architecture (ALSA) that is used to configure sound settings and adjust the volume.

alsamixer

The Left and right arrow keys are used to select the channel or device and the Up and Down Arrows control the volume for the currently selected device. Quit the program with ALT+Q, or by hitting the Esc key. More information

caution

Please use the F6 to select seeed-2mic-voicecard device first.

Usage overview

To get started, clone https://github.com/respeaker/mic_hat.git repository to your Raspberry Pi.

git clone https://github.com/respeaker/mic_hat.git
cd mic_hat

All the Python scripts, mentioned in the examples below can be found inside this repository. To install the necessary dependencies, from mic_hat repository folder, run

sudo apt-get install portaudio19-dev libatlas-base-dev
pip3 install -r requirements.txt

APA102 LEDs

To use the LEDs, you need enable SPI interface first. To enable SPI interface, open the Raspberry Pi software configuration tool:

sudo raspi-config

Choose "3 Interface Options" -> "I4 SPI" to enable SPI interface. Then reboot your Raspberry Pi.

sudo reboot

Each on-board APA102 LED has an additional driver chip. The driver chip takes care of receiving the desired color via its input lines, and then holding this color until a new command is received.

cd mic_hat
python3 interfaces/pixels.py

User Button

There is an on-board User Button, which is connected to GPIO_17.

caution

The demo code from repository is not available for Raspberry Pi 5 due to RPI.GPIO incompatibility. But we have provided an alternative demo code for Raspberry Pi 5 using gpiozero library.

Non-Raspberry Pi 5 device

Execute the example script from the repository which you cloned at Step 4, and it should display "on" when you press the button:

$ python3 button.py
off
off
on
on
off

Raspberry Pi 5 device

Copy the following code and save it to ~/button.py:

from gpiozero import DigitalInputDevice
from time import sleep

def main():
pin = DigitalInputDevice(pin=17, pull_up=True)
try:
while True:
print("on" if pin.value == 1 else "off")
sleep(1)
finally:
pin.close()

if __name__ == '__main__':
main()

It should also display "on" when you press the button:

$ python3 ~/button.py
off
on
on
off
on
off
note

It does not work in a virtual environment, you need to exit it first:

deactivate
python3 ~/button.py

Record sound with Python

We use PyAudio python library to record sound with Python.

First, run the following script to get the device index number of ReSpeaker:

cd mic_hit
python3 recording_examples/get_device_index.py

You will see the device ID as below.

Input Device id  1  -  seeed2micvoicec: 1f000a4000.i2s-tlv320aic3x-hifi tlv320aic3x-hifi-0 (hw:2,0)

To record the sound, open recording_examples/record.py file with nano, vim or other text editor and change RESPEAKER_INDEX = 2 to index number of ReSpeaker on your system. Then run python script record.py to make a recording:

python3 recording_examples/record.py

If you want to extract channel 0 data from 2 channels, have a look at the content of record_one_channel.py. For other channel X, please change [0::2] to [X::2].

python3 recording_examples/record_one_channel.py

To play the recorded samples you can either use aplay system utility, for example

aplay -f cd -D hw:2,0 output.wav # for Stereo sound
aplay -D plughw:2,0 output_one_channel.wav #for Mono sound from one channel

Alternatively you can use recording_examples/play.py script to play the .wav files with PyAudio.

python3 recording_examples/play.py path-to-wav-file

Make sure to specify the right output device index in play.py - otherwise PyAudio will freeze!

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...