DoA and VAD with reSpeaker XVF3800 44mm and XIAO ESP32-S3 Plus
The XVF3800 computes Direction of Arrival (DoA) and Voice Activity Detection (VAD) inside the chip. A host MCU can read both results over I2C using resource-based commands — no raw audio processing needed on the host. This sketch polls the DoA angle and the speech flag every 250 ms, streams I2S audio at the same time, and prints the RMS level of each channel so you can see when sound is present.

Prerequisites
- The array must be running the I2S firmware — I2C control is available in this mode.
- Arduino IDE with the ESP32 board package and the Arduino Audio Tools library. See Software Preparation.
- Board selected as XIAO_ESP32S3_Plus, Port number need to be selected.
How It Works
The XVF3800 exposes controls through servicers. A read is a two-step I2C transaction:
- Write
resid,cmd | 0x80, and the expected payload length plus one. - Read
statusfollowed by the payload bytes.
| Service | RESID | Command | Payload |
|---|---|---|---|
| Application servicer — firmware version | 48 | 0 | 3 bytes: major, minor, patch |
| GPO servicer — DoA | 20 | 18 | 4 bytes: angle (little-endian), speech flag (little-endian) |
The loop reads 256 stereo frames at a time from I2S, computes RMS for left and right, and polls DoA/VAD on a 250 ms interval. A DoA value above 359 is printed as N/A with the raw hex value, and any non-zero XMOS status byte is reported instead of being decoded.
Arduino Sketch
#include <Wire.h>
#include <math.h>
#include "AudioTools.h"
// =====================================================
// I2C CONFIGURATION
// =====================================================
#define XMOS_ADDR 0x2C
#define I2C_SDA_PIN 5
#define I2C_SCL_PIN 6
#define GPO_SERVICER_RESID 20
#define GPO_SERVICER_RESID_DOA 18
#define DOA_READ_NUM_BYTES 4
#define DOA_RESPONSE_BYTES 5 // Status + 4-byte payload
// =====================================================
// I2S CONFIGURATION
// =====================================================
#define I2S_BCK_PIN 8
#define I2S_WS_PIN 7
#define I2S_DATA_TX_PIN 44
#define I2S_DATA_RX_PIN 43
#define SAMPLE_RATE 48000
#define CHANNELS 2
#define BITS 32
// 256 stereo frames per block
#define BLOCK_FRAMES 256
#define FRAME_BYTES (CHANNELS * (BITS / 8))
#define BLOCK_BYTES (BLOCK_FRAMES * FRAME_BYTES)
// =====================================================
// DOA POLLING
// =====================================================
#define DOA_INTERVAL_MS 250
unsigned long lastDoaMs = 0;
// =====================================================
// AUDIO OBJECTS
// =====================================================
AudioInfo audioInfo(SAMPLE_RATE, CHANNELS, BITS);
I2SStream i2s;
I2SConfig cfg;
int32_t audioBuf[BLOCK_FRAMES * CHANNELS];
float rmsLeft = 0.0f;
float rmsRight = 0.0f;
// =====================================================
// GENERIC XMOS I2C READ
// =====================================================
// Returns true if the complete I2C response was received.
// The XMOS status byte is checked separately.
bool xmosReadBytes(
uint8_t resid,
uint8_t cmd,
uint8_t *payload,
uint8_t payloadLen,
uint8_t &status,
uint8_t &txError,
size_t &bytesReceived
) {
status = 0xFF;
txError = 0xFF;
bytesReceived = 0;
// Step 1: Send read command
Wire.beginTransmission(XMOS_ADDR);
Wire.write(resid);
Wire.write(cmd | 0x80);
Wire.write(payloadLen + 1);
txError = Wire.endTransmission();
if (txError != 0) {
return false;
}
// Step 2: Read status + payload
bytesReceived = Wire.requestFrom(
(uint8_t)XMOS_ADDR,
(uint8_t)(payloadLen + 1)
);
if (bytesReceived != (size_t)(payloadLen + 1)) {
while (Wire.available()) {
Wire.read();
}
return false;
}
// First byte is XMOS status
status = Wire.read();
// Remaining bytes are payload
for (uint8_t i = 0; i < payloadLen; i++) {
payload[i] = Wire.read();
}
return true;
}
// =====================================================
// READ FIRMWARE VERSION
// =====================================================
void readFirmwareVersion() {
uint8_t version[3] = {0};
uint8_t status;
uint8_t txError;
size_t received;
bool success = xmosReadBytes(
48, // Application Servicer
0, // VERSION command
version,
3,
status,
txError,
received
);
Serial.println("\nXMOS Firmware:");
if (!success) {
Serial.printf(
"I2C transport error: TX=%u, RX=%u/4\n",
txError,
(unsigned int)received
);
return;
}
if (status != 0) {
Serial.printf(
"Firmware version read failed. Status: 0x%02X\n",
status
);
return;
}
Serial.printf(
"Version: %u.%u.%u\n",
version[0],
version[1],
version[2]
);
}
// =====================================================
// READ DOA + SPEECH DETECTION
// =====================================================
bool readDOA(
uint16_t &doaAngle,
uint16_t &speech,
uint8_t &status,
uint8_t &txError,
size_t &bytesReceived,
uint8_t rawData[4]
) {
bool transportOK = xmosReadBytes(
GPO_SERVICER_RESID,
GPO_SERVICER_RESID_DOA,
rawData,
DOA_READ_NUM_BYTES,
status,
txError,
bytesReceived
);
if (!transportOK) {
return false;
}
// Do not decode payload if XMOS reports an error.
if (status != 0) {
return false;
}
// Little-endian payload
doaAngle =
(uint16_t)rawData[0] |
((uint16_t)rawData[1] << 8);
speech =
(uint16_t)rawData[2] |
((uint16_t)rawData[3] << 8);
return true;
}
// =====================================================
// AUDIO RMS CALCULATION
// =====================================================
// Channel 0 = Left
// Channel 1 = Right
float computeRMS(
const int32_t *samples,
size_t frames,
uint8_t channel
) {
if (frames == 0) {
return 0.0f;
}
double sum = 0.0;
for (size_t i = 0; i < frames; i++) {
double sample =
(double)samples[i * CHANNELS + channel]
/ 2147483648.0;
sum += sample * sample;
}
return (float)sqrt(sum / frames);
}
// =====================================================
// PRINT DOA ERROR INFORMATION
// =====================================================
void printDOAError(
uint8_t status,
uint8_t txError,
size_t bytesReceived,
const uint8_t rawData[4]
) {
if (txError != 0) {
Serial.printf(
"I2C write error: %u\n",
txError
);
return;
}
if (bytesReceived != DOA_RESPONSE_BYTES) {
Serial.printf(
"I2C response incomplete: %u / %u bytes\n",
(unsigned int)bytesReceived,
DOA_RESPONSE_BYTES
);
return;
}
Serial.printf(
"XMOS returned status: 0x%02X\n",
status
);
Serial.printf(
"Raw payload: %02X %02X %02X %02X\n",
rawData[0],
rawData[1],
rawData[2],
rawData[3]
);
}
// =====================================================
// SETUP
// =====================================================
void setup() {
Serial.begin(115200);
while (!Serial) {
delay(10);
}
AudioLogger::instance().begin(
Serial,
AudioLogger::Info
);
Serial.println("\n================================");
Serial.println("ReSpeaker 44mm I2S + DOA TEST");
Serial.println("================================");
// -----------------------------------------------
// Initialize I2C
// -----------------------------------------------
Wire.begin(
I2C_SDA_PIN,
I2C_SCL_PIN
);
Wire.setClock(100000);
delay(500);
Serial.println("I2C initialized");
// Read XMOS firmware version
readFirmwareVersion();
// -----------------------------------------------
// Initialize I2S
// -----------------------------------------------
Serial.println("\nStarting I2S...");
cfg = i2s.defaultConfig(RX_MODE);
cfg.copyFrom(audioInfo);
cfg.pin_bck = I2S_BCK_PIN;
cfg.pin_ws = I2S_WS_PIN;
// Retain both data pin assignments
cfg.pin_data = I2S_DATA_TX_PIN;
cfg.pin_data_rx = I2S_DATA_RX_PIN;
// XIAO = I2S slave
cfg.is_master = false;
if (!i2s.begin(cfg)) {
Serial.println("ERROR: I2S initialization failed!");
while (true) {
delay(1000);
}
}
Serial.println("I2S initialized successfully");
Serial.println("Sample rate : 48000 Hz");
Serial.println("Channels : Stereo");
Serial.println("Bit depth : 32-bit");
Serial.println("BCLK : GPIO8");
Serial.println("LRCLK : GPIO7");
Serial.println("TX : GPIO44");
Serial.println("RX : GPIO43");
Serial.println("\nDOA polling started");
Serial.println("Ready!");
lastDoaMs = millis();
}
// =====================================================
// MAIN LOOP
// =====================================================
void loop() {
// -----------------------------------------------
// STEP 1: Receive I2S audio
// -----------------------------------------------
size_t bytesRead = i2s.readBytes(
(uint8_t *)audioBuf,
BLOCK_BYTES
);
size_t framesRead =
bytesRead / FRAME_BYTES;
// -----------------------------------------------
// STEP 2: Calculate audio RMS
// -----------------------------------------------
if (framesRead > 0) {
rmsLeft = computeRMS(
audioBuf,
framesRead,
0
);
rmsRight = computeRMS(
audioBuf,
framesRead,
1
);
}
// -----------------------------------------------
// STEP 3: Poll DOA every 250 ms
// -----------------------------------------------
unsigned long now = millis();
if (now - lastDoaMs >= DOA_INTERVAL_MS) {
lastDoaMs = now;
uint16_t doaAngle = 0;
uint16_t speech = 0;
uint8_t status = 0xFF;
uint8_t txError = 0xFF;
size_t bytesReceived = 0;
uint8_t rawData[4] = {0};
bool success = readDOA(
doaAngle,
speech,
status,
txError,
bytesReceived,
rawData
);
// -------------------------------------------
// STEP 4: Print results
// -------------------------------------------
if (success) {
Serial.print("DOA: ");
if (doaAngle <= 359) {
Serial.printf(
"%3u deg",
doaAngle
);
} else {
Serial.printf(
"N/A (0x%04X)",
doaAngle
);
}
Serial.printf(
" | Speech: %s",
speech == 1 ? "DETECTED" :
speech == 0 ? "SILENT" : "UNKNOWN"
);
Serial.printf(
" | RMS L: %.5f | RMS R: %.5f\n",
rmsLeft,
rmsRight
);
} else {
Serial.print("DOA read failed: ");
printDOAError(
status,
txError,
bytesReceived,
rawData
);
}
}
if (bytesRead == 0) {
delay(1);
}
}
Expected Output
================================
ReSpeaker 44mm I2S + DOA TEST
================================
XMOS Firmware:
Version: 1.0.0
Starting I2S...
I2S initialized successfully
Sample rate : 48000 Hz
Channels : Stereo
Bit depth : 32-bit
BCLK : GPIO8
LRCLK : GPIO7
TX : GPIO44
RX : GPIO43
DOA polling started
Ready!
DOA: 135 deg | Speech: DETECTED | RMS L: 0.00321 | RMS R: 0.00298
DOA: 136 deg | Speech: DETECTED | RMS L: 0.00344 | RMS R: 0.00301
DOA: N/A (0xFFFF) | Speech: SILENT | RMS L: 0.00002 | RMS R: 0.00002
When nobody is speaking, Speech: SILENT and the reported angle is not meaningful — the XVF3800 reports an out-of-range value.
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.