Skip to main content

reSpeaker Clip Firmware Development Guide

The comprehensive reference for the reSpeaker Clip device-side firmware: how it is put together, the AT/GATT/UDP protocol it speaks, how it is built, updated, recovered, validated, and shipped. For the build-to-smoke-test path from a clean machine, see Getting Started with the reSpeaker Clip Firmware SDK; for full build/flash/power/pitfalls, see CLAUDE.md.

The checked-out firmware source is authoritative; this guide summarizes it. When they disagree, the source wins.

Introduction​

The Firmware SDK is an event-driven Zephyr RTOS application on the Nordic nRF5340 (application core + network core) with a PDM microphone array, BLE, Wi-Fi AP (nRF7002), USB, SD storage, and an OLED. It is for developers modifying device-side behavior. This guide covers the design and the operational reference (protocol, update, validation, production) in one place so that each fact has exactly one home — cross-references point back here rather than duplicating.

System Architecture​

Layered Architecture​

The firmware is organized in five layers, each depending only on the layer below:

LayerResponsibilityKey source
App / eventState machine, UI, button, the single place side effects happenclip_event.c, display.c, button.c, main.c
Service / transport-transfer-configMoving bytes (BLE/UDP/USB), file transfer engine, persistent configtransport.c, transport_ble.c, transport_udp.c, usb_cdc.c, transfer.c, config.c
Processing / audioPDM capture → DSP → Opus → framed file writesaudio.c, storage.c
HAL / driversBoard devices: OLED, PMIC, mic/regulators, SPI flash, SD, WiFi/BLE radioboards/seeed/clip/, drivers/, battery.c, haptic.c
Zephyr kernelThreads, message queues, semaphores, mutexes, power managementNCS v3.3.0

The invariant: the app layer is the only place that mutates state and triggers side effects. Button presses and AT commands do not start the mic or write the SD card directly — they post an event, and clip_event.c decides whether it is legal in the current state and executes it.

A request flows: button ISR / AT command → clip_post_event[_sync]() → [k_msgq] → clip_event_process() (main thread) → execute_transition() → side effects (audio_*, storage_*, display_*, haptic_*, ble_notify_*). Buttons post async (K_NO_WAIT, ISR-safe); AT commands post sync (block on a per-event semaphore so AT+START can return the session id synchronously).

Event and State Model​

The dispatcher in clip_event.c is a table-driven state machine:

  • clip_post_event(event) — async, non-blocking, ISR-safe; drops if the 8-slot queue is full.
  • clip_post_event_sync(event, &info) — blocking; returns OK/INVALID/ BUSY/ERROR through info.

States: UNINITIALIZED → IDLE → RECORDING → TRANSMITTING / WIFI_SYNC → IDLE, plus PAUSED, ERROR, OTA. transition_table[current_state][event] returns a next state, TRANS_SAME (stay, e.g. MARK), or TRANS_INVALID (reject). Two pre-gated rejections: START while WIFI_SYNC ("WiFi blocked"), START while USB MSC exposes the SD ("USB blocked" — mounting over USB while writing would corrupt FAT). State is committed only in execute_transition() via atomic_set(&g_state, new) — the one place state changes.

Notable side effects: START calls storage_ensure_mounted(), refuses if full, then audio_start_recording(AUDIO_MODE_MERGE). STOP waits ≤5 s for the audio thread to flush/close; if the SD is busy, stop commits IDLE anyway so the machine never deadlocks in RECORDING (the recording tail may be cut). POWER_OFF_EXEC cancels any active transfer (bounded wait), stops a recording, saves fuel-gauge state, puts the PMIC into ship mode.

Thread Model​

Five application threads (Zephyr priorities: lower number = higher priority, preemptible at 0+; Bluetooth RX runs higher still):

ThreadPriStackRole
Main(main)—Event loop clip_event_wait()→clip_event_process(), UI, time. Waits K_FOREVER idle or K_MSEC(1000) recording.
Audio audio_rec032768PDM read → DSP → Opus → storage. Highest-priority app thread (20 ms Opus deadline is hard).
Transfer516384File transfer engine: reads SD, sends via transport, retransmits.
UDP server54096Wi-Fi UDP socket server (port 8089).
AT server74096Parses AT on BLE/UDP/USB, posts sync events, sends JSON.

Synchronization pattern: volatile/atomic flags for "should I stop?" (transfer_cancel_requested, pause_requested), semaphores for "are you done?" (stop_done_sem, file_closed_sem, transfer_trigger_sem), mutexes for data structures (audio_state_mutex, sd_lifecycle_mutex, session_json_mutex, transport_lock), one message queue for the producer→consumer path that matters (clip_ev_msgq, events → main). A k_mem_slab of 32 × 1280 B buffers gives 640 ms of DMIC queue depth to absorb scheduling jitter (including BT RX preemption).

Audio and Recording Architecture​

Audio Pipeline​

Per 20 ms frame: dmic_read() (L+R stereo, 1280 B) → process_pcm_frame() (merge + DSP, mode-dependent) → opus_encode() (≤4000 B packet) → storage_write_frame() (2-byte length-prefixed, 4 KiB buffered writes).

Constants (audio.h): 16 kHz, 16-bit, 2-channel PDM; 20 ms frames → 320 samples/frame, 1280 B/block; 32 DMIC buffers (640 ms queue).

Recording Modes​

Older docs describe MODE_NORMAL as stereo. That is wrong. Both modes record mono.

  • Both modes record mono via an L+R merge. clip_event.c hardcodes audio_start_recording(AUDIO_MODE_MERGE). MODE_NORMAL is not stereo — the name is legacy.
  • MODE_NORMAL (default): delay-aligned L+R merge → hand-rolled 100 Hz high-pass → integer AGC (envelope + gain computer + smoother) → soft limiter. No SpeexDSP.
  • MODE_ENHANCED: the same merge + hand-rolled DSP, plus SpeexDSP noise suppression + dereverberation, gated on mode == ENHANCED && noise_suppress > 0 (audio.c:506). SpeexDSP AGC is not used (the build is FIXED_POINT; a float FFT AGC would cost ~15 ms/frame; the integer AGC replaces it).
  • The merge step cross-correlates L vs R over lags {−1, 0, +1} (2.85 cm mic spacing → ≤1 sample ITD at 16 kHz) and delay-aligns before summing, preventing comb filtering. The AGC is a classic compressor: ~30 ms attack / ~300 ms release, target ≈−14.7 dBFS, gain clamped ±12/24 dB, soft limiter (knee −2 dBFS, hard limit −0.5 dBFS).
  • Opus: OPUS_APPLICATION_AUDIO (preserves fricatives better than VOIP for STT), VBR unconstrained, voice signal hint, 16-bit depth, DTX/FEC/packet-loss off. Bitrate/complexity are per-mode Kconfig (CLIP_NORMAL_*/CLIP_ENHANCED_*), not runtime-settable. Encoder + SpeexDSP state are cached, reinitialized only when parameters change.
  • Set the mode with AT+MODE=normal|enhanced (persisted) or AT+START mode=enhanced (session-only, not persisted).

Session, Chunking, and Storage Model​

Each recording is one session with a 14-digit session_id: YYYYMMDDHHMMSS (UTC) when the clock is synced, else 0 + 13 uptime digits. The 14-digit form is enforced everywhere (validate_session_id) because the storage layout shards it into path components.

A session is a directory tree: session.json (metadata: id, duration, files, synced, size, channels, sample_rate, mode), marks.bin (binary bookmarks: "BMRK" magic + count + offsets), and chunk files 0/0001.opus, 0/0002.opus … 1/0101.opus (group = (file_index−1)/100, 100 files per subdir). Opus files are length-prefixed frame streams (2-byte LE length + packet, not OGG); a 4 KiB write buffer coalesces frames before fs_write.

Segment chunking: 300 s per segment when not syncing (CLIP_AUDIO_SEGMENT_DURATION_NO_SYNC), 60 s during an active transfer (CLIP_AUDIO_SEGMENT_DURATION_SYNC) — when recording while transferring (continuous mode), the transfer thread can only read a closed file, so 60 s caps the client's wait for the next file; if sync starts mid-file and the current file already exceeds 60 s, the engine slices immediately (audio.c:868). Each PAUSE/RESUME cycle also opens a new file. session.json's synced field tracks acknowledged files so a download resumes from the first unsynced file.

Storage: microSD (FAT32, /SD:) holds recordings under /SD:/REC/ in a bucket layout sharding the session id (/SD:/REC/<YYYYMMDD>/<HH>/<MM>/<SS>/…). External 8 MiB SPI flash (LittleFS, ~6.8 MiB) holds settings (/lfs/settings/run) and OTA slots — separate from the SD so corrupt settings or an interrupted OTA never take recordings down. The SD is lazily remounted via storage_ensure_mounted() and idle power-gated after CLIP_SD_IDLE_DELAY_MS (45 s) when genuinely idle (checked under lock to close the TOCTOU with a recording/transfer starting mid-check).

Power Management​

Battery device (170 mAh "240" cell, NPM1300 + nRF Fuel Gauge); idle current is the dominant constraint. Production build at the 3V3 rail:

SourceBehaviorCost
nRF5340 main + radio regulatorsDCDC (NRF5X_REG_MODE_DCDC)~500–600 µA vs LDO
SD cardIdle power-gated after 45 s~0 when idle
Debug UART consoleUARTE stays enabled between prints~570 µA leak
BLE slow advertising~1 s interval~0.1 mA averaged
nRF70 QSPICONFIG_NRF70_QSPI_LOW_POWER when WiFi unusedminimal

Production idle ≈ 170 µA. The largest leak after the regulators and SD were fixed is the debug UART console (~570 µA); the production snippet disables the console + UART log backend (CONFIG_CONSOLE=n, CONFIG_UART_CONSOLE=n, CONFIG_LOG_BACKEND_UART=n), which is what reaches ~170 µA. CONFIG_PM_DEVICE_RUNTIME=y auto-suspends UART/I2C/SPI drivers when idle. Recording/transfer briefly raise current (CPU boost to 128 MHz, reference-counted; mic + SD rail on; released on completion).

Communication Protocol​

BLE GATT Service​

CharacteristicUUID (suffix of 6E40xxxx-B5A3-F393-E0A9-E50E24DCCA9E)Role
Service0001The reSpeaker Clip service
Command Receive0002Host writes AT commands here
Response Send0003Device notifies JSON responses
File Data0004Device notifies binary file-transfer frames
Audio Visualization0005Device notifies recording energy levels

AT Command Grammar​

TypeFormatExampleNotes
EXECAT+XXAT+GSTATAction / default read
SETAT+XX=<value>AT+MODE=enhancedSet a parameter / act with args
READAT+XX?AT+MODE?Query current value

Parsing is shared: parse_command() (in at_server.c) owns the AT+NAME=args grammar and the =/? type detection; handlers receive ctx->args already split (past the =). AT+LIST?2&10 is a paginated read.

JSON Response Contract​

  • Success: {"ok":true,"data":{...}}
  • Failure: {"ok":false,"msg":"..."}
  • No numeric error codes, no error field, no request ID. Failures use msg. The same JSON goes out identically over BLE, UDP, and USB (routed by the command's originating transport via the SEND_RESPONSE() macro — your handler only fills the response buffer).

Registered Command Reference​

The registered commands live in applications/clip/src/at_commands.c (the .name = "..." table). Verified set:

GroupCommands
Device statusGSTAT, BATT, DEVICE, VERSION
RecordingSTART, STOP, PAUSE, RESUME, MARK
File managementLIST, MARKS, DOWNLOAD, CANCEL, DELETE
ConfigMODE, AUTODEL, BRIGHTNESS, TIME, NAME
ConnectivityWIFI, WIFICFG, USB, PAIR, DFU
MaintenanceLOG, STORAGE, FORMAT, REBOOT, POWEROFF, FACTORY

Removed legacy — do not document as available: BITRATE, COMPLEXITY, NOISE, AGC, DEREVERB, PURGE. Noise suppression / dereverb are boot-time Kconfig defaults (CLIP_DEFAULT_NOISE, CLIP_DEFAULT_DEREVERB), persisted in config.c, but have no runtime AT command; AGC is hand-rolled, always-on, not configurable. When you change an AT response, command, or transfer frame, update docs/protocol.md and sdk/ in the same change.

UDP Frame Types​

Wi-Fi UDP file transfer uses a binary frame protocol (port 8089) with per-frame CRC32:

TypeValueStructure
DATA0x01type(1) + seq(2) + len(2) + data
FILE_ACK0x03type(1) + status(1) + received_count(2) + crc32(4)
FILE_START0x10type(1) + fn_len(1) + filename + file_size(4)
FILE_END0x11type(1) + crc32(4)
TRANSFER_DONE0x12type(1) + sid_len(1) + session_id + file_count(4)
AT_RESP0x20AT response carried over UDP
HEARTBEAT0x30keepalive

BLE has no per-frame CRC (the link layer guarantees delivery) — only the full-file CRC32 in FILE_END for end-to-end check. UDP has per-frame CRC32 + FILE_ACK with a selective-repeat bitmap NACK: the client reports which frames it is missing as a bitmap and the engine resends only those, paced by CLIP_UDP_REPAIR_PACE_US (halves each retry round). A repair-pace that fails falls back to whole-file retransmit; TRANSFER_MAX_FILE_RETRIES (10) caps attempts before ERROR.

Session and File Addressing​

Host-visible session ids are exactly 14 decimal digits YYYYMMDDHHMMSS; physical FAT paths are never exposed in the protocol. AT+DOWNLOAD accepts session or session:NNNN.opus. Validate user-controlled arguments before storage, path, or transfer access.

Firmware Configuration and Build Profiles​

Stock and Development Builds​

The default (no-snippet) debug build keeps the UART console on and writes logs to /SD:/LOG (rotating 64 KiB files) at INF level (CONFIG_LOG_BACKEND_FS=y). Build:

source ~/ncs/v3.3.0/zephyr/zephyr-env.sh
export ZEPHYR_EXTRA_MODULES=$PWD # env var, not -D — Kconfig discovery runs before CMake
west build --build-dir build-clip --board clip/nrf5340/cpuapp applications/clip
# pristine (required after MCUboot/devicetree/sysbuild/partition changes):
west build --build-dir build-clip --pristine --board clip/nrf5340/cpuapp applications/clip

Every app builds as a sysbuild (MCUboot + app core + net-core radio) by default; the board supplies the glue. Key prj.conf / devicetree / Kconfig knobs: feature switches, log levels, BLE/Wi-Fi/FS config; GPIO/I2C/SPI/PDM/PMIC/ OLED mappings; buffer sizes, thread stacks, power policy.

Production Build​

Console + UART log off, idle ≈170 µA:

west build --build-dir build-clip-prod --board clip/nrf5340/cpuapp applications/clip \
-- -DSNIPPET_ROOT=$(pwd)/applications/clip -DSNIPPET=production

SNIPPET_ROOT must be absolute. The production snippet lives in applications/clip/snippets/production/. The project builds with zero warnings — fix every compiler warning before committing.

Firmware Update and Recovery​

Update Method Selection​

ScenarioRecommendedPackage
End-user upgrade (enclosed device)App BLE OTA or USB serial DFU*-signed.bin / *-ota.zip
Serial recovery (no app)mcumgr serial*-signed.bin
Dev debugwest flash / J-Linkmerged.hex
Production flashJ-Link / programmerfull merged.hex + merged_CPUNET.hex
App-core-only tweakmcumgr serial*-signed.bin (a single.zip is not yet shipped)

USB Serial DFU​

The app keeps USB off by default — send AT+USB=on over BLE first (samples with default CDC auto-enable USB, or hold the user button while plugging in). Open the CDC-ACM port at 1200 baud to trigger MCUboot serial recovery; a new port appears with PID 0x8069 (running app 0x0069; the 0x8000 bit marks bootloader; both Seeed VID 0x2886). Upload + reset:

nrfutil mcu-manager serial image-upload --firmware clip-<version>-signed.bin --serial-port /dev/ttyACMx
nrfutil mcu-manager serial reset --serial-port /dev/ttyACMx

MCUboot verifies the RSA signature and boots the new app; the bootloader partition is never touched.

BLE OTA​

nrfutil mcu-manager ble image-upload --firmware clip-<version>-ota.zip --address <BLE-MAC>

Or use nRF Connect Device Manager / SenseCraft Voice on a phone.

For dev/production/when USB+BLE recovery fails:

nrfutil device program --firmware clip-<version>-merged.hex --serial-number <JLINK-SN>
nrfutil device reset --serial-number <JLINK-SN>

Package Manifest​

Each release should carry a manifest so users don't guess package ranges from filenames:

firmware_version:
hardware_revision:
ncs_version: # v3.3.0
bootloader_version: # mcuboot
app_core_version:
net_core_version:
package_type: # debug | production
included_partitions: # [mcuboot, app, netcore]
upgrade_method: # serial-dfu | ble-ota | programmer
sha256:
rollback_supported:

Recovery Decision Tree​

flowchart TD
A["Upgrade failed"] --> B{"App boots?"}
B -->|"yes"| C["Check version, retry OTA"]
B -->|"no"| D{"Enters recovery?"}
D -->|"yes"| E["USB serial DFU"]
D -->|"no"| F["J-Link full recovery"]
E --> G["Reboot + verify"]
F --> G

Reset Command Matrix​

MethodCommandWhen
mcumgr serial resetnrfutil mcu-manager serial reset --serial-port …After serial DFU
BLE mcumgr resetnrfutil mcu-manager ble reset --address …After BLE OTA
J-Link resetnrfutil device reset --serial-number <JLINK-SN>Dev/production
west runner resetwest flash --build-dir … && nrfutil device resetDev — note west flash --reset does NOT work here

--recover erases both cores (clears the b0n access-port lock) — use only when net-core AP is locked, never routinely.

Safety Rules​

Never, unprepared: full-chip erase; UICR modify; overwrite the bootloader; partition-table change; flash a wrong-hardware-revision merged image; recover a production device without backing up its config.

Validation and Debugging​

Regression Matrix by Change Type​

ChangeMust test
Audio pipelineSNR, STOI, WER; buffer overflow; CPU; real-time (20 ms deadline)
OpusDecode; frame format; file size; transfer compat
AT / GATTOld commands; response format; error paths; Python SDK
FilesystemLong recording; power-loss; space-full; CRC
BLE / Wi-FiConnect; fragmentation; resume; timeout
PowerIdle; recording; Wi-Fi; wake
Firmware updateOTA; recovery; version readback; rollback

Audio Quality Metrics​

SNR (signal vs noise clarity), STOI (intelligibility), WER (ASR error rate — the business metric), THD (DSP/hardware distortion). Test scenarios: quiet near/far, office, café, car, street; both Normal and Enhanced; cover Chinese, English, digit sequences, silence.

PESQ/STOI need a clean reference + alignment. Do not compute them on arbitrary field recordings and claim a conclusion — without a matched reference, the number is not meaningful.

Serial, Logging, Storage, and Timing Debug​

minicom -D /dev/ttyACM0 -b 921600   # ttyACM1 if a J-Link also connected

Log levels: AT+LOG=off|info|debug (debug default: info). CONFIG_LOG_BACKEND_FS=y writes to /SD:/LOG (rotating 64 KiB) for post-mortem; AT+LOG=off lets the SD idle power-gate. The audio thread prints DWT cycle-counter stats (enc avg/min/max, dsp) every 500 frames (10 s). Known pitfalls (CLAUDE.md): %llu not supported on nRF5340 (use %u + cast); UDP sendto() returns success even on silent TX drops; FAT directory order is not chronological; corrupt /lfs/settings/run blocks settings_load (watchdog wipes + reboots after 3 s).

Host-side Test Tools​

python applications/clip/tests/tools/clip-cli.py status        # BLE default; --transport wifi
python applications/clip/tests/tools/clip-cli.py record --duration 5
python applications/clip/tests/tools/clip-cli.py list
python applications/clip/tests/tools/clip-cli.py sync --session <id>
python applications/clip/tests/tools/clip-cli.py terminal # interactive AT shell
python applications/clip/tests/tools/udp_sync.py --session <id>
python applications/clip/tests/tools/decode_opus.py <file>.opus out.wav

"Build passes" is not "hardware verified." A clean compile says nothing about on-device behavior.

Production Release​

Release Artifacts and Manifest​

Manual export today (tag-triggered scripts/build_release.sh + .github/workflows/release.yml are not yet implemented). Debug and production each produce four artifacts:

ArtifactUse
merged.hexApp-core full image (programmer / J-Link)
merged_CPUNET.hexNetwork-core full image
dfu_application.zip (release name *-ota.zip)mcumgr OTA package (BLE / USB serial)
clip/zephyr/zephyr.signed.bin (release name *-signed.bin)MCUboot-signed app image (USB serial DFU)

A single.zip (app-core-only) is not yet shipped — until build_release.sh lands, use *-signed.bin for app-only updates. Publish: add docs/release_notes/v$VERSION.md, commit, git tag vX.Y.Z && git push origin vX.Y.Z → CI builds the GitHub Release.

Signing Keys​

boards/seeed/clip/sysbuild/root-rsa-2048.pem is a copy of the MCUboot default key. Anyone with the public source can sign images for your devices. Generate your own key for production and keep the private half secret; rotate by replacing the key and re-flashing the bootloader.

CI​

.github/workflows/firmware.yml builds the clip app on push/PR to main (compilation check; applies the MCUboot patches + west build). mobile-ci.yml (analyze + unit tests, on PR) and mobile-verify.yml (debug APK / iOS smoke, push + manual) cover mobile/.

Factory Programming and Test Firmware​

Each test image is a standalone sysbuild under tests/<name>, built like west build --build-dir build-test --pristine --board clip/nrf5340/cpuapp tests/clip. Tests opt out of MCUboot (factory/cert firmware, flashed directly via J-Link) via SB_CONFIG_BOOTLOADER_NONE=y:

TestPurpose
tests/clipMulti-image hardware test suite (hosts the lfxo/hfxo crystal-tuning shell)
tests/dtmBLE Direct Test Mode (RF conformance; 2-wire UART @19200)
tests/wifi_radionRF70 Wi-Fi radio test (TX/RX, tone, IQ, FICR)
tests/otpnRF70 OTP programming (factory)
tests/reReference-board bring-up

Mass flash uses nrfutil device program --firmware …-merged.hex --serial-number <JLINK-SN>.

Compatibility Rules​

  • Keep the AT response shape: {"ok":true,"data":{...}} / {"ok":false,"msg":"..."}. No numeric error codes, no error field.
  • Don't break the file format (length-prefixed Opus, session.json schema).
  • Update docs/protocol.md and sdk/ whenever an AT response, command, or transfer frame changes.
  • Don't auto-execute a full-chip erase; don't auto-flash a production device.
  • The firmware source is the source of truth.

NCS v3.2.1 to v3.3.0 Migration​

main migrated to v3.3.0-only Kconfig (e.g. the WPA3 ..._WPA3_IMPLEMENTATION_NONE choice) and will no longer build against NCS v3.2.1. The ncs/v3.3.0 branch is an older diverged line (~12 commits behind main); local master is only the ancient initial import. Target NCS v3.3.0.

AI-Assisted Development​

The repo ships a firmware-dev skill at skills/clip-dev/ for AI agents (Claude Code, etc.) that work on this firmware. It encodes the project's real constraints so an agent does not re-derive them — and does not guess facts that are easy to get wrong. Use it; do not duplicate its rules into the docs.

For a complete, copyable example of AI-assisted AT command customization, see Customization: Add a Custom AT Command. That article shows how to prompt an AI agent to load the repository skill, add AT+ECHO, build the firmware, and validate the command on-device.

What the skill provides — SKILL.md plus nine references under skills/clip-dev/references/ (audio, build-flash, ble-at, storage, wifi-udp, mcuboot, power, display, hardware):

  • active NCS version, board sysbuild defaults, build/flash commands;
  • the current AT command set (registered in at_commands.c) and the response contract {"ok":true,"data":...} / {"ok":false,"msg":...};
  • the audio pipeline truth — both modes are mono L+R merge; runtime commands for bitrate, codec complexity, AGC, noise suppression, and dereverb do not exist;
  • power constraints (console leak, the production snippet, SD idle gating);
  • a firmware workflow: confirm the contract in source before editing docs or clients, validate user-controlled args, flash only the requested image, update docs/protocol.md + sdk/ whenever an AT response changes.

How to load it. In Claude Code the skill is auto-discovered; otherwise point the agent at the file:

@clip-dev
Analyze how to add distinct haptic patterns for recording start vs stop.
Give the modification plan first; do not edit code yet.

Standard task template — fill this in before asking an agent to change firmware:

## Goal
<device behavior to implement>

## Baseline
- Firmware commit/tag: v0.0.9
- NCS version: v3.3.0
- Board target: clip/nrf5340/cpuapp
- Build config: debug | production

## Constraints
- Keep which AT/GATT interfaces compatible
- New protocol fields allowed? (yes/no)
- File format changes allowed? (yes/no)
- Devicetree/Kconfig changes allowed? (yes/no)
- MCUboot / partition table / signing key edits forbidden

## Acceptance criteria
- Firmware builds (pristine, zero new warnings)
- Basic-SDK regression passes
- Expected serial log
- On-device behavior
- RAM/Flash delta
- Power or real-time constraint

Safety rules the skill enforces. Do not guess files, functions, Kconfig, or board targets — search the real source first. Do not infer a public interface from an internal module name. Do not modify MCUboot, the partition table, or signing keys without explicit confirmation. Do not auto-erase the whole chip or flash a production device. Do not break existing AT responses or file formats. "Build passes" is not "hardware verified" — claim only what was actually tested on a device. For audio/protocol changes, report CPU, buffer, flash, RAM, and output-format impact; for protocol changes, update the Python sdk/ and docs/protocol.md in the same change.

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...