Skip to main content

ROS2 Voice Pipeline on reSpeaker

Introduction​

pir

This project turns your voice into TurtleSim control using a reSpeaker microphone array and ROS2. Say “Hey Jarvis” followed by a command, and Jarvis records audio, transcribes it with Groq Whisper, interprets intent with Groq LLaMA, and responds with Groq Orpheus TTS. It supports forward/backward motion, angle turns, DoA-based facing, and instant stop commands. The system integrates wake-word detection, audio capture, ROS2 topics, and simulator command publishing in one seamless pipeline. It is designed for fast setup with Ubuntu and ROS2 Humble, making voice-driven robot experiments easy to run.

reSpeaker Flex XVF3800 CircularreSpeaker XVF3800

OR

Part 1 — Install ROS2 Humble​

Skip this part if ROS2 Humble is already installed on your machine. Check by running: ros2 --version

1.1 Set up the ROS2 apt repository

# Make sure your system is up to date
sudo apt update && sudo apt upgrade -y

# Install required tools
sudo apt install -y software-properties-common curl

# Add the ROS2 GPG key
sudo curl -sSL https://raw.githubusercontent.com/ros/rosdistro/master/ros.key \
-o /usr/share/keyrings/ros-archive-keyring.gpg

# Add the ROS2 repository to your sources
echo "deb [arch=$(dpkg --print-architecture) signed-by=/usr/share/keyrings/ros-archive-keyring.gpg] \
http://packages.ros.org/ros2/ubuntu $(. /etc/os-release && echo $UBUNTU_CODENAME) main" \
| sudo tee /etc/apt/sources.list.d/ros2.list > /dev/null

1.2 Install ROS2 Humble Desktop

sudo apt update
sudo apt install -y ros-humble-desktop

The desktop variant includes TurtleSim, RViz, and all tools you need. This download is around 1 GB — it may take a few minutes.

1.3 Install build tools

sudo apt install -y python3-colcon-common-extensions python3-rosdep

1.4 Source ROS2 automatically on every terminal

echo "source /opt/ros/humble/setup.bash" >> ~/.bashrc
source ~/.bashrc

1.5 Verify the installation

ros2 --version
# Expected output: ros2 cli version 0.18.x (or similar)

Then test TurtleSim to confirm everything works:

# Terminal 1
ros2 run turtlesim turtlesim_node

# Terminal 2
ros2 run turtlesim turtle_teleop_key

You should see a window with a turtle you can drive with arrow keys. Press Ctrl+C in both terminals when done.

Part 2 — Create a udev Rule for the Device​

Create a new udev rule to ensure proper permissions for the reSpeaker USB Mic Array:

sudo nano /etc/udev/rules.d/50-respeaker.rules

Add the following lines to the file:

# ReSpeaker USB Mic Array
SUBSYSTEM=="usb", ATTR{idVendor}=="2886", ATTR{idProduct}=="0018", MODE="0666", GROUP="plugdev"
SUBSYSTEM=="usb", ATTR{idVendor}=="2886", ATTR{idProduct}=="001a", MODE="0666", GROUP="plugdev"

Reload udev Rules and Restart the Service

Reload the udev rules and restart the service for changes to take effect:

sudo udevadm control --reload-rules
sudo udevadm trigger
sudo service udev restart

Unplug and replug your reSpeaker USB Mic Array to apply the new rules.


Part 3 — Get a Groq API Key​

This project uses Groq's free cloud API for:

  • Whisper — speech-to-text
  • LLaMA 3 — understanding your commands
  • Orpheus — Jarvis's voice reply
  1. Go to console.groq.com and create a free account
  2. Click API Keys in the left sidebar
  3. Click Create API Key, give it a name (e.g. "jarvis"), and copy it
  4. Save it somewhere safe — you will paste it into config.env shortly

The Groq free tier is generous enough for development and testing. No credit card is required to get started.


Part 4 — Install Python Dependencies (System-Wide)​

Important: Do NOT use a virtual environment for this project. ROS2 uses the system Python and cannot see packages installed inside a venv. We install everything with --break-system-packages to make them available to ROS2 nodes.

pip install \
groq \
openwakeword \
pyaudio \
numpy<2 \
python-dotenv \
pyusb \

Download the "Hey Jarvis" wake word model

python3 -c "import openwakeword; openwakeword.utils.download_models()"

This downloads pre-trained models to ~/.openwakeword/. It takes about 30 seconds.

Install PortAudio (required by PyAudio)

sudo apt install -y portaudio19-dev python3-pyaudio

Part 5 — Create Your ROS2 Workspace​

Skip to Part 6 if you already have a ~/ros2_ws workspace.

# Create the workspace directory
mkdir -p ~/ros2_ws/src
cd ~/ros2_ws

# Build the empty workspace to set it up
colcon build

# Source it and add to .bashrc so it loads automatically
echo "source ~/ros2_ws/install/setup.bash" >> ~/.bashrc
source ~/.bashrc

Part 6 — Clone and Configure the Project​

6.1 Clone the repository

If you are using Flex

cd ~/ros2_ws/src
git clone https://github.com/KasunThushara/ros_voice_controller_flex.git my_robot_controller

If you are using XVF3800

cd ~/ros2_ws/src
git clone https://github.com/KasunThushara/ros_voice_controller.git my_robot_controller

Your workspace should now look like this:

~/ros2_ws/
└── src/
└── my_robot_controller/
├── my_robot_controller/
│ ├── voice_node.py
│ ├── rotate_doa.py
│ ├── wakeword.py
│ └── ...
├── launch/
│ └── jarvis.launch.py
└── config.env.example

6.2 Create your config file

cd ~/ros2_ws/src/my_robot_controller
cp config.env.example config.env
nano config.env

Open the file and fill in your values:

# ── Groq API (required) ────────────────────────────────
GROQ_API_KEY=gsk_xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx ← paste your key here

# ── Microphone ─────────────────────────────────────────
MIC_INDEX=1 ← find the correct number in Step 6.3 below
WAKEWORD_THRESHOLD=0.5
WAKEWORD_COOLDOWN=2

# ── Recording ──────────────────────────────────────────
RECORDING_SECONDS=4
SAMPLE_RATE=16000

# ── Models ─────────────────────────────────────────────
WAKEWORD_MODEL=hey jarvis
LLM_MODEL=llama-3.1-8b-instant
STT_MODEL=whisper-large-v3-turbo
TTS_MODEL=canopylabs/orpheus-v1-english
TTS_VOICE=autumn

Save with Ctrl+O, Enter, Ctrl+X.

6.3 Find your correct MIC_INDEX

Run this helper to list all audio input devices:

python3 -c "
import pyaudio
p = pyaudio.PyAudio()
print('\nAvailable INPUT devices:\n')
for i in range(p.get_device_count()):
d = p.get_device_info_by_index(i)
if d['maxInputChannels'] > 0:
print(f' [{i}] {d[\"name\"]}')
print(f' channels={int(d[\"maxInputChannels\"])} rate={int(d[\"defaultSampleRate\"])}Hz')
p.terminate()
"

Example output:

Available INPUT devices:

[0] HDA Intel PCH: ALC897 Analog
channels=2 rate=44100Hz

[1] reSpeaker Flex XVF3800
channels=6 rate=16000Hz ← this is the one you want

[2] USB PnP Sound Device
channels=2 rate=16000Hz

Find the line that says reSpeaker Flex or reSpeaker Flex XVF3800. Note the number in brackets — that is your MIC_INDEX. Update config.env with that number.


Part 7 — Build the Package​

cd ~/ros2_ws
colcon build --packages-select my_robot_controller
source ~/.bashrc

Expected output:

Starting >>> my_robot_controller
Finished <<< my_robot_controller [3.2s]

Summary: 1 package finished [3.5s]

You must run colcon build and source ~/.bashrc every time you change any Python file.


Part 8 — Run the Project​

ros2 launch my_robot_controller jarvis.launch.py

You should see three processes start:

[turtlesim_node-1]   [INFO] Spawning turtle [turtle1] at x=[5.54], y=[5.54]
[angle_controller-2] [INFO] AngleController ready — listening on /target_angle
[voice_command-3] [INFO] reSpeaker Flex XVF3800 found — DoA ready
[voice_command-3] [WakeWord] Listening on device 1 (6ch → mono) for 'hey jarvis' ...
[voice_command-3] [INFO] Jarvis is listening ...

A window will open showing the turtle. Now speak:

"Hey Jarvis, move forward"

Jarvis will reply "Moving forward!" and the turtle will move.


pir

Voice Command Reference​

Say thisWhat happens
"Hey Jarvis, move forward"Turtle moves forward 1 step
"Hey Jarvis, move backward"Turtle moves backward 1 step
"Hey Jarvis, turn left"Turtle rotates left 90°
"Hey Jarvis, turn left 45"Turtle rotates left 45°
"Hey Jarvis, turn right"Turtle rotates right 90°
"Hey Jarvis, turn right 30 degrees"Turtle rotates right 30°
"Hey Jarvis, turn to my direction"Turtle faces toward your voice (DoA)
"Hey Jarvis, face me"Same as above
"Hey Jarvis, turn to 90"Turtle rotates to absolute 90°
"Hey Jarvis, face 180 degrees"Turtle rotates to absolute 180°
"Hey Jarvis, spin around"Turtle does a full 360° spin
"Hey Jarvis, do a 360"Same as above
"Hey Jarvis, stop"Turtle stops immediately

Project File Structure​

my_robot_controller/
│
├── my_robot_controller/ # Python package (ROS2 nodes)
│ ├── __init__.py
│ ├── voice_node.py # Main voice pipeline node
│ ├── rotate_doa.py # PID angle controller node
│ ├── wakeword.py # Wake word detection (openwakeword)
│ ├── audio_recorder.py # Mic recording after wake word
│ ├── stt.py # Speech-to-text (Groq Whisper)
│ ├── llm.py # Intent parsing (Groq LLaMA)
│ ├── tts.py # Text-to-speech (Groq Orpheus)
│ └── config.py # Loads settings from config.env
│
├── launch/
│ └── jarvis.launch.py # Starts all 3 nodes together
│
├── config.env # Your secrets (not in git)
├── config.env.example # Template — copy to config.env
├── package.xml
└── setup.py

How the nodes connect​

reSpeaker Flex (USB)
│
├── [voice_command node]
│ openwakeword → Groq Whisper → Groq LLaMA → Groq Orpheus
│ │ │
│ │ publishes /target_angle (Float32) │ speaks reply
│ │ publishes /turtle1/cmd_vel (Twist) │
│ │ ▼
│ ▼ Speaker output
└── [angle_controller node]
subscribes /target_angle
subscribes /turtle1/pose
PID control → publishes /turtle1/cmd_vel
│
▼
[turtlesim_node]

Configuration Reference​

All settings live in config.env. Edit and rebuild to apply changes.

VariableDefaultDescription
GROQ_API_KEY(required)Your Groq API key
MIC_INDEX1PyAudio device index of the reSpeaker
WAKEWORD_MODELhey jarvisWake word phrase
WAKEWORD_THRESHOLD0.5Detection sensitivity (0.0–1.0, lower = more sensitive)
WAKEWORD_COOLDOWN2Seconds before wake word can re-trigger
RECORDING_SECONDS4How long to record after wake word fires
SAMPLE_RATE16000Audio sample rate in Hz
LLM_MODELllama-3.1-8b-instantGroq LLM model for intent parsing
STT_MODELwhisper-large-v3-turboGroq Whisper model for transcription
TTS_MODELcanopylabs/orpheus-v1-englishGroq TTS model
TTS_VOICEautumnVoice for speech output (tara, leah, leo, dan, mia)

Resources​

Built with:

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...