Skip to main content

Add Voice Interaction to Your SO-ARM10x with reSpeaker

Overview​

pir

The LeRobot SO-ARM Voice Controller lets you control a SO-ARM100 robotic arm using natural voice commands powered by AI. The system combines wake word detection, Groq Whisper speech-to-text, LLaMA 3 language understanding, and Orpheus text-to-speech to create a fully interactive hands-free robotics experience. Built on top of the LeRobot framework, it runs on Ubuntu x86 systems and NVIDIA Jetson devices using a ReSpeaker USB microphone array for voice input. Users can create custom arm poses, gestures, and conversational triggers to build intelligent robotic interactions for research, education, and robotics development.

Hardware Required​

SO-ARM101reComputer Super J4012
reSpeaker Flex XVF3800 CircularreSpeaker XVF3800

OR

How It Works​

You speak → Wake word detected → Audio recorded → Whisper STT → LLaMA LLM → Orpheus TTS speaks back → SO-ARM100 moves

Services Required​

ServicePurposeCost
GroqWhisper STT, LLaMA LLM, Orpheus TTSFree tier is enough

Part 1 — Install LeRobot​

Install Miniforge​

For Jetson (ARM64):

wget https://github.com/conda-forge/miniforge/releases/latest/download/Miniforge3-Linux-aarch64.sh
chmod +x Miniforge3-Linux-aarch64.sh
./Miniforge3-Linux-aarch64.sh
source ~/.bashrc

For x86 Ubuntu 22.04:

wget "https://github.com/conda-forge/miniforge/releases/latest/download/Miniforge3-$(uname)-$(uname -m).sh"
bash Miniforge3-$(uname)-$(uname -m).sh
source ~/.bashrc
conda init --all

Create the Conda Environment​

conda create -y -n lerobot python=3.12
conda activate lerobot

Clone and Install LeRobot​

git clone https://github.com/KasunThushara/lerobot
conda install ffmpeg -c conda-forge
cd lerobot
pip install -e ".[feetech]"

Part 2 — Set Up the Arms​

Configure Motor IDs​

Each servo needs a unique ID assigned before assembly. Follow the official guide: Configure the Motors

Assemble the Arms​

Follow the assembly tutorial for the SO-ARM100: Assembly Guide

Find the USB Ports​

Plug in each arm and run this utility to identify which port belongs to which arm:

lerobot-find-port

Run it once per arm (plug one in at a time). Note down the port paths — typically /dev/ttyACM0 and /dev/ttyACM1.

Calibrate Both Arms​

Calibration maps raw motor values to normalized positions. Follow the guide for both the leader and follower arms: Calibration Guide

The calibration file will be saved automatically at:

~/.cache/huggingface/lerobot/calibration/robots/so_follower/<your_arm_id>.json


Part 3 — Set Up the Voice Controller​

cd ~/lerobot/examples/voice_arm

Install Dependencies​

# System dependency required for PyAudio
sudo apt-get install -y portaudio19-dev

pip install -r requirements.txt

Download the Wake Word Model​

Downloads the pre-trained "Hey Jarvis" model from openwakeword into ~/.openwakeword/:

python download_model.py

Find Your Microphone Index​

Plug in your reSpeaker , then run:

python list_mics.py

Example output:

Available audio INPUT devices:

[0] bcm2835 Headphones (rate=44100Hz)
[1] ReSpeaker 4 Mic Array (rate=16000Hz)
[2] USB PnP Sound Device (rate=16000Hz)

Note the index number next to your ReSpeaker — that's your MIC_INDEX.

Configure the Project​

cp config.env.example config.env
nano config.env

At minimum, update these two values:

# Your Groq API key (required) — get one free at console.groq.com
GROQ_API_KEY=gsk_xxxxxxxxxxxxxxxxxxxxxxxx

# The number from list_mics.py
MIC_INDEX=1

Part 4 — Define Your Arm Actions​

Step 1 — Read Current Joint Positions​

Move the arm physically into a pose you want to save, then run:

python read_positions.py

The script prints live normalized joint values as you move the arm. When you're happy with the pose, press Ctrl+C and the final position will be printed for you to copy.

Step 2 — Add the Pose to robot_arm.py​

Open robot_arm.py and find the ACTION_MAP dictionary. Add your pose:

pir

"my_custom_pose": _pose(**{
"shoulder_pan.pos": 20.0,
"shoulder_lift.pos": 40.0,
"elbow_flex.pos": 60.0,
"wrist_flex.pos": -30.0,
"gripper.pos": 80.0,
}),

For animated gestures (like a wave), use a list of poses — each step runs with ARM_GESTURE_DELAY between them:

"wave_hi": [
_pose(**{"shoulder_lift.pos": -70.0, "wrist_flex.pos": 60.0, ...}),
_pose(**{"shoulder_lift.pos": -70.0, "wrist_flex.pos": -60.0, ...}),
_HOME, # return to neutral
],

Step 3 — Update the LLM System Prompt in llm.py​

Add your new action to the valid actions list and trigger rules so the LLM knows about it:

pir

Valid actions:
my_custom_pose = describe what it does

Trigger rules:
- "your trigger phrase" → my_custom_pose

Run the Voice Controller​

Make sure your conda environment is active, then:

conda activate lerobot
python pipeline.py

You should see:

======================================================
SO100 Arm Voice Controller — Ready
Wake word : hey jarvis
LLM model : llama-3.1-8b-instant
STT model : whisper-large-v3-turbo
TTS voice : autumn
Arm port : /dev/ttyACM0 id='my_awesome_follower_arm'
======================================================
[WakeWord] Listening for 'hey jarvis' ...

Now say "Hey Jarvis" and give a command!

Example Voice Commands​

You sayWhat happens
"Hey Jarvis, open the gripper"Gripper opens fully
"Hey Jarvis, grab it"Gripper closes
"Hey Jarvis, go to pick up mode"Arm moves to grasp pose
"Hey Jarvis, can you turn around"Base rotates to the side
"Hey Jarvis, wave at the camera"Arm waves, returns to neutral
"Hey Jarvis, go home"All joints return to neutral

Project File Overview​

examples/voice_arm/
├── pipeline.py # Main entry point — orchestrates the full flow
├── robot_arm.py # SO100 arm controller — add your poses here
├── llm.py # LLM prompt — add your voice triggers here
├── wakeword.py # Listens for "Hey Jarvis" in a background thread
├── audio_recorder.py # Records audio after wake word fires
├── stt.py # Sends audio to Groq Whisper → returns text
├── tts.py # Sends reply to Groq Orpheus → plays audio
├── config.py # Loads all settings from config.env
├── config.env.example # Template — copy to config.env and fill in
├── read_positions.py # Helper: read live joint positions for tuning poses
├── list_mics.py # Helper: find your MIC_INDEX
└── download_model.py # Downloads the openwakeword model files

Configuration Reference​

VariableDefaultDescription
GROQ_API_KEY(required)Your Groq API key
WAKEWORD_MODELhey jarvisWake word phrase
MIC_INDEX1PyAudio device index
WAKEWORD_THRESHOLD0.5Detection sensitivity (0.0–1.0)
WAKEWORD_COOLDOWN2Seconds between re-triggers
RECORDING_SECONDS3How long to record after wake word
LLM_MODELllama-3.1-8b-instantGroq LLM model
STT_MODELwhisper-large-v3-turboGroq Whisper model
TTS_VOICEautumnVoice for speech output
ARM_PORT/dev/ttyACM0Follower arm USB port
ARM_IDmy_awesome_follower_armArm ID (matches calibration filename)
ARM_MOVE_DELAY1.5Seconds to wait after a pose move
ARM_GESTURE_DELAY0.4Seconds between gesture sequence steps

Troubleshooting​

PyAudio fails to install Install the PortAudio system library first:

sudo apt-get install -y portaudio19-dev

Wake word never triggers Run list_mics.py again and confirm MIC_INDEX matches your ReSpeaker. Try lowering WAKEWORD_THRESHOLD to 0.3. Speak clearly within ~1 metre of the mic.

Arm not moving after a command Check that ARM_PORT is correct (lerobot-find-port). Verify the calibration file exists at ~/.cache/huggingface/lerobot/calibration/robots/so_follower/<ARM_ID>.json.

Arm moves to wrong position The default pose values in ACTION_MAP are starting estimates. Run read_positions.py, physically move the arm to the desired pose, and copy the printed values into robot_arm.py.

TTS / STT errors Double-check GROQ_API_KEY in config.env. The Groq free tier has rate limits — wait a few seconds between commands if you hit errors.

Audio plays but sounds distorted On Raspberry Pi, set audio output to the correct device via raspi-config → System Options → Audio.


Credits​

Built with:

  • LeRobot — open-source robotics framework by Hugging Face
  • SO-ARM100 — low-cost open-source robotic arm by Seeed Studio
  • openwakeword — local wake word detection
  • Groq — ultra-fast Whisper STT, LLaMA LLM, and Orpheus TTS
  • ReSpeaker Flex — USB microphone array
Loading Comments...