RGB test
Functionality
The RGB light on the ReSpeaker Lite board is using the WS2812 chip and controlled via the GPIO1 pin. The project cycles through different colors (red, green, blue, and white) to ensure that the RGB light is functioning properly.
Code
#include <Adafruit_NeoPixel.h>
// Define parameters for the LED strip
#define PIN 1 // Pin connected to the RGB LED
#define NUMPIXELS 1 // Number of LEDs
Adafruit_NeoPixel strip(NUMPIXELS, PIN, NEO_GRB + NEO_KHZ800); // Initialize the LED strip object
void setup() {
// Initialize the serial monitor for debugging
Serial.begin(115200);
// Initialize the RGB LED strip
strip.begin();
strip.show(); // Initialize all pixels to the off state
}
void loop() {
// Red color test
Serial.println("Red color test");
strip.setPixelColor(0, strip.Color(255, 0, 0)); // Set the first pixel to red
strip.show(); // Update the strip display
delay(1000); // Delay for 1 second
// Green color test
Serial.println("Green color test");
strip.setPixelColor(0, strip.Color(0, 255, 0)); // Set the first pixel to green
strip.show();
delay(1000);
// Blue color test
Serial.println("Blue color test");
strip.setPixelColor(0, strip.Color(0, 0, 255)); // Set the first pixel to blue
strip.show();
delay(1000);
// White color test
Serial.println("White color test");
strip.setPixelColor(0, strip.Color(255, 255, 255)); // Set the first pixel to white
strip.show();
delay(1000);
// Turn off the LED
Serial.println("Turn off the LED");
strip.setPixelColor(0, strip.Color(0, 0, 0)); // Turn off the first pixel
strip.show();
delay(1000);
}

Configuration
strip.setPixelColor: set the color LED in the strip.
strip.show: applies the color changes to the LED.