MQTT Audio Streaming
This project demonstrates how to use the reSpeaker Lite board, which includes an integrated XIAO ESP32S3 microcontroller, to generate and send audio data to an MQTT broker.
Library Required
Functionality
The sketch performs the following tasks:
- Connects to the specified WiFi network.
- Connects to the specified MQTT broker.
- Generates white noise audio using the WhiteNoiseGenerator class from the reSpeaker Lite library.
- Encodes the audio data as a WAV file using the WAVEncoder class from the reSpeaker Lite library.
- Sends the encoded audio data to the specified MQTT topic using the MqttClient class from the ArduinoMqttClient library.
- Maintains the MQTT connection by regularly calling the poll() function.
Code
Modify the following lines in the sketch to match your WiFi and MQTT broker settings:
const char* ssid = "SSID"; // your Wi-FI SSID (name)
const char* password = "PASSWORD"; // your Wi-Fi password (use for WPA, or use as key for WEP)
const char* broker = "test.mosquitto.org";
const char* topic = "audio.wav";
int port = 1883;
Code
#include "WiFi.h"
#include "ArduinoMqttClient.h"
#include "AudioTools.h"
#define SIZE 1024
#define N 100
// Communication
const char* ssid = "SSID"; // your Wi-FI SSID (name)
const char* password = "PASSWORD"; // your Wi-Fi password (use for WPA, or use as key for WEP)
const char* broker = "test.mosquitto.org";
const char* topic = "audio.wav";
int port = 1883;
WiFiClient wifiClient;
MqttClient mqttClient(wifiClient);
// Audio
AudioInfo info(16000, 1, 32);
WhiteNoiseGenerator<int16_t> noise(32000); // subclass of SoundGenerator with max amplitude of 32000
GeneratedSoundStream<int16_t> in_stream(noise); // Stream generated from noise
EncodedAudioStream out_stream(&mqttClient, new WAVEncoder()); // encode as wav file
StreamCopy copier(out_stream, in_stream, SIZE); // copies sound to MQTT client
// Connect to Wifi
void connectWIFI() {
// attempt to connect to WiFi network:
Serial.print("Attempting to connect to WPA SSID: ");
Serial.println(ssid);
WiFi.begin(ssid, password);
Serial.print("Connecting to WiFi ..");
while (WiFi.status() != WL_CONNECTED) {
Serial.print('.');
delay(1000);
}
Serial.println("You're connected to the network");
Serial.println();
}
// Connect to MQTT Server
void connectMQTT() {
// You can provide a unique client ID, if not set the library uses Arduino-millis()
// Each client must have a unique client ID
mqttClient.setId("reSpeaker");
// You can provide a username and password for authentication
// mqttClient.setUsernamePassword("username", "password");
Serial.print("Attempting to connect to the MQTT broker: ");
Serial.println(broker);
if (!mqttClient.connect(broker, port)) {
Serial.print("MQTT connection failed! Error code = ");
Serial.println(mqttClient.connectError());
stop();
}
Serial.println("You're connected to the MQTT broker!");
Serial.println();
}
// Send audio to MQTT Server
void sendMQTT() {
// make sure that we write wav header
out_stream.begin(info);
// send message, the Print interface can be used to set the message contents
mqttClient.beginMessage(topic, SIZE * N, true);
// copy audio data to mqtt: 100 * 1024 bytes
copier.copyN(N);
mqttClient.endMessage();
}
void setup() {
// Initialize logger
Serial.begin(115200);
AudioLogger::instance().begin(Serial, AudioLogger::Info);
// connect
connectWIFI();
connectMQTT();
// setup audio
noise.begin(info);
in_stream.begin(info);
// send Audio
sendMQTT();
}
void loop() {
// call poll() regularly to allow the library to send MQTT keep alives which
// avoids being disconnected by the broker
mqttClient.poll();
delay(10000);
}
Open the Serial Monitor to check the output and logs.

Then you can see the data on your MQTT server.

Customization
You can customize the audio generation and encoding by modifying the following lines in the sketch:
WhiteNoiseGenerator<int16_t> noise(32000);
GeneratedSoundStream<int16_t> in_stream(noise);
EncodedAudioStream out_stream(&mqttClient, new WAVEncoder());
WhiteNoiseGeneratorgenerates white noise audio with a specified maximum amplitude.GeneratedSoundStreamcreates an input stream from the generated audio.EncodedAudioStreamencodes the audio data using the specified encoder (WAV in this case).
You can also adjust the size of the audio data being sent by modifying the SIZE and N constants:
#define SIZE 1024
#define N 100
SIZErepresents the size of each audio data chunk.Nrepresents the number of audio data chunks to send.