Volume Adjustment
Functionality
This example project demonstrates how to adjust the volume of the ReSpeaker Lite via I2C command.
AIC3204 I2C address: 0x18
Code
#include "AudioTools.h"
#include "Wire.h"
#define AIC3204_ADDR 0x18
AudioInfo info_16k(16000, 2, 32);
SineWaveGenerator<int16_t> sineWave(1000); // subclass of SoundGenerator with max amplitude of 32000
GeneratedSoundStream<int16_t> sound(sineWave); // Stream generated from sine wave
I2SStream out;
I2SConfig config_i2s1;
//FormatConverterStream converter(in);
//StreamCopy copier(out, converter);
StreamCopy copier(out, sound);
uint32_t now_time = 0;
uint8_t level_index = 0;
int8_t level[10] = {0x3A, 0x3B, 0x3C, 0x3D, 0x3E, 0x3F, 0x00, 0x01, 0x02, 0x03};
void aic3204_write_reg(uint8_t reg, uint8_t value)
{
Wire.beginTransmission(AIC3204_ADDR);
Wire.write(reg);
Wire.write(value);
Wire.endTransmission();
}
void setup(void) {
// Open Serial
Serial.begin(115200);
Wire.begin(5,6);
// while(!Serial);
// AudioLogger::instance().begin(Serial, AudioLogger::Info);
// start I2S
Serial.println("starting I2S...");
config_i2s1 = out.defaultConfig(TX_MODE);
config_i2s1.copyFrom(info_16k);
// Custom I2S output pins
config_i2s1.pin_bck = 8;
config_i2s1.pin_ws = 7;
config_i2s1.pin_data = 43;
config_i2s1.pin_data_rx = 44;
config_i2s1.is_master = false;
out.begin(config_i2s1);
// converter.begin(info_16k, info_48k);
sineWave.begin(info_16k, N_B4);
Serial.println("started...");
}
// Arduino loop - copy sound to out
void loop() {
copier.copy();
if (millis() - now_time > 1000) {
now_time = millis();
aic3204_write_reg(0x00, 0x01);
aic3204_write_reg(0x12, level[level_index]);
aic3204_write_reg(0x13, level[level_index]);
Serial.print("level: ");
Serial.println(level_index);
level_index = level_index + 2;
if (level_index >= 10) level_index = 0;
}
}