reSpeaker XVF3000 FAQ
This page contains verified answers for the reSpeaker XVF3000. Each answer states the product variant and firmware mode it applies to, together with the date it was last verified against current official sources.
Before you begin
- Confirm the exact product variant and the firmware mode (USB or I2S) the device is running.
- Check the current firmware version before applying version-specific steps.
- Answers on this page were last verified on 2026-11-02; re-check the linked official sources if you are reading this later.
Connectivity & Detection
Does the XVF3000 provide a unique serial number for device identification?
Applies to: reSpeaker USB 4-Mic Array XVF3000 v3.0/v3.2 and ReSpeaker Mic Array v2.0 running the official USB audio firmware on Linux, Windows, or macOS hosts
Last verified: 2026-11-02
No. The official XVF3000 USB firmware does not expose a unique serial number: iSerialNumber is empty, DFU reports serial="UNKNOWN", and tuning.py exposes only the firmware version and DSP parameters. For fixed installations, identify the device by its host USB port path. If the identifier must stay with the device, use a product with a factory-programmed serial number such as the XVF3800, or custom firmware with a production-written serial.
Prerequisites:
- Access to the host USB descriptors and the physical USB port used by the device
- A host application or inventory record that can store the device's port or instance identifier
- Confirm that the device has no stock serial:
lsusb -v -d 2886:0018 | grep iSerialshould returniSerial 0, anddfu-util -lshould reportserial="UNKNOWN". - On Linux, read the stable port path with
udevadm info -q property -n /dev/bus/usb/001/002 | grep ID_PATH. The device node number can change, butID_PATHstays the same while the device remains on that port. For ALSA, use/dev/snd/by-path/, notby-idor the card index. - On Windows use the device instance ID, and on macOS use the USB Location ID. Record that value with the unit's asset label.
- For a fixed installation, bind the recorded port path to the asset ID in the host application or inventory database. If the identifier must be read from the device itself, use a product with a factory serial number such as the XVF3800, or plan custom firmware and a production step that writes the serial.
Success criteria:
- The device reports no stock serial number (
iSerial 0and DFUserial="UNKNOWN"). - The host resolves the same port path after reconnecting the device to the same port.
- The application maps that port path to the intended physical unit or asset record.
Notes:
- The port path identifies the USB port, not the device; moving the device to another port or host requires re-binding.
- Do not use
version,bcdDevice, DOA angle, RT60, or noise floor as a unique identifier; these values are shared across units or change with the environment. - ALSA
by-idnames and card indexes are not stable when multiple identical devices are connected.
References:
- ReSpeaker USB 4-Mic Array XVF3000 v3.0/v3.2 Wiki
- Official XVF3000 tuning tool (tuning.py)
- reSpeaker XVF3800 FAQ: unique device serial number
Algorithm Tuning
How can I inspect the built-in DSP tuning controls on ReSpeaker Mic Array v2.0?
Applies to: ReSpeaker Mic Array v2.0 with XVF3000 and the matching official firmware
Last verified: 2026-09-01
Use the official usb_4_mic_array repository's tuning.py tool. The current v2.0 Wiki documents python tuning.py -p to list available parameters and shows parameter reads and writes, but it does not provide a universal preset or guaranteed pickup distance for every noisy room.
Prerequisites:
- Confirm the hardware is ReSpeaker Mic Array v2.0 rather than another ReSpeaker revision
- Install the USB control dependency and host driver required by the official guide
- Keep a record of the starting parameter values and use a repeatable audio test
- Clone the official
respeaker/usb_4_mic_arrayrepository and enter its directory. - Run
python tuning.py -pto print the parameter names, types, ranges, access mode, and descriptions exposed by the active firmware. - Use the documented
python tuning.py <PARAMETER>form to read a value, and change only a writable parameter whose public range and meaning are shown. - Repeat the same speech, distance, noise, and room test after each single change; keep the change only if the captured result improves without introducing a regression.
Success criteria:
- The parameter list is returned without a USB-control error
- The selected value reads back and the before/after recordings are compared under the same test conditions
Notes:
- The public parameter table is an interface reference, not a validated noisy-room tuning recipe.
- Poor pickup at a particular distance does not by itself prove a hardware defect; microphone placement, background noise, reverberation, firmware, and the host capture path must be controlled first.
References:
- ReSpeaker Mic Array v2.0 tuning guide and parameter table
- Official XVF3000 USB 4-Mic Array tools repository
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.