Skip to main content

ROS2 on reSpeaker XVF3800

Introduction

pir

This project demonstrates the integration of the ReSpeaker XVF3800 with ROS2 for robotic applications, focusing on speech detection and Direction of Arrival (DOA) estimation. Using the Turtlesim node, we simulate robotic control based on speech input, enabling precise movement through PID control. The tutorial covers the setup of the ROS2 environment, configuration of the ReSpeaker XVF3800, and how to apply speech commands for controlling a robot. By the end, users will understand how to connect voice interfaces with robotics and use basic control algorithms for navigation.

pir

How to Install ROS 2 on the Host Computer

For this project, we use ROS 2 Humble as the middleware. If you are installing ROS 2 for the first time, please follow the official installation guide for detailed steps:

ROS 2 Humble Installation Guide (Ubuntu)

Set Up ReSpeaker USB Mic Array

If you're using the ReSpeaker USB Mic Array for your robot or voice applications, follow these steps to configure it on your Ubuntu system.

Find Your Device's Vendor and Product IDs

To find your device's IDs, run:

lsusb

Look for the ReSpeaker device (e.g., vendor 0x2886, product 0x001A).

Create a udev Rule for the Device

Create a new udev rule to ensure proper permissions for the ReSpeaker Mic Array:

sudo nano /etc/udev/rules.d/50-respeaker.rules

Add the following lines to the file:

# ReSpeaker USB Mic Array
SUBSYSTEM=="usb", ATTR{idVendor}=="2886", ATTR{idProduct}=="0018", MODE="0666", GROUP="plugdev"
SUBSYSTEM=="usb", ATTR{idVendor}=="2886", ATTR{idProduct}=="001a", MODE="0666", GROUP="plugdev"

Reload udev Rules and Restart the Service

Reload the udev rules and restart the service for changes to take effect:

sudo udevadm control --reload-rules
sudo udevadm trigger
sudo service udev restart

Unplug and replug your ReSpeaker USB Mic Array to apply the new rules.

Setting Up ROS2 Workspace and Controlling Your Robot with ROS2

This guide walks you through the process of setting up a ROS2 workspace, creating a custom ROS2 package, controlling a robot using Python, and configuring the ReSpeaker USB Mic Array for use in your ROS2 project.

Install Required Dependencies

Install Python Colcon Extension

First, ensure that the necessary Python extensions for building ROS2 packages are installed:

sudo apt install python3-colcon-common-extensions

Configure Colcon Auto-completion (Optional)

If you need to set up auto-completion for colcon:

cd /usr/share/colcon_argcomplete/hook/
ls
gedit ~/.bashrc
clear

Then, add source ~/.bashrc to reload the environment:

source ~/.bashrc

Create a ROS2 Workspace

Create a new ROS2 workspace and prepare the environment:

mkdir ros2_ws
cd ros2_ws/
mkdir src
colcon build

Source the ROS2 Workspace

After building the workspace, source it to set up the environment variables:

source ~/ros2_ws/install/setup.bash

You can add this line to your ~/.bashrc to source the workspace automatically every time you open a new terminal:

echo "source ~/ros2_ws/install/setup.bash" >> ~/.bashrc
source ~/.bashrc

Create a New ROS2 Package

Now, let's create a new ROS2 package for your robot controller. This package will use ament_python for building and rclpy as a dependency:

cd ~/ros2_ws/src
ros2 pkg create my_robot_controller --build-type ament_python --dependencies rclpy

Add Python Script for Robot Control

Navigate into your newly created package, and create a Python script (e.g., rotate_doa.py) to control the robot:

cd my_robot_controller/
touch rotate_doa.py
chmod +x rotate_doa.py

Edit the script with your desired control logic (e.g., using an editor like VS Code):

cd ..
code .
rotate_doa.py
import sys
import struct
import usb.core
import usb.util
import time
import rclpy
from rclpy.node import Node
from geometry_msgs.msg import Twist
from turtlesim.msg import Pose
from std_msgs.msg import Float32
import math

# name, resid, cmdid, length, type
PARAMETERS = {
"VERSION": (48, 0, 4, "ro", "uint8"),
"AEC_AZIMUTH_VALUES": (33, 75, 16 + 1, "ro", "radians"),
"DOA_VALUE": (20, 18, 4 + 1, "ro", "uint16"),
}

class ReSpeaker:
TIMEOUT = 100000

def __init__(self, dev):
self.dev = dev

def write(self, name, value):
pass

def read(self, name):
try:
data = PARAMETERS[name]
except KeyError:
return

resid = data[0]
cmdid = 0x80 | data[1]
length = data[2]

response = self.dev.ctrl_transfer(
usb.util.CTRL_IN | usb.util.CTRL_TYPE_VENDOR | usb.util.CTRL_RECIPIENT_DEVICE,
0, cmdid, resid, length, self.TIMEOUT)

if data[4] == 'uint8':
result = response.tolist()
elif data[4] == 'radians':
byte_data = response.tobytes()
float1, float2, float3, float4 = struct.unpack('<ffff', byte_data[1:17])
result = [float1 * 180 / 3.1415926,
float2 * 180 / 3.1415926,
float3 * 180 / 3.1415926,
float4 * 180 / 3.1415926]
elif data[4] == 'uint16':
result = response.tolist()

return result

def close(self):
"""
close the interface
"""
usb.util.dispose_resources(self.dev)


def find(vid=0x2886, pid=0x001A):
dev = usb.core.find(idVendor=vid, idProduct=pid)
if not dev:
return None
return ReSpeaker(dev)


class AngleController(Node):
def __init__(self):
super().__init__('angle_controller')
self.target_angle = 0.0
self.pose_sub = self.create_subscription(Pose, '/turtle1/pose', self.pose_callback, 10)
self.cmd_pub = self.create_publisher(Twist, '/turtle1/cmd_vel', 10)

# PID params
self.kp = 1.5
self.ki = 0.0
self.kd = 0.2

self.integral = 0.0
self.prev_error = 0.0
self.prev_time = self.get_clock().now()

def publish_angle(self, angle_deg: float):
self.target_angle = math.radians(angle_deg) # Convert to radians
self.get_logger().info(f"New target angle: {angle_deg:.2f}°")

def pose_callback(self, msg: Pose):
current_yaw = msg.theta
error = self.normalize_angle(self.target_angle - current_yaw)

now = self.get_clock().now()
dt = (now - self.prev_time).nanoseconds / 1e9
self.prev_time = now

self.integral += error * dt
derivative = (error - self.prev_error) / dt if dt > 0 else 0.0

control = self.kp * error + self.ki * self.integral + self.kd * derivative

twist = Twist()
twist.angular.z = control
self.cmd_pub.publish(twist)

self.prev_error = error

@staticmethod
def normalize_angle(angle):
while angle > math.pi:
angle -= 2.0 * math.pi
while angle < -math.pi:
angle += 2.0 * math.pi
return angle


def main(args=None):
rclpy.init(args=args)
node = AngleController()

# Setup ReSpeaker device
dev = find()
if not dev:
node.get_logger().error("No ReSpeaker device found")
return

# Function to handle publishing DOA angle when speech is detected
def publish_doa_angle():
result = dev.read("DOA_VALUE")
if result:
speech_detected = result[3]
doa_angle = result[1]
if speech_detected: # If speech is detected
node.publish_angle(doa_angle)
node.get_logger().info(f"Speech detected, DOA angle: {doa_angle}°")

# Timer to check for DOA updates every 1 second
timer = node.create_timer(1.0, publish_doa_angle)

rclpy.spin(node)
node.destroy_node()
rclpy.shutdown()
dev.close()


if __name__ == '__main__':
main()

Add this dependancies to package.xml

  <depend>rclpy</depend>
<depend>geometry_msgs</depend>
<depend>turtlesim</depend>
<depend>std_msgs</depend>

Add this endpoint to package.xml


entry_points={
'console_scripts': [
'rotate_doa = my_controller.rotate_doa:main',
],
},

Build and Run the Package

After editing your Python script, build the package:

colcon build
source ~/ros2_ws/install/setup.bash

Finally, run the package with:

ros2 run my_robot_controller rotate_doa

In another terminal, you can also run a basic ROS2 node (e.g., turtlesim for testing):

ros2 run turtlesim turtlesim_node

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...