reTerminal DM Flash Raspbian OS to eMMC

reTerminal DM is A 10.1" open-source industrial HMI - an Integrated Device Master to unify data flow and manage the onsite device.
Based on Raspberry Pi CM4, and as a Panel PC, HMI, PLC, IIoT Gateway all-in-one device, reTerminal DM is a new generation of interactive sensing hub with an IP65 industrial-grade large screen.
It is equipped with rich scalability and hybrid connectivity, supporting CAN bus, RS485, RS232, Gigabit Ethernet port, and other interfaces, as well as powerful wireless communication capabilities such as 4G, LoRa®, WiFi, and BLE.
*4G and LoRa® modules does not come with reTerminal DM by default, please purchase the relevant modules accordingly, for 4G bundle
The Sensecraft Edge OS can be download from Here, please note that this Sensecraft Edge OS is currently developed based on reTerminal DM and only works with Production version reTerminal DM
Hardware Requirements
You need to prepare the following hardware
- reTerminal DM x 1
- Host Computer (Windows/Mac/Linux) x 1
- Ethernet cable x 1
- Power adapter (12V-24V) BYO
- USB Type-C cable x 1
Software Requirements
Steps for Flashing Raspbian OS
Note: The latest system image packaged by Seeed, including the appropriate drivers: pi-gen-expand
- Step 1. Flip the
boot mode switchlocated next to the USB Type-C port, make sure switch is set todisable eMMC boot modeaccording to the diagram below:

-
Step 2. Please use the USB Type-C data cable connect to the Type-C port on the reTerminal DM, as shown in the above image,
-
Step 3. Please connect the Power Cord from the power supply to the reTerminal DM power port.
Please make sure you have connected the power cord in the right polarity.

Now let's move on to software set up on your host computer. Please follow the steps according to your desired operating system
For Windows
-
Step 1. Download the rpiboot setup installer by click here to install the necessary drivers and the boot tool
-
Step 2. Connect reTerminal DM to the PC via USB Type-C cable
Windows will now find the hardware and install the necessary drivers
-
Step 3. Search for rpiboot tool that we installed before and open it
-
Step 4. Open file explorer and you will see the eMMC of the Computer Module 4 shown as a USB mass storage device
-
Step 5. Download Raspberry Pi Imager software from here
-
Step 6. Open Raspberry Pi Imager software

- Step 7. Press CTRL + SHIFT + X on the keyboard to open Advanced options window

Here you can set a hostname, enable SSH, set a password, configure wiFi, set locale settings and more
- Step 8. Click CHOOSE OS and select your preferred OS

NOTE: You can select other OS such as 64-bit Ubuntu by navigating into Other general purpose OS

-
Step 9. Click CHOOSE STORAGE and select the connected eMMC drive
-
Step 10. Finally, click WRITE

Please wait a few minutes until the flashing process is complete.
- Step 11. Flip the Boot Mode switch back to the original position
Now you can skip to here
Once the above steps finished and you have reapply the power to the reTerminal DM, the Power LED should turn on yellow color and the ACT LED should flashing green color, but the screen is blank and no backlight. please do not panic, you just need to following the install drivers steps to revive the screen.
For MAC
You need to install homebrew before proceed the following steps.
Please open a terminal and type brew -V to check if you have setup the correct homebrew environment, you should see the version of the homebrew environment you have installed.
- Step 1. Clone the usbboot repository
git clone --depth=1 https://github.com/raspberrypi/usbboot
cd usbboot
- Step 2. Install libusb
brew install libusb
- Step 3. Install pkg-config
brew install pkg-config
- Step 4. Build using make
make
- Step 5. Run the binary
sudo ./rpiboot
-
Step 6. Connect reTerminal to the your Mac computer via USB Type-C cable
-
Step 7. Download and Install Raspberry Pi Imager Application by visiting this link
-
Step 8. Open the Raspberry Pi Imager Application

- Step 9. Press CTRL + SHIFT + X on the keyboard to open Advanced options window

Here you can set a hostname, enable SSH, set a password, configure wifi, set locale settings and more
- Step 10. Click CHOOSE OS and select your preferred OS

NOTE: You can select OS such as 64-bit Ubuntu by navigating into Other general purpose OS

-
Step 11. Click CHOOSE STORAGE and select the connected eMMC drive
-
Step 12. Finally, click WRITE

Please wait a few minutes until the flashing process is complete.
- Step 13. Flip the Boot Mode switch back to the original position
Now you can skip to here
Once the above steps finished and you have reapply the power to the reTerminal DM, you should experience that the Power LED should turn on yellow color and the ACT LED should flashing green color, but the screen is blank and no backlight. please do not panic, you just need to following the install drivers steps to revive the screen.
For Linux
We will use Git to obtain the rpiboot source code, so make sure Git is installed
- Step 1. Open a Terminal window and type the following to update the packages list
sudo apt-get update
- Step 2. Install Git by the following command
sudo apt install git libusb-1.0-0-dev pkg-config build-essential
- Step 3. Git might produce an error if the date is not set properly. Type the following to correct this
sudo date MMDDhhmm
NOTE: Where MM is the month, DD is the date, and hh and mm are hours and minutes respectively.
- Step 4. Clone the usbboot tool repository
git clone --depth=1 https://github.com/raspberrypi/usbboot
cd usbboot
- Step 5. Build and install the usbboot tool
make
- Step 6. Run the usbboot tool and it will wait for a connection
sudo ./rpiboot
The result is shown as below:

-
Step 7. Connect reTerminal to the PC via USB Type-C cable
-
Step 8. Download snap
sudo apt install snap
- Step 9. Download rpi-imager
snap install rpi-imager
- Step 10. Open Raspberry Pi Imager software
rpi-imager
The result is shown as below:

- Step 11. Press CTRL + SHIFT + X on the keyboard to open Advanced options window
Set a hostname, set a password, configure wifi, set locale settings

Enable SSH

Here you can set a hostname, enable SSH, set a password, configure wifi, set locale settings and more
- Step 11. Click CHOOSE OS and select your preferred OS

NOTE: You can select OS such as 64-bit Ubuntu by navigating into Other general purpose OS

-
Step 12. Click CHOOSE STORAGE and select the connected eMMC drive
-
Step 13. Finally, click NEXT and YES

Please wait a few minutes until the flashing process is complete. The result is shown as below:

- Step 14. Flip the Boot Mode Switch back to the original position
Once the above steps finished and you have reapply the power to the reTerminal DM, you should experience that the Power LED should turn on yellow color and the ACT LED should flashing green color, but the screen is blank and no backlight. please do not panic, you just need to following the install drivers steps to revive the screen.
Install Drivers
Access reTerminal DM via SSH
The following steps require some basic Linux command line knowledge, Please prepare yourself a cup of coffee and getting ready.
As following the above flashing OS steps, the reTerminal DM should have SSH enabled with the hostname of raspberrypi.local.
Now please connect the Ethernet cable to the reTerminal DM and a router which is on the same network as your host computer.
To test if your reTerminal DM is on the same network with host computer, you can use ping raspberrypi.local
if you see the following output after the ping command which means both devices are on the same network:

For Windows
- Step 1. Open Command Prompt and type the following
# ssh username@hostname
ssh pi@raspberrypi.local
- Step 2. Type yes for the prompt

- Step 3. Enter the password as follows
raspberry
- Step 4. If you have sucessfully logged into the Raspberry Pi OS, you will see the following output

For Mac/Linux
- Step 1. Open Terminal on the computer and type the following
ssh pi@raspberrypi.local
- Step 2. Type yes for the following message
ECDSA key fingerprint is SHA256:XXXXXXX.
Are you sure you want to continue connecting (yes/no/[fingerprint])?
- Step 3. When it asks for the password, type the following
raspberry
- Step 4. If you have sucessfully logged into the Raspberry Pi OS, you will see the following output

Install reTerminal drivers after flashing new Raspbian OS
reTerminal DM comes with the necessary drivers pre-installed out-of-the-box so you don't need to install any additional drivers. However, if you flash new OS by yourself, you need to install the necessary drivers separately.
For install 32-bit OS driver, Please carefully follow the steps below:
The Operating System that pre-installed on reTerminal DM is 64-bit, if you wish to install 32-bit OS please use the following method to install the DTS drivers.
⚠️Note : Please reboot your reTerminal DM after you flash 32-bit OS.
Please follow the Access reTerminal DM via SSH step, and then enter the following command:
echo arm_64bit=0 | sudo tee -a /boot/config.txt
Then continue the Install drivers after flashing new Raspbian OS process
Meanwhile, if you are using the latest official 32-bit Raspberry Pi OS, its new kernel is incompatible with this product, which will result in failed driver updates and a blank screen. If you do need a 32-bit OS image for development, we recommend using an older 32-bit image version.
- Step 1. Clone the following repo in the ssh shell you have connected to reTerminal DM from the above steps
sudo apt install git -y
git clone --depth 1 https://github.com/Seeed-Studio/seeed-linux-dtoverlays
- Step 2. Enter the repo
cd seeed-linux-dtoverlays
- Step 3. Type the following to install the drivers
sudo ./scripts/reTerminal.sh --device reTerminal-DM
- Step 4. Reboot the reTerminal DM
sudo reboot
Now your screen should light up and run normally.
FAQ
Touch Screen orientation
Q: The screen touch panel is orientate differently from the screen display?
A: Please carefully follow the steps below:
Please follow the access reTerminal DM via SSH step, and then enter the following command:
echo 'ATTRS{name}=="gt9271", ENV{LIBINPUT_CALIBRATION_MATRIX}="0 1.0 0 -1.0 0 1.0 0 0 1.0"' | sudo tee -a /etc/udev/rules.d/98-touchscreen-cal.rules
Then reboot:
sudo reboot
If the screen orientation is still incorrect, additional options for the ENV{LIBINPUT_CALIBRATION_MATRIX} can be found here.
Tech Support & Product Discussion
Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.