Skip to main content

ESPHome Cookbook: Buttons, Buzzer, LED, Battery, Touch & Low Power (reTerminal E Series)

Prerequisites

This page assumes you've already worked through the ESPHome display cookbook for reTerminal E Series (device on Wi-Fi, Home Assistant integration online, first dashboard rendered). For the platform-level YAML skeleton and Home Assistant integration steps, see Work with ESPHome. For RTC, microSD card detect, and microphone setup, see ESPHome Cookbook: RTC, SD Card & Microphone. Capacitive touch (GT911) is covered later on this page and applies to reTerminal E1003 only.

Generate ESPHome YAML or flash demos in the browser

Want a ready-made ESPHome configuration without assembling every pin by hand? Open the reTerminal E-Series Firmware Hub, choose the ESPHome card, pick your device (E1001 / E1002 / E1003 / E1004), then check the onboard features you need — display, buttons, battery, sensors, RTC, SD card, microphone, touch, deep sleep, and more. The Hub generates matching ESPHome YAML you can copy or download into your ESPHome dashboard.

The same Hub can also flash demo firmware directly from the browser (desktop Chrome or Edge). For the shared ESPHome workflow, see Work with ESPHome.



This article covers the onboard I/O and power-related ESPHome configurations for your reTerminal E Series ePaper Display device, building upon the foundational concepts covered in our ESPHome display cookbook. If you're new to ESPHome or the reTerminal E Series, we recommend starting with the display guide before using these hardware examples.

Hardware Capabilities​

The reTerminal E Series ePaper Display includes several hardware components that can be leveraged in Home Assistant through ESPHome:

  • Three programmable buttons (GPIO3, GPIO4, GPIO5)

  • Buzzer (GPIO45)

  • Battery level monitoring (GPIO1 for voltage; enable pin differs by model)

  • On-board LED (GPIO6 on E1001/E1002, GPIO16 on E1003, GPIO48 on E1004)

  • Temperature and humidity sensor (I²C interface)

  • Capacitive touchscreen (GT911 on reTerminal E1003 only)

Let's explore how to use each of these components in practical applications.

Supported models & ESPHome version

Examples on this page cover E1001 / E1002 / E1003 / E1004. For E1003 and E1004 display drivers, use ESPHome 2026.7.0 or later.

reTerminal E Series ePaper Display Hardware Component Control​

Let's explore how to use each of the hardware components on the reTerminal E Series ePaper Display in Home Assistant.

Buttons and LED​

This example demonstrates how to use the three buttons on your reTerminal E Series ePaper Display to control functions and provide visual feedback with the on-board LED.

You can use this example by copying the code below and pasting it after the captive_portal code line in your Yaml file.

Onboard LED pin by model
  • E1001 / E1002: GPIO6
  • E1003: GPIO16
  • E1004: GPIO48

Update the output pin in the snippet above to match your device.

# Button configuration
binary_sensor:
- platform: gpio
pin:
number: GPIO3 # Green button
mode: INPUT_PULLUP
inverted: true
id: button_1
name: "Button 1"
on_press:
then:
- light.turn_on: onboard_led
- delay: 500ms
- light.turn_off: onboard_led

- platform: gpio
pin:
number: GPIO4 # Right white button
mode: INPUT_PULLUP
inverted: true
id: button_2
name: "Button 2"
on_press:
then:
- light.turn_on: onboard_led
- delay: 200ms
- light.turn_off: onboard_led
- delay: 200ms
- light.turn_on: onboard_led
- delay: 200ms
- light.turn_off: onboard_led

- platform: gpio
pin:
number: GPIO5 # Left white button
mode: INPUT_PULLUP
inverted: true
id: button_3
name: "Button 3"
on_press:
then:
- light.toggle: onboard_led

# LED configuration
output:
- platform: gpio
pin: GPIO6
id: led_output
inverted: true

light:
- platform: binary
name: "Onboard LED"
output: led_output
id: onboard_led

This configuration:

  • Sets up all three buttons as inputs with pull-up resistors
  • Configures Button 1 to briefly flash the LED
  • Configures Button 2 to flash the LED in a double-blink pattern
  • Configures Button 3 to toggle the LED on/off
  • Makes the LED available in Home Assistant as a controllable light entity

Buzzer Control​

The reTerminal E Series ePaper Display includes a buzzer on GPIO45 that can be used to provide audible feedback. Here's how to configure it:

You can use this example by copying the code below and pasting it after the captive_portal code line in your Yaml file.

# This component creates a raw PWM (Pulse Width Modulation) output signal.
# For ESP32, the correct platform is 'ledc', which uses the dedicated LED Control hardware peripheral.
output:
- platform: ledc # CORRECTED: 'ledc' is the correct platform for ESP32 PWM.
pin: GPIO45
id: buzzer_pwm
# The frequency determines the pitch of the buzzer's sound. 1000Hz is a mid-range tone.
frequency: 1000Hz

# Create a light entity to provide a user-friendly way to control the buzzer.
# The 'brightness' of the light will control the PWM duty cycle, which effectively changes the buzzer's volume.
light:
- platform: monochromatic
output: buzzer_pwm
name: "Buzzer"
id: buzzer
# Setting transition length to 0s makes the buzzer turn on and off instantly.
default_transition_length: 0s

# This section defines the physical button that will trigger the buzzer.
binary_sensor:
- platform: gpio
pin:
number: GPIO3 # The GPIO pin connected to the green button.
mode: INPUT_PULLUP # Use the internal pull-up resistor.
inverted: true # The signal is low when pressed.
id: button_1
# 'on_press' defines the sequence of actions to execute when the button is pressed.
on_press:
then:
# First beep: turn on at 50% volume (brightness) for 200 milliseconds.
- light.turn_on:
id: buzzer
brightness: 50%
- delay: 200ms
- light.turn_off: buzzer
# Pause for 100 milliseconds between beeps.
- delay: 100ms
# Second beep: turn on at 70% volume for 200 milliseconds.
- light.turn_on:
id: buzzer
brightness: 70%
- delay: 200ms
- light.turn_off: buzzer

This configuration:

  • Sets up the buzzer as a PWM output
  • Creates a light entity to control the buzzer
  • Configures Button 1 to play a short beep pattern when pressed
tip

You can adjust the frequency parameter to change the tone of the buzzer. Higher values create higher-pitched tones.

Battery Monitoring​

The reTerminal E Series ePaper Display can monitor its battery level through the analog input on GPIO1. Here's how to set it up:

Battery measurement enable pin by model

To measure the battery level, you must turn on the battery enable output before reading GPIO1. Use the pin that matches your device:

  • E1001 / E1002 / E1004: GPIO21
  • E1003: GPIO40
esphome:
name: reterminal-e10xx
friendly_name: reTerminal_E10xx
on_boot:
priority: 600
then:
- output.turn_on: bsp_battery_enable

esp32:
board: esp32-s3-devkitc-1
framework:
type: arduino

# Enable logging
logger:

# Enable Home Assistant API
api:
encryption:
key: "REPLACE_WITH_YOUR_API_KEY"

ota:
- platform: esphome
password: "REPLACE_WITH_YOUR_OTA_PASSWORD"

wifi:
ssid: !secret wifi_ssid
password: !secret wifi_password

# Enable fallback hotspot (captive portal) in case wifi connection fails
ap:
ssid: "Reterminal-E10Xx"
password: "ChangeMe123"

captive_portal:

output:
- platform: gpio
pin: GPIO21
id: bsp_battery_enable

sensor:
- platform: adc
pin: GPIO1
name: "Battery Voltage"
id: battery_voltage
update_interval: 60s
attenuation: 12db
filters:
- multiply: 2.0 # Voltage divider compensation

- platform: template
name: "Battery Level"
id: battery_level
unit_of_measurement: "%"
icon: "mdi:battery"
device_class: battery
state_class: measurement
lambda: 'return id(battery_voltage).state;'
update_interval: 10s
filters:
- calibrate_linear:
- 4.15 -> 100.0
- 3.96 -> 90.0
- 3.91 -> 80.0
- 3.85 -> 70.0
- 3.80 -> 60.0
- 3.75 -> 50.0
- 3.68 -> 40.0
- 3.58 -> 30.0
- 3.49 -> 20.0
- 3.41 -> 10.0
- 3.30 -> 5.0
- 3.27 -> 0.0
- clamp:
min_value: 0
max_value: 100

This configuration:

  • Reads the battery voltage through the ADC
  • Converts the voltage to a battery percentage using a calibration curve
  • Makes both the raw voltage and the percentage available in Home Assistant

Demo 2. Take the Home Assistant Dashboard as a Screenshot​

This example demonstrates how to capture screenshots of your Home Assistant dashboard and display them on your reTerminal E Series.

Installing the Puppet Add-on​

Step 1. First, you need to install the Puppet add-on. Click the button below, which will take you directly to the add-on installation page in your Home Assistant instance:

Step 2. On the add-on page, click the "INSTALL" button and wait for the installation to complete.

Creating an Access Token​

Step 3. After installation, go to the Configuration page of the Puppet add-on. As you can see, here we need to enter the token. You'll need to create an access token for this add-on.

Step 4. Navigate to your profile in Home Assistant by clicking on your username in the bottom left corner, then select "Long-Lived Access Tokens" at the bottom of the page.

Step 5. Create a new token with a descriptive name like "Puppet Screenshot" and copy the generated token.

Step 6. Return to the Puppet add-on configuration and paste the token in the "Long-Lived Access Token" field.

Step 7. Save the configuration and restart the Puppet add-on.

Understanding the Screenshot API​

The Puppet add-on launches a server on port 10000 that generates screenshots of any Home Assistant page. Here's how to use it:

Basic Screenshot URL Format​

http://homeassistant.local:10000/lovelace/0?viewport=800x480

This URL will capture a screenshot of your default dashboard at 800x480 resolution (perfect for reTerminal E Series).

E-Paper Optimization​

For e-paper displays, add the eink parameter to reduce the color palette:

http://homeassistant.local:10000/lovelace/0?viewport=800x480&eink=2

The value 2 represents a 2-color (black and white) palette.

Inverting Colors​

Add the invert parameter to invert black and white:

http://homeassistant.local:10000/lovelace/0?viewport=800x480&eink=2&invert

Capturing Different Pages​

You can capture any Home Assistant page by changing the URL path:

http://homeassistant.local:10000/todo?viewport=800x480&eink=2&invert

Test your screenshot URL by entering it in a web browser. You should see the screenshot of your selected Home Assistant page.

ESPHome Configuration​

Step 11. Add the following code to your ESPHome configuration after the captive_portal section:


……
psram:
mode: octal
speed: 80MHz

……

captive_portal:

spi:
clk_pin: GPIO7
mosi_pin: GPIO9

http_request:
verify_ssl: false
timeout: 20s
watchdog_timeout: 25s

online_image:
- id: dashboard_image
format: PNG
type: GRAYSCALE
buffer_size: 65536
url: http://homeassistant.local:10000/lovelace/0?viewport=800x480&eink=2&invert
update_interval: 1min
on_download_finished:
- component.update: epaper_display

display:
- platform: waveshare_epaper
id: epaper_display
model: 7.50inv2 # You can use 7.50inv2alt when you draw complex info and it display not good.
cs_pin: GPIO10
dc_pin: GPIO11
reset_pin:
number: GPIO12
inverted: false
busy_pin:
number: GPIO13
inverted: true
update_interval: 300s
lambda: |-
it.image(0, 0, id(dashboard_image));
caution

Replace homeassistant.local with your Home Assistant's actual IP address if local DNS resolution doesn't work in your network.

When your configuration is successfully uploaded and running, your reTerminal E Series ePaper Display will display a screenshot of your Home Assistant dashboard:

Demo 3: Deep Sleep Mode​

tip

If you start using the Deep Sleep program, we recommend that you use it preferably with the white button on the right side and set the white button on the right side as the Sleep Wake button. This way, when you want to update the program, you won't encounter the awkward situation where the device is sleeping and you can't upload the program through the serial port.

This example demonstrates how to use deep sleep mode to significantly reduce power consumption, making your reTerminal E Series ePaper Display suitable for battery-powered applications.

You can use this example by copying the code below and pasting it after the captive_portal code line in your Yaml file.

globals:
- id: sleep_counter
type: int
restore_value: yes # Use RTC storage to maintain counter during sleep
initial_value: '0'

# Deep sleep configuration
deep_sleep:
id: deep_sleep_1
run_duration: 30s # Device remains awake for 30 seconds
sleep_duration: 5min # Then sleeps for 5 minutes
# Optional: Use a button to wake from sleep
wakeup_pin: GPIO4
wakeup_pin_mode: INVERT_WAKEUP

interval:
- interval: 29s # Schedule sleep just before run_duration ends
then:
- logger.log: "Entering deep sleep now..."

font:
- file: "gfonts://Inter@700"
id: font1
size: 24

spi:
clk_pin: GPIO7
mosi_pin: GPIO9

display:
- platform: waveshare_epaper
id: epaper_display
model: 7.50inv2
cs_pin: GPIO10
dc_pin: GPIO11
reset_pin:
number: GPIO12
inverted: false
busy_pin:
number: GPIO13
inverted: true
update_interval: 5min
lambda: |-
id(sleep_counter) += 1;
ESP_LOGD("main", "Wakeup count: %d", id(sleep_counter));
it.printf(100, 100, id(font1), "Wakeup count: %d", id(sleep_counter));

This configuration:

  • Creates a counter that persists across sleep cycles
  • Configures the device to wake for 30 seconds, then sleep for 3 minutes
  • Updates the display with the current wake-up count
  • Optionally configures a button to wake the device

When running, you'll see a counter increment each time the device wakes from sleep:

Demo 4: Comprehensive Example​

tip

For a better understanding, we strongly recommend that you run the basic examples above first before trying this comprehensive example.

This advanced example combines multiple features into a complete dashboard solution for the reTerminal E Series. It demonstrates:

  1. Weather and indoor climate display
  2. Battery monitoring with icons
  3. Time and date display
  4. Page switching using buttons
  5. Battery monitoring
Click here to view the full code
esphome:
name: reterminal_e1001
friendly_name: reTerminal_E1001
on_boot:
priority: 600
then:
- output.turn_on: bsp_sd_enable
- output.turn_on: bsp_battery_enable
- delay: 200ms
- component.update: battery_voltage
- component.update: battery_level


esp32:
board: esp32-s3-devkitc-1
framework:
type: arduino

# Enable logging
logger:

# Enable Home Assistant API
api:
encryption:
key: "REPLACE_WITH_YOUR_API_KEY"

ota:
- platform: esphome
password: "REPLACE_WITH_YOUR_OTA_PASSWORD"

wifi:
ssid: !secret wifi_ssid
password: !secret wifi_password

# Enable fallback hotspot (captive portal) in case wifi connection fails
ap:
ssid: "reTerminal-E1001"
password: "ChangeMe123"

captive_portal:

# Deep-sleep, wake by GPIO4
deep_sleep:
id: deep_sleep_1
run_duration: 1min
sleep_duration: 60min
wakeup_pin: GPIO4 # Right white button
wakeup_pin_mode: INVERT_WAKEUP

# SPI / I²C
spi:
clk_pin: GPIO7
mosi_pin: GPIO9
i2c:
scl: GPIO20
sda: GPIO19

# Fonts
font:
- file: "gfonts://Inter@700"
id: small_font
size: 24
- file: "gfonts://Inter@700"
id: mid_font
size: 36
- file: "gfonts://Inter@700"
id: big_font
size: 180
- file: "gfonts://Inter@700"
id: time_font
size: 96 # for the big time display
- file: 'fonts/materialdesignicons-webfont.ttf'
id: font_mdi_large
size: 70
glyphs:
- "\U000F050F" # thermometer
- "\U000F058E" # humidity
- file: 'fonts/materialdesignicons-webfont.ttf'
id: font_bat_icon
size: 24
glyphs:
- "\U000F007A" # mdi-battery-10
- "\U000F007B" # mdi-battery-20
- "\U000F007C" # mdi-battery-30
- "\U000F007D" # mdi-battery-40
- "\U000F007E" # mdi-battery-50
- "\U000F007F" # mdi-battery-60
- "\U000F0080" # mdi-battery-70
- "\U000F0081" # mdi-battery-80
- "\U000F0082" # mdi-battery-90
- "\U000F0079" # mdi-battery

globals:
- id: page_index
type: int
restore_value: true
initial_value: '0'
- id: battery_glyph
type: std::string
restore_value: no
initial_value: "\"\\U000F0079\"" # default full battery

sensor:
- platform: sht4x
temperature:
name: "Temperature"
id: temp_sensor
humidity:
name: "Relative Humidity"
id: hum_sensor
- platform: adc
pin: GPIO1
name: "Battery Voltage"
id: battery_voltage
update_interval: 60s
attenuation: 12db
filters:
- multiply: 2.0
- platform: template
name: "Battery Level"
id: battery_level
unit_of_measurement: "%"
icon: "mdi:battery"
device_class: battery
state_class: measurement
lambda: 'return id(battery_voltage).state;'
update_interval: 60s
on_value:
then:
- lambda: |-
int pct = int(x);
if (pct <= 10) id(battery_glyph) = "\U000F007A";
else if (pct <= 20) id(battery_glyph) = "\U000F007B";
else if (pct <= 30) id(battery_glyph) = "\U000F007C";
else if (pct <= 40) id(battery_glyph) = "\U000F007D";
else if (pct <= 50) id(battery_glyph) = "\U000F007E";
else if (pct <= 60) id(battery_glyph) = "\U000F007F";
else if (pct <= 70) id(battery_glyph) = "\U000F0080";
else if (pct <= 80) id(battery_glyph) = "\U000F0081";
else if (pct <= 90) id(battery_glyph) = "\U000F0082";
else id(battery_glyph) = "\U000F0079";
filters:
- calibrate_linear:
- 4.15 -> 100.0
- 3.96 -> 90.0
- 3.91 -> 80.0
- 3.85 -> 70.0
- 3.80 -> 60.0
- 3.75 -> 50.0
- 3.68 -> 40.0
- 3.58 -> 30.0
- 3.49 -> 20.0
- 3.41 -> 10.0
- 3.30 -> 5.0
- 3.27 -> 0.0
- clamp:
min_value: 0
max_value: 100

output:
- platform: gpio
pin: GPIO6
id: bsp_led
inverted: true
- platform: gpio
pin: GPIO16
id: bsp_sd_enable
- platform: gpio
pin: GPIO21
id: bsp_battery_enable

# Onboard LED
light:
- platform: binary
name: "Onboard LED"
output: bsp_led
id: onboard_led

binary_sensor:
- platform: gpio # Next page
pin:
number: GPIO3
mode: INPUT_PULLUP
inverted: true
id: key1
name: "Key1"
on_press:
then:
- lambda: |-
id(page_index) = (id(page_index) + 1) % 2;
id(epaper_display).update();

- platform: gpio # Prev page
pin:
number: GPIO5
mode: INPUT_PULLUP
inverted: true
id: key2
name: "Key2"
on_press:
then:
- lambda: |-
id(page_index) = (id(page_index) - 1 + 2) % 2;
id(epaper_display).update();

# - platform: gpio
# pin:
# number: GPIO4
# mode: INPUT_PULLUP
# inverted: true
# id: key2
# name: "Key2"
# on_press:
# then:
# - lambda: |-
# id(page_index) = (id(page_index) - 1 + 3) % 3;
# id(epaper_display).update();

# Home Assistant time
time:
- platform: homeassistant
id: ha_time

# e-paper
display:
- platform: waveshare_epaper
id: epaper_display
model: 7.50inv2
cs_pin: GPIO10
dc_pin: GPIO11
reset_pin:
number: GPIO12
inverted: false
busy_pin:
number: GPIO13
inverted: true
update_interval: never
lambda: |-
// ---------- PAGE 0 ----------
if (id(page_index) == 0) {
const int scr_w = 800;
const int scr_h = 480;

// Battery in upper-right corner
it.printf(670, 13, id(font_bat_icon), "%s", id(battery_glyph).c_str());
it.printf(700, 10, id(small_font), "%.0f%%", id(battery_level).state);

//line
it.filled_rectangle(400, 100, 2, 280);

// Convert °C to °F
float temp_f = id(temp_sensor).state * 9.0 / 5.0 + 32.0;

// ---------------------------------------------------------
// Horizontal split: two 400 px columns
const int col_w = scr_w / 2;

const int icon_y = 100; // Icon baseline
const int value_y = 220; // Number baseline
const int unit_y = 300; // Unit baseline
const int label_y = 380; // Text label baseline

const int icon_size = 70; // icon font size
const int val_size = 120; // number font size
const int unit_size = 44; // unit font size
const int label_size= 36; // label font size

// --- Left column : Temperature -----------------------------
const int left_mid = col_w / 2 - 30; // 200 px

// Icon
it.printf(left_mid, icon_y, id(font_mdi_large), TextAlign::CENTER, "\U000F050F");
// Value
it.printf(left_mid, value_y, id(big_font), TextAlign::CENTER, "%.0f", temp_f);
// Unit
it.printf(left_mid + 150, unit_y, id(mid_font), TextAlign::CENTER, "°F");
// Label
it.printf(left_mid, label_y, id(mid_font), TextAlign::CENTER, "Temperature");

// --- Right column : Humidity -------------------------------
const int right_mid = col_w + col_w / 2; // 600 px

// Icon
it.printf(right_mid, icon_y, id(font_mdi_large), TextAlign::CENTER, "\U000F058E");
// Value
it.printf(right_mid, value_y, id(big_font), TextAlign::CENTER, "%.0f", id(hum_sensor).state);
// Unit
it.printf(right_mid + 150, unit_y, id(mid_font), TextAlign::CENTER, "%%");
// Label
it.printf(right_mid, label_y, id(mid_font), TextAlign::CENTER, "Humidity");
}
// ---------- PAGE 1 ----------
else{
// Battery top-right
it.printf(670, 13, id(font_bat_icon), "%s", id(battery_glyph).c_str());
it.printf(700, 10, id(small_font), "%.0f%%", id(battery_level).state);

auto now = id(ha_time).now();
struct tm timeinfo = now.to_c_tm();

// centering time HH:MM
char timeStr[6];
strftime(timeStr, sizeof(timeStr), "%H:%M", &timeinfo);
it.printf(400, 180, id(time_font), TextAlign::CENTER, timeStr);

// Date: Day of week
const char *weekday[] = {"Sun","Mon","Tue","Wed","Thu","Fri","Sat"};
const char *wday = weekday[timeinfo.tm_wday];

// Date: month - day
char dateStr[12];
strftime(dateStr, sizeof(dateStr), "%b %d", &timeinfo); // e.g. Jun 15

// Day of the week + date below the time
it.printf(400, 280, id(mid_font), TextAlign::CENTER, "%s, %s", wday, dateStr);
}

When your configuration is successfully uploaded and running, your reTerminal E Series ePaper Display will display a comprehensive dashboard with environment data, time, and battery status:

Understanding the Comprehensive Example​

This example implements:

  1. Multiple Pages: The display toggles between two pages - a climate dashboard and a time/date display
  2. Button Navigation: Buttons on GPIO3 and GPIO5 are used to navigate between pages
  3. Battery Monitoring: Battery level is shown with appropriate icons that change based on the charge level
  4. Hardware Initialization: SD card and battery monitoring circuits are enabled on boot
  5. Temperature and Humidity Display: Using the onboard SHT4x sensor via I²C
  6. Dynamic Icons: Material Design Icons change based on sensor values

Capacitive Touch (reTerminal E1003 only)​

E1003 only

The GT911 capacitive touchscreen is available on reTerminal E1003. reTerminal E1001, E1002, and E1004 do not include this touch controller, so skip this section on those models.

reTerminal E1003 uses a GT911 touch controller on the shared I2C bus. In ESPHome you attach it to the it8951 display with the touchscreen component, then log or act on touch events.

Wiring summary​

FunctionPin / Bus
Touch interruptGPIO2
Touch resetGPIO48
I2CSDA GPIO19, SCL GPIO20 (shared with SHT4x / PCF8563)

Minimal touch example​

Add the following after your E1003 display configuration (the display block must use id: epaper_display). Requires ESPHome 2026.7.0 or later.

i2c:
scl: GPIO20
sda: GPIO19

touchscreen:
- platform: gt911
id: e1003_touch
display: epaper_display
interrupt_pin: GPIO2
reset_pin: GPIO48
transform:
mirror_x: true
on_touch:
- logger.log:
format: "Touch: x=%d, y=%d"
args: ["touch.x", "touch.y"]

What you should see​

  1. Flash an E1003 configuration that includes both the it8951 display and the gt911 touchscreen blocks.
  2. Open the ESPHome logs over USB (logger with hardware_uart: UART0).
  3. Tap the panel — you should see Touch: x=..., y=... lines in the log.

You can extend on_touch with automations such as page changes, button-like hotspots, or Home Assistant events. Keep transform.mirror_x: true aligned with the E1003 display transform so touch coordinates match what you draw on screen.

FAQ​

Q1: Why is there no data?​

In this case, you should go to Settings -> Devices & Services -> Integrations to RECONGFIGURE device. Haven't found your ePaper Panel? Try to reboot Home Assistant.

Q2: Why can't I get those data in Home Assistant?​

In this case, you should go to Settings -> Devices & Services -> Integrations to ADD your device to Home Assistant.

Q3: Wi-Fi upload program failed?​

In this case, your device is either offline or in deep sleep mode. Please ensure it's connected to your network or wake it up from sleep mode before attempting to upload.

Q4: Why is there no serial log over USB?​

The reTerminal E Series uses a CH340K USB-to-UART bridge on UART0. Keep this logger setting in your YAML:

logger:
hardware_uart: UART0

Tech Support & Product Discussion​

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...