Skip to main content

ESPHome Cookbook: RTC, SD Card & Microphone (reTerminal E Series)


Prerequisites

This page assumes you have already completed the ESPHome display cookbook for reTerminal E Series and your device is online in Home Assistant. For buttons, buzzer, LED, battery monitoring, SHT4x, capacitive touch (E1003), and deep sleep, see ESPHome Cookbook: Buttons, Buzzer, LED, Battery, Touch & Low Power.

Generate ESPHome YAML or flash demos in the browser

Want a ready-made ESPHome configuration without assembling every pin by hand? Open the reTerminal E-Series Firmware Hub, choose the ESPHome card, pick your device (E1001 / E1002 / E1003 / E1004), then check the onboard features you need — display, buttons, battery, sensors, RTC, SD card, microphone, touch, deep sleep, and more. The Hub generates matching ESPHome YAML you can copy or download into your ESPHome dashboard.

The same Hub can also flash demo firmware directly from the browser (desktop Chrome or Edge). For the shared ESPHome workflow, see Work with ESPHome.


This cookbook continues the reTerminal E Series ESPHome examples with three onboard hardware blocks that are not covered in the display and I/O cookbooks:

  • PCF8563 RTC - read hardware time from the onboard RTC and sync it from Home Assistant.
  • microSD card slot - enable the SD power rail and report whether a card is inserted.
  • PDM microphone - enable the onboard microphone power rail and initialize the PDM microphone through ESPHome.

Each section below is organized as a small standalone ESPHome demo. You can copy one complete YAML example, replace the API and OTA placeholders, and upload it directly from ESPHome.

Model coverage

The ready-to-copy examples in this page cover reTerminal E1001 / E1002 / E1003 / E1004. E1003 and E1004 require ESPHome 2026.7.0 or later. The onboard microphone examples apply to models that include the PDM microphone hardware (E1001 / E1002 / E1003); reTerminal E1004 does not include the microphone.

Hardware Capabilities

The following pins are used by the demos in this cookbook.

FunctionESPHome ComponentPin / Address
PCF8563 RTCtime.pcf8563I2C address 0x51, SDA GPIO19, SCL GPIO20
microSD card detectbinary_sensor.gpioGPIO15, active LOW
microSD power enableoutput.gpioGPIO16 (E1001 / E1002 / E1004), GPIO39 (E1003)
PDM microphone power enableoutput.gpioGPIO38
PDM microphone clocki2s_audioGPIO42
PDM microphone datamicrophone.i2s_audioGPIO41
Shared SPI busspiCLK GPIO7, MOSI GPIO9, MISO GPIO8
Keep your secrets private

The examples use placeholders such as REPLACE_WITH_YOUR_API_KEY and REPLACE_WITH_YOUR_OTA_PASSWORD. Do not publish your real API encryption key, OTA password, Wi-Fi password, or Home Assistant token.

RTC Time Sync

This demo reads time from the onboard PCF8563 RTC and displays it on the ePaper screen. When Home Assistant syncs time to the device, ESPHome writes that time back to the hardware RTC.

The RTC uses the shared I2C bus:

  • SDA: GPIO19
  • SCL: GPIO20
  • RTC address: 0x51

You can use this example by replacing the placeholder values and uploading the complete YAML to your device.

esphome:
name: reterminal-e1001-rtc-demo
friendly_name: reTerminal_E1001_RTC_Demo
on_boot:
priority: 600
then:
- pcf8563.read_time:

esp32:
board: esp32-s3-devkitc-1
framework:
type: arduino

logger:
hardware_uart: UART0

api:
encryption:
key: "REPLACE_WITH_YOUR_API_KEY"

ota:
- platform: esphome
password: "REPLACE_WITH_YOUR_OTA_PASSWORD"

wifi:
ssid: !secret wifi_ssid
password: !secret wifi_password
ap:
ssid: "E1001-RTC-Demo"
password: "ChangeMe123"

captive_portal:

i2c:
scl: GPIO20
sda: GPIO19

spi:
clk_pin: GPIO7
mosi_pin: GPIO9

time:
- platform: pcf8563
id: rtc_time
address: 0x51
update_interval: never

- platform: homeassistant
on_time_sync:
then:
- pcf8563.write_time:
- component.update: epaper_display

font:
- file: "gfonts://Inter@700"
id: font_title
size: 32
- file: "gfonts://Inter@700"
id: font_body
size: 26

display:
- platform: waveshare_epaper
id: epaper_display
model: 7.50inv2
cs_pin: GPIO10
dc_pin: GPIO11
reset_pin:
number: GPIO12
inverted: false
busy_pin:
number: GPIO13
inverted: true
update_interval: 300s
lambda: |-
it.printf(400, 40, id(font_title), TextAlign::TOP_CENTER, "RTC Time Sync Demo");
auto now = id(rtc_time).now();
if (now.is_valid()) {
it.strftime(400, 135, id(font_title), TextAlign::TOP_CENTER, "%Y-%m-%d", now);
it.strftime(400, 190, id(font_title), TextAlign::TOP_CENTER, "%H:%M:%S", now);
ESP_LOGD("rtc_demo", "RTC time is valid");
} else {
it.printf(400, 150, id(font_body), TextAlign::TOP_CENTER, "RTC: waiting for sync");
ESP_LOGW("rtc_demo", "RTC time is not valid yet");
}

This configuration:

  • Reads the PCF8563 RTC once during boot.
  • Uses Home Assistant time as the source of truth after the device connects.
  • Writes the Home Assistant time back to the hardware RTC.
  • Displays the current date and time on the ePaper screen.

The following image shows the expected result on reTerminal E1002. The same demo pattern works across the reTerminal E Series. Choose the matching device tab above. Monochrome / grayscale panels (E1001, E1003) and color panels (E1002, E1004) differ mainly in the display platform and color drawing API.

tip

If the RTC time does not stay correct after a full power cycle, install or replace the CR1220 coin cell for the RTC backup holder.

MicroSD Card Detection

This demo reports whether a microSD card is inserted. It also turns on the SD card power rail through GPIO16 (E1001 / E1002 / E1004) or GPIO39 (E1003).

The card detect pin is active LOW, so the binary sensor uses inverted: true.

You can use this example by replacing the placeholder values and uploading the complete YAML to your device.

esphome:
name: reterminal-e1001-sd-demo
friendly_name: reTerminal_E1001_SD_Demo
on_boot:
priority: 600
then:
- output.turn_on: bsp_sd_enable
- delay: 200ms
- component.update: epaper_display

esp32:
board: esp32-s3-devkitc-1
framework:
type: arduino

logger:
hardware_uart: UART0

api:
encryption:
key: "REPLACE_WITH_YOUR_API_KEY"

ota:
- platform: esphome
password: "REPLACE_WITH_YOUR_OTA_PASSWORD"

wifi:
ssid: !secret wifi_ssid
password: !secret wifi_password
ap:
ssid: "E1001-SD-Demo"
password: "ChangeMe123"

captive_portal:

spi:
id: epaper_spi_bus
clk_pin: GPIO7
mosi_pin: GPIO9
miso_pin: GPIO8

output:
- platform: gpio
pin: GPIO16
id: bsp_sd_enable

binary_sensor:
- platform: gpio
pin:
number: GPIO15
mode: INPUT_PULLUP
inverted: true
id: sd_card_detect
name: "SD Card Detected"
on_press:
then:
- logger.log: "SD card inserted"
- component.update: epaper_display
on_release:
then:
- logger.log: "SD card removed"
- component.update: epaper_display

font:
- file: "gfonts://Inter@700"
id: font_title
size: 32
- file: "gfonts://Inter@700"
id: font_body
size: 28

display:
- platform: waveshare_epaper
id: epaper_display
model: 7.50inv2
cs_pin: GPIO10
dc_pin: GPIO11
reset_pin:
number: GPIO12
inverted: false
busy_pin:
number: GPIO13
inverted: true
update_interval: 300s
lambda: |-
it.printf(400, 40, id(font_title), TextAlign::TOP_CENTER, "microSD Card Detection");
if (id(sd_card_detect).state) {
it.printf(400, 160, id(font_body), TextAlign::TOP_CENTER, "SD Card: inserted");
} else {
it.printf(400, 160, id(font_body), TextAlign::TOP_CENTER, "SD Card: not detected");
}
it.printf(400, 230, id(font_body), TextAlign::TOP_CENTER, "Detect pin: GPIO15");

This configuration:

  • Enables SD card power through GPIO16 (E1001 / E1002 / E1004) or GPIO39 (E1003).
  • Reads the card-detect signal from GPIO15.
  • Shows the card state on the ePaper screen.
  • Exposes SD Card Detected to Home Assistant as a binary sensor.

The following image shows the expected result on reTerminal E1002. The same demo pattern works across the reTerminal E Series. Choose the matching device tab above. Monochrome / grayscale panels (E1001, E1003) and color panels (E1002, E1004) differ mainly in the display platform and color drawing API.

How ESPHome uses the microSD card

In this ESPHome cookbook, the microSD card is used as a device status signal. The demo checks whether a card is inserted, shows the result on the screen, and exposes the same state to Home Assistant.

This is because ESPHome is mainly designed for sensors, switches, displays, and Home Assistant automation. It is not usually used as a local file manager on the device. Tasks such as opening files, creating folders, writing logs, or recording WAV audio directly to the SD card are better handled with Arduino, where your firmware controls the SD card filesystem directly.

In a typical ESPHome setup, the SD card status can be used to:

  • show whether storage is physically available;
  • trigger Home Assistant automations when a card is inserted or removed;
  • display hardware health information together with RTC, battery, and microphone status.

If your goal is direct SD card file read/write, refer to the Arduino SD card cookbook instead.

PDM Microphone Power Check

This demo enables the onboard PDM microphone power rail and displays the microphone pin assignment on the ePaper screen. It keeps the YAML minimal so you can verify the display update first, then add the optional ESPHome I2S microphone configuration if you want to use the microphone with Home Assistant Voice Assistant.

The microphone uses these pins:

  • Power enable: GPIO38
  • PDM clock: GPIO42
  • PDM data: GPIO41

You can use this example by replacing the placeholder values and uploading the complete YAML to your device.

esphome:
name: reterminal-e1001-mic-demo
friendly_name: reTerminal_E1001_Mic_Demo
on_boot:
priority: 600
then:
- output.turn_on: mic_power_enable
- delay: 200ms
- logger.log: "PDM microphone power enabled"
- component.update: epaper_display

esp32:
board: esp32-s3-devkitc-1
framework:
type: arduino

logger:
hardware_uart: UART0

api:
encryption:
key: "REPLACE_WITH_YOUR_API_KEY"

ota:
- platform: esphome
password: "REPLACE_WITH_YOUR_OTA_PASSWORD"

wifi:
ssid: !secret wifi_ssid
password: !secret wifi_password
ap:
ssid: "E1001-Mic-Demo"
password: "ChangeMe123"

captive_portal:

spi:
clk_pin: GPIO7
mosi_pin: GPIO9

output:
- platform: gpio
pin: GPIO38
id: mic_power_enable

font:
- file: "gfonts://Inter@700"
id: font_title
size: 32
- file: "gfonts://Inter@700"
id: font_body
size: 26

display:
- platform: waveshare_epaper
id: epaper_display
model: 7.50inv2
cs_pin: GPIO10
dc_pin: GPIO11
reset_pin:
number: GPIO12
inverted: false
busy_pin:
number: GPIO13
inverted: true
update_interval: 300s
lambda: |-
it.printf(400, 40, id(font_title), TextAlign::TOP_CENTER, "PDM Microphone Power");
it.printf(400, 135, id(font_body), TextAlign::TOP_CENTER, "Mic Power: ON");
it.printf(400, 190, id(font_body), TextAlign::TOP_CENTER, "CLK GPIO42 / DATA GPIO41");
it.printf(400, 245, id(font_body), TextAlign::TOP_CENTER, "I2S microphone: optional");

This configuration:

  • Enables microphone power through GPIO38.
  • Shows the PDM clock pin GPIO42 and data pin GPIO41 on the ePaper screen.
  • Keeps the main demo close to the RTC and microSD demos, so the display refresh can be verified before adding the audio component.

If you want to expose the onboard PDM microphone to ESPHome, add the following optional block after confirming that the screen demo refreshes correctly:

i2s_audio:
i2s_lrclk_pin: GPIO42

microphone:
- platform: i2s_audio
id: onboard_mic
adc_type: external
pdm: true
i2s_din_pin: GPIO41

The following image shows the expected result on reTerminal E1002. The same demo pattern works across the reTerminal E Series. Choose the matching device tab above. Monochrome / grayscale panels (E1001, E1003) and color panels (E1002, E1004) differ mainly in the display platform and color drawing API.

note

This demo only verifies microphone power control and the related pin assignment on the ePaper screen. A complete Home Assistant Assist voice pipeline requires the optional microphone block above and additional voice assistant configuration. Recording audio directly to the SD card is better handled by the Arduino microphone examples.

Demo 4: Complete RTC, SD Card and Microphone Status Dashboard

This demo combines the three features above into one hardware status page:

  1. RTC date and time from the PCF8563.
  2. microSD card insertion status from GPIO15.
  3. PDM microphone initialization status.

For a better understanding, run the single-function demos first before trying this combined example.

Click here to view the full code
esphome:
name: reterminal-e1001-hardware-status
friendly_name: reTerminal_E1001_Hardware_Status
on_boot:
priority: 600
then:
- output.turn_on: bsp_sd_enable
- output.turn_on: mic_power_enable
- delay: 200ms
- pcf8563.read_time:
- component.update: epaper_display

esp32:
board: esp32-s3-devkitc-1
framework:
type: arduino

logger:
hardware_uart: UART0

api:
encryption:
key: "REPLACE_WITH_YOUR_API_KEY"

ota:
- platform: esphome
password: "REPLACE_WITH_YOUR_OTA_PASSWORD"

wifi:
ssid: !secret wifi_ssid
password: !secret wifi_password
ap:
ssid: "E1001-HW-Status"
password: "ChangeMe123"

captive_portal:

spi:
id: epaper_spi_bus
clk_pin: GPIO7
mosi_pin: GPIO9
miso_pin: GPIO8

i2c:
scl: GPIO20
sda: GPIO19

i2s_audio:
i2s_lrclk_pin: GPIO42

output:
- platform: gpio
pin: GPIO16
id: bsp_sd_enable

- platform: gpio
pin: GPIO38
id: mic_power_enable

time:
- platform: pcf8563
id: rtc_time
address: 0x51
update_interval: never

- platform: homeassistant
on_time_sync:
then:
- pcf8563.write_time:
- component.update: epaper_display

microphone:
- platform: i2s_audio
id: onboard_mic
adc_type: external
pdm: true
i2s_din_pin: GPIO41

binary_sensor:
- platform: gpio
pin:
number: GPIO15
mode: INPUT_PULLUP
inverted: true
id: sd_card_detect
name: "SD Card Detected"
on_press:
then:
- component.update: epaper_display
on_release:
then:
- component.update: epaper_display

font:
- file: "gfonts://Inter@700"
id: font_small
size: 20
- file: "gfonts://Inter@700"
id: font_medium
size: 32

display:
- platform: waveshare_epaper
id: epaper_display
model: 7.50inv2
cs_pin: GPIO10
dc_pin: GPIO11
reset_pin:
number: GPIO12
inverted: false
busy_pin:
number: GPIO13
inverted: true
update_interval: 300s
lambda: |-
it.printf(400, 20, id(font_medium), TextAlign::TOP_CENTER,
"reTerminal E1001 Hardware Status");
it.line(20, 60, 780, 60);

auto now = id(rtc_time).now();
if (now.is_valid()) {
it.strftime(30, 95, id(font_medium), "%Y-%m-%d %H:%M", now);
ESP_LOGD("status", "RTC time is valid");
} else {
it.printf(30, 95, id(font_medium), "RTC: waiting for sync");
ESP_LOGW("status", "RTC time is not valid yet");
}

if (id(sd_card_detect).state) {
it.printf(30, 155, id(font_medium), "SD Card: inserted");
} else {
it.printf(30, 155, id(font_medium), "SD Card: not detected");
}

it.printf(30, 215, id(font_medium), "PDM Mic: initialized");
it.printf(30, 265, id(font_small), "RTC: I2C address 0x51");
it.printf(30, 295, id(font_small), "SD: DET GPIO15 / EN GPIO16");
it.printf(30, 325, id(font_small), "Mic: CLK GPIO42 / DATA GPIO41 / EN GPIO38");

When the firmware is running, the screen shows the RTC time and SD card state on one page. Models with an onboard PDM microphone (E1001 / E1002 / E1003) also show microphone initialization status; E1004 shows that the microphone is not available.

The following image shows the expected result on reTerminal E1002. The same demo pattern works across the reTerminal E Series. Choose the matching device tab above. Monochrome / grayscale panels (E1001, E1003) and color panels (E1002, E1004) differ mainly in the display platform and color drawing API.

FAQ

Q1: Why does the screen show "RTC: waiting for sync"?

The device has not received valid time yet. Confirm that Wi-Fi is connected, the ESPHome API is connected to Home Assistant, and Home Assistant has the correct system time. After Home Assistant syncs time, ESPHome writes the time back to the PCF8563 RTC.

Q2: Why is there no serial log over USB?

The reTerminal E Series uses a CH340K USB-to-UART bridge on UART0. Keep this logger setting in your YAML:

logger:
hardware_uart: UART0

Q3: Why does the screen not refresh in the RTC or microphone demo?

If a microSD card is inserted, remove the card first and restart the device. Except for the microSD card detection demo, the other demos on this page do not need the card to be inserted. Keeping a card inserted may affect the shared SPI bus and prevent the ePaper screen from refreshing correctly.

After removing the card, upload or restart the RTC or microphone demo again. The ePaper screen should refresh normally.

Resources

Tech Support & Product Discussion

Thank you for choosing our products! We are here to provide you with different support to ensure that your experience with our products is as smooth as possible. We offer several communication channels to cater to different preferences and needs.

Loading Comments...