Skip to main content
SEEED STUDIO · HANDS-ON DEPLOYMENT

How to Deploy and Evaluate ACT on reBot Arm

Run ACT on a real robot, understand preprocessing and action-chunk execution, measure success, and improve data by analyzing failures.

  • On-robot inference
  • Action-chunk execution
  • Evaluation
  • Data iteration

Inference Data Flow at a Glance​

Deploy an ACT Model: Inference Data Flow at a Glance (Figure 1)


Preprocessing and Denormalization​

The model was trained with normalized data, so inference must apply the same input and output rules:

DirectionProcessingStatistics
Into the modelResize images and apply ImageNet normalization; subtract state means and divide by standard deviations (z-score).Training dataset meta/stats.json
Out of the modelMultiply actions by standard deviations and add means to recover physical joint angles.The same statistics

Deploy an ACT Model: Preprocessing and Denormalization (Figure 2)


Start On-Robot Inference and Iterate on Data​

Load the policy with lerobot-record. Use exactly the same robot and camera parameters as during collection:

RS version:

lerobot-record \
--robot.type=seeed_b601_rs_follower \
--robot.port=can0 \
--robot.can_adapter=socketcan \
--robot.cameras='{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"} }' \
--robot.id=follower1 \
--display_data=false \
--dataset.repo_id=seeed/eval_test18 \
--dataset.single_task="Grab the crayfish into the box" \
--dataset.num_episodes=10 \
--dataset.episode_time_s=60 \
--dataset.reset_time_s=10 \
--policy.path=outputs/train/act_rebot_test/checkpoints/last/pretrained_model \
--policy.push_to_hub=false

DM version:

lerobot-record \
--robot.type=seeed_b601_dm_follower \
--robot.port=/dev/ttyACM0 \
--robot.can_adapter=damiao \
--robot.cameras='{ front: {type: opencv, index_or_path: 0, width: 640, height: 480, fps: 30, fourcc: "MJPG"}, side: {type: opencv, index_or_path: 2, width: 640, height: 480, fps: 30, fourcc: "MJPG"} }' \
--robot.id=follower1 \
--display_data=false \
--dataset.repo_id=seeed/eval_test18 \
--dataset.single_task="Grab the crayfish into the box" \
--dataset.num_episodes=10 \
--dataset.episode_time_s=60 \
--dataset.reset_time_s=10 \
--policy.path=outputs/train/act_rebot_test/checkpoints/last/pretrained_model \
--policy.push_to_hub=false
  • --dataset.num_episodes=10: record 10 evaluation episodes.

  • --dataset.episode_time_s=60: allow at most 60 seconds per episode. Set this for the task duration: if putting the crayfish in the box takes 20–30 seconds, allow 30–40 seconds. For extended observation without waiting between episodes, you can use a longer duration such as 300 seconds.

  • --dataset.reset_time_s=10: allow 10 seconds between episodes to restore object positions. Keep starting conditions as consistent as possible during evaluation.


Executing an Action Chunk​

  • One inference predicts a 100-step action chunk. Execute only the first n steps open-loop (n_action_steps), then observe again: predictions become less reliable further into the future.

  • With temporal ensembling (temporal_ensemble_coeff), the action at each timestep is a weighted average of overlapping predictions, producing smoother trajectories.

  • Visible pauses often occur when a chunk finishes before the next inference is ready. Increasing n_action_steps can reduce these pauses, at the cost of slower responses to disturbances.


Safety: Limits, Speed, and Emergency Stops​

  • Use ESC to end the session; do not use Ctrl+C. Before stopping, let the arm finish its current action chunk or manually return it to a safe pose (although Ctrl+C currently also returns the robot to zero), to avoid leaving it suspended under load.

  • Be ready to disconnect power immediately if the arm behaves abnormally.


Evaluate Success Rate and Completion Time​

Fix the starting conditions and run 20 trials, recording each result.

  • Success rate = successful trials ÷ 20. For the first trained model, above 50% is a normal starting point and above 80% is excellent.

  • Completion time indicates consistency. Successful trials should take similar amounts of time; large variations suggest hesitation.

  • For failures, record the failure mode, rather than only marking a cross.


Test Generalization​

After testing standard conditions, change one condition at a time and measure the success-rate drop. An ACT model trained on 50 episodes has limited generalization; broader coverage requires more demonstrations.

TestMethodExpected behavior
Position generalizationPlace the block away from the five marked points, but within the demonstrated region.Little degradation; a drop suggests insufficient position diversity.
Mild distractionAdd unrelated objects to the table.A model with clean visual understanding should be unaffected.
Clear distribution shiftUse a completely new object or a reflective tabletop.Failure is expected outside the training distribution.

The purpose is to map the model's capability boundary, then extend it gradually with more data.


Analyze Failure Types​

FailureMost likely causeResponse
Reaches toward the wrong positionInsufficient data coverage at that position; distribution shift.Collect more demonstrations in that region.
Contacts the object but cannot hold it, or drops itPoorly learned closing timing or too few grasp examples.Add high-quality demonstrations of the grasping moment.
Moves erratically throughoutTraining has not converged, or the scene and lighting have changed substantially.Check that the scene and lighting during collection match inference.

Rule out configuration problems before blaming the data. Erratic motion often calls for configuration checks; inaccurate reaching often calls for better coverage.


Data Iteration: Collect for Failure Cases​

Close the loop by turning failures into data:

  1. Classify the failure and the scene in which it occurs.

  2. Collect 10–20 new demonstrations targeting that case. For missed reaches, record the problematic location; for unstable grasps, emphasize the closing motion. Expand the covered region gradually, for example with new points spaced 5–10 cm around the original cross.

  3. Retrain using the updated dataset.

Deploy an ACT Model: Data Iteration: Collect for Failure Cases (Figure 3)

Loading Comments...